Difference between revisions of "Wiki archives"

[unchecked revision] [quality revision]
m
m
 

This page aims to provide links to archived wikis.
Each ecosystem releases release flow has its corresponding wiki.

An ecosystem releases release flow designates all the ecosystem releases which are based on the same versions of the major software components (e.g. Linux® kernel) of the OpenSTLinux distribution (see details in the table below table).
Each vx flow groups together all the vx.y.z ecosystem releases, and has its own wiki.

The most recent flow is associated with this flagship/ latest wiki also known as flagship wiki (whose URL is "https://wiki.st.com/stm32mpu"), while the previous flows are associated with archived wikis (whose URLs are "https://wiki.st.com/stm32mpu-ecosystem-vx").

This flagship /latest wiki is for the v2 flow (v2.y.z ecosystem releases): if you discover the STM32 Arm® Cortex®-based MPUs, it is highly recommended to continue browsing this wiki that contains the latest major ecosystem release.


However, if you need information about any previous ecosystem releases flow, browse the associated wiki thanks to the below table:

STM32 MPU wiki by ST.png

ecosystem-v1

STM32 MPU archived wiki for the v1.y.z ecosystem releases


Wikis and software components
Wiki Major ecosystem releases Major software components (OpenSTLinux distribution)
This wiki

v2.1.0
v2.0.0

Linux® kernel v5.4 (LTS)
U-Boot v2020.01
TF-A v2.2
OP-TEE v3.9.0
OpenEmbedded v3.1 (Dunfell)

Archived wiki for the v1 flow

v1.2.0
v1.1.0
v1.0.0

Linux® kernel v4.19 (LTS)
U-Boot v2018.11
TF-A v2.0
OP-TEE v3.3.0
OpenEmbedded v2.6 (Thud)


This page aims to provide links to archived wikis.<br>

Each ecosystem releasesrelease flow has its corresponding wiki.

An '''ecosystem releasesrelease flow''' designates all the '''ecosystem releases''' which are based on the '''same versions of the major software components''' (e.g. Linux<sup>&reg;</sup> kernel) of the OpenSTLinux distribution (see details in the table below table).<br>

Each '''v''x''''' flow groups together all the '''v''x''.''y''.''z''''' ecosystem releases, and has '''its own wiki'''.

The most recent flow is associated with this '''flagship/latestlatest wiki also known as '''flagship wiki''' (whose URL is "<nowiki>https:</nowiki>//wiki.st.com/stm32mpu"), while the previous flows are associated with '''archived wikis''' (whose URLs are "<nowiki>https:</nowiki>//wiki.st.com/stm32mpu-ecosystem-v''x''").

{{Highlight|This flagship/latest wiki is for the '''v2''' flow ('''v2.''y''.''z''''' ecosystem releases)}}: if you discover the STM32 Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-based MPUs, it is highly recommended to continue browsing this wiki that contains the [[STM32MP15 ecosystem release note|latest major ecosystem release]].

However, if you need information about any previous ecosystem releases flow, browse the associated wiki thanks to the below table:
{| class="st-table"
|- style="vertical-align:top;"
| style="text-align:center;" | [[File:STM32_MPU_wiki_by_ST.png|center|x70px|link=stm32mpuv1:Main Page]]
[[stm32mpuv1:Main Page|ecosystem-v1]]
|  style="vertical-align:middle;" | STM32 MPU archived wiki for the {{Highlight|v1.''y''.''z''}} ecosystem releases
|}


{| class="st-table"
|+ Wikis and software components
! Wiki !! Major ecosystem releases !! Major software components (OpenSTLinux distribution)
|-
| [[Main_Page|This wiki]]
|
v2.1.0<br>

v2.0.0
|
Linux<sup>&reg;</sup> kernel v5.4 (LTS)<br>

U-Boot v2020.01<br>

TF-A v2.2<br>

OP-TEE v3.9.0<br>

OpenEmbedded v3.1 (Dunfell)
|-
|  [[stm32mpuv1:Main Page|Archived wiki for the v1 flow]]
|
v1.2.0<br>

v1.1.0<br>

v1.0.0
|
Linux<sup>&reg;</sup> kernel v4.19 (LTS)<br>

U-Boot v2018.11<br>

TF-A v2.0<br>

OP-TEE v3.3.0<br>

OpenEmbedded v2.6 (Thud)
|}
<noinclude>

[[Category:Wiki archives tab]]
{{PublicationRequestId | 18177 | 2020-11-19 | }}</noinclude>
Line 1: Line 1:
 
This page aims to provide links to archived wikis.<br>
 
This page aims to provide links to archived wikis.<br>
Each ecosystem releases flow has its corresponding wiki.
+
Each ecosystem release flow has its corresponding wiki.
   
An '''ecosystem releases flow''' designates all the '''ecosystem releases''' which are based on the '''same versions of the major software components''' (e.g. Linux<sup>&reg;</sup> kernel) of the OpenSTLinux distribution (see details in the below table).<br>
+
An '''ecosystem release flow''' designates all the '''ecosystem releases''' which are based on the '''same versions of the major software components''' (e.g. Linux<sup>&reg;</sup> kernel) of the OpenSTLinux distribution (see details in the table below).<br>
 
Each '''v''x''''' flow groups together all the '''v''x''.''y''.''z''''' ecosystem releases, and has '''its own wiki'''.
 
Each '''v''x''''' flow groups together all the '''v''x''.''y''.''z''''' ecosystem releases, and has '''its own wiki'''.
   
The most recent flow is associated with this '''flagship/latest wiki''' (whose URL is "<nowiki>https:</nowiki>//wiki.st.com/stm32mpu"), while the previous flows are associated with '''archived wikis''' (whose URLs are "<nowiki>https:</nowiki>//wiki.st.com/stm32mpu-ecosystem-v''x''").
+
The most recent flow is associated with this latest wiki also known as '''flagship wiki''' (whose URL is "<nowiki>https:</nowiki>//wiki.st.com/stm32mpu"), while the previous flows are associated with '''archived wikis''' (whose URLs are "<nowiki>https:</nowiki>//wiki.st.com/stm32mpu-ecosystem-v''x''").
   
{{Highlight|This flagship/latest wiki is for the '''v2''' flow ('''v2.''y''.''z''''' ecosystem releases)}}: if you discover the STM32 Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-based MPUs, it is highly recommended to continue browsing this wiki that contains the [[STM32MP15 ecosystem release note|latest major ecosystem release]].
+
{{Highlight|This flagship wiki is for the '''v2''' flow ('''v2.''y''.''z''''' ecosystem releases)}}: if you discover the STM32 Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-based MPUs, it is highly recommended to continue browsing this wiki that contains the [[STM32MP15 ecosystem release note|latest major ecosystem release]].