Difference between revisions of "V4L2 camera overview"
[quality revision] | [quality revision] |
m
|
m
|
This article gives information about the Linux® V4L2 camera framework.
Contents
1 Framework purpose[edit]
The V4L2 Linux kernel framework[1] allows to control both an external camera sensor and the camera interface in order to capture raw frames in various pixel formats or encoded stream data such as JPEG.
This could be typically used, with the help of other Linux multimedia frameworks and applications, to take snapshot, to make preview, to make a video recording or even remotely stream images from the camera sensor.
2 System overview[edit]
2.1 Component description[edit]
- Application (User space)
Any application relying on V4L2 Linux kernel interface or libv4l abstraction layer. GStreamer framework provides such application.
- V4L2 utilities (User space)
A set of tools to test, configure and use the whole camera subsystem, including the external camera sensor and the camera interface. V4l2-ctl is one of the most usefull utility.
- V4L2 libraries (libv4l) (User space)
A set of libraries on top of the V4L2 Linux kernel interface which abstract the kernel interface in order to simplify, keep compatibility or add some hooks between V4L-based applications and the V4L2 kernel interface.
- yavta (User space)
Yavta is a test tool which relies on the V4L2 Linux kernel interface.
- V4L2 core (Kernel space)
This layer represents the standard Linux kernel V4L2 Framework.
- stm32-dcmi (Kernel space)
This V4L2 DCMI Linux device driver handles the DCMI hardware block.
- Camera sensor X driver (Kernel space)
This V4L2 Linux device driver handles the camera sensor X external peripheral, handles some GPIOs lines and potentially power supplies to power-up/down the camera sensor. The communication with camera sensor is done through the i2c bus.
- DCMI (Hardware)
The Digital Camera Memory Interface hardware block.
- Camera sensor X (Hardware)
The camera sensor external peripheral.
2.2 APIs description[edit]
The V4L2 userland API is documented in the Linux Media subsystem documentation[2]
The V4L2 kernel framework internal API is documented in the V4L2 Kernel Support section of the Linux Kernel documentation[3]
3 Configuration[edit]
3.1 Kernel configuration[edit]
The STM32 camera interface and OV5640 camera sensor are enabled by default in STMicroelectronics deliveries.
Nevertheless this is not the case when using upstream kernel version. In this case, the DCMI V4L2 driver can be enabled using Linux kernel menuconfig tool:
[*] Device Drivers ---> [*] Multimedia support ---> [*] V4L platform devices ---> [*] STM32 Digital Camera Memory Interface (DCMI) support
The external camera sensor connected to the camera interface must also be enabled, here is an example with the OV5640 Omnivision camera sensor located on the MB1379 camera daughter board[4] connected to the CN7 camera connector[5] of the STM32MP15 evaluation board[6]:
[*] Device Drivers ---> [*] Multimedia support ---> I2C Encoders, decoders, sensors and other helper chips ---> [*] OmniVision OV5640 sensor support
3.2 Device tree configuration[edit]
Refer to DCMI device tree configuration article for a complete view of DCMI & sensor configuration thanks to Linux kernel device tree mechanism.
4 How to use the framework[edit]
The use cases described here are enabled using V4l2-ctl, gst-launch or gst-play command line utilities.
4.1 List the video devices and their capabilities[edit]
List all the available video devices using --list-devices option:
v4l2-ctl --list-devices
STM32 Camera Memory Interface (platform:dcmi): /dev/video0
If several devices are available, use -d option after any V4l2-ctl commands to target a specific device. If -d option is not specified, /dev/video0 is targeted by default.
In order to have information on a specific device, use -D option:
v4l2-ctl -d /dev/video0 -D
Driver Info (not using libv4l2): Driver name : stm32-dcmi Card type : STM32 Camera Memory Interface Bus info : platform:dcmi Driver version: X.Y.Z Capabilities : 0x85200001 Video Capture Read/Write Streaming Extended Pix Format Device Capabilities Device Caps : 0x05200001 Video Capture Read/Write Streaming Extended Pix Format
4.2 Controlling camera[edit]
Use V4l2-ctl with -L option to get the list of supported controls:
v4l2-ctl -L
User Controls contrast (int) : min=0 max=255 step=1 default=0 value=0 flags=slider saturation (int) : min=0 max=255 step=1 default=64 value=64 flags=slider hue (int) : min=0 max=359 step=1 default=0 value=0 flags=slider white_balance_automatic (bool) : default=1 value=1 flags=update red_balance (int) : min=0 max=4095 step=1 default=0 value=128 flags=inactive, slider blue_balance (int) : min=0 max=4095 step=1 default=0 value=128 flags=inactive, slider exposure (int) : min=0 max=65535 step=1 default=0 value=885 flags=inactive, volatile gain_automatic (bool) : default=1 value=1 flags=update gain (int) : min=0 max=1023 step=1 default=0 value=32 flags=inactive, volatile horizontal_flip (bool) : default=0 value=0 vertical_flip (bool) : default=0 value=0 Camera Controls auto_exposure (menu) : min=0 max=1 default=0 value=0 flags=update 0: Auto Mode 1: Manual Mode Image Processing Controls test_pattern (menu) : min=0 max=1 default=0 value=0 0: Disabled 1: Color bars
![]() |
"value=" field returns the current value of the control |
The control value can be changed thanks to --set-ctrl option, for example:
v4l2-ctl --set-ctrl test_pattern=1
The control value can be changed dynamically. In the following example, the color bar is enabled/disabled while preview is running:
- Start preview in background
gst-launch-1.0 v4l2src ! "video/x-raw, width=1280, Height=720, framerate=(fraction)15/1" ! queue ! autovideosink -e &
- Then alternate the color bar activation or not
v4l2-ctl --set-ctrl test_pattern=1;sleep 1;v4l2-ctl --set-ctrl test_pattern=0;sleep 1;v4l2-ctl --set-ctrl test_pattern=1;sleep 1;v4l2-ctl --set-ctrl test_pattern=0;killall gst-launch-1.0
- Horizontal/vertical flip can also be changed while preview is running:
v4l2-ctl --set-ctrl horizontal_flip=1;sleep 2;v4l2-ctl --set-ctrl horizontal_flip=0;sleep 2;v4l2-ctl --set-ctrl vertical_flip=1;sleep 2;v4l2-ctl --set-ctrl vertical_flip=0;killall gst-launch-1.0
4.3 Set the pixel format, resolution and framerate[edit]
Use --list-formats-ext option to get the supported pixel format, resolution and framerate:
v4l2-ctl --list-formats-ext
ioctl: VIDIOC_ENUM_FMT Index : 0 Type : Video Capture Pixel Format: 'JPEG' (compressed) Name : JFIF JPEG Size: Discrete 176x144 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 320x240 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 640x480 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 720x480 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 720x576 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 1024x768 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 1280x720 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 1920x1080 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 2592x1944 Interval: Discrete 0.067s (15.000 fps) Index : 1 Type : Video Capture Pixel Format: 'UYVY' Name : UYVY 4:2:2 Size: Discrete 176x144 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 320x240 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 640x480 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 720x480 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 720x576 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 1024x768 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 1280x720 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 1920x1080 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 2592x1944 Interval: Discrete 0.067s (15.000 fps) Index : 2 Type : Video Capture Pixel Format: 'YUYV' Name : YUYV 4:2:2 Size: Discrete 176x144 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 320x240 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 640x480 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 720x480 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 720x576 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 1024x768 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 1280x720 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 1920x1080 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 2592x1944 Interval: Discrete 0.067s (15.000 fps) Index : 3 Type : Video Capture Pixel Format: 'RGBP' Name : 16-bit RGB 5-6-5 Size: Discrete 176x144 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 320x240 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 640x480 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 720x480 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 720x576 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 1024x768 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 1280x720 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 1920x1080 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 2592x1944 Interval: Discrete 0.067s (15.000 fps)
In order to change the camera configuration, select first the framerate using --set-parm option:
v4l2-ctl --set-parm=30
Then select the wanted resolution and/or pixel format using --set-fmt-video option:
v4l2-ctl --set-fmt-video=width=320,height=240,pixelformat=RGBP
4.4 Set the framerate[edit]
- With V4l2-ctl, use --set-parm option giving the framerate numerator only, the denominator is fixed to 1 (only integer framerate values are allowed):
v4l2-ctl --set-parm=<framerate numerator>
Take 100 VGA pictures at 30fps:
v4l2-ctl --set-parm=30;v4l2-ctl --set-fmt-video=width=640,height=480,pixelformat=JPEG --stream-mmap --stream-count=100 --stream-to=pics@30fps.jpeg
Replay at 30fps using gst-play:
gst-play-1.0 pics@30fps.jpeg --videosink="videorate ! video/x-raw, framerate=(fraction)30/1 ! autovideosink"
Take 100 VGA pictures at 15fps:
v4l2-ctl --set-parm=15;v4l2-ctl --set-fmt-video=width=640,height=480,pixelformat=JPEG --stream-mmap --stream-count=100 --stream-to=pics@15fps.jpeg
Replay at 15fps using gst-play:
gst-play-1.0 pics@15fps.jpeg --videosink="videorate ! video/x-raw, framerate=(fraction)15/1 ! autovideosink"
- With GStreamer, using framerate caps:
gst-launch-1.0 v4l2src ! "video/x-raw, ... framerate=(fraction)<numerator>/<denominator>" ! ...
Preview VGA@30fps
gst-launch-1.0 v4l2src ! "video/x-raw, width=640, Height=480, framerate=(fraction)30/1" ! queue ! autovideosink -e
Preview VGA@15fps
gst-launch-1.0 v4l2src ! "video/x-raw, width=640, Height=480, framerate=(fraction)15/1" ! queue ! autovideosink -e
4.5 Grab a raw frame[edit]
Capture a QVGA RGB565 raw frame on disk:
v4l2-ctl --set-fmt-video=width=320,height=240,pixelformat=RGBP --stream-mmap --stream-count=1 --stream-to=grab-320x240-rgb565.raw
In order to display it, this raw frame must be converted first to JPEG:
gst-launch-1.0 filesrc location= grab-320x240-rgb565.raw blocksize=153600 ! "video/x-raw, format=(string)RGB16, width=(int)320, height=(int)240, framerate=(fraction)30/1" ! videoconvert ! jpegenc ! filesink location=grab-320x240-rgb565.jpeg
Then weston-image utility can be used to display this JPEG file:
weston-image grab-320x240-rgb565.jpeg
4.6 Fullscreen preview[edit]
gst-launch-1.0 v4l2src ! "video/x-raw, width=1280, Height=720, framerate=(fraction)15/1" ! queue ! autovideosink -e
![]() |
Please note that GStreamer overwrites all the parameters that could have been previously set on the video device (for ex. parameters set through V4l2-ctl commands such as resolution, pixel format, framerate, ...) |
4.7 Take a picture[edit]
Capture a 5Mp JPEG:
v4l2-ctl --set-parm=15; v4l2-ctl --set-fmt-video=width=2592,height=1944,pixelformat=JPEG --stream-mmap --stream-count=1 --stream-skip=3 --stream-to=pic-5Mp.jpeg; v4l2-ctl --set-parm=30
Then display it:
weston-image pic-5Mp.jpeg
You can check the picture resolution using gst-typefind:
gst-typefind-1.0 pic-5Mp.jpeg
pic-5Mp.jpeg - image/jpeg, width=(int)2592, height=(int)1944, sof-marker=(int)0
4.8 Pictures streaming over network[edit]
Refer to How to stream camera over network article to get some examples on how to stream camera content over network.
5 How to trace and debug[edit]
5.1 How to monitor[edit]
5.1.1 Check of devicetree configuration[edit]
Here are some commands to verify that DCMI is enabled, check which camera sensor is used and log other details about devicetree settings:
rm devicetree.txt echo "[devicetree]" >> devicetree.txt echo "|-[dcmi]" >> devicetree.txt find /proc/device-tree/soc | grep dcmi | sed 's/\/proc\/device-tree\/soc\//| |-/' >> devicetree.txt echo "|" >> devicetree.txt echo "|-[camera:" | tr -d "\n" >> devicetree.txt cat /proc/device-tree/soc/i2c*/camera*/compatible >> devicetree.txt echo "]" >> devicetree.txt find /proc/device-tree/soc | grep camera | sed 's/\/proc\/device-tree\/soc\// |-/' >> devicetree.txt echo "" >> devicetree.txt cat devicetree.txt
[devicetree] |-[dcmi] | |-dcmi@4c006000 | |-dcmi@4c006000/compatible | |-dcmi@4c006000/clocks | |-dcmi@4c006000/resets | |-dcmi@4c006000/pinctrl-1 | |-dcmi@4c006000/port | |-dcmi@4c006000/port/endpoint | |-dcmi@4c006000/port/endpoint/hsync-active | |-dcmi@4c006000/port/endpoint/vsync-active | |-dcmi@4c006000/port/endpoint/remote-endpoint | |-dcmi@4c006000/port/endpoint/bus-width | |-dcmi@4c006000/port/endpoint/pclk-sample | |-dcmi@4c006000/port/endpoint/phandle | |-dcmi@4c006000/port/endpoint/linux,phandle | |-dcmi@4c006000/port/endpoint/name | |-dcmi@4c006000/port/name | |-dcmi@4c006000/clock-names | |-dcmi@4c006000/status | |-dcmi@4c006000/interrupts | |-dcmi@4c006000/dma-names | |-dcmi@4c006000/phandle | |-dcmi@4c006000/reg | |-dcmi@4c006000/pinctrl-0 | |-dcmi@4c006000/dmas | |-dcmi@4c006000/linux,phandle | |-dcmi@4c006000/name | |-dcmi@4c006000/pinctrl-names | |-pin-controller/dcmi-sleep@0 | |-pin-controller/dcmi-sleep@0/pins | |-pin-controller/dcmi-sleep@0/pins/pinmux | |-pin-controller/dcmi-sleep@0/pins/name | |-pin-controller/dcmi-sleep@0/phandle | |-pin-controller/dcmi-sleep@0/linux,phandle | |-pin-controller/dcmi-sleep@0/name | |-pin-controller/dcmi@0 | |-pin-controller/dcmi@0/pins | |-pin-controller/dcmi@0/pins/pinmux | |-pin-controller/dcmi@0/pins/bias-disable | |-pin-controller/dcmi@0/pins/name | |-pin-controller/dcmi@0/phandle | |-pin-controller/dcmi@0/linux,phandle | |-pin-controller/dcmi@0/name | |-[camera:ovti,ov5640] |-i2c@40013000/camera@3c |-i2c@40013000/camera@3c/compatible |-i2c@40013000/camera@3c/powerdown-gpios |-i2c@40013000/camera@3c/DOVDD-supply |-i2c@40013000/camera@3c/clocks |-i2c@40013000/camera@3c/rotation |-i2c@40013000/camera@3c/port |-i2c@40013000/camera@3c/port/endpoint |-i2c@40013000/camera@3c/port/endpoint/hsync-active |-i2c@40013000/camera@3c/port/endpoint/vsync-active |-i2c@40013000/camera@3c/port/endpoint/remote-endpoint |-i2c@40013000/camera@3c/port/endpoint/bus-width |-i2c@40013000/camera@3c/port/endpoint/pclk-sample |-i2c@40013000/camera@3c/port/endpoint/phandle |-i2c@40013000/camera@3c/port/endpoint/data-shift |-i2c@40013000/camera@3c/port/endpoint/linux,phandle |-i2c@40013000/camera@3c/port/endpoint/name |-i2c@40013000/camera@3c/port/name |-i2c@40013000/camera@3c/clock-names |-i2c@40013000/camera@3c/status |-i2c@40013000/camera@3c/reset-gpios |-i2c@40013000/camera@3c/phandle |-i2c@40013000/camera@3c/reg |-i2c@40013000/camera@3c/linux,phandle |-i2c@40013000/camera@3c/name
5.2 How to trace[edit]
5.2.1 V4L2 userland API tracing[edit]
Tracing of V4L2 userland API[2] can be enabled using command:
echo 0x3 > /sys/devices/platform/soc/*.dcmi/video4linux/video*/dev_debug
Traces are output in kernel log buffer:
dmesg
[10130.641469] video0: VIDIOC_TRY_FMT: type=vid-cap, width=640, height=480, pixelformat=YUYV, field=none, bytesperline= 1280, sizeimage=614400, colorspace=8, flags=0x0, ycbcr_enc=1, quantization=1, xfer_func=2 [10130.641550] video0: VIDIOC_S_FMT: type=vid-cap, width=640, height=480, pixelformat=YUYV, field=none, bytesperline=12 80, sizeimage=614400, colorspace=8, flags=0x0, ycbcr_enc=1, quantization=1, xfer_func=2 [10130.641597] video0: VIDIOC_G_PARM: type=vid-cap, capability=0x1000, capturemode=0x0, timeperframe=1/30, extendedmode =0, readbuffers=2 [10130.641638] video0: VIDIOC_G_PARM: type=vid-cap, capability=0x1000, capturemode=0x0, timeperframe=1/30, extendedmode =0, readbuffers=2 [10130.641681] video0: VIDIOC_S_PARM: type=vid-cap, capability=0x1000, capturemode=0x0, timeperframe=1/30, extendedmode =0, readbuffers=2 [10130.641740] video0: VIDIOC_G_CTRL: error -22: id=0x980927, value=0 [10130.642770] video0: VIDIOC_REQBUFS: count=0, type=vid-cap, memory=mmap [10130.642819] video0: VIDIOC_CREATE_BUFS: index=0, count=0, memory=mmap, type=vid-cap, width=640, height=480, pixelfor mat=YUYV, field=none, bytesperline=1280, sizeimage=614400, colorspace=8, flags=0x0, ycbcr_enc=1, quantization=1, xfer_f unc=2 [10130.658541] video0: VIDIOC_G_CTRL: error -22: id=0x980927, value=0 [10130.662770] video0: VIDIOC_REQBUFS: count=3, type=vid-cap, memory=mmap [10130.662852] video0: VIDIOC_QUERYBUF: 00:00:00.00000000 index=0, type=vid-cap, flags=0x00002000, field=any, sequence= 0, memory=mmap, bytesused=0, offset/userptr=0x0, length=614400 [10130.662892] timecode=00:00:00 type=0, flags=0x00000000, frames=0, userbits=0x00000000 [10130.662917] video0: VIDIOC_QUERYBUF: 00:00:00.00000000 index=1, type=vid-cap, flags=0x00002000, field=any, sequence= 0, memory=mmap, bytesused=0, offset/userptr=0x96000, length=614400 [10130.662952] timecode=00:00:00 type=0, flags=0x00000000, frames=0, userbits=0x00000000 [10130.662967] video0: VIDIOC_QUERYBUF: 00:00:00.00000000 index=2, type=vid-cap, flags=0x00002000, field=any, sequence= 0, memory=mmap, bytesused=0, offset/userptr=0x12c000, length=614400 [10130.663002] timecode=00:00:00 type=0, flags=0x00000000, frames=0, userbits=0x00000000 [10130.666880] video0: VIDIOC_STREAMON: type=vid-cap [10130.857484] video0: VIDIOC_CREATE_BUFS: index=3, count=1, memory=mmap, type=vid-cap, width=640, height=480, pixelfor mat=YUYV, field=none, bytesperline=1280, sizeimage=614400, colorspace=8, flags=0x0, ycbcr_enc=1, quantization=1, xfer_f unc=2 [10130.857585] video0: VIDIOC_QUERYBUF: 00:00:00.00000000 index=3, type=vid-cap, flags=0x00002000, field=any, sequence= 0, memory=mmap, bytesused=0, offset/userptr=0x1c2000, length=614400 [10130.857627] timecode=00:00:00 type=0, flags=0x00000000, frames=0, userbits=0x00000000 [10131.022069] video0: VIDIOC_STREAMOFF: type=vid-cap
5.2.2 V4L2 core framework tracing[edit]
Tracing of the V4L2 core framework[3] can be enabled using commands:
echo 0x3 > /sys/module/videobuf2_core/parameters/debug echo 0x3 > /sys/module/videobuf2_v4l2/parameters/debug
Traces are output in kernel log buffer:
dmesg
[11875.487933] vb2-core: __setup_offsets: buffer 0, plane 0 offset 0x00000000 [11875.501731] vb2-core: __setup_offsets: buffer 1, plane 0 offset 0x001fb000 [11875.514901] vb2-core: __setup_offsets: buffer 2, plane 0 offset 0x003f6000 [11875.532298] vb2-core: __setup_offsets: buffer 3, plane 0 offset 0x005f1000 [11875.540019] vb2-core: __vb2_queue_alloc: allocated 4 buffers, 1 plane(s) each [11875.563689] vb2_dc_mmap: mapped dma addr 0xf1900000 at 0xb4f05000, size 2076672 [11875.571174] vb2-core: vb2_mmap: buffer 0, plane 0 successfully mapped [11875.589656] vb2-core: vb2_core_qbuf: qbuf of buffer 0 succeeded [11875.595684] vb2_dc_mmap: mapped dma addr 0xf1b00000 at 0xb4d0a000, size 2076672 [11875.603062] vb2-core: vb2_mmap: buffer 1, plane 0 successfully mapped [11875.609668] vb2-core: vb2_core_qbuf: qbuf of buffer 1 succeeded [11875.615642] vb2_dc_mmap: mapped dma addr 0xf1d00000 at 0xb4b0f000, size 2076672 [11875.623016] vb2-core: vb2_mmap: buffer 2, plane 0 successfully mapped [11875.629628] vb2-core: vb2_core_qbuf: qbuf of buffer 2 succeeded [11875.635617] vb2_dc_mmap: mapped dma addr 0xf1f00000 at 0xb4914000, size 2076672 [11875.642952] vb2-core: vb2_mmap: buffer 3, plane 0 successfully mapped [11875.649715] vb2-core: vb2_core_qbuf: qbuf of buffer 3 succeeded [11875.734058] vb2-core: vb2_core_streamon: successful [11875.961291] vb2-core: vb2_buffer_done: done processing on buffer 0, state: 6 [11875.967036] vb2-core: vb2_core_dqbuf: returning done buffer [11875.972437] vb2-core: vb2_core_dqbuf: dqbuf of buffer 0, with state 0 [11876.094639] vb2-core: vb2_buffer_done: done processing on buffer 1, state: 6 [11876.100367] vb2-core: vb2_core_dqbuf: returning done buffer [11876.105788] vb2-core: vb2_core_dqbuf: dqbuf of buffer 1, with state 0
5.2.3 DCMI V4L2 kernel driver tracing[edit]
DCMI dynamic debug traces[7] can be enabled using command:
echo "module stm32_dcmi +p" > /sys/kernel/debug/dynamic_debug/control
Here is an example with a 5Mp jpeg capture:
gst-launch-1.0 v4l2src ! image/jpeg, width=2592, height=1944 ! fakesink dmesg
[12706.715949] stm32-dcmi 4c006000.dcmi: Sensor format set to 0x4001 2592x1944 [12706.721548] stm32-dcmi 4c006000.dcmi: Buffer format set to JPEG 2592x1944 [12707.365947] stm32-dcmi 4c006000.dcmi: Sensor format set to 0x4001 2592x1944 [12707.371551] stm32-dcmi 4c006000.dcmi: Buffer format set to JPEG 2592x1944 [12707.437537] stm32-dcmi 4c006000.dcmi: Sensor format set to 0x4001 2592x1944 [12707.443042] stm32-dcmi 4c006000.dcmi: Buffer format set to JPEG 2592x1944 [12707.459767] stm32-dcmi 4c006000.dcmi: Setup queue, count=4, size=5038848 [12707.518914] stm32-dcmi 4c006000.dcmi: buffer[0] phy=0xf1900000 size=5038848 [12707.526068] stm32-dcmi 4c006000.dcmi: buffer[1] phy=0xf1e00000 size=5038848 [12707.533299] stm32-dcmi 4c006000.dcmi: buffer[2] phy=0xf2300000 size=5038848 [12707.541456] stm32-dcmi 4c006000.dcmi: buffer[3] phy=0xf2800000 size=5038848 [12707.551443] stm32-dcmi 4c006000.dcmi: Start streaming, starting capture [12707.820885] stm32-dcmi 4c006000.dcmi: buffer[0] done seq=0, bytesused=499936 [12708.087436] stm32-dcmi 4c006000.dcmi: buffer[1] done seq=1, bytesused=447472 [12708.306415] stm32-dcmi 4c006000.dcmi: Stop streaming, errors=0 (overrun=0), buffers=2 [12708.319095] stm32-dcmi 4c006000.dcmi: Start streaming, starting capture [12708.333571] stm32-dcmi 4c006000.dcmi: Stop streaming, errors=0 (overrun=0), buffers=0
5.3 How to debug[edit]
5.3.1 Errors[edit]
Errors are unconditionnaly traced in kernel log:
dmesg [ 87.233672] stm32-dcmi 4c006000.dcmi: Some errors found while streaming: errors=1 (overrun=1), buffers=24
5.3.2 Memory tracking[edit]
Frames require large chunks of contiguous memory, they are allocated by V4L2 framework through DMA backend. Those allocations can be traced using:
echo "module dma_contiguous +p" > /sys/kernel/debug/dynamic_debug/control echo "module videobuf2_dma_contig +p" > /sys/kernel/debug/dynamic_debug/control
Here is the trace after a VGA preview
[11311.617688] vb2_dc_mmap: mapped dma addr 0xf1900000 at 0xb3b6a000, size 614400 [11311.617986] vb2_dc_mmap: mapped dma addr 0xf1a00000 at 0xb3ad4000, size 614400 [11311.618071] vb2_dc_mmap: mapped dma addr 0xf1b00000 at 0xb3a3e000, size 614400 [11311.764146] vb2_dc_mmap: mapped dma addr 0xf1c00000 at 0xb307c000, size 614400
4 frames of VGA YUV422 frames: 640x480x2=614400 bytes
6 Source code location[edit]
6.1 User space[edit]
6.2 Kernel space[edit]
7 References[edit]
- ↑ Information about V4L2 Linux kernel framework on wikipedia.
- ↑ 2.02.1 Linux Media Infrastructure userspace API » Part I - Video for Linux API
- ↑ 3.03.1 Media subsystem kernel internal API » 1. Video4Linux devices
- ↑ MB1379 camera daughter board
- ↑ STM32MP157x-EV1 Evaluation board CN7 Camera sensor connector
- ↑ STM32MP15 evaluation board
- ↑ How to use the kernel dynamic debug
This article gives information about the Linux<sup>®</sup> V4L2 camera framework. == Framework purpose == The V4L2 Linux kernel framework<ref>[https://en.wikipedia.org/wiki/Video4Linux Information about V4L2 Linux kernel framework on wikipedia].</ref> allows to control both an external camera sensor and the camera interface in order to capture raw frames in various pixel formats or encoded stream data such as JPEG. This could be typically used, with the help of other Linux multimedia frameworks and applications, to take snapshot, to make preview, to make a video recording or even remotely stream images from the camera sensor. == System overview == [[File:CAMERAOverview.png|link=]] === Component description === *'''Application''' (User space) Any application relying on V4L2 Linux kernel interface or libv4l abstraction layer. [[GStreamer overview|GStreamer]] framework provides such application. *'''V4L2 utilities''' (User space) A set of tools to test, configure and use the whole camera subsystem, including the external camera sensor and the camera interface. [[V4l2-ctl]] is one of the most usefull utility. *'''V4L2 libraries (libv4l)''' (User space) A set of libraries on top of the V4L2 Linux kernel interface which abstract the kernel interface in order to simplify, keep compatibility or add some hooks between V4L-based applications and the V4L2 kernel interface. *'''yavta''' (User space) [[Yavta]] is a test tool which relies on the V4L2 Linux kernel interface. *'''V4L2 core''' (Kernel space) This layer represents the standard Linux kernel V4L2 Framework. *'''stm32-dcmi''' (Kernel space) This V4L2 DCMI Linux device driver handles the [[DCMI internal peripheral|DCMI hardware block]]. *'''Camera sensor X driver''' (Kernel space) This V4L2 Linux device driver handles the camera sensor X external peripheral, handles some GPIOs lines and potentially power supplies to power-up/down the camera sensor. The communication with camera sensor is done through the i2c bus. *'''DCMI''' (Hardware) The [[DCMI internal peripheral|Digital Camera Memory Interface hardware block]]. *'''Camera sensor X''' (Hardware) The camera sensor external peripheral. === APIs description === The V4L2 userland API is documented in the Linux Media subsystem documentation<ref name=API>[https://www.linuxtvkernel.org/downloads/v4l-dvb-apis-new/uapidoc/html/latest/userspace-api/media/v4l/v4l2.html Linux Media Infrastructure userspace API » Part I - Video for Linux API]</ref> The V4L2 kernel framework internal API is documented in the V4L2 Kernel Support section of the Linux Kernel documentation<ref name=core>[https://www.kernel.org/doc/html/latest/{{DocSource | domain=Linux kernel | path=media/kapi/v4l2-core.html | text=Media subsystem kernel internal API » 1. Video4Linux devices]}}</ref> == Configuration == === Kernel configuration === The STM32 camera interface and OV5640 camera sensor are enabled by default in STMicroelectronics deliveries. Nevertheless this is not the case when using upstream kernel version. In this case, the DCMI V4L2 driver can be enabled using [[Menuconfig or how to configure kernel|Linux kernel menuconfig tool]]:<pre> [*] Device Drivers ---> [*] Multimedia support ---> [*] V4L platform devices ---> [*] STM32 Digital Camera Memory Interface (DCMI) support</pre> The external camera sensor connected to the camera interface must also be enabled, here is an example with the OV5640 Omnivision camera sensor located on the MB1379 camera daughter board<ref>[[MB1379 | MB1379 camera daughter board]]</ref> connected to the CN7 camera connector<ref>[[STM32MP157x-EV1 - hardware description#MB1262-CN7|STM32MP157x-EV1 Evaluation board CN7 Camera sensor connector]]</ref> of the STM32MP15 evaluation board<ref>[[STM32MP157x-EV1 - hardware description | STM32MP15 evaluation board]]</ref>: :{{UpdateNeededForNewBoard|Point to the camera connector (if any) of the new board}}<pre> [*] Device Drivers ---> [*] Multimedia support ---> I2C Encoders, decoders, sensors and other helper chips ---> [*] OmniVision OV5640 sensor support</pre> === Device tree configuration === Refer to [[DCMI device tree configuration]] article for a complete view of DCMI & sensor configuration thanks to Linux kernel device tree mechanism. == How to use the framework == The use cases described here are enabled using [[V4l2-ctl]], [https://gstreamer.freedesktop.org/documentation/tools/gst-launch.html# gst-launch] or [[Gst-play|gst-play]] command line utilities. ==== List the video devices and their capabilities ==== List all the available video devices using {{highlight|'''--list-devices'''}} option: {{Board$}} v4l2-ctl {{highlight|'''--list-devices'''}}<pre> STM32 Camera Memory Interface (platform:dcmi): /dev/video0</pre> If several devices are available, use {{HighlightParam|'''-d'''}} option after any [[V4l2-ctl]] commands to target a specific device. If {{HighlightParam|'''-d'''}} option is not specified, /dev/video0 is targeted by default. In order to have information on a specific device, use {{highlight|'''-D'''}} option: {{Board$}} v4l2-ctl {{HighlightParam|'''-d'''}} /dev/video0 {{highlight|'''-D'''}}<pre> Driver Info (not using libv4l2): Driver name : stm32-dcmi Card type : STM32 Camera Memory Interface Bus info : platform:dcmi Driver version: X.Y.Z Capabilities : 0x85200001 Video Capture Read/Write Streaming Extended Pix Format Device Capabilities Device Caps : 0x05200001 Video Capture Read/Write Streaming Extended Pix Format</pre> <br> <br> === Controlling camera === Use [[V4l2-ctl]] with {{highlight|'''-L'''}} option to get the list of supported controls: {{Board$}} v4l2-ctl {{highlight|'''-L'''}}<pre> User Controls contrast (int) : min=0 max=255 step=1 default=0 value=0 flags=slider saturation (int) : min=0 max=255 step=1 default=64 value=64 flags=slider hue (int) : min=0 max=359 step=1 default=0 value=0 flags=slider white_balance_automatic (bool) : default=1 value=1 flags=update red_balance (int) : min=0 max=4095 step=1 default=0 value=128 flags=inactive, slider blue_balance (int) : min=0 max=4095 step=1 default=0 value=128 flags=inactive, slider exposure (int) : min=0 max=65535 step=1 default=0 value=885 flags=inactive, volatile gain_automatic (bool) : default=1 value=1 flags=update gain (int) : min=0 max=1023 step=1 default=0 value=32 flags=inactive, volatile horizontal_flip (bool) : default=0 value=0 vertical_flip (bool) : default=0 value=0 Camera Controls auto_exposure (menu) : min=0 max=1 default=0 value=0 flags=update 0: Auto Mode 1: Manual Mode Image Processing Controls test_pattern (menu) : min=0 max=1 default=0 value=0 0: Disabled 1: Color bars</pre> {{Info|'''"value{{=}}"''' field returns the current value of the control}} The control value can be changed thanks to {{highlight|'''--set-ctrl'''}} option, for example: {{Board$}} v4l2-ctl {{highlight|'''--set-ctrl test_pattern{{=}}1'''}} The control value can be changed dynamically. In the following example, the color bar is enabled/disabled while preview is running: * Start preview in background {{Board$}} gst-launch-1.0 v4l2src ! "video/x-raw, width=1280, Height=720, framerate=(fraction)15/1" ! queue ! autovideosink -e & * Then alternate the color bar activation or not {{Board$}} v4l2-ctl {{highlight|'''--set-ctrl test_pattern{{=}}1'''}};sleep 1;v4l2-ctl {{highlight|'''--set-ctrl test_pattern{{=}}0'''}};sleep 1;v4l2-ctl {{highlight|'''--set-ctrl test_pattern{{=}}1'''}};sleep 1;v4l2-ctl {{highlight|'''--set-ctrl test_pattern{{=}}0'''}};killall gst-launch-1.0 * Horizontal/vertical flip can also be changed while preview is running: {{Board$}} v4l2-ctl {{highlight|'''--set-ctrl horizontal_flip{{=}}1'''}};sleep 2;v4l2-ctl {{highlight|'''--set-ctrl horizontal_flip{{=}}0'''}};sleep 2;v4l2-ctl {{highlight|'''--set-ctrl vertical_flip{{=}}1'''}};sleep 2;v4l2-ctl {{highlight|'''--set-ctrl vertical_flip{{=}}0'''}};killall gst-launch-1.0 === Set the pixel format, resolution and framerate === Use {{highlight|'''--list-formats-ext'''}} option to get the supported pixel format, resolution and framerate: {{Board$}} v4l2-ctl {{highlight|'''--list-formats-ext'''}}<pre> ioctl: VIDIOC_ENUM_FMT Index : 0 Type : Video Capture Pixel Format: 'JPEG' (compressed) Name : JFIF JPEG Size: Discrete 176x144 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 320x240 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 640x480 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 720x480 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 720x576 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 1024x768 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 1280x720 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 1920x1080 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 2592x1944 Interval: Discrete 0.067s (15.000 fps) Index : 1 Type : Video Capture Pixel Format: 'UYVY' Name : UYVY 4:2:2 Size: Discrete 176x144 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 320x240 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 640x480 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 720x480 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 720x576 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 1024x768 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 1280x720 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 1920x1080 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 2592x1944 Interval: Discrete 0.067s (15.000 fps) Index : 2 Type : Video Capture Pixel Format: 'YUYV' Name : YUYV 4:2:2 Size: Discrete 176x144 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 320x240 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 640x480 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 720x480 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 720x576 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 1024x768 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 1280x720 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 1920x1080 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 2592x1944 Interval: Discrete 0.067s (15.000 fps) Index : 3 Type : Video Capture Pixel Format: 'RGBP' Name : 16-bit RGB 5-6-5 Size: Discrete 176x144 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 320x240 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 640x480 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 720x480 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 720x576 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 1024x768 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 1280x720 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 1920x1080 Interval: Discrete 0.067s (15.000 fps) Interval: Discrete 0.033s (30.000 fps) Size: Discrete 2592x1944 Interval: Discrete 0.067s (15.000 fps)</pre> In order to change the camera configuration, select first the framerate using {{highlight|'''--set-parm'''}} option: {{Board$}} v4l2-ctl {{highlight|'''--set-parm{{=}}30'''}} Then select the wanted resolution and/or pixel format using {{highlight|'''--set-fmt-video'''}} option: {{Board$}} v4l2-ctl {{highlight|'''--set-fmt-video{{=}}width{{=}}320,height{{=}}240,pixelformat{{=}}RGBP'''}} === Set the framerate === * With [[V4l2-ctl]], use {{highlight|'''--set-parm'''}} option giving the framerate numerator only, the denominator is fixed to 1 (only integer framerate values are allowed): {{Board$}} v4l2-ctl {{highlight|'''--set-parm{{=}}<framerate numerator>'''}} Take 100 VGA pictures at 30fps: {{Board$}} v4l2-ctl {{highlight|'''--set-parm{{=}}30'''}};v4l2-ctl --set-fmt-video=width=640,height=480,pixelformat=JPEG --stream-mmap --stream-count=100 --stream-to=pics@30fps.jpeg Replay at 30fps using [[Gst-play|gst-play]]: {{Board$}} gst-play-1.0 pics@30fps.jpeg --videosink="videorate ! video/x-raw, framerate=(fraction)30/1 ! autovideosink" Take 100 VGA pictures at 15fps: {{Board$}} v4l2-ctl {{highlight|'''--set-parm{{=}}15'''}};v4l2-ctl --set-fmt-video=width=640,height=480,pixelformat=JPEG --stream-mmap --stream-count=100 --stream-to=pics@15fps.jpeg Replay at 15fps using [[Gst-play|gst-play]]: {{Board$}} gst-play-1.0 pics@15fps.jpeg --videosink="videorate ! video/x-raw, framerate=(fraction)15/1 ! autovideosink" * With [[:Category:GStreamer|GStreamer]], using {{highlight|'''framerate'''}} caps: {{Board$}} gst-launch-1.0 v4l2src ! "video/x-raw, ... {{highlight|'''framerate{{=}}(fraction)<numerator>/<denominator>'''}}" ! ... Preview VGA@30fps {{Board$}} gst-launch-1.0 v4l2src ! "video/x-raw, width=640, Height=480, {{highlight|'''framerate{{=}}(fraction)30/1'''}}" ! queue ! autovideosink -e Preview VGA@15fps {{Board$}} gst-launch-1.0 v4l2src ! "video/x-raw, width=640, Height=480, {{highlight|'''framerate{{=}}(fraction)15/1'''}}" ! queue ! autovideosink -e === Grab a raw frame === Capture a QVGA RGB565 raw frame on disk: {{Board$}} v4l2-ctl --set-fmt-video=width=320,height=240,pixelformat=RGBP --stream-mmap --stream-count=1 --stream-to=grab-320x240-rgb565.raw In order to display it, this raw frame must be converted first to JPEG: {{Board$}} gst-launch-1.0 filesrc location= grab-320x240-rgb565.raw blocksize=153600 ! "video/x-raw, format=(string)RGB16, width=(int)320, height=(int)240, framerate=(fraction)30/1" ! videoconvert ! jpegenc ! filesink location=grab-320x240-rgb565.jpeg Then [[Wayland Weston overview#Display_some_images|weston-image]] utility can be used to display this JPEG file: {{Board$}} weston-image grab-320x240-rgb565.jpeg === Fullscreen preview === {{Board$}} gst-launch-1.0 v4l2src ! "video/x-raw, width=1280, Height=720, framerate=(fraction)15/1" ! queue ! autovideosink -e {{Info|Please note that GStreamer overwrites all the parameters that could have been previously set on the video device (for ex. parameters set through [[V4l2-ctl]] commands such as resolution, pixel format, framerate, ...)}} === Take a picture === Capture a 5Mp JPEG: {{Board$}} v4l2-ctl --set-parm=15; v4l2-ctl --set-fmt-video=width=2592,height=1944,pixelformat=JPEG --stream-mmap --stream-count=1 --stream-skip=3 --stream-to=pic-5Mp.jpeg; v4l2-ctl --set-parm=30 Then display it: {{Board$}} weston-image pic-5Mp.jpeg You can check the picture resolution using [[Gst-typefind|gst-typefind]]: {{Board$}} gst-typefind-1.0 pic-5Mp.jpeg pic-5Mp.jpeg - image/jpeg, width=(int)2592, height=(int)1944, sof-marker=(int)0 === Pictures streaming over network === Refer to [[How to stream camera over network]] article to get some examples on how to stream camera content over network. == How to trace and debug == === How to monitor === ==== Check of devicetree configuration ==== Here are some commands to verify that DCMI is enabled, check which camera sensor is used and log other details about devicetree settings:<pre> rm devicetree.txt echo "[devicetree]" >> devicetree.txt echo "|-[dcmi]" >> devicetree.txt find /proc/device-tree/soc | grep dcmi | sed 's/\/proc\/device-tree\/soc\//| |-/' >> devicetree.txt echo "|" >> devicetree.txt echo "|-[camera:" | tr -d "\n" >> devicetree.txt cat /proc/device-tree/soc/i2c*/camera*/compatible >> devicetree.txt echo "]" >> devicetree.txt find /proc/device-tree/soc | grep camera | sed 's/\/proc\/device-tree\/soc\// |-/' >> devicetree.txt echo "" >> devicetree.txt cat devicetree.txt</pre> <pre> [devicetree] |-[dcmi] | |-dcmi@4c006000 | |-dcmi@4c006000/compatible | |-dcmi@4c006000/clocks | |-dcmi@4c006000/resets | |-dcmi@4c006000/pinctrl-1 | |-dcmi@4c006000/port | |-dcmi@4c006000/port/endpoint | |-dcmi@4c006000/port/endpoint/hsync-active | |-dcmi@4c006000/port/endpoint/vsync-active | |-dcmi@4c006000/port/endpoint/remote-endpoint | |-dcmi@4c006000/port/endpoint/bus-width | |-dcmi@4c006000/port/endpoint/pclk-sample | |-dcmi@4c006000/port/endpoint/phandle | |-dcmi@4c006000/port/endpoint/linux,phandle | |-dcmi@4c006000/port/endpoint/name | |-dcmi@4c006000/port/name | |-dcmi@4c006000/clock-names | |-dcmi@4c006000/status | |-dcmi@4c006000/interrupts | |-dcmi@4c006000/dma-names | |-dcmi@4c006000/phandle | |-dcmi@4c006000/reg | |-dcmi@4c006000/pinctrl-0 | |-dcmi@4c006000/dmas | |-dcmi@4c006000/linux,phandle | |-dcmi@4c006000/name | |-dcmi@4c006000/pinctrl-names | |-pin-controller/dcmi-sleep@0 | |-pin-controller/dcmi-sleep@0/pins | |-pin-controller/dcmi-sleep@0/pins/pinmux | |-pin-controller/dcmi-sleep@0/pins/name | |-pin-controller/dcmi-sleep@0/phandle | |-pin-controller/dcmi-sleep@0/linux,phandle | |-pin-controller/dcmi-sleep@0/name | |-pin-controller/dcmi@0 | |-pin-controller/dcmi@0/pins | |-pin-controller/dcmi@0/pins/pinmux | |-pin-controller/dcmi@0/pins/bias-disable | |-pin-controller/dcmi@0/pins/name | |-pin-controller/dcmi@0/phandle | |-pin-controller/dcmi@0/linux,phandle | |-pin-controller/dcmi@0/name | |-[camera:ovti,ov5640] |-i2c@40013000/camera@3c |-i2c@40013000/camera@3c/compatible |-i2c@40013000/camera@3c/powerdown-gpios |-i2c@40013000/camera@3c/DOVDD-supply |-i2c@40013000/camera@3c/clocks |-i2c@40013000/camera@3c/rotation |-i2c@40013000/camera@3c/port |-i2c@40013000/camera@3c/port/endpoint |-i2c@40013000/camera@3c/port/endpoint/hsync-active |-i2c@40013000/camera@3c/port/endpoint/vsync-active |-i2c@40013000/camera@3c/port/endpoint/remote-endpoint |-i2c@40013000/camera@3c/port/endpoint/bus-width |-i2c@40013000/camera@3c/port/endpoint/pclk-sample |-i2c@40013000/camera@3c/port/endpoint/phandle |-i2c@40013000/camera@3c/port/endpoint/data-shift |-i2c@40013000/camera@3c/port/endpoint/linux,phandle |-i2c@40013000/camera@3c/port/endpoint/name |-i2c@40013000/camera@3c/port/name |-i2c@40013000/camera@3c/clock-names |-i2c@40013000/camera@3c/status |-i2c@40013000/camera@3c/reset-gpios |-i2c@40013000/camera@3c/phandle |-i2c@40013000/camera@3c/reg |-i2c@40013000/camera@3c/linux,phandle |-i2c@40013000/camera@3c/name</pre> === How to trace === ==== V4L2 userland API tracing ==== Tracing of V4L2 userland API<ref name=API/> can be enabled using command: {{Board$}} echo 0x3 > /sys/devices/platform/soc/*.dcmi/video4linux/video*/dev_debug Traces are output in kernel log buffer: {{Board$}} dmesg<pre> [10130.641469] video0: VIDIOC_TRY_FMT: type=vid-cap, width=640, height=480, pixelformat=YUYV, field=none, bytesperline= 1280, sizeimage=614400, colorspace=8, flags=0x0, ycbcr_enc=1, quantization=1, xfer_func=2 [10130.641550] video0: VIDIOC_S_FMT: type=vid-cap, width=640, height=480, pixelformat=YUYV, field=none, bytesperline=12 80, sizeimage=614400, colorspace=8, flags=0x0, ycbcr_enc=1, quantization=1, xfer_func=2 [10130.641597] video0: VIDIOC_G_PARM: type=vid-cap, capability=0x1000, capturemode=0x0, timeperframe=1/30, extendedmode =0, readbuffers=2 [10130.641638] video0: VIDIOC_G_PARM: type=vid-cap, capability=0x1000, capturemode=0x0, timeperframe=1/30, extendedmode =0, readbuffers=2 [10130.641681] video0: VIDIOC_S_PARM: type=vid-cap, capability=0x1000, capturemode=0x0, timeperframe=1/30, extendedmode =0, readbuffers=2 [10130.641740] video0: VIDIOC_G_CTRL: error -22: id=0x980927, value=0 [10130.642770] video0: VIDIOC_REQBUFS: count=0, type=vid-cap, memory=mmap [10130.642819] video0: VIDIOC_CREATE_BUFS: index=0, count=0, memory=mmap, type=vid-cap, width=640, height=480, pixelfor mat=YUYV, field=none, bytesperline=1280, sizeimage=614400, colorspace=8, flags=0x0, ycbcr_enc=1, quantization=1, xfer_f unc=2 [10130.658541] video0: VIDIOC_G_CTRL: error -22: id=0x980927, value=0 [10130.662770] video0: VIDIOC_REQBUFS: count=3, type=vid-cap, memory=mmap [10130.662852] video0: VIDIOC_QUERYBUF: 00:00:00.00000000 index=0, type=vid-cap, flags=0x00002000, field=any, sequence= 0, memory=mmap, bytesused=0, offset/userptr=0x0, length=614400 [10130.662892] timecode=00:00:00 type=0, flags=0x00000000, frames=0, userbits=0x00000000 [10130.662917] video0: VIDIOC_QUERYBUF: 00:00:00.00000000 index=1, type=vid-cap, flags=0x00002000, field=any, sequence= 0, memory=mmap, bytesused=0, offset/userptr=0x96000, length=614400 [10130.662952] timecode=00:00:00 type=0, flags=0x00000000, frames=0, userbits=0x00000000 [10130.662967] video0: VIDIOC_QUERYBUF: 00:00:00.00000000 index=2, type=vid-cap, flags=0x00002000, field=any, sequence= 0, memory=mmap, bytesused=0, offset/userptr=0x12c000, length=614400 [10130.663002] timecode=00:00:00 type=0, flags=0x00000000, frames=0, userbits=0x00000000 [10130.666880] video0: VIDIOC_STREAMON: type=vid-cap [10130.857484] video0: VIDIOC_CREATE_BUFS: index=3, count=1, memory=mmap, type=vid-cap, width=640, height=480, pixelfor mat=YUYV, field=none, bytesperline=1280, sizeimage=614400, colorspace=8, flags=0x0, ycbcr_enc=1, quantization=1, xfer_f unc=2 [10130.857585] video0: VIDIOC_QUERYBUF: 00:00:00.00000000 index=3, type=vid-cap, flags=0x00002000, field=any, sequence= 0, memory=mmap, bytesused=0, offset/userptr=0x1c2000, length=614400 [10130.857627] timecode=00:00:00 type=0, flags=0x00000000, frames=0, userbits=0x00000000 [10131.022069] video0: VIDIOC_STREAMOFF: type=vid-cap</pre> ==== V4L2 core framework tracing ==== Tracing of the V4L2 core framework<ref name=core/> can be enabled using commands: {{Board$}} echo 0x3 > /sys/module/videobuf2_core/parameters/debug {{Board$}} echo 0x3 > /sys/module/videobuf2_v4l2/parameters/debug Traces are output in kernel log buffer: {{Board$}} dmesg<pre> [11875.487933] vb2-core: __setup_offsets: buffer 0, plane 0 offset 0x00000000 [11875.501731] vb2-core: __setup_offsets: buffer 1, plane 0 offset 0x001fb000 [11875.514901] vb2-core: __setup_offsets: buffer 2, plane 0 offset 0x003f6000 [11875.532298] vb2-core: __setup_offsets: buffer 3, plane 0 offset 0x005f1000 [11875.540019] vb2-core: __vb2_queue_alloc: allocated 4 buffers, 1 plane(s) each [11875.563689] vb2_dc_mmap: mapped dma addr 0xf1900000 at 0xb4f05000, size 2076672 [11875.571174] vb2-core: vb2_mmap: buffer 0, plane 0 successfully mapped [11875.589656] vb2-core: vb2_core_qbuf: qbuf of buffer 0 succeeded [11875.595684] vb2_dc_mmap: mapped dma addr 0xf1b00000 at 0xb4d0a000, size 2076672 [11875.603062] vb2-core: vb2_mmap: buffer 1, plane 0 successfully mapped [11875.609668] vb2-core: vb2_core_qbuf: qbuf of buffer 1 succeeded [11875.615642] vb2_dc_mmap: mapped dma addr 0xf1d00000 at 0xb4b0f000, size 2076672 [11875.623016] vb2-core: vb2_mmap: buffer 2, plane 0 successfully mapped [11875.629628] vb2-core: vb2_core_qbuf: qbuf of buffer 2 succeeded [11875.635617] vb2_dc_mmap: mapped dma addr 0xf1f00000 at 0xb4914000, size 2076672 [11875.642952] vb2-core: vb2_mmap: buffer 3, plane 0 successfully mapped [11875.649715] vb2-core: vb2_core_qbuf: qbuf of buffer 3 succeeded [11875.734058] vb2-core: vb2_core_streamon: successful [11875.961291] vb2-core: vb2_buffer_done: done processing on buffer 0, state: 6 [11875.967036] vb2-core: vb2_core_dqbuf: returning done buffer [11875.972437] vb2-core: vb2_core_dqbuf: dqbuf of buffer 0, with state 0 [11876.094639] vb2-core: vb2_buffer_done: done processing on buffer 1, state: 6 [11876.100367] vb2-core: vb2_core_dqbuf: returning done buffer [11876.105788] vb2-core: vb2_core_dqbuf: dqbuf of buffer 1, with state 0</pre> ==== DCMI V4L2 kernel driver tracing ==== DCMI dynamic debug traces<ref>[[How to use the kernel dynamic debug]]</ref> can be enabled using command: {{Board$}} echo "module stm32_dcmi +p" > /sys/kernel/debug/dynamic_debug/control Here is an example with a 5Mp jpeg capture: {{Board$}} gst-launch-1.0 v4l2src ! image/jpeg, width=2592, height=1944 ! fakesink {{Board$}} dmesg<pre> [12706.715949] stm32-dcmi 4c006000.dcmi: Sensor format set to 0x4001 2592x1944 [12706.721548] stm32-dcmi 4c006000.dcmi: Buffer format set to JPEG 2592x1944 [12707.365947] stm32-dcmi 4c006000.dcmi: Sensor format set to 0x4001 2592x1944 [12707.371551] stm32-dcmi 4c006000.dcmi: Buffer format set to JPEG 2592x1944 [12707.437537] stm32-dcmi 4c006000.dcmi: Sensor format set to 0x4001 2592x1944 [12707.443042] stm32-dcmi 4c006000.dcmi: Buffer format set to JPEG 2592x1944 [12707.459767] stm32-dcmi 4c006000.dcmi: Setup queue, count=4, size=5038848 [12707.518914] stm32-dcmi 4c006000.dcmi: buffer[0] phy=0xf1900000 size=5038848 [12707.526068] stm32-dcmi 4c006000.dcmi: buffer[1] phy=0xf1e00000 size=5038848 [12707.533299] stm32-dcmi 4c006000.dcmi: buffer[2] phy=0xf2300000 size=5038848 [12707.541456] stm32-dcmi 4c006000.dcmi: buffer[3] phy=0xf2800000 size=5038848 [12707.551443] stm32-dcmi 4c006000.dcmi: Start streaming, starting capture [12707.820885] stm32-dcmi 4c006000.dcmi: buffer[0] done seq=0, bytesused=499936 [12708.087436] stm32-dcmi 4c006000.dcmi: buffer[1] done seq=1, bytesused=447472 [12708.306415] stm32-dcmi 4c006000.dcmi: Stop streaming, errors=0 (overrun=0), buffers=2 [12708.319095] stm32-dcmi 4c006000.dcmi: Start streaming, starting capture [12708.333571] stm32-dcmi 4c006000.dcmi: Stop streaming, errors=0 (overrun=0), buffers=0</pre> === How to debug === ==== Errors ==== Errors are unconditionnaly traced in kernel log: {{Board$}} dmesg [ 87.233672] stm32-dcmi 4c006000.dcmi: Some errors found while streaming: errors=1 (overrun=1), buffers=24 ==== Memory tracking ==== Frames require large chunks of contiguous memory, they are allocated by V4L2 framework through DMA backend. Those allocations can be traced using: {{Board$}} echo "module dma_contiguous +p" > /sys/kernel/debug/dynamic_debug/control {{Board$}} echo "module videobuf2_dma_contig +p" > /sys/kernel/debug/dynamic_debug/control Here is the trace after a VGA preview<pre> [11311.617688] vb2_dc_mmap: mapped dma addr 0xf1900000 at 0xb3b6a000, size 614400 [11311.617986] vb2_dc_mmap: mapped dma addr 0xf1a00000 at 0xb3ad4000, size 614400 [11311.618071] vb2_dc_mmap: mapped dma addr 0xf1b00000 at 0xb3a3e000, size 614400 [11311.764146] vb2_dc_mmap: mapped dma addr 0xf1c00000 at 0xb307c000, size 614400</pre> 4 frames of VGA YUV422 frames: 640x480x2=614400 bytes == Source code location == === User space === * [https://git.linuxtv.org/v4l-utils.git V4L2 utilities source code] * [https://git.linuxtv.org/v4l-utils.git V4L2 libraries source code] * [http://git.ideasonboard.org/yavta.git Yavta source code] === Kernel space === * {{CodeSource | Linux kernel | drivers/media/v4l2-core | V4L2 core source code}} * {{CodeSource | Linux kernel | drivers/media/platform/stm32/stm32-dcmi.c | stm32-dcmi V4L2 driver source code}} * {{CodeSource | Linux kernel | drivers/media/i2c | i2c camera sensor V4L2 drivers source code}} ==References== <references /> <noinclude> {{ArticleBasedOnModel | Framework overview article model}} {{PublicationRequestId | 7962 | 2018-07-05 | AlainF}} [[Category:V4L2]]</noinclude>
(One intermediate revision by one other user not shown) | |||
Line 40: | Line 40: | ||
=== APIs description === |
=== APIs description === |
||
− | The V4L2 userland API is documented in the Linux Media subsystem documentation<ref name=API>[https://www. |
+ | The V4L2 userland API is documented in the Linux Media subsystem documentation<ref name=API>[https://www.kernel.org/doc/html/latest/userspace-api/media/v4l/v4l2.html Linux Media Infrastructure userspace API » Part I - Video for Linux API]</ref> |
− | The V4L2 kernel framework internal API is documented in the V4L2 Kernel Support section of the Linux Kernel documentation<ref name=core> |
+ | The V4L2 kernel framework internal API is documented in the V4L2 Kernel Support section of the Linux Kernel documentation<ref name=core>{{DocSource | domain=Linux kernel | path=media/kapi/v4l2-core.html | text=Media subsystem kernel internal API » 1. Video4Linux devices}}</ref> |
== Configuration == |
== Configuration == |