This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1 Usage
The Green template is used to color text in pages, with the "classic MediaWiki orange" (█) color.
Usage: {{Orange|<text to color>}}
Where <text to color> is the text to format in orange. If this template is called with no text, the hexadecimal code of the color is returned.
2 Basic examples
You type | You get |
---|---|
Coloring text in "classic MediaWiki" orange
This is a {{Orange|"classic MediaWiki" color: orange: █}} |
This is a "classic MediaWiki" color: orange: █ |
Getting the hexadecimal code of the color
{{Orange}} is the hexadecimal code of the "classic MediaWiki" orange. |
#FFA500 is the hexadecimal code of the "classic MediaWiki" orange. |
3 More examples
You type | You get |
---|---|
Orange and bold
This is a {{Orange|'''"classic MediaWiki"'''}} color: '''{{Orange|orange: █}}''' |
This is a "classic MediaWiki" color: orange: █ |
Orange and italic
This is a {{Orange|''"classic MediaWiki"''}} color: ''{{Orange|orange: █}}'' |
This is a "classic MediaWiki" color: orange: █ |
4 Maintenance
This template is a template common to all ST wikis.
Modifications must be done into the WikiModel. They must be reviewed by all ST wikis maintainers.
When approved, the template can be pushed/merged towards all ST wikis.
5 Code
#FFA500