- Last edited 2 years ago ago
Component
Contents
1 Usage[edit]
The EcosystemRelease/Component template returns the version of a software component delivered by an ecosystem release revision of the flow associated with this wiki (e.g. v1.y.z ,or v2.y.z, or...).
Usage: {{EcosystemRelease/Component | revision=<revision> | component=<component> | name=<name>}}
Where:
- <revision> is the mandatory revision of the ecosystem release, for which the version of the software component is requested.
- The possible values for this parameter are available in the EcosystemRelease/Revision template.
- <component> is the mandatory software component delivered by the ecosystem release revision, for which the version of the component is requested. The possible values are:
- Linux kernel
- U-Boot
- TF-A
- OP-TEE
- STM32CubeMPU
- OpenEmbedded
- Android
- <name> is the optional parameter that allows to select the way the version name is displayed. Per default (if <name> is not set), the long board name (e.g; "Linux kernel vx.y-stm32mp-[...] (vx.y.z)") is displayed. The possible value for <name> is:
- short: the short version name (e.g. "x.y") is displayed
The returned value is:
- a string that contains the version of the software component delivered by the ecosystem release revision.
- an empty string, if the software component is not delivered by the ecosystem release revision.
- "unknown revision", if <<revision> is not supported.
- "unknown component", if <<component> is not supported.
2 Basic examples[edit]
You type | You get |
---|---|
All components for the v2.1.0 revision requested
Long version names:<br /> {{EcosystemRelease/Component | revision=2.1.0 | component=Linux kernel}}<br /> {{EcosystemRelease/Component | revision=2.1.0 | component=U-Boot}}<br /> {{EcosystemRelease/Component | revision=2.1.0 | component=TF-A}}<br /> {{EcosystemRelease/Component | revision=2.1.0 | component=OP-TEE}}<br /> {{EcosystemRelease/Component | revision=2.1.0 | component=STM32CubeMPU}}<br /> {{EcosystemRelease/Component | revision=2.1.0 | component=OpenEmbedded}}<br /> {{EcosystemRelease/Component | revision=2.1.0 | component=Android}}<br /> Short version names:<br /> {{EcosystemRelease/Component | revision=2.1.0 | component=Linux kernel | name=short}}<br /> {{EcosystemRelease/Component | revision=2.1.0 | component=U-Boot | name=short}}<br /> {{EcosystemRelease/Component | revision=2.1.0 | component=TF-A | name=short}}<br /> {{EcosystemRelease/Component | revision=2.1.0 | component=OP-TEE | name=short}}<br /> {{EcosystemRelease/Component | revision=2.1.0 | component=STM32CubeMPU | name=short}}<br /> {{EcosystemRelease/Component | revision=2.1.0 | component=OpenEmbedded | name=short}}<br /> {{EcosystemRelease/Component | revision=2.1.0 | component=Android | name=short}}<br /> |
Long version names: |
All components for the v2.0.0 revision requested
Long version names:<br /> {{EcosystemRelease/Component | revision=2.0.0 | component=Linux kernel}}<br /> {{EcosystemRelease/Component | revision=2.0.0 | component=U-Boot}}<br /> {{EcosystemRelease/Component | revision=2.0.0 | component=TF-A}}<br /> {{EcosystemRelease/Component | revision=2.0.0 | component=OP-TEE}}<br /> {{EcosystemRelease/Component | revision=2.0.0 | component=STM32CubeMPU}}<br /> {{EcosystemRelease/Component | revision=2.0.0 | component=OpenEmbedded}}<br /> {{EcosystemRelease/Component | revision=2.0.0 | component=Android}}<br /> Short version names:<br /> {{EcosystemRelease/Component | revision=2.0.0 | component=Linux kernel | name=short}}<br /> {{EcosystemRelease/Component | revision=2.0.0 | component=U-Boot | name=short}}<br /> {{EcosystemRelease/Component | revision=2.0.0 | component=TF-A | name=short}}<br /> {{EcosystemRelease/Component | revision=2.0.0 | component=OP-TEE | name=short}}<br /> {{EcosystemRelease/Component | revision=2.0.0 | component=STM32CubeMPU | name=short}}<br /> {{EcosystemRelease/Component | revision=2.0.0 | component=OpenEmbedded | name=short}}<br /> {{EcosystemRelease/Component | revision=2.0.0 | component=Android | name=short}}<br /> |
Long version names: |
Linux kernel version for vx.0.0 revision requested
{{EcosystemRelease/Component | revision=x.0.0 | component=Linux kernel}}<br /> {{EcosystemRelease/Component | revision=x.0.0 | component=Linux kernel | name=short}} |
Linux kernel vx.y (example) |
U-Boot version for vx.0.0 revision requested
{{EcosystemRelease/Component | revision=x.0.0 | component=U-Boot}}<br /> {{EcosystemRelease/Component | revision=x.0.0 | component=U-Boot | name=short}} |
U-Boot vx.y (example) |
TF-A version for vx.0.0 revision requested
{{EcosystemRelease/Component | revision=x.0.0 | component=TF-A}}<br /> {{EcosystemRelease/Component | revision=x.0.0 | component=TF-A | name=short}} |
TF-A vx.y (example) |
OP-TEE version for vx.0.0 revision requested
{{EcosystemRelease/Component | revision=x.0.0 | component=OP-TEE}}<br /> {{EcosystemRelease/Component | revision=x.0.0 | component=OP-TEE | name=short}} |
OP-TEE vx.y (example) |
STM32CubeMPU version for vx.0.0 revision requested
{{EcosystemRelease/Component | revision=x.0.0 | component=STM32CubeMPU}}<br /> {{EcosystemRelease/Component | revision=x.0.0 | component=STM32CubeMPU | name=short}} |
STM32CubeMP1 Package vx.y (example) |
OpenEmbedded version for vx.0.0 revision requested
{{EcosystemRelease/Component | revision=x.0.0 | component=OpenEmbedded}}<br /> {{EcosystemRelease/Component | revision=x.0.0 | component=OpenEmbedded | name=short}} |
OpenEmbedded vx.y (example) |
Android version for vx.1.0 revision requested
{{EcosystemRelease/Component | revision=x.1.0 | component=Android}}<br /> {{EcosystemRelease/Component | revision=x.1.0 | component=Android | name=short}} |
Android vx.y (example) |
3 More examples[edit]
You type | You get |
---|---|
Linux kernel version for vx.2.0 revision requested
{{EcosystemRelease/Component | revision=x.2.0 | component=Linux kernel}}
|
Linux kernel vx.y (example) |
Linux kernel version for vx.1.0 revision requested
{{EcosystemRelease/Component | revision=x.1.0 | component=Linux kernel}}
|
Linux kernel vx.y (example) |
Android version for the vx.0.0 revision requested: Android is not supported by this ecosystem release revision
{{EcosystemRelease/Component | revision=x.0.0 | component=Android}} |
|
U-Boot version for an unspecified revision requested
{{EcosystemRelease/Component | component=U-Boot}}
|
unknown revision |
TF-A version for an unknown revision requested
{{EcosystemRelease/Component | revision=10.20.30 | component=TF-A}}
|
unknown revision |
Unspecified component
{{EcosystemRelease/Component | revision=x.0.0}} |
unknown component |
Unknown component
{{EcosystemRelease/Component | revision=x.0.0 | component=not supported}} |
unknown component |
4 Code[edit]
unknown component