Last edited 3 years ago

Board

1 Usage[edit source]

The Board template is used to indicate for which board(s), an article part (chapter, paragraph, table...) is valid. Per default (i.e. if this template is not used), any part of an article is valid for all boards for which the entire article is valid.

It outputs a "standardized" string that might be used to name an article part.

Usage: {{Board | type=<type>}}
Where:
  • <type> is the mandatory identifier of the board type. The possible values are (see also the part number codification for the STM32MP15 MPUs):
    • 157A-EV1: STM32MP157A-EV1 Evaluation board
    • 157D-EV1: STM32MP157D-EV1 Evaluation board
    • 157C-EV1: STM32MP157C-EV1 Evaluation board
    • 157F-EV1: STM32MP157F-EV1 Evaluation board
    • 157A/D-EV1: STM32MP157A-EV1 or STM32MP157D-EV1 Evaluation board
    • 157C/F-EV1: STM32MP157C-EV1 or STM32MP157F-EV1 Evaluation board
    • 157x-EV1: any Evaluation board with a STM32MP157 MPU
    • 157A-DK1: STM32MP157A-DK1 Discovery kit
    • 157D-DK1: STM32MP157A-DK1 Discovery kit
    • 157C-DK2: STM32MP157C-DK2 Discovery kit
    • 157F-DK2: STM32MP157F-DK2 Discovery kit
    • 157A/D-DK1: STM32MP157A-DK1 or STM32MP157D-DK1 Discovery kit
    • 157C/F-DK2: STM32MP157C-DK2 or STM32MP157F-DK2 Discovery kit
    • 157x-DKx: any Discovery kit with a STM32MP157 MPU

Clicking on the More info.png icon displays the article about the board (e.g. STM32MP157x-DKx - hardware description).

2 Basic examples[edit source]

You type You get
STM32MP157F-EV1 Evaluation board
{{Board | type=157F-EV1}}

STM32MP157F-EV1 Evaluation board More info.png

STM32MP157F-DK2 Discovery kit
{{Board | type=157F-DK2}}

STM32MP157F-DK2 Discovery kit More info.png

3 More examples[edit source]

You type You get
Evaluation boards with a STM32MP157 MPU
{{Board | type=157A-EV1}}<br>
{{Board | type=157D-EV1}}<br>
{{Board | type=157C-EV1}}<br>
{{Board | type=157F-EV1}}<br>
{{Board | type=157A/D-EV1}}<br>
{{Board | type=157C/F-EV1}}<br>
{{Board | type=157x-EV1}}

STM32MP157A-EV1 Evaluation board More info.png
STM32MP157D-EV1 Evaluation board More info.png
STM32MP157C-EV1 Evaluation board More info.png
STM32MP157F-EV1 Evaluation board More info.png
STM32MP157A/D-EV1 Evaluation board More info.png
STM32MP157C/F-EV1 Evaluation board More info.png
STM32MP157x-EV1 Evaluation board More info.png

Discovery kits with a STM32MP157 MPU
{{Board | type=157A-DK1}}<br>
{{Board | type=157D-DK1}}<br>
{{Board | type=157C-DK2}}<br>
{{Board | type=157F-DK2}}<br>
{{Board | type=157A/D-DK1}}<br>
{{Board | type=157C/F-DK2}}<br>
{{Board | type=157x-DKx}}

STM32MP157A-DK1 Discovery kit More info.png
STM32MP157D-DK1 Discovery kit More info.png
STM32MP157C-DK2 Discovery kit More info.png
STM32MP157F-DK2 Discovery kit More info.png
STM32MP157A/D-DK1 Discovery kit More info.png
STM32MP157C/F-DK2 Discovery kit More info.png
STM32MP157x-DKx Discovery kit More info.png

Unspecified board
{{Board}}

STM32MP unknown board type identifier

Unknown boards
{{Board | type=153C-EV1}}<br>
{{Board | type=157C-DK3}}

STM32MP153C-EV1 unknown board type identifier
STM32MP157C-DK3 unknown board type identifier

Check that there's no space before and after the text
BEFORE{{Board | type=157C-EV1}}AFTER<br>
BEFORE{{Board | type=157C-DK2}}AFTER<br>

BEFORESTM32MP157C-EV1 Evaluation board More info.pngAFTER
BEFORESTM32MP157C-DK2 Discovery kit More info.pngAFTER

4 Code[edit source]

STM32MP unknown board type identifier

No categories assignedEdit