Difference between revisions of "TIM internal peripheral"
[quality revision] | [quality revision] |
m
|
m
|
![]() |
This section has not been yet updated for the STM32 MPU ecosystem-v2 flow, so information provided in this section may not be not applicable for v2. We apologize for this inconvenient. |
Contents
1 Article purpose[edit]
The purpose of this article is to
- briefly introduce the TIM peripheral and its main features
- indicate the level of security supported by this hardware block
- explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components
- explain how to configure the TIM peripheral
2 Peripheral overview[edit]
The TIM peripheral is a multi-channel timer unit, available in various configurations, depending on the instance used. There are basically following categories: advanced-control timers, general-purpose timers and basic timers.
The TIM can provide: PWM with complementary output and dead-time insertion, break detection, input capture[1], quadrature encoder[2] interface (typically used for rotary encoders), trigger source for other internal peripherals like: ADC[3], DAC[4], DFSDM[5].
2.1 Features[edit]
The TIM peripheral is available in different configurations, depending on the selected instance :
- TIM1 and TIM8 are advanced-control timers, with 6 independent channels.
- TIM2, TIM3, TIM4 and TIM5 are general-purpose timers, with 4 independent channels.
- TIM12, TIM13 and TIM14 are general-purpose timers, with 2 (TIM12) or 1 (TIM13 and TIM14) independent channels.
- TIM15, TIM16 and TIM17 are also general-purpose timers, with 2 (TIM15) or 1 (TIM16 and TIM17) independent channels. Compare to TIM12, TIM13 and TIM14, this configuration brings some features that are very useful for motor control (like break function, DMA burst mode control, complementary output with dead-time insertion, ...)
- TIM6 and TIM7 are basic timers
Refer to STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to know which features are really implemented.
2.2 Security support[edit]
The TIM is a non-secure peripheral.
3 Peripheral usage and associated software[edit]
3.1 Boot time[edit]
The TIM is not used at boot time.
3.2 Runtime[edit]
3.2.1 Overview[edit]
TIM12 and/or TIM15 can be allocated to:
- the Arm® Cortex®-A7 secure core to be controlled in the secure monitor (TF-A or OP-TEE), to perform HSI and CSI calibrations[6] in RCC.
All TIM instances can be allocated to:
- the Arm® Cortex®-A7 non-secure to be controlled in Linux® by the PWM, the IIO, and/or the IIO Counter frameworks.
or
- the Arm® Cortex®-M4 to be controlled in STM32Cube MPU Package by TIM HAL driver
Note that RCC[7] owns one prescaler per TIM group corresponding to APB1 and APB2 buses: TIMG1PRE and TIMG2PRE, respectively. The allocation to Cortex-A7 or the Cortex-M4 should ideally be done on a per group basis to get independent clocking setup on each side, this is why the TIM instances groups are shown in the summary table below (#Peripheral assignment).
3.2.2 Software frameworks[edit]
Domain | Peripheral | Software frameworks | Comment | ||
---|---|---|---|---|---|
Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) |
Cortex-M4 (STM32Cube) |
|||
Core/Timers | TIM |
TF-A TIM driver
OP-TEE TIM driver |
Linux PWM framework
Linux IIO framework, Counter framework |
STM32Cube TIM driver |
3.2.3 Peripheral configuration[edit]
The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration by itself can be performed via the STM32CubeMX tool for all internal peripherals. It can then be manually completed (especially for external peripherals) according to the information given in the corresponding software framework article.
For Linux kernel configuration, please refer to TIM device tree configuration and TIM Linux driver articles.
3.2.4 Peripheral assignment[edit]
Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:
- ☐ means that the peripheral can be assigned (☑) to the given runtime context.
- ✓ is used for system peripherals that cannot be unchecked because they are statically connected in the device.
Refer to How to assign an internal peripheral to a runtime context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.
Domain | Peripheral | Runtime allocation | Comment | |||
---|---|---|---|---|---|---|
Instance |
Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) |
Cortex-M4 (STM32Cube) |
|||
Core/Timers | TIM | TIM1 (APB2 group) | ☐ | ☐ | Assignment (single choice) | |
TIM2 (APB1 group) | ☐ | ☐ | Assignment (single choice) | |||
TIM3 (APB1 group) | ☐ | ☐ | Assignment (single choice) | |||
TIM4 (APB1 group) | ☐ | ☐ | Assignment (single choice) | |||
TIM5 (APB1 group) | ☐ | ☐ | Assignment (single choice) | |||
TIM6 (APB1 group) | ☐ | ☐ | Assignment (single choice) | |||
TIM7 (APB1 group) | ☐ | ☐ | Assignment (single choice) | |||
TIM8 (APB2 group) | ☐ | ☐ | Assignment (single choice) | |||
TIM12 (APB1 group) | ☐ | ☐ | ☐ | Assignment (single choice) | ||
TIM13 (APB1 group) | ☐ | ☐ | Assignment (single choice) | |||
TIM14 (APB1 group) | ☐ | ☐ | Assignment (single choice) | |||
TIM15 (APB2 group) | ☐ | ☐ | ☐ | Assignment (single choice) | ||
TIM16 (APB2 group) | ☐ | ☐ | Assignment (single choice) | |||
TIM17 (APB2 group) | ☐ | ☐ | Assignment (single choice) |
4 How to go further[edit]
STM32 cross-series timer overview[8] application note.
5 References[edit]
{{EcosystemFlow/Warning| flow=Current}} ====Article purpose== The purpose of this article is to * briefly introduce the '''TIM''' peripheral and its main features * indicate the level of security supported by this hardware block * explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components * explain how to configure the TIM peripheral {{ReviewsComments|-- [[User:Nathalie Sangouard|Nathalie Sangouard]] ([[User talk:Nathalie Sangouard|talk]]) 16:47, 13 November 2020 (CET)<br />Article to be updated to be compliant with ecosystem v2.0.0 (BZ 80500)}} ==Peripheral overview== The TIM peripheral is a multi-channel timer unit, available in various configurations, depending on the instance used. There are basically following categories: advanced-control timers, general-purpose timers and basic timers. The TIM can provide: PWM with complementary output and dead-time insertion, break detection, input capture<ref name="input_capture">[https://en.wikipedia.org/wiki/Input_capture Input capture]</ref>, quadrature encoder<ref name="quadrature_encoder">[https://en.wikipedia.org/wiki/Rotary_encoder#Incremental_encoder Quadrature encoder]</ref> interface (typically used for rotary encoders), trigger source for other internal peripherals like: ADC<ref name="adc_internal">[[ADC internal peripheral]]</ref>, DAC<ref name="dac_internal">[[DAC internal peripheral]]</ref>, DFSDM<ref name="dfsdm_internal">[[DFSDM internal peripheral]]</ref>. ===Features=== The '''TIM''' peripheral is available in different configurations, depending on the selected instance : * TIM1 and TIM8 are advanced-control timers, with 6 independent channels. * TIM2, TIM3, TIM4 and TIM5 are general-purpose timers, with 4 independent channels. * TIM12, TIM13 and TIM14 are general-purpose timers, with 2 (TIM12) or 1 (TIM13 and TIM14) independent channels. * TIM15, TIM16 and TIM17 are also general-purpose timers, with 2 (TIM15) or 1 (TIM16 and TIM17) independent channels. Compare to TIM12, TIM13 and TIM14, this configuration brings some features that are very useful for motor control (like break function, DMA burst mode control, complementary output with dead-time insertion, ...) * TIM6 and TIM7 are basic timers Refer to [[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]] for the complete list of features, and to the software components, introduced below, to know which features are really implemented. ===Security support=== The TIM is a '''non-secure''' peripheral. ==Peripheral usage and associated software== ===Boot time=== The TIM is not used at boot time. ===Runtime=== ====Overview==== '''TIM12''' and/or '''TIM15''' can be allocated to: * the Arm<sup>®</sup> Cortex<sup>®</sup>-A7 secure core to be controlled in the secure monitor ([[TF-A overview|TF-A]] or [[OP-TEE overview|OP-TEE]]), to perform HSI and CSI calibrations<ref>[[How to activate HSI and CSI oscillators calibration]]</ref> in [[RCC internal peripheral|RCC]].<br /> '''All TIM instances''' can be allocated to: *the Arm<sup>®</sup> Cortex<sup>®</sup>-A7 non-secure to be controlled in Linux<sup>®</sup> by the [[PWM overview|PWM]] and/or , the [[IIO overview|IIO]] , and/or the ''Counter'' frameworks. or * the Arm<sup>®</sup> Cortex<sup>®</sup>-M4 to be controlled in STM32Cube MPU Package by [[STM32CubeMP1 architecture|TIM HAL driver]]<br /> Note that RCC<ref name="rcc">[[RCC internal peripheral]]</ref> owns one prescaler per '''TIM group''' corresponding to '''APB1''' and '''APB2''' buses: TIMG1PRE and TIMG2PRE, respectively. The allocation to Cortex-A7 or the Cortex-M4 should ideally be done on a per group basis to get independent clocking setup on each side, this is why the TIM instances groups are shown in the summary table below ([[#Peripheral assignment]]). ====Software frameworks==== {{:Internal_peripherals_software_table_template}} | Core/Timers | [[TIM internal peripheral|TIM]] | [[TF-A_overview|TF-A TIM driver]]<br />[[OP-TEE_overview|OP-TEE TIM driver]] | [[PWM overview|Linux PWM framework]]<br>[[IIO overview|Linux IIO framework]] ,<br>''Counter'' framework| [[STM32CubeMP1 architecture|STM32Cube TIM driver]] | |- |} ====Peripheral configuration==== The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration by itself can be performed via the [[STM32CubeMX]] tool for all internal peripherals. It can then be manually completed (especially for external peripherals) according to the information given in the corresponding software framework article. For Linux kernel configuration, please refer to [[TIM device tree configuration]] and [[TIM Linux driver]] articles. ====Peripheral assignment==== {{:Internal_peripherals_assignment_table_template}}<onlyinclude> | rowspan="14" | Core/Timers | rowspan="14" | [[TIM internal peripheral|TIM]] | TIM1 (APB2 group) | | <span title="assignable peripheral" style="font-size:21px">☐</span> | <span title="assignable peripheral" style="font-size:21px">☐</span> | Assignment (single choice) |- | TIM2 (APB1 group) | | <span title="assignable peripheral" style="font-size:21px">☐</span> | <span title="assignable peripheral" style="font-size:21px">☐</span> | Assignment (single choice) |- | TIM3 (APB1 group) | | <span title="assignable peripheral" style="font-size:21px">☐</span> | <span title="assignable peripheral" style="font-size:21px">☐</span> | Assignment (single choice) |- | TIM4 (APB1 group) | | <span title="assignable peripheral" style="font-size:21px">☐</span> | <span title="assignable peripheral" style="font-size:21px">☐</span> | Assignment (single choice) |- | TIM5 (APB1 group) | | <span title="assignable peripheral" style="font-size:21px">☐</span> | <span title="assignable peripheral" style="font-size:21px">☐</span> | Assignment (single choice) |- | TIM6 (APB1 group) | | <span title="assignable peripheral" style="font-size:21px">☐</span> | <span title="assignable peripheral" style="font-size:21px">☐</span> | Assignment (single choice) |- | TIM7 (APB1 group) | | <span title="assignable peripheral" style="font-size:21px">☐</span> | <span title="assignable peripheral" style="font-size:21px">☐</span> | Assignment (single choice) |- | TIM8 (APB2 group) | | <span title="assignable peripheral" style="font-size:21px">☐</span> | <span title="assignable peripheral" style="font-size:21px">☐</span> | Assignment (single choice) |- | TIM12 (APB1 group) | <span title="assignable peripheral" style="font-size:21px">☐</span> | <span title="assignable peripheral" style="font-size:21px">☐</span> | <span title="assignable peripheral" style="font-size:21px">☐</span> | Assignment (single choice) |- | TIM13 (APB1 group) | | <span title="assignable peripheral" style="font-size:21px">☐</span> | <span title="assignable peripheral" style="font-size:21px">☐</span> | Assignment (single choice) |- | TIM14 (APB1 group) | | <span title="assignable peripheral" style="font-size:21px">☐</span> | <span title="assignable peripheral" style="font-size:21px">☐</span> | Assignment (single choice) |- | TIM15 (APB2 group) | <span title="assignable peripheral" style="font-size:21px">☐</span> | <span title="assignable peripheral" style="font-size:21px">☐</span> | <span title="assignable peripheral" style="font-size:21px">☐</span> | Assignment (single choice) |- | TIM16 (APB2 group) | | <span title="assignable peripheral" style="font-size:21px">☐</span> | <span title="assignable peripheral" style="font-size:21px">☐</span> | Assignment (single choice) |- | TIM17 (APB2 group) | | <span title="assignable peripheral" style="font-size:21px">☐</span> | <span title="assignable peripheral" style="font-size:21px">☐</span> | Assignment (single choice) |-</onlyinclude> |} ==How to go further== STM32 cross-series timer overview<ref name="stm32_cross_series_timer_overview">[http://www.st.com/content/ccc/resource/technical/document/application_note/54/0f/67/eb/47/34/45/40/DM00042534.pdf/files/DM00042534.pdf/jcr:content/translations/en.DM00042534.pdf STM32 cross-series timer overview application note]</ref> application note. ==References==<references/> <noinclude> [[Category:Timers peripherals]] {{ArticleBasedOnModel| Internal peripheral article model}} {{PublicationRequestId | 7895 | 2018-07-03 | AlainF}}</noinclude>
Line 1: | Line 1: | ||
− | |||
==Article purpose== |
==Article purpose== |
||
The purpose of this article is to |
The purpose of this article is to |
||
Line 6: | Line 5: | ||
* explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components |
* explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components |
||
* explain how to configure the TIM peripheral |
* explain how to configure the TIM peripheral |
||
− | |||
− | |||
==Peripheral overview== |
==Peripheral overview== |
||
Line 37: | Line 34: | ||
<br /> |
<br /> |
||
'''All TIM instances''' can be allocated to: |
'''All TIM instances''' can be allocated to: |
||
− | *the Arm<sup>®</sup> Cortex<sup>®</sup>-A7 non-secure to be controlled in Linux<sup>®</sup> by the [[PWM overview|PWM]] |
+ | *the Arm<sup>®</sup> Cortex<sup>®</sup>-A7 non-secure to be controlled in Linux<sup>®</sup> by the [[PWM overview|PWM]], the [[IIO overview|IIO]], and/or the ''Counter'' frameworks. |
or |
or |
||
* the Arm<sup>®</sup> Cortex<sup>®</sup>-M4 to be controlled in STM32Cube MPU Package by [[STM32CubeMP1 architecture|TIM HAL driver]] |
* the Arm<sup>®</sup> Cortex<sup>®</sup>-M4 to be controlled in STM32Cube MPU Package by [[STM32CubeMP1 architecture|TIM HAL driver]] |
||
Line 49: | Line 46: | ||
| [[TIM internal peripheral|TIM]] |
| [[TIM internal peripheral|TIM]] |
||
| [[TF-A_overview|TF-A TIM driver]]<br />[[OP-TEE_overview|OP-TEE TIM driver]] |
| [[TF-A_overview|TF-A TIM driver]]<br />[[OP-TEE_overview|OP-TEE TIM driver]] |
||
− | | [[PWM overview| |
+ | | [[PWM overview|PWM framework]]<br>[[IIO overview|IIO framework]],<br>''Counter'' framework
|
| [[STM32CubeMP1 architecture|STM32Cube TIM driver]] |
| [[STM32CubeMP1 architecture|STM32Cube TIM driver]] |
||
| |
| |