Approved version. Approved on: 14:12, 15 April 2020
- Last edited 2 years ago ago
Standard SDK directory structure
This article describes the structure of the OpenSTLinux standard SDK installation directory:
SDK ├── environment-setup-<target>-<distro>-linux-gnueabi Environment setup script ├── site-config-<target>-<distro>-linux-gnueabi Configuration file for the target ├── sysroots Root file systems │ ├── <target>-<distro>-linux-gnueabi Target sysroot (libraries, headers, and symbols) │ │ ├── bin │ │ ├── boot │ │ ├── config │ │ ├── dev │ │ ├── etc │ │ ├── home │ │ ├── lib │ │ ├── media │ │ ├── mnt │ │ ├── proc │ │ ├── run │ │ ├── sbin │ │ ├── sys │ │ ├── tmp │ │ ├── usr │ │ └── var │ └── <host machine>-<distro>_sdk-linux Native sysroot (libraries, headers, and symbols) │ ├── bin │ ├── environment-setup.d │ ├── etc │ ├── lib │ ├── sbin │ ├── usr │ └── var └── version-<target>-<distro>-linux-gnueabi Version file for the target
Where:
<target> | Target architecture for cross-toolchain; examples (non exhaustive list):
|
<distro> | Distribution; examples (non-exhaustive list):
|
<host machine> | Host machine on which the SDK is installed; examples (non-exhaustive list):
|
The installed SDK consists of:
- an environment setup script for the SDK
- a configuration file for the target
- a version file for the target
- the root file systems (sysroots) needed to develop objects for the target system