This article describes the content of OpenSTLinux distribution software release version openstlinux-5.4-dunfell-mp1-20-11-12, which is part of STM32MP15 ecosystem release note - v2.1.0.
1 Intended audience
The targeted audience is STM32MP15 customers or partners.
2 Delivery scope and purpose
The OpenSTLinux distribution is a Linux® distribution based on the OpenEmbedded build Framework. It runs on the Arm®Cortex®-A7 processors, and is a fundamental part of the STM32MPU Embedded Software distribution.
This delivery of OpenSTLinux distribution is part of STM32MP15-Ecosystem-v2.1.0 (see the STM32MP15 ecosystem release note - v2.1.0).
3 Licensing
This software package is licensed under a LIMITED LICENSE AGREEMENT FOR ST MATERIALS EVALUATION (LLA). Customers may not use this package except in compliance with the software license agreement (SLA).
All of the packages use the same source components. All components and their respective licenses are listed here.
4 Supported hardware
This software delivery is compatible with the following boards:
5 Delivered features
5.1 Main software components
-
Linux kernel v5.4-stm32mp-r2 (v5.4.56)
-
TF-A v2.2-stm32mp-r2
-
U-Boot v2020.01-stm32mp-r2
-
OP-TEE v3.9.0-stm32mp-r2
- STM32CubeMP1 Package v1.3.0
- OpenEmbedded v3.1.3 (Dunfell)
- Weston version v8.0.0
- Wayland version 1.18.0
- GStreamer version v1.16.2
- GCC version v9.3
- OpenOCD version v0.10.0
- GCnano version v6.4.3
5.2 Detailed features
5.2.1 Kernel part
- Rebase on Linux kernel v5.4.56
- Add OP-TEE support in remoteproc
- Add FMC2 EBI support
- Add serial modem control gpio support
- Add vbus-supply support through usbphyc
- Add SAI PM_runtime support
- Other fixes
5.2.2 U-boot part
- Activate DCache in SPL and in pre-reloc step to reduce boot time
- Handle I2C FastMode+ for STM32MP15x
- Backport ETH patches and solve instability due to DCache managment
- Handle OP-TEE reserved memory and fixup the associated node in kernel device tree device tree
- Add EBI support in FMC2 driver
- Fixup DBGMCU init to avoid boot crash
- Use SCMI for MCU_HOLD_BOOT in remoteproc
- Add VBus support in USB PHYC driver
- Add Cortex-M4 firmware load with OP-TEE remoteproc TA
- Other minor fixes
5.2.3 TF-A part
- FMC2: Update bindings for EBI support
-
SMC: return correct error
- TAMPER: Add PINCTRL management for tamper if defined
- USB OTG: regulator mode update
- Update firewall on DDR CTRL and PHY (Allow read access for non-secure)
- Manage MCU reset through SCMI
- Add a new RETRAM property to configure state during low power
- Correct STGEN counter restore when returning from stop mode
- Add support of auto stop mode management
- Correct the exception fault return address
- Other minor fixes + all fixes already published after STM32MP15 ecosystem release v2.0.0
5.2.4 OP-TEE part
-
TA: Authenticated firmware management, used for Cortex-M4 firmware loading
- Update firewall on DDR CTRL and PHY (Allow read access for non-secure)
- Manage MCU reset through SCMI
-
SMC: return correct error
- USB OTG: regulator mode update
- Other minor fixes + all fixes already published after STM32MP15 ecosystem release v2.0.0
6 Recommendations for use
6.1 Safe use
- Flash programming and boot from all supported Flash devices: SDCard, eMMC, ONFI NAND and NOR Flash memories
- Develop Linux® applications, libraries, kernel modules based on OpenSTLinux delivery
- Develop coprocessor Cube applications based on STM32CubeMP1 delivery
- Develop boards based on STM32MP15
- Prototype applications based on ST boards
6.2 Non-recommended use
7 Main restrictions list
- M-CAN Bus is not functional if power management is activated ("sleep" state defined in pinctrl): the issue is corrected thanks to this patch.
8 Minor release updates
STMicroelectronics regularly delivers corrections through github® components which are U-Boot, OP-TEE, TF-A, Linux kernel.
The corrections can be incorporated into the Developer Package (refer to STM32MP1 Developer Package) or Distribution Package (see below).
Two possibilities exist to update a Distribution Package:
- Update your existing Distribution Package:
- Switch your Distribution Package to # github® mode .
- Use the devtool modify <recipe name> command to set up an environment. It will fetch and unpack the source code.
- In the extracted source code, use a git command such as git checkout -b WORK <github® TAG> to point to a new revision of the component.
- More rarely STMicroelectronics also delivers fixes on layers through github®. These changes can be integrated (via git commands: git checkout -b WORK <github® commit SHA1>) into the local STM32MP1 Distribution Package environment. See below the github® links of the quoted layers :
- - meta-st-stm32mp
- - meta-st-openstlinux
- - meta-st-stm32mp-addons
- Get a new Distribution Package:
- Refer to Installing_the_OpenSTLinux_distribution page for install instructions, and use the repo command given for the minor version below, if it exists.
8.1 v2.1.5
- Update to Yocto 3.1.16 (dunfell-23.0.16)
-
BSP update:
- New manifest tag available to get the release: openstlinux-5.4-dunfell-mp1-22-05-20
repo init -u https://github.com/STMicroelectronics/oe-manifest -b refs/tags/openstlinux-5.4-dunfell-mp1-22-05-20
repo sync
8.2 v2.1.4
- Update to Yocto 3.1.11 (dunfell-23.0.11)
-
BSP update:
- New manifest tag available to get the release: openstlinux-5.4-dunfell-mp1-21-12-22
repo init -u https://github.com/STMicroelectronics/oe-manifest -b refs/tags/openstlinux-5.4-dunfell-mp1-21-12-22
repo sync
8.3 v2.1.3
- Update to Yocto 3.1.9 (2020-04.9-dunfell)
- Correct syntax changed for fit
repo init -u https://github.com/STMicroelectronics/oe-manifest -b dunfell-2.x
repo sync
8.4 v2.1.2
8.5 v2.1.1
9 How to get started with openstlinux-5.4-dunfell-mp1-20-11-12
Refer to How to download the software and start with this release?
10 Associated tools
Refer to the Referenced tools release notes .
11 Detailed delivery content
11.1 Detailed description of STMicroelectronics layers
OpenSTLinux distribution is based on the build framework OpenEmbedded.
OpenEmbedded build framework engine is named OE-Core.
A layer is a collection of recipes and/or configurations applied on top of OE-Core.
Typically, each layer is organized around a specific theme, such as adding recipes for building web browser software.
The implemented layers are listed below, together with the list of recipes contained in each layer and the related information.
11.1.1 meta-st-stm32mp
Name of layer |
Description
|
meta-st-stm32mp |
BSP Layer for stm32mp
|
Recipe Name |
Path of recipe |
License |
Description
|
alsa-state-stm32mp1 |
meta-st/meta-st-stm32mp/recipes-bsp/alsa/alsa-state-stm32mp1.bb |
MIT |
Alsa scenario files to enable alsa state restoration
|
gcnano-driver-stm32mp |
meta-st/meta-st-stm32mp/recipes-bsp/drivers/gcnano-driver-stm32mp_6.4.3.bb |
GPLv1 & MIT |
GCNano kernel drivers
|
tf-a-stm32mp |
meta-st/meta-st-stm32mp/recipes-bsp/trusted-firmware-a/tf-a-stm32mp_2.2.bb |
BSD-3-Clause |
Trusted Firmware-A for STM32MP1
|
u-boot-stm32mp-extlinux |
meta-st/meta-st-stm32mp/recipes-bsp/u-boot/u-boot-stm32mp-extlinux.bb |
MIT |
Generate 'extlinux.conf' file for U-boot
|
u-boot-stm32mp-splash |
meta-st/meta-st-stm32mp/recipes-bsp/u-boot/u-boot-stm32mp-splash_2018.11.bb |
Proprietary |
Universal Boot Loader Splash Screen for stm32mp embedded devices
|
u-boot-stm32mp |
meta-st/meta-st-stm32mp/recipes-bsp/u-boot/u-boot-stm32mp_2020.01.bb |
GPLv2+ |
Universal Boot Loader for embedded devices for stm32mp (trusted)
|
wifi-suspend |
meta-st/meta-st-stm32mp/recipes-connectivity/wifi/wifi-suspend.bb |
MIT |
Systemd service to suspend/resume correctly the wifi
|
gcc-arm-none-eabi-native |
meta-st/meta-st-stm32mp/recipes-devtools/gcc-arm-none-eabi/gcc-arm-none-eabi-native_7.bb |
GPL-3.0-with-GCC-exception & GPLv3 |
Baremetal GCC for ARM
|
nativesdk-gcc-arm-none-eabi |
meta-st/meta-st-stm32mp/recipes-devtools/gcc-arm-none-eabi/nativesdk-gcc-arm-none-eabi_7.bb |
GPL-3.0-with-GCC-exception & GPLv3 |
Baremetal GCC for ARM
|
openocd-stm32mp |
meta-st/meta-st-stm32mp/recipes-devtools/openocd/openocd-stm32mp_0.10.0.bb |
GPLv2 |
Free and Open On-Chip Debugging, In-System Programming and Boundary-Scan Testing
|
sdcard-raw-tools |
meta-st/meta-st-stm32mp/recipes-devtools/sdcard-raw-tools/sdcard-raw-tools.bb |
MIT |
script for creating raw SDCARD image ready to flash
|
linux-examples-stm32mp1 |
meta-st/meta-st-stm32mp/recipes-extended/linux-examples/linux-examples-stm32mp1.bb |
Proprietary |
ST STM32MP1 projects for Linux examples
|
m4fwcoredump |
meta-st/meta-st-stm32mp/recipes-extended/m4coredump/m4fwcoredump.bb |
MIT |
Script to manage coredump of cortexM4
|
m4projects-stm32mp1 |
meta-st/meta-st-stm32mp/recipes-extended/m4projects/m4projects-stm32mp1.bb |
Proprietary |
ST STM32MP1 Examples for CM4
|
gcnano-userland-multi-binary-debug-stm32mp |
meta-st/meta-st-stm32mp/recipes-graphics/gcnano-userland/gcnano-userland-multi-binary-debug-stm32mp.bb |
Proprietary |
[DEBUG] Vivante libraries OpenGL ES, OpenVG and EGL (multi backend)
|
gcnano-userland-multi-binary-stm32mp |
meta-st/meta-st-stm32mp/recipes-graphics/gcnano-userland/gcnano-userland-multi-binary-stm32mp.bb |
Proprietary |
Vivante libraries OpenGL ES, OpenVG and EGL (multi backend)
|
linux-firmware-bluetooth-bcm4343 |
meta-st/meta-st-stm32mp/recipes-kernel/linux-firmware/linux-firmware-bluetooth-bcm4343.bb |
Firmware-cypress-bcm4343 |
Bluetooth firrmware for BCM4343
|
linux-stm32mp |
meta-st/meta-st-stm32mp/recipes-kernel/linux/linux-stm32mp_5.4.bb |
GPLv2 |
Linux STM32MP Kernel
|
optee-os-stm32mp |
meta-st/meta-st-stm32mp/recipes-security/optee/optee-os-stm32mp_3.9.0.bb |
BSD |
OPTEE OS for stm32mp
|
st-image-bootfs |
meta-st/meta-st-stm32mp/recipes-st/images/st-image-bootfs.bb |
MIT |
STM32MP bootfs Image
|
st-image-userfs |
meta-st/meta-st-stm32mp/recipes-st/images/st-image-userfs.bb |
MIT |
STM32MP userfs Image
|
st-image-vendorfs |
meta-st/meta-st-stm32mp/recipes-st/images/st-image-vendorfs.bb |
MIT |
STM32MP vendorfs Image
|
hidapi-stm32mp |
meta-st/meta-st-stm32mp/recipes-support/hidapi/hidapi-stm32mp_0.8.0-rc1.bb |
BSD-3-Clause GPLv3 |
Multi-platform library to interface with USB and Bluetooth HID-Class devices
|
libopencsd |
meta-st/meta-st-stm32mp/recipes-support/libopencsd/libopencsd_0.10.0.bb |
BSD-3-Clause |
SUMMARY=CoreSight Trace Decode library
|
Addons on recipes: configuration, patch, ..
|
Recipe Name |
Path of recipe
|
alsa-lib |
meta-st/meta-st-stm32mp/recipes-bsp/alsa/alsa-lib_%.bbappend
|
base-files |
meta-st/meta-st-stm32mp/recipes-core/base-files/base-files_%.bbappend
|
busybox |
meta-st/meta-st-stm32mp/recipes-core/busybox/busybox_%.bbappend
|
systemd-conf |
meta-st/meta-st-stm32mp/recipes-core/systemd/systemd-conf.bbappend
|
bison |
meta-st/meta-st-stm32mp/recipes-devtools/bison/bison_%.bbappend
|
gdb-cross-canadian |
meta-st/meta-st-stm32mp/recipes-devtools/gdb/gdb-cross-canadian_%.bbappend
|
gdb-cross |
meta-st/meta-st-stm32mp/recipes-devtools/gdb/gdb-cross_%.bbappend
|
libdrm |
meta-st/meta-st-stm32mp/recipes-graphics/drm/libdrm_%.bbappend
|
weston-init |
meta-st/meta-st-stm32mp/recipes-graphics/wayland/weston-init.bbappend
|
weston |
meta-st/meta-st-stm32mp/recipes-graphics/wayland/weston_5.0.0.bbappend
|
linux-firmware |
meta-st/meta-st-stm32mp/recipes-kernel/linux-firmware/linux-firmware_git.bbappend
|
pulseaudio |
meta-st/meta-st-stm32mp/recipes-multimedia/pulseaudio/pulseaudio_%.bbappend
|
11.1.2 meta-st-stm32mp-addons
Name of layer |
Description
|
meta-st-stm32mp-addons |
BSP addons layer for stm32mp
|
Addons on recipes: configuration, patch, ..
|
Recipe Name |
Path of recipe
|
alsa-state-stm32mp1 |
meta-st/meta-st-stm32mp-addons/recipes-bsp/alsa/alsa-state-stm32mp1.bbappend
|
tf-a-stm32mp |
meta-st/meta-st-stm32mp-addons/recipes-bsp/trusted-firmware-a/tf-a-stm32mp_%.bbappend
|
u-boot-stm32mp |
meta-st/meta-st-stm32mp-addons/recipes-bsp/u-boot/u-boot-stm32mp_%.bbappend
|
linux-stm32mp |
meta-st/meta-st-stm32mp-addons/recipes-kernel/linux/linux-stm32mp_%.bbappend
|
m4projects-stm32mp1 |
meta-st/meta-st-stm32mp-addons/recipes-extended/m4projects/m4projects-stm32mp1.bbappend
|
11.1.3 meta-st-openstlinux
Name of layer |
Description
|
meta-st-openstlinux
|
OpenSTLinux layer - framework/image settings
|
Recipe Name |
Path of recipe |
License |
Description
|
resize-helper |
meta-st/meta-st-openstlinux/recipes-bsp/tools/resize-helper.bb |
GPLv2+ |
Tools for resizing the file system
|
usbotg-gadget-config |
meta-st/meta-st-openstlinux/recipes-bsp/tools/usbotg-gadget-config.bb |
MIT |
The goal is to enable USB Ethernet & MSC gadget
|
psplash-drm |
meta-st/meta-st-openstlinux/recipes-core/psplash/psplash-drm.bb |
MIT |
Basic splash screen displaying a picture on DRM/KMS
|
systemd-mount-partitions |
meta-st/meta-st-openstlinux/recipes-core/systemd/systemd-mount-partitions.bb |
MIT |
Mount partitions
|
systemd-networkd-configuration |
meta-st/meta-st-openstlinux/recipes-core/systemd/systemd-networkd-configuration.bb |
MIT |
Basic networkd configuration
|
lsb-openstlinux |
meta-st/meta-st-openstlinux/recipes-extended/lsb/lsb-openstlinux.bb |
GPLv2+ |
LSB support for checking gpu provider
|
openstlinux-qt-eglfs |
meta-st/meta-st-openstlinux/recipes-qt/qt5/openstlinux-qt-eglfs.bb |
MIT |
add script and material to help with eglfs qt configuration
|
ai-hand-char-reco-launcher |
meta-st/meta-st-openstlinux/recipes-samples/ai-nn-application/ai-hand-char-reco-launcher.bb |
GPLv2 & BSD-3-Clause |
Hand writing character recognition launcher based on HCR Neural Network
|
demo-launcher |
meta-st/meta-st-openstlinux/recipes-samples/demo/demo-launcher.bb |
Proprietary |
Python script which launch several use-cases
|
sensors-iks01a2 |
meta-st/meta-st-openstlinux/recipes-samples/demo/sensors-iks01a2.bb |
Proprietary |
Python script which monitors the temperature measured by the Nucleo extension board iks01a2a on-board sensor
|
demo-hotspot-wifi |
meta-st/meta-st-openstlinux/recipes-samples/hotspot-wifi/demo-hotspot-wifi.bb |
MIT |
Shell script to enable/disable hotsopt wifi configuration
|
st-example-image-qt |
meta-st/meta-st-openstlinux/recipes-samples/images/st-example-image-qt.bb |
Proprietary |
STMicroelectronics example of image based on QT framework.
|
st-example-image-qtwayland |
meta-st/meta-st-openstlinux/recipes-samples/images/st-example-image-qtwayland.bb |
Proprietary |
STMicroelectronics example of image based on QT framework over Weston/Wayland.
|
optee-client |
meta-st/meta-st-openstlinux/recipes-security/optee/optee-client_git.bb |
BSD |
OPTEE client
|
optee-examples |
meta-st/meta-st-openstlinux/recipes-security/optee/optee-examples.bb |
GPLv2 |
OP-TEE examples
|
optee-test |
meta-st/meta-st-openstlinux/recipes-security/optee/optee-test_git.bb |
BSD & GPLv2 |
OP-TEE sanity testsuite
|
packagegroup-optee-core |
meta-st/meta-st-openstlinux/recipes-security/packagegroups/packagegroup-optee-core.bb |
LGPLv2+ |
OP-TEE core packagegroup
|
packagegroup-optee-test |
meta-st/meta-st-openstlinux/recipes-security/packagegroups/packagegroup-optee-test.bb |
LGPLv2+ |
OP-TEE test packagegroup
|
libsmaf |
meta-st/meta-st-openstlinux/recipes-security/smaf/libsmaf.bb |
LGPLv2.1 |
SMAF library
|
st-image-core |
meta-st/meta-st-openstlinux/recipes-st/images/st-image-core.bb |
Proprietary |
OpenSTLinux core image.
|
st-image-weston |
meta-st/meta-st-openstlinux/recipes-st/images/st-image-weston.bb |
Proprietary |
OpenSTLinux weston image with basic Wayland support (if enable in distro).
|
packagegroup-framework-tools |
meta-st/meta-st-openstlinux/recipes-st/packagegroups/packagegroup-framework-tools.bb |
MIT |
Frameworks components
|
packagegroup-gstreamer1-0 |
meta-st/meta-st-openstlinux/recipes-st/packagegroups/packagegroup-gstreamer1-0.bb |
LGPLv2+ |
Gstreamer 1.0 components
|
Recipes addons, such as configurations and patches.
Recipe name |
Recipe path
|
openssh |
meta-st/meta-st-openstlinux/oe-core/recipes-connectivity/openssh/openssh_%.bbappend
|
packagegroup-core-ssh-openssh |
meta-st/meta-st-openstlinux/oe-core/recipes-core/packagegroups/packagegroup-core-ssh-openssh.bbappend
|
dpkg |
meta-st/meta-st-openstlinux/oe-core/recipes-devtools/dpkg/dpkg_%.bbappend
|
ckermit |
meta-st/meta-st-openstlinux/oe-core/recipes-support/ckermit/ckermit_%.bbappend
|
libiio |
meta-st/meta-st-openstlinux/oe-core/recipes-support/libiio/libiio_git.bbappend
|
glmark2 |
meta-st/meta-st-openstlinux/recipes-benchmark/glmark2/glmark2_%.bbappend
|
bluez5 |
meta-st/meta-st-openstlinux/recipes-connectivity/bluez5/bluez5_%.bbappend
|
connman |
meta-st/meta-st-openstlinux/recipes-connectivity/connman/connman_%.bbappend
|
busybox |
meta-st/meta-st-openstlinux/recipes-core/busybox/busybox_%.bbappend
|
meta-environment |
meta-st/meta-st-openstlinux/recipes-core/meta/meta-environment.bbappend
|
packagegroup-core-eclipse-debug |
meta-st/meta-st-openstlinux/recipes-core/packagegroups/packagegroup-core-eclipse-debug.bbappend
|
packagegroup-core-tools-profile |
meta-st/meta-st-openstlinux/recipes-core/packagegroups/packagegroup-core-tools-profile.bbappend
|
systemd-conf |
meta-st/meta-st-openstlinux/recipes-core/systemd/systemd-conf.bbappend
|
systemd-serialgetty |
meta-st/meta-st-openstlinux/recipes-core/systemd/systemd-serialgetty.bbappend
|
systemd |
meta-st/meta-st-openstlinux/recipes-core/systemd/systemd_%.bbappend
|
cairo |
meta-st/meta-st-openstlinux/recipes-graphics/cairo/cairo_%.bbappend
|
kmscube |
meta-st/meta-st-openstlinux/recipes-graphics/kmscube/kmscube_git.bbappend
|
lxdm |
meta-st/meta-st-openstlinux/recipes-graphics/lxdm/lxdm_0.5.3.bbappend
|
wayland-protocols |
meta-st/meta-st-openstlinux/recipes-graphics/wayland/wayland-protocols_1.10.bbappend
|
weston-init |
meta-st/meta-st-openstlinux/recipes-graphics/wayland/weston-init.bbappend
|
xserver-nodm-init |
meta-st/meta-st-openstlinux/recipes-graphics/x11-common/xserver-nodm-init_%.bbappend
|
xinit |
meta-st/meta-st-openstlinux/recipes-graphics/xorg-app/xinit_%.bbappend
|
pixman |
meta-st/meta-st-openstlinux/recipes-graphics/xorg-lib/pixman_0.34.0.bbappend
|
alsa-utils |
meta-st/meta-st-openstlinux/recipes-multimedia/alsa/alsa-utils_1.1.4.bbappend
|
gstreamer1.0-libav |
meta-st/meta-st-openstlinux/recipes-multimedia/gstreamer/gstreamer1.0-libav_1.14.2.bbappend
|
gstreamer1.0-plugins-bad |
meta-st/meta-st-openstlinux/recipes-multimedia/gstreamer/gstreamer1.0-plugins-bad_1.12.2.bbappend
|
gstreamer1.0-plugins-base |
meta-st/meta-st-openstlinux/recipes-multimedia/gstreamer/gstreamer1.0-plugins-base_1.12.2.bbappend
|
gstreamer1.0-plugins-good |
meta-st/meta-st-openstlinux/recipes-multimedia/gstreamer/gstreamer1.0-plugins-good_1.12.2.bbappend
|
pulseaudio |
meta-st/meta-st-openstlinux/recipes-multimedia/pulseaudio/pulseaudio_10.0.bbappend
|
v4l-utils |
meta-st/meta-st-openstlinux/recipes-multimedia/v4l2apps/v4l-utils_1.12.3.bbappend
|
packagegroup-qt5-toolchain-target |
meta-st/meta-st-openstlinux/recipes-qt/packagegroups/packagegroup-qt5-toolchain-target.bbappend
|
qtbase |
meta-st/meta-st-openstlinux/recipes-qt/qt5/qtbase_git.bbappend
|
qtmultimedia |
meta-st/meta-st-openstlinux/recipes-qt/qt5/qtmultimedia_git.bbappend
|
st-image-userfs |
meta-st/meta-st-openstlinux/recipes-samples/images/st-image-userfs.bbappend
|
packagegroup-framework-tools |
meta-st/meta-st-openstlinux/recipes-st/packagegroups/packagegroup-framework-tools.bbappend
|
ntp |
meta-st/meta-st-openstlinux/recipes-support/ntp/ntp_%.bbappend
|
netdata |
meta-st/meta-st-openstlinux/recipes-webadmin/netdata/netdata_git.bbappend
|
12 Archives