Approved version. Approved on: 11:02, 10 October 2019
You are viewing an old version of this page. Return to the latest version.
Difference between revisions of "STM32MP15 U-Boot"
[quality revision] | [quality revision] |
(Undo revision 63268 by Patrick Delaunay (talk))
(Tag: Undo)
|
m
|
This article briefly describes the STM32MP15x lines support in U-Boot.
Contents
1 STM32MP15x lines
support[edit]
For detailed information, please read the file in the delivered U-Boot code = board/st/stm32mp1/README
Also available in official U-Boot Git.
Code :
-
arch/arm/mach-stm32mp : arch specific code for STM32 Arm® Cortex® MPUs
- board/st/stm32mp1 : generic STMicroelectronics board for STM32MP1 Series
- drivers/*/*stm32* : drivers
Configuration Files:
- defconfig file
- config files
- Device tree in arch/arm/dts
- stm32mp157*-<board>.dts : same as kernel
- stm32mp157*-<board>-u-boot.dtsi : addition for u-boot ( <<device tree>>-u-boot.dtsi automatically included in build process)
2 Selecting targets : choose defconfig and Device Tree[edit]
Each boot chain is supported by one U-Boot configuration with defconfig
Boot chain | defconfig | FSBL | SSBL | TEE support |
---|---|---|---|---|
Trusted Boot | stm32mp15_trusted_defconfig | TF-A |
U-Boot
u-boot.stm32 |
- |
Trusted Boot with OP-TEE | stm32mp15_optee_defconfig | TF-A |
U-Boot
u-boot.stm32 |
yes |
Basic Boot | stm32mp15_basic_defconfig |
SPL
u-boot-spl.stm32 |
U-Boot
u-boot.img |
- |
![]() |
The basic boot chain is not supported/promoted by STMicroelectronics to make product (see Boot chains overview for details). |
Several targets/ boards are supported with the associated device-tree (same name as kernel):
Board part number | Description | Device tree |
---|---|---|
STM32MP157C-EV1 Evaluation board ![]() |
MB1262+MB1263 | stm32mp157c-ev1 |
STM32MP157C-ED1 Evaluation daughterboard | MB1263 | stm32mp157c-ed1 |
STM32MP157A-DK1 Discovery kit ![]() |
MB1272 | stm32mp157a-dk1 |
STM32MP157C-DK2 Discovery kit ![]() |
MB1272+MB1407 | stm32mp157c-dk2 |
3 Compilation[edit]
see U-Boot_overview#U-Boot_build
With <mode> = 'basic', 'trusted' or 'optee'
make stm32mp15_<mode>_defconfig make DEVICE_TREE=<device tree name> all
- DEVICE_TREE: select in arch/arm/dts the device tree that is used
- KBUILD_OUTPUT: change the destination directory for the build
- EXT_DTB: select external device tree
4 Examples[edit]
4.1 STM32MP157C-EV1 Evaluation board
trusted boot[edit]
make stm32mp15_trusted_defconfig make DEVICE_TREE=stm32mp157c-ev1 all
4.2 STM32MP157C-DK2 Discovery kit
trusted boot[edit]
Using export to select the device tree
export KBUILD_OUTPUT=../build/trusted export DEVICE_TREE=stm32mp157c-dk2 make stm32mp15_trusted_defconfig make all
4.3 STM32MP157C-ED1 Evaluation daughterboard basic boot[edit]
export KBUILD_OUTPUT=../build/basic make stm32mp15_basic_defconfig make DEVICE_TREE=stm32mp157c-ed1 all
4.4 Trusted boot chain with external device tree[edit]
make stm32mp15_trusted_defconfig make EXT_DTB=boot/stm32mp157c-myboard.dtb all
This article briefly describes the {{MicroprocessorDevice | device=15}} support in [[U-Boot_overview|U-Boot]]. == {{MicroprocessorDevice | device=15}} support == For detailed information, please read the file in the delivered U-Boot code = {{CodeSource | U-Boot | board/st/stm32mp1/README}} Also available in official U-Boot Git. Code : * {{CodeSource | U-Boot | arch/arm/mach-stm32mp}}: arch specific code for {{MicroprocessorDevice | device=Class}} * {{CodeSource | U-Boot | board/st/stm32mp1}}: generic STMicroelectronics board for {{MicroprocessorDevice | device=1}} * drivers/*/*stm32* : drivers Configuration Files: * defconfig file ** {{CodeSource | U-Boot | configs/stm32mp15_basic_defconfig}} ** {{CodeSource | U-Boot | configs/stm32mp15_optee_defconfig}} ** {{CodeSource | U-Boot | configs/stm32mp15_trusted_defconfig}} * config files ** {{CodeSource | U-Boot | include/configs/stm32mp1.h}} * Device tree in {{CodeSource | U-Boot | arch/arm/dts }} ** stm32mp157*-<board>.dts : same as kernel ** stm32mp157*-<board>-u-boot.dtsi : addition for u-boot ( <<device tree>>-u-boot.dtsi automatically included in build process) == Selecting targets : choose defconfig and Device Tree == Each [[Boot_chains_overview|boot chain]] is supported by one [[U-Boot_overview#Kbuild|U-Boot configuration with defconfig]] {| class="wikitablest-table" |- ! Boot chain !! defconfig !! FSBL !! SSBL !! TEE support |- | [[Boot_chains_overview#STM32MP boot chains|''' Trusted Boot''']] || stm32mp15_trusted_defconfig || TF-A || '''U-Boot'''<br>[[U-Boot_overview#Output_files|u-boot.stm32]] || - |- | [[Boot_chains_overview#STM32MP boot chains|''' Trusted Boot''']] with [[OP-TEE_overview|'''OP-TEE''']] || stm32mp15_optee_defconfig || TF-A || '''U-Boot'''<br>[[U-Boot_overview#Output_files|u-boot.stm32]] || yes |- | [[Boot_chains_overview#STM32MP boot chains|'''Basic Boot''']] || stm32mp15_basic_defconfig || SPL<br>[[U-Boot_overview#Output_files|u-boot-spl.stm32]] || '''U-Boot'''<br>[[U-Boot_overview#Output_files|u-boot.img]] || - |} {{Warning | The basic boot chain is not supported/promoted by STMicroelectronics to make product (see [[Boot_chains_overview#Boot_chains_features_set|Boot chains overview]] for details).}} Several [[STM32MP15_boards|targets/ boards]] are supported with the associated device-tree (same name as kernel): {| class="wikitablest-table" |- ! Board part number !! Description !! Device tree |- | '''{{Board | type=157C-EV1}}''' || [[MB1262]]+[[MB1263]] || {{CodeSource | U-Boot | arch/arm/dts/stm32mp157c-ev1.dts|'''stm32mp157c-ev1'''}} |- | STM32MP157C-ED1 Evaluation daughterboard || [[MB1263]] || {{CodeSource | U-Boot | arch/arm/dts/stm32mp157c-ed1.dts|stm32mp157c-ed1}} |- | '''{{Board | type=157A-DK1}}''' || [[MB1272]] || {{CodeSource | U-Boot | arch/arm/dts/stm32mp157a-dk1.dts|'''stm32mp157a-dk1'''}} |- | '''{{Board | type=157C-DK2}}''' || [[MB1272]]+[[MB1407]] || {{CodeSource | U-Boot | arch/arm/dts/stm32mp157c-dk2.dts|'''stm32mp157c-dk2'''}} |} == Compilation == see [[U-Boot_overview#U-Boot_build]] With <mode> = 'basic', 'trusted' or 'optee' {{PC$}} make stm32mp15_<mode>_defconfig {{PC$}} make DEVICE_TREE=<device tree name> all *'''DEVICE_TREE''': select in arch/arm/dts the device tree that is used * '''KBUILD_OUTPUT''': change the destination directory for the build * '''EXT_DTB''': select external device tree == Examples == === {{Board | type=157C-EV1}} trusted boot === {{PC$}} make stm32mp15_trusted_defconfig {{PC$}} make DEVICE_TREE=stm32mp157c-ev1 all === {{Board | type=157C-DK2}} trusted boot === Using export to select the device tree {{PC$}} export KBUILD_OUTPUT=../build/trusted {{PC$}} export DEVICE_TREE=stm32mp157c-dk2 {{PC$}} make stm32mp15_trusted_defconfig {{PC$}} make all === STM32MP157C-ED1 Evaluation daughterboard basic boot === {{PC$}} export KBUILD_OUTPUT=../build/basic {{PC$}} make stm32mp15_basic_defconfig {{PC$}} make DEVICE_TREE=stm32mp157c-ed1 all === Trusted boot chain with external device tree === {{PC$}} make stm32mp15_trusted_defconfig {{PC$}} make EXT_DTB=boot/stm32mp157c-myboard.dtb all <noinclude> [[Category:U-Boot]] {{PublicationRequestId | 12895 | 2019-08-01}}</noinclude>
Line 27: | Line 27: | ||
Each [[Boot_chains_overview|boot chain]] is supported by one [[U-Boot_overview#Kbuild|U-Boot configuration with defconfig]] |
Each [[Boot_chains_overview|boot chain]] is supported by one [[U-Boot_overview#Kbuild|U-Boot configuration with defconfig]] |
||
− | {| class=" |
+ | {| class="st-table" |
|- |
|- |
||
! Boot chain !! defconfig !! FSBL !! SSBL !! TEE support |
! Boot chain !! defconfig !! FSBL !! SSBL !! TEE support |
||
Line 42: | Line 42: | ||
Several [[STM32MP15_boards|targets/ boards]] are supported with the associated device-tree (same name as kernel): |
Several [[STM32MP15_boards|targets/ boards]] are supported with the associated device-tree (same name as kernel): |
||
− | {| class=" |
+ | {| class="st-table" |
|- |
|- |
||
! Board part number !! Description !! Device tree |
! Board part number !! Description !! Device tree |