Difference between revisions of "STM32MP15 OpenSTLinux release note - v2.1.0"
[unchecked revision] | [quality revision] |
Lionel Vitte (talk | contribs)
m (→v2.1.4)
|
Lionel Vitte (talk | contribs)
m (→v2.1.4)
|
This article describes the content of OpenSTLinux distribution software release version openstlinux-5.4-dunfell-mp1-20-11-12, which is part of STM32MP15 ecosystem release note - v2.1.0.
Contents
1 Intended audience[edit]
The targeted audience is STM32MP15 customers or partners.
2 Delivery scope and purpose[edit]
The OpenSTLinux distribution is a Linux® distribution based on the OpenEmbedded build Framework. It runs on the Arm® Cortex®-A7 processors, and is a fundamental part of the STM32MPU Embedded Software distribution.
This delivery of OpenSTLinux distribution is part of STM32MP15-Ecosystem-v2.1.0 (see the STM32MP15 ecosystem release note - v2.1.0).
3 Licensing[edit]
This software package is licensed under a LIMITED LICENSE AGREEMENT FOR ST MATERIALS EVALUATION (LLA). Customers may not use this package except in compliance with the software license agreement (SLA).
All of the packages use the same source components. All components and their respective licenses are listed here.
4 Supported hardware[edit]
This software delivery is compatible with the following boards:
- STM32MP157A-EV1, STM32MP157C-EV1, STM32MP157D-EV1 and STM32MP157F-EV1 Evaluation boards. For more information on this board, please read the article STM32MP157x-EV1 - hardware description
- STM32MP157A-DK1, STM32MP157D-DK1, STM32MP157C-DK2 and STM32MP157F-DK2 Discovery kit. For more information on these boards, please read the article STM32MP157x-DKx - hardware description
5 Delivered features[edit]
5.1 Main software components[edit]
- Linux kernel v5.4-stm32mp-r2 (v5.4.56)
- TF-A v2.2-stm32mp-r2
- U-Boot v2020.01-stm32mp-r2
- OP-TEE v3.9.0-stm32mp-r2
- STM32CubeMP1 Package v1.3.0
- OpenEmbedded v3.1.3 (Dunfell)
- Weston version v8.0.0
- Wayland version 1.18.0
- GStreamer version v1.16.2
- GCC version v9.3
- OpenOCD version v0.10.0
- GCnano version v6.4.3
5.2 Detailed features[edit]
5.2.1 Kernel part[edit]
- Rebase on Linux kernel v5.4.56
- Add OP-TEE support in remoteproc
- Add FMC2 EBI support
- Add serial modem control gpio support
- Add vbus-supply support through usbphyc
- Add SAI PM_runtime support
- Other fixes
5.2.2 U-boot part[edit]
- Activate DCache in SPL and in pre-reloc step to reduce boot time
- Handle I2C FastMode+ for STM32MP15x
- Backport ETH patches and solve instability due to DCache managment
- Handle OP-TEE reserved memory and fixup the associated node in kernel device tree device tree
- Add EBI support in FMC2 driver
- Fixup DBGMCU init to avoid boot crash
- Use SCMI for MCU_HOLD_BOOT in remoteproc
- Add VBus support in USB PHYC driver
- Add Cortex-M4 firmware load with OP-TEE remoteproc TA
- Other minor fixes
5.2.3 TF-A part[edit]
- FMC2: Update bindings for EBI support
- SMC: return correct error
- TAMPER: Add PINCTRL management for tamper if defined
- USB OTG: regulator mode update
- Update firewall on DDR CTRL and PHY (Allow read access for non-secure)
- Manage MCU reset through SCMI
- Add a new RETRAM property to configure state during low power
- Correct STGEN counter restore when returning from stop mode
- Add support of auto stop mode management
- Correct the exception fault return address
- Other minor fixes + all fixes already published after STM32MP15 ecosystem release v2.0.0
- Rebase TF-A SSP
5.2.4 OP-TEE part[edit]
- TA: Authenticated firmware management, used for Cortex-M4 firmware loading
- Update firewall on DDR CTRL and PHY (Allow read access for non-secure)
- Manage MCU reset through SCMI
- SMC: return correct error
- USB OTG: regulator mode update
- Other minor fixes + all fixes already published after STM32MP15 ecosystem release v2.0.0
6 Recommendations for use[edit]
6.1 Safe use[edit]
- Flash programming and boot from all supported Flash devices: SDCard, eMMC, ONFI NAND and NOR Flash memories
- Develop Linux® applications, libraries, kernel modules based on OpenSTLinux delivery
- Develop coprocessor Cube applications based on STM32CubeMP1 delivery
- Develop boards based on STM32MP15
- Prototype applications based on ST boards
6.2 Non-recommended use[edit]
- None
7 Main restrictions list[edit]
- M-CAN Bus is not functional if power management is activated ("sleep" state defined in pinctrl): the issue is corrected thanks to this patch.
8 Minor release updates[edit]
STMicroelectronics regularly delivers corrections through github® components which are u-boot, optee-os, tf-a, Linux kernel.
You can decide to incorporate them into your developer package (please refer to STM32MP1 Developer Package) or Distribution package.
To update Distribution package please proceed as follow:
-
- Switch to github® mode your Distribution package.
- Use the command devtool modify <recipe name> to set up an environment. It will fetch and unpack the source code.
- In extracted source code, use git command such as git checkout -b WORK <github® TAG> to point on new revision of component.
More rarely STMicroelectronics also delivers fixes on layers through github®. These changes can be integrated (via git commands) into your local STM32MP1 Distribution Package environment. Please find below the github® links of the quoted layers :
8.1 v2.1.4[edit]
- Update to Yocto 3.1.11 (dunfell-23.0.11)
- BSP update
Layer name | github® commit SHA1 reference |
---|---|
meta-st-stm32mp | bd643ba8654010628fbcf093666fe3d184a9df34 |
meta-st-openstlinux | 2dc988821b19d2eb75cfad4d543b674cdadd77bb |
oe-manifest | 0acb085ce0c7dfe01cd03c766620eba8851f7cb0 6d8f11172136624905da984a96e0ac29f36decec |
Component | Recipe name | new github® release |
---|---|---|
tf-a | tf-a-stm32mp | v2.2-stm32mp-r2.3 |
u-boot | u-boot-stm32mp | v2020.01-stm32mp-r2.2 |
kernel | linux-stm32mp | v5.4-stm32mp-r2.3 |
optee-os | optee-os-stm32mp | 3.9.0-stm32mp-r2.3" |
repo init -u https://github.com/STMicroelectronics/oe-manifest -b dunfell-2.x repo sync
8.2 v2.1.3[edit]
- Update to Yocto 3.1.9 (2020-04.9-dunfell)
- Correct syntax changed for fit
Layer name | github® commit SHA1 reference |
---|---|
meta-st-stm32mp | 86260861f4bffd9fb97541e83d5f1c2db34e2e84 |
oe-manifest | 0acb085ce0c7dfe01cd03c766620eba8851f7cb0 |
repo init -u https://github.com/STMicroelectronics/oe-manifest -b dunfell-2.x repo sync
8.3 v2.1.2[edit]
Component | Recipe name | new github® release |
---|---|---|
tf-a | tf-a-stm32mp | v2.2-stm32mp-r2.2 |
u-boot | u-boot-stm32mp | v2020.01-stm32mp-r2.1 |
kernel | linux-stm32mp | v5.4-stm32mp-r2.2 |
optee-os | optee-os-stm32mp | 3.9.0-stm32mp-r2.2 |
8.4 v2.1.1[edit]
Component | Recipe name | new github® release |
---|---|---|
tf-a | tf-a-stm32mp | v2.2-stm32mp-r2.1 |
u-boot | u-boot-stm32mp | v2020.01-stm32mp-r2.1 |
kernel | linux-stm32mp | v5.4-stm32mp-r2.1 |
optee-os | optee-os-stm32mp | 3.9.0-stm32mp-r2.1 |
9 How to get started with openstlinux-5.4-dunfell-mp1-20-11-12[edit]
Refer to How to download the software and start with this release?
10 Associated tools[edit]
Refer to the Referenced tools release notes .
11 Detailed delivery content[edit]
11.1 Detailed description of STMicroelectronics layers[edit]
OpenSTLinux distribution is based on the build framework OpenEmbedded.
OpenEmbedded build framework engine is named OE-Core.
A layer is a collection of recipes and/or configurations applied on top of OE-Core.
Typically, each layer is organized around a specific theme, such as adding recipes for building web browser software.
The implemented layers are listed below, together with the list of recipes contained in each layer and the related information.
11.1.1 meta-st-stm32mp[edit]
Name of layer | Description |
---|---|
meta-st-stm32mp | BSP Layer for stm32mp |
Recipe Name | Path of recipe | License | Description |
---|---|---|---|
alsa-state-stm32mp1 | meta-st/meta-st-stm32mp/recipes-bsp/alsa/alsa-state-stm32mp1.bb | MIT | Alsa scenario files to enable alsa state restoration |
gcnano-driver-stm32mp | meta-st/meta-st-stm32mp/recipes-bsp/drivers/gcnano-driver-stm32mp_6.4.3.bb | GPLv1 & MIT | GCNano kernel drivers |
tf-a-stm32mp | meta-st/meta-st-stm32mp/recipes-bsp/trusted-firmware-a/tf-a-stm32mp_2.2.bb | BSD-3-Clause | Trusted Firmware-A for STM32MP1 |
u-boot-stm32mp-extlinux | meta-st/meta-st-stm32mp/recipes-bsp/u-boot/u-boot-stm32mp-extlinux.bb | MIT | Generate 'extlinux.conf' file for U-boot |
u-boot-stm32mp-splash | meta-st/meta-st-stm32mp/recipes-bsp/u-boot/u-boot-stm32mp-splash_2018.11.bb | Proprietary | Universal Boot Loader Splash Screen for stm32mp embedded devices |
u-boot-stm32mp | meta-st/meta-st-stm32mp/recipes-bsp/u-boot/u-boot-stm32mp_2020.01.bb | GPLv2+ | Universal Boot Loader for embedded devices for stm32mp (trusted) |
wifi-suspend | meta-st/meta-st-stm32mp/recipes-connectivity/wifi/wifi-suspend.bb | MIT | Systemd service to suspend/resume correctly the wifi |
gcc-arm-none-eabi-native | meta-st/meta-st-stm32mp/recipes-devtools/gcc-arm-none-eabi/gcc-arm-none-eabi-native_7.bb | GPL-3.0-with-GCC-exception & GPLv3 | Baremetal GCC for ARM |
nativesdk-gcc-arm-none-eabi | meta-st/meta-st-stm32mp/recipes-devtools/gcc-arm-none-eabi/nativesdk-gcc-arm-none-eabi_7.bb | GPL-3.0-with-GCC-exception & GPLv3 | Baremetal GCC for ARM |
openocd-stm32mp | meta-st/meta-st-stm32mp/recipes-devtools/openocd/openocd-stm32mp_0.10.0.bb | GPLv2 | Free and Open On-Chip Debugging, In-System Programming and Boundary-Scan Testing |
sdcard-raw-tools | meta-st/meta-st-stm32mp/recipes-devtools/sdcard-raw-tools/sdcard-raw-tools.bb | MIT | script for creating raw SDCARD image ready to flash |
linux-examples-stm32mp1 | meta-st/meta-st-stm32mp/recipes-extended/linux-examples/linux-examples-stm32mp1.bb | Proprietary | ST STM32MP1 projects for Linux examples |
m4fwcoredump | meta-st/meta-st-stm32mp/recipes-extended/m4coredump/m4fwcoredump.bb | MIT | Script to manage coredump of cortexM4 |
m4projects-stm32mp1 | meta-st/meta-st-stm32mp/recipes-extended/m4projects/m4projects-stm32mp1.bb | Proprietary | ST STM32MP1 Examples for CM4 |
gcnano-userland-multi-binary-debug-stm32mp | meta-st/meta-st-stm32mp/recipes-graphics/gcnano-userland/gcnano-userland-multi-binary-debug-stm32mp.bb | Proprietary | [DEBUG] Vivante libraries OpenGL ES, OpenVG and EGL (multi backend) |
gcnano-userland-multi-binary-stm32mp | meta-st/meta-st-stm32mp/recipes-graphics/gcnano-userland/gcnano-userland-multi-binary-stm32mp.bb | Proprietary | Vivante libraries OpenGL ES, OpenVG and EGL (multi backend) |
linux-firmware-bluetooth-bcm4343 | meta-st/meta-st-stm32mp/recipes-kernel/linux-firmware/linux-firmware-bluetooth-bcm4343.bb | Firmware-cypress-bcm4343 | Bluetooth firrmware for BCM4343 |
linux-stm32mp | meta-st/meta-st-stm32mp/recipes-kernel/linux/linux-stm32mp_5.4.bb | GPLv2 | Linux STM32MP Kernel |
optee-os-stm32mp | meta-st/meta-st-stm32mp/recipes-security/optee/optee-os-stm32mp_3.9.0.bb | BSD | OPTEE OS for stm32mp |
st-image-bootfs | meta-st/meta-st-stm32mp/recipes-st/images/st-image-bootfs.bb | MIT | STM32MP bootfs Image |
st-image-userfs | meta-st/meta-st-stm32mp/recipes-st/images/st-image-userfs.bb | MIT | STM32MP userfs Image |
st-image-vendorfs | meta-st/meta-st-stm32mp/recipes-st/images/st-image-vendorfs.bb | MIT | STM32MP vendorfs Image |
hidapi-stm32mp | meta-st/meta-st-stm32mp/recipes-support/hidapi/hidapi-stm32mp_0.8.0-rc1.bb | BSD-3-Clause GPLv3 | Multi-platform library to interface with USB and Bluetooth HID-Class devices |
libopencsd | meta-st/meta-st-stm32mp/recipes-support/libopencsd/libopencsd_0.10.0.bb | BSD-3-Clause | SUMMARY=CoreSight Trace Decode library |
Addons on recipes: configuration, patch, .. | |
---|---|
Recipe Name | Path of recipe |
alsa-lib | meta-st/meta-st-stm32mp/recipes-bsp/alsa/alsa-lib_%.bbappend |
base-files | meta-st/meta-st-stm32mp/recipes-core/base-files/base-files_%.bbappend |
busybox | meta-st/meta-st-stm32mp/recipes-core/busybox/busybox_%.bbappend |
systemd-conf | meta-st/meta-st-stm32mp/recipes-core/systemd/systemd-conf.bbappend |
bison | meta-st/meta-st-stm32mp/recipes-devtools/bison/bison_%.bbappend |
gdb-cross-canadian | meta-st/meta-st-stm32mp/recipes-devtools/gdb/gdb-cross-canadian_%.bbappend |
gdb-cross | meta-st/meta-st-stm32mp/recipes-devtools/gdb/gdb-cross_%.bbappend |
libdrm | meta-st/meta-st-stm32mp/recipes-graphics/drm/libdrm_%.bbappend |
weston-init | meta-st/meta-st-stm32mp/recipes-graphics/wayland/weston-init.bbappend |
weston | meta-st/meta-st-stm32mp/recipes-graphics/wayland/weston_5.0.0.bbappend |
linux-firmware | meta-st/meta-st-stm32mp/recipes-kernel/linux-firmware/linux-firmware_git.bbappend |
pulseaudio | meta-st/meta-st-stm32mp/recipes-multimedia/pulseaudio/pulseaudio_%.bbappend |
11.1.2 meta-st-stm32mp-addons[edit]
Name of layer | Description |
---|---|
meta-st-stm32mp-addons | BSP addons layer for stm32mp |
Addons on recipes: configuration, patch, .. | |
---|---|
Recipe Name | Path of recipe |
alsa-state-stm32mp1 | meta-st/meta-st-stm32mp-addons/recipes-bsp/alsa/alsa-state-stm32mp1.bbappend |
tf-a-stm32mp | meta-st/meta-st-stm32mp-addons/recipes-bsp/trusted-firmware-a/tf-a-stm32mp_%.bbappend |
u-boot-stm32mp | meta-st/meta-st-stm32mp-addons/recipes-bsp/u-boot/u-boot-stm32mp_%.bbappend |
linux-stm32mp | meta-st/meta-st-stm32mp-addons/recipes-kernel/linux/linux-stm32mp_%.bbappend |
m4projects-stm32mp1 | meta-st/meta-st-stm32mp-addons/recipes-extended/m4projects/m4projects-stm32mp1.bbappend |
11.1.3 meta-st-openstlinux[edit]
Name of layer | Description |
---|---|
meta-st-openstlinux | OpenSTLinux layer - framework/image settings |
Recipe Name | Path of recipe | License | Description |
---|---|---|---|
resize-helper | meta-st/meta-st-openstlinux/recipes-bsp/tools/resize-helper.bb | GPLv2+ | Tools for resizing the file system |
usbotg-gadget-config | meta-st/meta-st-openstlinux/recipes-bsp/tools/usbotg-gadget-config.bb | MIT | The goal is to enable USB Ethernet & MSC gadget |
psplash-drm | meta-st/meta-st-openstlinux/recipes-core/psplash/psplash-drm.bb | MIT | Basic splash screen displaying a picture on DRM/KMS |
systemd-mount-partitions | meta-st/meta-st-openstlinux/recipes-core/systemd/systemd-mount-partitions.bb | MIT | Mount partitions |
systemd-networkd-configuration | meta-st/meta-st-openstlinux/recipes-core/systemd/systemd-networkd-configuration.bb | MIT | Basic networkd configuration |
lsb-openstlinux | meta-st/meta-st-openstlinux/recipes-extended/lsb/lsb-openstlinux.bb | GPLv2+ | LSB support for checking gpu provider |
openstlinux-qt-eglfs | meta-st/meta-st-openstlinux/recipes-qt/qt5/openstlinux-qt-eglfs.bb | MIT | add script and material to help with eglfs qt configuration |
ai-hand-char-reco-launcher | meta-st/meta-st-openstlinux/recipes-samples/ai-nn-application/ai-hand-char-reco-launcher.bb | GPLv2 & BSD-3-Clause | Hand writing character recognition launcher based on HCR Neural Network |
demo-launcher | meta-st/meta-st-openstlinux/recipes-samples/demo/demo-launcher.bb | Proprietary | Python script which launch several use-cases |
sensors-iks01a2 | meta-st/meta-st-openstlinux/recipes-samples/demo/sensors-iks01a2.bb | Proprietary | Python script which monitors the temperature measured by the Nucleo extension board iks01a2a on-board sensor |
demo-hotspot-wifi | meta-st/meta-st-openstlinux/recipes-samples/hotspot-wifi/demo-hotspot-wifi.bb | MIT | Shell script to enable/disable hotsopt wifi configuration |
st-example-image-qt | meta-st/meta-st-openstlinux/recipes-samples/images/st-example-image-qt.bb | Proprietary | STMicroelectronics example of image based on QT framework. |
st-example-image-qtwayland | meta-st/meta-st-openstlinux/recipes-samples/images/st-example-image-qtwayland.bb | Proprietary | STMicroelectronics example of image based on QT framework over Weston/Wayland. |
optee-client | meta-st/meta-st-openstlinux/recipes-security/optee/optee-client_git.bb | BSD | OPTEE client |
optee-examples | meta-st/meta-st-openstlinux/recipes-security/optee/optee-examples.bb | GPLv2 | OP-TEE examples |
optee-test | meta-st/meta-st-openstlinux/recipes-security/optee/optee-test_git.bb | BSD & GPLv2 | OP-TEE sanity testsuite |
packagegroup-optee-core | meta-st/meta-st-openstlinux/recipes-security/packagegroups/packagegroup-optee-core.bb | LGPLv2+ | OP-TEE core packagegroup |
packagegroup-optee-test | meta-st/meta-st-openstlinux/recipes-security/packagegroups/packagegroup-optee-test.bb | LGPLv2+ | OP-TEE test packagegroup |
libsmaf | meta-st/meta-st-openstlinux/recipes-security/smaf/libsmaf.bb | LGPLv2.1 | SMAF library |
st-image-core | meta-st/meta-st-openstlinux/recipes-st/images/st-image-core.bb | Proprietary | OpenSTLinux core image. |
st-image-weston | meta-st/meta-st-openstlinux/recipes-st/images/st-image-weston.bb | Proprietary | OpenSTLinux weston image with basic Wayland support (if enable in distro). |
packagegroup-framework-tools | meta-st/meta-st-openstlinux/recipes-st/packagegroups/packagegroup-framework-tools.bb | MIT | Frameworks components |
packagegroup-gstreamer1-0 | meta-st/meta-st-openstlinux/recipes-st/packagegroups/packagegroup-gstreamer1-0.bb | LGPLv2+ | Gstreamer 1.0 components |
Recipes addons, such as configurations and patches.
Recipe name | Recipe path |
---|---|
openssh | meta-st/meta-st-openstlinux/oe-core/recipes-connectivity/openssh/openssh_%.bbappend |
packagegroup-core-ssh-openssh | meta-st/meta-st-openstlinux/oe-core/recipes-core/packagegroups/packagegroup-core-ssh-openssh.bbappend |
dpkg | meta-st/meta-st-openstlinux/oe-core/recipes-devtools/dpkg/dpkg_%.bbappend |
ckermit | meta-st/meta-st-openstlinux/oe-core/recipes-support/ckermit/ckermit_%.bbappend |
libiio | meta-st/meta-st-openstlinux/oe-core/recipes-support/libiio/libiio_git.bbappend |
glmark2 | meta-st/meta-st-openstlinux/recipes-benchmark/glmark2/glmark2_%.bbappend |
bluez5 | meta-st/meta-st-openstlinux/recipes-connectivity/bluez5/bluez5_%.bbappend |
connman | meta-st/meta-st-openstlinux/recipes-connectivity/connman/connman_%.bbappend |
busybox | meta-st/meta-st-openstlinux/recipes-core/busybox/busybox_%.bbappend |
meta-environment | meta-st/meta-st-openstlinux/recipes-core/meta/meta-environment.bbappend |
packagegroup-core-eclipse-debug | meta-st/meta-st-openstlinux/recipes-core/packagegroups/packagegroup-core-eclipse-debug.bbappend |
packagegroup-core-tools-profile | meta-st/meta-st-openstlinux/recipes-core/packagegroups/packagegroup-core-tools-profile.bbappend |
systemd-conf | meta-st/meta-st-openstlinux/recipes-core/systemd/systemd-conf.bbappend |
systemd-serialgetty | meta-st/meta-st-openstlinux/recipes-core/systemd/systemd-serialgetty.bbappend |
systemd | meta-st/meta-st-openstlinux/recipes-core/systemd/systemd_%.bbappend |
cairo | meta-st/meta-st-openstlinux/recipes-graphics/cairo/cairo_%.bbappend |
kmscube | meta-st/meta-st-openstlinux/recipes-graphics/kmscube/kmscube_git.bbappend |
lxdm | meta-st/meta-st-openstlinux/recipes-graphics/lxdm/lxdm_0.5.3.bbappend |
wayland-protocols | meta-st/meta-st-openstlinux/recipes-graphics/wayland/wayland-protocols_1.10.bbappend |
weston-init | meta-st/meta-st-openstlinux/recipes-graphics/wayland/weston-init.bbappend |
xserver-nodm-init | meta-st/meta-st-openstlinux/recipes-graphics/x11-common/xserver-nodm-init_%.bbappend |
xinit | meta-st/meta-st-openstlinux/recipes-graphics/xorg-app/xinit_%.bbappend |
pixman | meta-st/meta-st-openstlinux/recipes-graphics/xorg-lib/pixman_0.34.0.bbappend |
alsa-utils | meta-st/meta-st-openstlinux/recipes-multimedia/alsa/alsa-utils_1.1.4.bbappend |
gstreamer1.0-libav | meta-st/meta-st-openstlinux/recipes-multimedia/gstreamer/gstreamer1.0-libav_1.14.2.bbappend |
gstreamer1.0-plugins-bad | meta-st/meta-st-openstlinux/recipes-multimedia/gstreamer/gstreamer1.0-plugins-bad_1.12.2.bbappend |
gstreamer1.0-plugins-base | meta-st/meta-st-openstlinux/recipes-multimedia/gstreamer/gstreamer1.0-plugins-base_1.12.2.bbappend |
gstreamer1.0-plugins-good | meta-st/meta-st-openstlinux/recipes-multimedia/gstreamer/gstreamer1.0-plugins-good_1.12.2.bbappend |
pulseaudio | meta-st/meta-st-openstlinux/recipes-multimedia/pulseaudio/pulseaudio_10.0.bbappend |
v4l-utils | meta-st/meta-st-openstlinux/recipes-multimedia/v4l2apps/v4l-utils_1.12.3.bbappend |
packagegroup-qt5-toolchain-target | meta-st/meta-st-openstlinux/recipes-qt/packagegroups/packagegroup-qt5-toolchain-target.bbappend |
qtbase | meta-st/meta-st-openstlinux/recipes-qt/qt5/qtbase_git.bbappend |
qtmultimedia | meta-st/meta-st-openstlinux/recipes-qt/qt5/qtmultimedia_git.bbappend |
st-image-userfs | meta-st/meta-st-openstlinux/recipes-samples/images/st-image-userfs.bbappend |
packagegroup-framework-tools | meta-st/meta-st-openstlinux/recipes-st/packagegroups/packagegroup-framework-tools.bbappend |
ntp | meta-st/meta-st-openstlinux/recipes-support/ntp/ntp_%.bbappend |
netdata | meta-st/meta-st-openstlinux/recipes-webadmin/netdata/netdata_git.bbappend |
This article describes the content of [[OpenSTLinux distribution]] '''software''' release version '''{{EcosystemRelease/Package | revision=2.1.0 | package=OpenSTLinux distribution | request=name}}''', which is part of [[STM32MP15 ecosystem release note - v2.1.0]]. ==Intended audience== The targeted audience is STM32MP15 customers or partners. ==Delivery scope and purpose== The OpenSTLinux distribution is a Linux<sup>®</sup> distribution based on the OpenEmbedded build Framework. It runs on the Arm<sup>®</sup> Cortex<sup>®</sup>-A7 processors, and is a fundamental part of the [[STM32MPU Embedded Software distribution]]. This delivery of OpenSTLinux distribution is part of STM32MP15-Ecosystem-v2.1.0 (see the [[STM32MP15 ecosystem release note - v2.1.0]]). ==Licensing== This software package is licensed under a LIMITED LICENSE AGREEMENT FOR ST MATERIALS EVALUATION (LLA). Customers may not use this package except in compliance with the [[LegalInformation:OpenSTLinux licenses - v2.1.0#Top Software license agreement (SLA) and third-party licences|software license agreement (SLA)]]. All of the packages use the same source components. All components and their respective licenses are listed [[LegalInformation:OpenSTLinux licenses - v2.1.0|here]]. ==Supported hardware== This software delivery is compatible with the following boards: * STM32MP157A-EV1, STM32MP157C-EV1, STM32MP157D-EV1 and STM32MP157F-EV1 Evaluation boards. For more information on this board, please read the article [[STM32MP157x-EV1 - hardware description]] * STM32MP157A-DK1, STM32MP157D-DK1, STM32MP157C-DK2 and STM32MP157F-DK2 Discovery kit. For more information on these boards, please read the article [[STM32MP157x-DKx - hardware description]] ==Delivered features== ===Main software components=== * {{EcosystemRelease/Component | revision=2.1.0 | component=Linux kernel}} * {{EcosystemRelease/Component | revision=2.1.0 | component=TF-A}} * {{EcosystemRelease/Component | revision=2.1.0 | component=U-Boot}} * {{EcosystemRelease/Component | revision= 2.1.0| component=OP-TEE}} * {{EcosystemRelease/Component | revision= 2.1.0| component=STM32CubeMPU}} * {{EcosystemRelease/Component | revision= 2.1.0| component=OpenEmbedded}} * Weston version v8.0.0 * Wayland version 1.18.0 * GStreamer version v1.16.2 * GCC version v9.3 * OpenOCD version v0.10.0 * GCnano version v6.4.3 ===Detailed features=== ====Kernel part==== * Rebase on Linux kernel v5.4.56 * Add OP-TEE support in remoteproc * Add FMC2 EBI support * Add serial modem control gpio support * Add vbus-supply support through usbphyc * Add SAI PM_runtime support * Other fixes ====U-boot part==== * Activate DCache in SPL and in pre-reloc step to reduce boot time * Handle I2C FastMode+ for STM32MP15x * Backport ETH patches and solve instability due to DCache managment * Handle OP-TEE reserved memory and fixup the associated node in kernel device tree device tree * Add EBI support in FMC2 driver * Fixup DBGMCU init to avoid boot crash * Use SCMI for MCU_HOLD_BOOT in remoteproc * Add VBus support in USB PHYC driver * Add Cortex-M4 firmware load with OP-TEE remoteproc TA * Other minor fixes ====TF-A part==== * FMC2: Update bindings for EBI support * SMC: return correct error * TAMPER: Add PINCTRL management for tamper if defined * USB OTG: regulator mode update * Update firewall on DDR CTRL and PHY (Allow read access for non-secure) * Manage MCU reset through SCMI * Add a new RETRAM property to configure state during low power * Correct STGEN counter restore when returning from stop mode * Add support of auto stop mode management * Correct the exception fault return address * Other minor fixes + all fixes already published after STM32MP15 ecosystem release v2.0.0 * Rebase TF-A SSP ====OP-TEE part==== * TA: Authenticated firmware management, used for Cortex-M4 firmware loading * Update firewall on DDR CTRL and PHY (Allow read access for non-secure) * Manage MCU reset through SCMI * SMC: return correct error * USB OTG: regulator mode update * Other minor fixes + all fixes already published after STM32MP15 ecosystem release v2.0.0 ==Recommendations for use== ===Safe use=== * Flash programming and boot from all supported Flash devices: SDCard, eMMC, ONFI NAND and NOR Flash memories * Develop Linux<sup>®</sup> applications, libraries, kernel modules based on OpenSTLinux delivery * Develop coprocessor Cube applications based on STM32CubeMP1 delivery * Develop boards based on STM32MP15 * Prototype applications based on ST boards ===Non-recommended use=== * None ==Main restrictions list== * M-CAN Bus is not functional if power management is activated ("sleep" state defined in pinctrl): the issue is corrected thanks to [https://git.kernel.org/pub/scm/linux/kernel/git/stable/linux.git/commit/?id=b0342b87cad88894a989604df549e88ff47fb513 this patch]. ==Minor release updates==<section begin=OpenSTLinux_release/> STMicroelectronics regularly delivers corrections through github<sup>®</sup> components which are [https://github.com/STMicroelectronics/u-boot/ u-boot], [https://github.com/STMicroelectronics/optee_os optee-os], [https://github.com/STMicroelectronics/arm-trusted-firmware tf-a], [https://github.com/STMicroelectronics/linux Linux kernel]. <br> You can decide to incorporate them into your developer package (please refer to [[STM32MP1 Developer Package]]) or Distribution package.<br/> To update Distribution package please proceed as follow: :# [[OpenSTLinux_distribution#Reference_source_code| Switch to github<sup>®</sup> mode]] your Distribution package. :# Use the command ''' [[OpenEmbedded_-_devtool#devtool_modify|devtool modify]] <recipe name>''' to set up an environment. It will fetch and unpack the source code. :# In extracted source code, use git command such as '''git checkout -b WORK <github<sup>®</sup> TAG>''' to point on new revision of component. More rarely STMicroelectronics also delivers fixes on layers through github<sup>®</sup>. These changes can be integrated (via [[git]] commands) into your local [[STM32MP1 Distribution Package]] environment. Please find below the github<sup>®</sup> links of the quoted layers : * [https://github.com/STMicroelectronics/meta-st-stm32mp/ meta-st-stm32mp] * [https://github.com/STMicroelectronics/meta-st-openstlinux/ meta-st-openstlinux ] * [https://github.com/STMicroelectronics/meta-st-stm32mp-addons/ meta-st-stm32mp-addons] ===v2.1.4=== * Update to Yocto 3.1.11 (dunfell-23.0.11) * BSP update {| ! Layer name !! github<sup>®</sup> commit SHA1 reference |- | meta-st-stm32mp || [https://github.com/STMicroelectronics/meta-st-stm32mp/commit/bd643ba8654010628fbcf093666fe3d184a9df34 bd643ba8654010628fbcf093666fe3d184a9df34] |- | meta-st-openstlinux || [https://github.com/STMicroelectronics/meta-st-openstlinux/commit/2dc988821b19d2eb75cfad4d543b674cdadd77bb 2dc988821b19d2eb75cfad4d543b674cdadd77bb] |- | oe-manifest || [https://github.com/STMicroelectronics/oe-manifest/commit/0acb085ce0c7dfe01cd03c766620eba8851f7cb0 0acb085ce0c7dfe01cd03c766620eba8851f7cb06d8f11172136624905da984a96e0ac29f36decec 6d8f11172136624905da984a96e0ac29f36decec] |} {| ! Component !! Recipe name !! new github<sup>®</sup> release |- | tf-a || tf-a-stm32mp || [https://github.com/STMicroelectronics/arm-trusted-firmware/releases/tag/v2.2-stm32mp-r2.3 '''v2.2-stm32mp-r2.3'''] |- | u-boot || u-boot-stm32mp || [https://github.com/STMicroelectronics/u-boot/releases/tag/v2020.01-stm32mp-r2.2 '''v2020.01-stm32mp-r2.2'''] |- | kernel || linux-stm32mp || [https://github.com/STMicroelectronics/linux/releases/tag/v5.4-stm32mp-r2.3 '''v5.4-stm32mp-r2.3'''] |- | optee-os || optee-os-stm32mp || [https://github.com/STMicroelectronics/optee_os/releases/tag/3.9.0-stm32mp-r2.3 '''3.9.0-stm32mp-r2.3"'''] |} repo init -u https://github.com/STMicroelectronics/oe-manifest -b dunfell-2.x repo sync ===v2.1.3=== * Update to Yocto 3.1.9 (2020-04.9-dunfell) * Correct syntax changed for fit {| ! Layer name !! github<sup>®</sup> commit SHA1 reference |- | meta-st-stm32mp || [https://github.com/STMicroelectronics/meta-st-stm32mp/commit/86260861f4bffd9fb97541e83d5f1c2db34e2e84 86260861f4bffd9fb97541e83d5f1c2db34e2e84] |- | oe-manifest || [https://github.com/STMicroelectronics/oe-manifest/commit/0acb085ce0c7dfe01cd03c766620eba8851f7cb0 0acb085ce0c7dfe01cd03c766620eba8851f7cb0] |} repo init -u https://github.com/STMicroelectronics/oe-manifest -b dunfell-2.x repo sync ===v2.1.2=== {| ! Component !! Recipe name !! new github<sup>®</sup> release |- | tf-a || tf-a-stm32mp || [https://github.com/STMicroelectronics/arm-trusted-firmware/releases/tag/v2.2-stm32mp-r2.2 '''v2.2-stm32mp-r2.2'''] |- | u-boot || u-boot-stm32mp || [https://github.com/STMicroelectronics/u-boot/releases/tag/v2020.01-stm32mp-r2.1 ''v2020.01-stm32mp-r2.1''] |- | kernel || linux-stm32mp || [https://github.com/STMicroelectronics/linux/releases/tag/v5.4-stm32mp-r2.2 '''v5.4-stm32mp-r2.2'''] |- | optee-os || optee-os-stm32mp || [https://github.com/STMicroelectronics/optee_os/releases/tag/3.9.0-stm32mp-r2.2 '''3.9.0-stm32mp-r2.2'''] |} ===v2.1.1=== {| ! Component !! Recipe name !! new github<sup>®</sup> release |- | tf-a || tf-a-stm32mp || [https://github.com/STMicroelectronics/arm-trusted-firmware/releases/tag/v2.2-stm32mp-r2.1 '''v2.2-stm32mp-r2.1'''] |- | u-boot || u-boot-stm32mp || [https://github.com/STMicroelectronics/u-boot/releases/tag/v2020.01-stm32mp-r2.1 '''v2020.01-stm32mp-r2.1'''] |- | kernel || linux-stm32mp || [https://github.com/STMicroelectronics/linux/releases/tag/v5.4-stm32mp-r2.1 '''v5.4-stm32mp-r2.1'''] |- | optee-os || optee-os-stm32mp || [https://github.com/STMicroelectronics/optee_os/releases/tag/3.9.0-stm32mp-r2.1 '''3.9.0-stm32mp-r2.1'''] |}<section end=OpenSTLinux_release/> ==How to get started with {{EcosystemRelease/Package | revision=2.1.0 | package=OpenSTLinux distribution | request=name}}== Refer to [[STM32MP15_ecosystem_release_note_-_v2.1.0#How_to_download_the_software_and_start_with_this_release-3F|How to download the software and start with this release?]] ==Associated tools== Refer to the [[STM32MP15 ecosystem release note - v2.1.0#Referenced tools release notes | Referenced tools release notes ]]. ==Detailed delivery content== ===Detailed description of STMicroelectronics layers === OpenSTLinux distribution is based on the build framework OpenEmbedded.<br /> OpenEmbedded build framework engine is named OE-Core. <br /> A layer is a collection of recipes and/or configurations applied on top of OE-Core. Typically, each layer is organized around a specific theme, such as adding recipes for building web browser software. The implemented layers are listed below, together with the list of recipes contained in each layer and the related information. ==== meta-st-stm32mp ==== {| ! Name of layer !! Description |- | meta-st-stm32mp || BSP Layer for stm32mp |- |} {| |- ! Recipe Name !! Path of recipe !! License !! Description |- | alsa-state-stm32mp1 || meta-st/meta-st-stm32mp/recipes-bsp/alsa/alsa-state-stm32mp1.bb || MIT || Alsa scenario files to enable alsa state restoration |- | gcnano-driver-stm32mp || meta-st/meta-st-stm32mp/recipes-bsp/drivers/gcnano-driver-stm32mp_6.4.3.bb || GPLv1 & MIT || GCNano kernel drivers |- | tf-a-stm32mp || meta-st/meta-st-stm32mp/recipes-bsp/trusted-firmware-a/tf-a-stm32mp_2.2.bb || BSD-3-Clause || Trusted Firmware-A for STM32MP1 |- | u-boot-stm32mp-extlinux || meta-st/meta-st-stm32mp/recipes-bsp/u-boot/u-boot-stm32mp-extlinux.bb || MIT || Generate 'extlinux.conf' file for U-boot |- | u-boot-stm32mp-splash || meta-st/meta-st-stm32mp/recipes-bsp/u-boot/u-boot-stm32mp-splash_2018.11.bb || Proprietary || Universal Boot Loader Splash Screen for stm32mp embedded devices |- | u-boot-stm32mp || meta-st/meta-st-stm32mp/recipes-bsp/u-boot/u-boot-stm32mp_2020.01.bb || GPLv2+ || Universal Boot Loader for embedded devices for stm32mp (trusted) |- | wifi-suspend || meta-st/meta-st-stm32mp/recipes-connectivity/wifi/wifi-suspend.bb || MIT || Systemd service to suspend/resume correctly the wifi |- | gcc-arm-none-eabi-native || meta-st/meta-st-stm32mp/recipes-devtools/gcc-arm-none-eabi/gcc-arm-none-eabi-native_7.bb || GPL-3.0-with-GCC-exception & GPLv3 || Baremetal GCC for ARM |- | nativesdk-gcc-arm-none-eabi || meta-st/meta-st-stm32mp/recipes-devtools/gcc-arm-none-eabi/nativesdk-gcc-arm-none-eabi_7.bb || GPL-3.0-with-GCC-exception & GPLv3 || Baremetal GCC for ARM |- | openocd-stm32mp || meta-st/meta-st-stm32mp/recipes-devtools/openocd/openocd-stm32mp_0.10.0.bb || GPLv2 || Free and Open On-Chip Debugging, In-System Programming and Boundary-Scan Testing |- | sdcard-raw-tools || meta-st/meta-st-stm32mp/recipes-devtools/sdcard-raw-tools/sdcard-raw-tools.bb || MIT || script for creating raw SDCARD image ready to flash |- | linux-examples-stm32mp1 || meta-st/meta-st-stm32mp/recipes-extended/linux-examples/linux-examples-stm32mp1.bb || Proprietary || ST STM32MP1 projects for Linux examples |- | m4fwcoredump || meta-st/meta-st-stm32mp/recipes-extended/m4coredump/m4fwcoredump.bb || MIT || Script to manage coredump of cortexM4 |- | m4projects-stm32mp1 || meta-st/meta-st-stm32mp/recipes-extended/m4projects/m4projects-stm32mp1.bb || Proprietary || ST STM32MP1 Examples for CM4 |- | gcnano-userland-multi-binary-debug-stm32mp || meta-st/meta-st-stm32mp/recipes-graphics/gcnano-userland/gcnano-userland-multi-binary-debug-stm32mp.bb || Proprietary || [DEBUG] Vivante libraries OpenGL ES, OpenVG and EGL (multi backend) |- | gcnano-userland-multi-binary-stm32mp || meta-st/meta-st-stm32mp/recipes-graphics/gcnano-userland/gcnano-userland-multi-binary-stm32mp.bb || Proprietary || Vivante libraries OpenGL ES, OpenVG and EGL (multi backend) |- | linux-firmware-bluetooth-bcm4343 || meta-st/meta-st-stm32mp/recipes-kernel/linux-firmware/linux-firmware-bluetooth-bcm4343.bb || Firmware-cypress-bcm4343 || Bluetooth firrmware for BCM4343 |- | linux-stm32mp || meta-st/meta-st-stm32mp/recipes-kernel/linux/linux-stm32mp_5.4.bb || GPLv2 || Linux STM32MP Kernel |- | optee-os-stm32mp || meta-st/meta-st-stm32mp/recipes-security/optee/optee-os-stm32mp_3.9.0.bb || BSD || OPTEE OS for stm32mp |- | st-image-bootfs || meta-st/meta-st-stm32mp/recipes-st/images/st-image-bootfs.bb || MIT || STM32MP bootfs Image |- | st-image-userfs || meta-st/meta-st-stm32mp/recipes-st/images/st-image-userfs.bb || MIT || STM32MP userfs Image |- | st-image-vendorfs || meta-st/meta-st-stm32mp/recipes-st/images/st-image-vendorfs.bb || MIT || STM32MP vendorfs Image |- | hidapi-stm32mp || meta-st/meta-st-stm32mp/recipes-support/hidapi/hidapi-stm32mp_0.8.0-rc1.bb || BSD-3-Clause GPLv3 || Multi-platform library to interface with USB and Bluetooth HID-Class devices |- | libopencsd || meta-st/meta-st-stm32mp/recipes-support/libopencsd/libopencsd_0.10.0.bb || BSD-3-Clause || SUMMARY=CoreSight Trace Decode library |} {| |- ! Addons on recipes: configuration, patch, .. |- ! Recipe Name !! Path of recipe |- | alsa-lib || meta-st/meta-st-stm32mp/recipes-bsp/alsa/alsa-lib_%.bbappend |- | base-files || meta-st/meta-st-stm32mp/recipes-core/base-files/base-files_%.bbappend |- | busybox || meta-st/meta-st-stm32mp/recipes-core/busybox/busybox_%.bbappend |- | systemd-conf || meta-st/meta-st-stm32mp/recipes-core/systemd/systemd-conf.bbappend |- | bison || meta-st/meta-st-stm32mp/recipes-devtools/bison/bison_%.bbappend |- | gdb-cross-canadian || meta-st/meta-st-stm32mp/recipes-devtools/gdb/gdb-cross-canadian_%.bbappend |- | gdb-cross || meta-st/meta-st-stm32mp/recipes-devtools/gdb/gdb-cross_%.bbappend |- | libdrm || meta-st/meta-st-stm32mp/recipes-graphics/drm/libdrm_%.bbappend |- | weston-init || meta-st/meta-st-stm32mp/recipes-graphics/wayland/weston-init.bbappend |- | weston || meta-st/meta-st-stm32mp/recipes-graphics/wayland/weston_5.0.0.bbappend |- | linux-firmware || meta-st/meta-st-stm32mp/recipes-kernel/linux-firmware/linux-firmware_git.bbappend |- | pulseaudio || meta-st/meta-st-stm32mp/recipes-multimedia/pulseaudio/pulseaudio_%.bbappend |} ==== meta-st-stm32mp-addons ==== {| ! Name of layer !! Description |- | meta-st-stm32mp-addons || BSP addons layer for stm32mp |- |} {| |- ! Addons on recipes: configuration, patch, .. |- ! Recipe Name !! Path of recipe |- | alsa-state-stm32mp1 || meta-st/meta-st-stm32mp-addons/recipes-bsp/alsa/alsa-state-stm32mp1.bbappend |- | tf-a-stm32mp || meta-st/meta-st-stm32mp-addons/recipes-bsp/trusted-firmware-a/tf-a-stm32mp_%.bbappend |- | u-boot-stm32mp || meta-st/meta-st-stm32mp-addons/recipes-bsp/u-boot/u-boot-stm32mp_%.bbappend |- | linux-stm32mp || meta-st/meta-st-stm32mp-addons/recipes-kernel/linux/linux-stm32mp_%.bbappend |- | m4projects-stm32mp1 || meta-st/meta-st-stm32mp-addons/recipes-extended/m4projects/m4projects-stm32mp1.bbappend |} ==== meta-st-openstlinux ==== {| ! Name of layer !! Description |- | meta-st-openstlinux || OpenSTLinux layer - framework/image settings |- |} {| |- ! Recipe Name !! Path of recipe !! License !! Description |- | resize-helper || meta-st/meta-st-openstlinux/recipes-bsp/tools/resize-helper.bb || GPLv2+ || Tools for resizing the file system |- | usbotg-gadget-config || meta-st/meta-st-openstlinux/recipes-bsp/tools/usbotg-gadget-config.bb || MIT || The goal is to enable USB Ethernet & MSC gadget |- | psplash-drm || meta-st/meta-st-openstlinux/recipes-core/psplash/psplash-drm.bb || MIT || Basic splash screen displaying a picture on DRM/KMS |- | systemd-mount-partitions || meta-st/meta-st-openstlinux/recipes-core/systemd/systemd-mount-partitions.bb || MIT || Mount partitions |- | systemd-networkd-configuration || meta-st/meta-st-openstlinux/recipes-core/systemd/systemd-networkd-configuration.bb || MIT || Basic networkd configuration |- | lsb-openstlinux || meta-st/meta-st-openstlinux/recipes-extended/lsb/lsb-openstlinux.bb || GPLv2+ || LSB support for checking gpu provider |- | openstlinux-qt-eglfs || meta-st/meta-st-openstlinux/recipes-qt/qt5/openstlinux-qt-eglfs.bb || MIT || add script and material to help with eglfs qt configuration |- | ai-hand-char-reco-launcher || meta-st/meta-st-openstlinux/recipes-samples/ai-nn-application/ai-hand-char-reco-launcher.bb || GPLv2 & BSD-3-Clause || Hand writing character recognition launcher based on HCR Neural Network |- | demo-launcher || meta-st/meta-st-openstlinux/recipes-samples/demo/demo-launcher.bb || Proprietary || Python script which launch several use-cases |- | sensors-iks01a2 || meta-st/meta-st-openstlinux/recipes-samples/demo/sensors-iks01a2.bb || Proprietary || Python script which monitors the temperature measured by the Nucleo extension board iks01a2a on-board sensor |- | demo-hotspot-wifi || meta-st/meta-st-openstlinux/recipes-samples/hotspot-wifi/demo-hotspot-wifi.bb || MIT || Shell script to enable/disable hotsopt wifi configuration |- | st-example-image-qt || meta-st/meta-st-openstlinux/recipes-samples/images/st-example-image-qt.bb || Proprietary || STMicroelectronics example of image based on QT framework. |- | st-example-image-qtwayland || meta-st/meta-st-openstlinux/recipes-samples/images/st-example-image-qtwayland.bb || Proprietary || STMicroelectronics example of image based on QT framework over Weston/Wayland. |- | optee-client || meta-st/meta-st-openstlinux/recipes-security/optee/optee-client_git.bb || BSD || OPTEE client |- | optee-examples || meta-st/meta-st-openstlinux/recipes-security/optee/optee-examples.bb || GPLv2 || OP-TEE examples |- | optee-test || meta-st/meta-st-openstlinux/recipes-security/optee/optee-test_git.bb || BSD & GPLv2 || OP-TEE sanity testsuite |- | packagegroup-optee-core || meta-st/meta-st-openstlinux/recipes-security/packagegroups/packagegroup-optee-core.bb || LGPLv2+ || OP-TEE core packagegroup |- | packagegroup-optee-test || meta-st/meta-st-openstlinux/recipes-security/packagegroups/packagegroup-optee-test.bb || LGPLv2+ || OP-TEE test packagegroup |- | libsmaf || meta-st/meta-st-openstlinux/recipes-security/smaf/libsmaf.bb || LGPLv2.1 || SMAF library |- | st-image-core || meta-st/meta-st-openstlinux/recipes-st/images/st-image-core.bb || Proprietary || OpenSTLinux core image. |- | st-image-weston || meta-st/meta-st-openstlinux/recipes-st/images/st-image-weston.bb || Proprietary || OpenSTLinux weston image with basic Wayland support (if enable in distro). |- | packagegroup-framework-tools || meta-st/meta-st-openstlinux/recipes-st/packagegroups/packagegroup-framework-tools.bb || MIT || Frameworks components |- | packagegroup-gstreamer1-0 || meta-st/meta-st-openstlinux/recipes-st/packagegroups/packagegroup-gstreamer1-0.bb || LGPLv2+ || Gstreamer 1.0 components |} Recipes addons, such as configurations and patches. {| |- ! Recipe name !! Recipe path |- | openssh || meta-st/meta-st-openstlinux/oe-core/recipes-connectivity/openssh/openssh_%.bbappend |- | packagegroup-core-ssh-openssh || meta-st/meta-st-openstlinux/oe-core/recipes-core/packagegroups/packagegroup-core-ssh-openssh.bbappend |- | dpkg || meta-st/meta-st-openstlinux/oe-core/recipes-devtools/dpkg/dpkg_%.bbappend |- | ckermit || meta-st/meta-st-openstlinux/oe-core/recipes-support/ckermit/ckermit_%.bbappend |- | libiio || meta-st/meta-st-openstlinux/oe-core/recipes-support/libiio/libiio_git.bbappend |- | glmark2 || meta-st/meta-st-openstlinux/recipes-benchmark/glmark2/glmark2_%.bbappend |- | bluez5 || meta-st/meta-st-openstlinux/recipes-connectivity/bluez5/bluez5_%.bbappend |- | connman || meta-st/meta-st-openstlinux/recipes-connectivity/connman/connman_%.bbappend |- | busybox || meta-st/meta-st-openstlinux/recipes-core/busybox/busybox_%.bbappend |- | meta-environment || meta-st/meta-st-openstlinux/recipes-core/meta/meta-environment.bbappend |- | packagegroup-core-eclipse-debug || meta-st/meta-st-openstlinux/recipes-core/packagegroups/packagegroup-core-eclipse-debug.bbappend |- | packagegroup-core-tools-profile || meta-st/meta-st-openstlinux/recipes-core/packagegroups/packagegroup-core-tools-profile.bbappend |- | systemd-conf || meta-st/meta-st-openstlinux/recipes-core/systemd/systemd-conf.bbappend |- | systemd-serialgetty || meta-st/meta-st-openstlinux/recipes-core/systemd/systemd-serialgetty.bbappend |- | systemd || meta-st/meta-st-openstlinux/recipes-core/systemd/systemd_%.bbappend |- | cairo || meta-st/meta-st-openstlinux/recipes-graphics/cairo/cairo_%.bbappend |- | kmscube || meta-st/meta-st-openstlinux/recipes-graphics/kmscube/kmscube_git.bbappend |- | lxdm || meta-st/meta-st-openstlinux/recipes-graphics/lxdm/lxdm_0.5.3.bbappend |- | wayland-protocols || meta-st/meta-st-openstlinux/recipes-graphics/wayland/wayland-protocols_1.10.bbappend |- | weston-init || meta-st/meta-st-openstlinux/recipes-graphics/wayland/weston-init.bbappend |- | xserver-nodm-init || meta-st/meta-st-openstlinux/recipes-graphics/x11-common/xserver-nodm-init_%.bbappend |- | xinit || meta-st/meta-st-openstlinux/recipes-graphics/xorg-app/xinit_%.bbappend |- | pixman || meta-st/meta-st-openstlinux/recipes-graphics/xorg-lib/pixman_0.34.0.bbappend |- | alsa-utils || meta-st/meta-st-openstlinux/recipes-multimedia/alsa/alsa-utils_1.1.4.bbappend |- | gstreamer1.0-libav || meta-st/meta-st-openstlinux/recipes-multimedia/gstreamer/gstreamer1.0-libav_1.14.2.bbappend |- | gstreamer1.0-plugins-bad || meta-st/meta-st-openstlinux/recipes-multimedia/gstreamer/gstreamer1.0-plugins-bad_1.12.2.bbappend |- | gstreamer1.0-plugins-base || meta-st/meta-st-openstlinux/recipes-multimedia/gstreamer/gstreamer1.0-plugins-base_1.12.2.bbappend |- | gstreamer1.0-plugins-good || meta-st/meta-st-openstlinux/recipes-multimedia/gstreamer/gstreamer1.0-plugins-good_1.12.2.bbappend |- | pulseaudio || meta-st/meta-st-openstlinux/recipes-multimedia/pulseaudio/pulseaudio_10.0.bbappend |- | v4l-utils || meta-st/meta-st-openstlinux/recipes-multimedia/v4l2apps/v4l-utils_1.12.3.bbappend |- | packagegroup-qt5-toolchain-target || meta-st/meta-st-openstlinux/recipes-qt/packagegroups/packagegroup-qt5-toolchain-target.bbappend |- | qtbase || meta-st/meta-st-openstlinux/recipes-qt/qt5/qtbase_git.bbappend |- | qtmultimedia || meta-st/meta-st-openstlinux/recipes-qt/qt5/qtmultimedia_git.bbappend |- | st-image-userfs || meta-st/meta-st-openstlinux/recipes-samples/images/st-image-userfs.bbappend |- | packagegroup-framework-tools || meta-st/meta-st-openstlinux/recipes-st/packagegroups/packagegroup-framework-tools.bbappend |- | ntp || meta-st/meta-st-openstlinux/recipes-support/ntp/ntp_%.bbappend |- | netdata || meta-st/meta-st-openstlinux/recipes-webadmin/netdata/netdata_git.bbappend |} <noinclude> {{PublicationRequestId | Auto}} [[Category:Release notes archives]]</noinclude>
Line 123: | Line 123: | ||
| meta-st-openstlinux || [https://github.com/STMicroelectronics/meta-st-openstlinux/commit/2dc988821b19d2eb75cfad4d543b674cdadd77bb 2dc988821b19d2eb75cfad4d543b674cdadd77bb] |
| meta-st-openstlinux || [https://github.com/STMicroelectronics/meta-st-openstlinux/commit/2dc988821b19d2eb75cfad4d543b674cdadd77bb 2dc988821b19d2eb75cfad4d543b674cdadd77bb] |
||
|- |
|- |
||
− | | oe-manifest || [https://github.com/STMicroelectronics/oe-manifest/commit/ |
+ | | oe-manifest || [https://github.com/STMicroelectronics/oe-manifest/commit/6d8f11172136624905da984a96e0ac29f36decec 6d8f11172136624905da984a96e0ac29f36decec] |
|} |
|} |
||
{| |
{| |