Approved version. Approved on: 15:14, 18 May 2020
Difference between revisions of "STM32MP15 Discovery kits - starting for the first time"
[unchecked revision] | [quality revision] |
m
|
m
|
This article aims to present how to configure and start for the first time a STM32MP157x-DKx Discovery kit that has just been flashed. It is valid for the STM32MP157A-DK1 , STM32MP157D-DK1
, STM32MP157C-DK2
and STM32MP157F-DK2
Discovery kits: the part numbers are specified in the STM32MP15 microprocessor part numbers article.
![]() |
For assistance with starting up the boards, it is recommended to go through the related Starter Package articles: Category:Starter Package |
Now that the image is flashed on the STM32MP157x-DKx Discovery kit, let's finalize the system configuration:
-
Step 1: check the configuration of the switches
- The figure below shows the position of the boot switches in order to boot from the microSD card.
- Step 2: (optional) connect a USB keyboard and/or a USB mouse (not provided) using the USB type A ports (3 and 4)
- Step 3: (optional) connect an Ethernet cable (not provided) to the dedicated connector (7)
- Step 4: check that the microSD card is inserted into the dedicated slot (2)
- Step 5: connect the provided power supply (5 V, 3 A) to the USB type C connector (8)
-
Step 6: (optional) connect the ST-LINK/V2-1 USB micro-B port (5) to a host PC that runs a Terminal program with ST-LINK/V2-1 virtual port (e.g. Minicom on Ubuntu Linux PC or Tera Term on Windows PC)
- install and configure a remote Terminal program onto your host PC
-
Step 7: (optional) connect a HDMI monitor (or TV) to the HDMI connector. This option is particularly useful for the STM32MP157A-DK1
and STM32MP157D-DK1
Discovery kits that do not include any DSI display daughterboard
- Step 8: press the reset button (6) to reset the board
The board boots and the system will be available after few seconds.
<noinclude> This article aims to present how to configure and start for the first time a STM32MP157x-DKx Discovery kit that has just been flashed. It is valid for the STM32MP157A-DK1, STM32MP157D-DK1, STM32MP157C-DK2 and STM32MP157F-DK2 {{Board | type=157A-DK1 | name=short}}, {{Board | type=157D-DK1 | name=short}}, {{Board | type=157C-DK2 | name=short}} and {{Board | type=157F-DK2 | name=short}} Discovery kits: the part numbers are specified in the [[STM32MP15 microprocessor#Part number codification|STM32MP15 microprocessor part numbers]] article. {{Warning|For assistance with starting up the boards, it is recommended to go through the related Starter Package articles: [[:Category:Starter Package]]}}</noinclude> Now that the image is flashed on the STM32MP157x-DKx Discovery kit, let's finalize the system configuration: *<span id{{=}}"step1">'''Step 1'''</span>: check the configuration of the [[STM32MP157x-DKx - hardware description#Boot related switches | switches]] ** The figure below shows the position of the boot switches in order to boot from the microSD card. [[File:STM32MP157x-DKx_boot_switches_microSD_card.png|thumb|center|300px|link=|Boot from microSD card]] *<span id{{=}}"step2">'''Step 2'''</span>: {{highlight|'''(optional)'''}} connect a USB keyboard and/or a USB mouse (not provided) using the USB type A ports ('''3''' and '''4''') *<span id{{=}}"step3">'''Step 3'''</span>: {{highlight|'''(optional)'''}} connect an Ethernet cable (not provided) to the dedicated connector ('''7''') {{:STM32MP157x-DKx - board connections}} <br> *<span id{{=}}"step4">'''Step 4'''</span>: check that the microSD card is inserted into the dedicated slot ('''2''') *<span id{{=}}"step5">'''Step 5'''</span>: connect the provided power supply (5 V, 3 A) to the USB type C connector ('''8''') *<span id{{=}}"step6">'''Step 6'''</span>: {{highlight|'''(optional)'''}} connect the ST-LINK/V2-1 USB micro-B port ('''5''') to a host PC that runs a Terminal program with ST-LINK/V2-1 virtual port (e.g. Minicom on Ubuntu Linux PC or Tera Term on Windows PC) ** install and configure a [[How to get Terminal | remote Terminal program]] onto your host PC *<span id{{=}}"step7">'''Step 7'''</span>: {{highlight|'''(optional)'''}} connect a HDMI monitor (or TV) to the HDMI connector. This option is particularly useful for the '''STM32MP157A-DK1''' and '''STM32MP157D-DK1{{Board | type=157A-DK1 | name=short}}''' and '''{{Board | type=157D-DK1 | name=short}}''' Discovery kits that do not include any DSI display daughterboard [[File: STM32MP157x-DKx_HDMI.png|600px|link=]] *<span id{{=}}"step">'''Step 8'''</span>: press the reset button ('''6''') to reset the board The board boots and the system will be available after few seconds. <noinclude> {{NoIndex}} [[Category:Sub-articles]] {{PublicationRequestId | 8423 | 2018-09-14 | BrunoB}}</noinclude>
Line 1: | Line 1: | ||
<noinclude> |
<noinclude> |
||
− | This article aims to present how to configure and start for the first time a STM32MP157x-DKx Discovery kit that has just been flashed. It is valid for the |
+ | This article aims to present how to configure and start for the first time a STM32MP157x-DKx Discovery kit that has just been flashed. It is valid for the {{Board | type=157A-DK1 | name=short}}, {{Board | type=157D-DK1 | name=short}}, {{Board | type=157C-DK2 | name=short}} and {{Board | type=157F-DK2 | name=short}} Discovery kits: the part numbers are specified in the [[STM32MP15 microprocessor#Part number codification|STM32MP15 microprocessor part numbers]] article. |
{{Warning|For assistance with starting up the boards, it is recommended to go through the related Starter Package articles: [[:Category:Starter Package]]}} |
{{Warning|For assistance with starting up the boards, it is recommended to go through the related Starter Package articles: [[:Category:Starter Package]]}} |
||
</noinclude> |
</noinclude> |
||
Line 22: | Line 22: | ||
** install and configure a [[How to get Terminal | remote Terminal program]] onto your host PC |
** install and configure a [[How to get Terminal | remote Terminal program]] onto your host PC |
||
− | *<span id{{=}}"step7">'''Step 7'''</span>: {{highlight|'''(optional)'''}} connect a HDMI monitor (or TV) to the HDMI connector. This option is particularly useful for the ''' |
+ | *<span id{{=}}"step7">'''Step 7'''</span>: {{highlight|'''(optional)'''}} connect a HDMI monitor (or TV) to the HDMI connector. This option is particularly useful for the '''{{Board | type=157A-DK1 | name=short}}''' and '''{{Board | type=157D-DK1 | name=short}}''' Discovery kits that do not include any DSI display daughterboard |
[[File: STM32MP157x-DKx_HDMI.png|600px|link=]] |
[[File: STM32MP157x-DKx_HDMI.png|600px|link=]] |
||