Difference between revisions of "RTC device tree configuration"
[quality revision] | [quality revision] |
(Created page with "<noinclude> {{ArticleBasedOnModel | Peripheral or framework device tree configuration model}} {{ArticleMainWriter | AmelieD}} {{ArticleApprovedVersion | Jean-ChristopheT |...")
|
m
|
![]() |
Coming soon |
Contents
1 Article purpose[edit]
This article explains how to configure the RTC internal peripheral when it is assigned to the Linux® OS. In this case, it is controlled by the RTC framework.
The configuration is performed using the device tree mechanism that provides a hardware description of the RTC peripheral used by the STM32 RTC Linux driver.
2 DT bindings documentation[edit]
The RTC is represented by the STM32 RTC device tree bindings[1]
3 DT configuration[edit]
This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device tree file split.
STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.
3.1 DT configuration (STM32 level)[edit]
The RTC node is declared in the file stm32mp151.dtsi [2]. It describes the hardware register address, clocks and interrupts.
rtc: rtc@5c004000 { compatible = "st,stm32mp1-rtc"; reg = <0x5c004000 0x400>; --> Register location and length clocks = <&rcc RTCAPB>, <&rcc RTC>; clock-names = "pclk", "rtc_ck"; interrupts-extended = <&intc GIC_SPI 3 IRQ_TYPE_LEVEL_HIGH>, <&exti 19 1>; status = "disabled"; };
![]() |
This device tree part is related to STM32 microprocessors. It should be kept as is, without being modified by the end-user. |
3.2 DT configuration (board level)[edit]
This part is used to enable the RTC used on a board, which is done by setting the status property to okay.
An "st,lsco" property is available to select and enable the RTC output on which RTC low-speed clock is output. The valid ouput values are defined in [3]. A pinctrl state named "default" can be defined to reserve a pin for the RTC output.
3.3 DT configuration examples[edit]
#include <dt-bindings/rtc/rtc-stm32.h>
...
&rtc {
st,lsco = <RTC_OUT2_RMP>;
pinctrl-0 = <&rtc_out2_rmp_pins_a>;
pinctrl-names = "default";
};
4 How to configure the DT using STM32CubeMX[edit]
The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
STM32CubeMX might not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.
5 References[edit]
Please refer to the following links for additional information:
<noinclude> {{ArticleBasedOnModel | [[Peripheral or framework device tree configuration model]]}} {{ArticleMainWriter | AmelieD}} {{ArticleApprovedVersion | Jean-ChristopheT | Nobody | No previous approved version | Automatic approval (article under construction) | 28Jan’19}} [[ == Article purpose == This article explains how to configure the [[RTC internal peripheral|'''RTC''' internal peripheral]] when it is assigned to the Linux<sup>®</sup> OS. In this case, it is controlled by the '''RTC framework'''. The configuration is performed using the [[Device tree|device tree]] mechanism that provides a hardware description of the RTC peripheral used by the STM32 RTC Linux driver. == DT bindings documentation == The [[RTC internal peripheral|'''RTC''']] is represented by the ''STM32 RTC device tree bindings''<ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/rtc/st,stm32-rtc.txt | Device tree bindings}}</ref> == DT configuration == This hardware description is a combination of the '''STM32 microprocessor''' device tree files (''.dtsi'' extension) and '''board''' device tree files (''.dts'' extension). See the [[Device tree]] for an explanation of the device tree file split. '''STM32CubeMX''' can be used to generate the board device tree. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX|How to configure the DT using STM32CubeMX]] for more details. ===DT configuration (STM32 level) === The '''RTC''' node is declared in the file ''stm32mp151.dtsi'' <ref>{{CodeSource|Linux kernel|arch/arm/boot/dts/stm32mp151.dtsi|STM32MP151 device tree}}</ref>. It describes the hardware register address, clocks and interrupts. rtc: rtc@5c004000 { compatible = "st,stm32mp1-rtc"; reg = <0x5c004000 0x400>; {{highlight|--> Register location and length}} clocks = <&rcc RTCAPB>, <&rcc RTC>; clock-names = "pclk", "rtc_ck"; interrupts-extended = <&intc GIC_SPI 3 IRQ_TYPE_LEVEL_HIGH>,<&exti 19 1>; status = "disabled"; }; {{Warning|This device tree part is related to STM32 microprocessors. It should be kept as is, without being modified by the end-user.}} === DT configuration (board level) === This part is used to enable the '''RTC''' used on a board, which is done by setting the '''status''' property to '''okay'''. An "st,lsco" property is available to select and enable the RTC output on which RTC low-speed clock is output. The valid ouput values are defined in <ref>{{CodeSource|Linux kernel|include/dt-bindings/rtc/rtc-stm32.h|STM32 RTC bindings constants}}</ref>. A pinctrl state named "default" can be defined to reserve a pin for the RTC output. === DT configuration examples === #include <dt-bindings/rtc/rtc-stm32.h> ... &rtc { st,lsco = <RTC_OUT2_RMP>; pinctrl-0 = <&rtc_out2_rmp_pins_a>; pinctrl-names = "default"; }; ==How to configure the DT using STM32CubeMX== The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree#STM32|platform configuration device tree]] files.<br /> STM32CubeMX might not support all the properties described in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to [[STM32CubeMX]] user manual for further information. ==References== Please refer to the following links for additional information: <references /> <noinclude> [[Category:Device tree configuration]] [[Category:RTC|1]]</noinclude> {{UnderConstruction}}{{PublicationRequestId | 15043 | 2020-02-21}} {{ArticleBasedOnModel|Peripheral or framework device tree configuration model}}</noinclude>
(9 intermediate revisions by 6 users not shown) | |||
Line 1: | Line 1: | ||
+ | |||
+ | == Article purpose == |
||
+ | This article explains how to configure the [[RTC internal peripheral|'''RTC''' internal peripheral]] when it is assigned to the Linux<sup>®</sup> OS. In this case, it is controlled by the '''RTC framework'''. |
||
+ | |||
+ | The configuration is performed using the [[Device tree|device tree]] mechanism that provides a hardware description of the RTC peripheral used by the STM32 RTC Linux driver. |
||
+ | |||
+ | == DT bindings documentation == |
||
+ | |||
+ | The [[RTC internal peripheral|'''RTC''']] is represented by the ''STM32 RTC device tree bindings''<ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/rtc/st,stm32-rtc.txt | Device tree bindings}}</ref> |
||
+ | |||
+ | == DT configuration == |
||
+ | This hardware description is a combination of the '''STM32 microprocessor''' device tree files (''.dtsi'' extension) and '''board''' device tree files (''.dts'' extension). See the [[Device tree]] for an explanation of the device tree file split. |
||
+ | |||
+ | '''STM32CubeMX''' can be used to generate the board device tree. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX|How to configure the DT using STM32CubeMX]] for more details. |
||
+ | |||
+ | ===DT configuration (STM32 level) === |
||
+ | The '''RTC''' node is declared in the file ''stm32mp151.dtsi'' <ref>{{CodeSource|Linux kernel|arch/arm/boot/dts/stm32mp151.dtsi|STM32MP151 device tree}}</ref>. It describes the hardware register address, clocks and interrupts. |
||
+ | |||
+ | rtc: rtc@5c004000 { |
||
+ | compatible = "st,stm32mp1-rtc"; |
||
+ | reg = <0x5c004000 0x400>; {{highlight|--> Register location and length}} |
||
+ | clocks = <&rcc RTCAPB>, <&rcc RTC>; |
||
+ | clock-names = "pclk", "rtc_ck"; |
||
+ | interrupts-extended = <&intc GIC_SPI 3 IRQ_TYPE_LEVEL_HIGH>, |
||
+ | <&exti 19 1>; |
||
+ | status = "disabled"; |
||
+ | }; |
||
+ | {{Warning|This device tree part is related to STM32 microprocessors. It should be kept as is, without being modified by the end-user.}} |
||
+ | |||
+ | === DT configuration (board level) === |
||
+ | This part is used to enable the '''RTC''' used on a board, which is done by setting the '''status''' property to '''okay'''. |
||
+ | |||
+ | An "st,lsco" property is available to select and enable the RTC output on which RTC low-speed clock is output. The valid ouput values are defined in <ref>{{CodeSource|Linux kernel|include/dt-bindings/rtc/rtc-stm32.h|STM32 RTC bindings constants}}</ref>. A pinctrl state named "default" can be defined to reserve a pin for the RTC output. |
||
+ | |||
+ | === DT configuration examples === |
||
+ | #include <dt-bindings/rtc/rtc-stm32.h> |
||
+ | ... |
||
+ | &rtc { |
||
+ | st,lsco = <RTC_OUT2_RMP>; |
||
+ | pinctrl-0 = <&rtc_out2_rmp_pins_a>; |
||
+ | pinctrl-names = "default"; |
||
+ | }; |
||
+ | |||
+ | ==How to configure the DT using STM32CubeMX== |
||
+ | The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree#STM32|platform configuration device tree]] files.<br /> |
||
+ | STM32CubeMX might not support all the properties described in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to [[STM32CubeMX]] user manual for further information. |
||
+ | |||
+ | ==References== |
||
+ | Please refer to the following links for additional information: |
||
+ | |||
+ | <references /> |
||
+ | |||
<noinclude> |
<noinclude> |
||
− | |||
− | |||
− | |||
[[Category:Device tree configuration]] |
[[Category:Device tree configuration]] |
||
[[Category:RTC|1]] |
[[Category:RTC|1]] |
||
+ | {{PublicationRequestId | 15043 | 2020-02-21}} |
||
+ | {{ArticleBasedOnModel|Peripheral or framework device tree configuration model}} |
||
</noinclude> |
</noinclude> |
||
− |