Difference between revisions of "RNG device tree configuration"
[quality revision] | [quality revision] |
m (→DT configuration (board level))
|
m
|
Contents
1 Article purpose[edit]
This article explains how to configure the RNG internal peripheral when it is assigned to the Linux® OS. In that case, it is controlled by the Hardware random framework.
The configuration is performed using the device tree mechanism that provides a hardware description of the RNG peripheral, used by the STM32 RNG Linux driver.
If the peripheral is assigned to another execution context, refer to How to assign an internal peripheral to a runtime context article for guidelines on peripheral assignment and configuration.
2 DT bindings documentation[edit]
The RNG is represented by the STM32 RNG device tree bindings[1]
3 DT configuration[edit]
This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device tree file split.
STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.
3.1 DT configuration (STM32 level)[edit]
The RNG node is declared in stm32mp157cstm32mp151.dtsi[2]. It describes the hardware register address, clock and reset.
rng1: rng@54003000 { Comments compatible = "st,stm32-rng"; reg = <0x54003000 0x400>; --> Register location and length clocks = <&rccscmi0_clk RNG1CK_K>SCMI0_RNG1>; resets = <&rccscmi0_reset RNG1RST_R>SCMI0_RNG1>; status = "disabled"; };
![]() |
This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user. |
3.2 DT configuration (board level)[edit]
This part is used to enable the RNG used on a board which is done by setting the status property to okay.
A clock-error-detect property is available depending the clock choosen for entropy. It can be enabled to manage the clock detection.
3.3 DT configuration examples[edit]
&rng1 { status = "okay"; clock-error-detect; };
4 How to configure the DT using STM32CubeMX[edit]
The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.
5 References[edit]
Please refer to the following links for additional information:
- ↑ Device tree bindings
- ↑ STM32MP157C STM32MP151 device tree
<noinclude> {{ArticleBasedOnModel|[[Peripheral or framework device tree configuration model]]}} {{ArticleMainWriter | LionelD}} {{ArticleApprovedVersion| LionelD| FabienD(Passed 26Jun'18)| No previous approved version | AlainF - 08Oct'18 - 8900| 29'Oct18}} [[Category:Device tree configuration]] [[Category:Security]]</noinclude> == Article purpose == This article explains how to configure the [[RNG internal peripheral|'''RNG''' internal peripheral]] when it is assigned to the Linux<sup>®</sup> OS. In that case, it is controlled by the [[Hardware random overview|Hardware random framework]]. The configuration is performed using the [[Device tree|device tree]] mechanism that provides a hardware description of the RNG peripheral, used by the STM32 RNG Linux driver. If the peripheral is assigned to another execution context, refer to [[How to assign an internal peripheral to a runtime context]] article for guidelines on peripheral assignment and configuration. == DT bindings documentation == The [[RNG internal peripheral|''RNG'']] is represented by the ''STM32 RNG device tree bindings''<ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/rng/st,stm32-rng.txt | Device tree bindings}}</ref> == DT configuration == This hardware description is a combination of the '''STM32 microprocessor''' device tree files (''.dtsi'' extension) and '''board''' device tree files (''.dts'' extension). See the [[Device tree]] for an explanation of the device tree file split. '''STM32CubeMX''' can be used to generate the board device tree. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX|How to configure the DT using STM32CubeMX]] for more details. ===DT configuration (STM32 level) === The RNG node is declared in stm32mp157cstm32mp151.dtsi<ref>{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp157cstm32mp151.dtsi | STM32MP157CSTM32MP151 device tree}}</ref>. It describes the hardware register address, clock and reset. rng1: rng@54003000 { {{highlight| Comments}} compatible = "st,stm32-rng"; reg = <0x54003000 0x400>; {{highlight|--> Register location and length}} clocks = <&rcc RNG1_K><&scmi0_clk CK_SCMI0_RNG1>; resets = <&rcc RNG1_R><&scmi0_reset RST_SCMI0_RNG1>; status = "disabled"; }; {{Warning|This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user.}} === DT configuration (board level) === This part is used to enable the RNG used on a board which is done by setting the '''status''' property to '''okay'''. A clock-error-detect property is available depending the clock choosen for entropy. It can be enabled to manage the clock detection. === DT configuration examples === &rng1 { status = "okay"; clock-error-detect; }; ==How to configure the DT using STM32CubeMX== The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree#STM32|platform configuration device tree]] files.<br /> The STM32CubeMX may not support all the properties described in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to [[STM32CubeMX]] user manual for further information. ==References== Please refer to the following links for additional information: <references/> <noinclude> {{ArticleBasedOnModel|Peripheral or framework device tree configuration model}} {{PublicationRequestId | 8900 | 2018-10-08 | AlainF}} [[Category:Device tree configuration]] [[Category:Security]]</noinclude>
(3 intermediate revisions by 3 users not shown) | |||
Line 1: | Line 1: | ||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
== Article purpose == |
== Article purpose == |
||
This article explains how to configure the [[RNG internal peripheral|'''RNG''' internal peripheral]] when it is assigned to the Linux<sup>®</sup> OS. In that case, it is controlled by the [[Hardware random overview|Hardware random framework]]. |
This article explains how to configure the [[RNG internal peripheral|'''RNG''' internal peripheral]] when it is assigned to the Linux<sup>®</sup> OS. In that case, it is controlled by the [[Hardware random overview|Hardware random framework]]. |
||
The configuration is performed using the [[Device tree|device tree]] mechanism that provides a hardware description of the RNG peripheral, used by the STM32 RNG Linux driver. |
The configuration is performed using the [[Device tree|device tree]] mechanism that provides a hardware description of the RNG peripheral, used by the STM32 RNG Linux driver. |
||
+ | |||
+ | If the peripheral is assigned to another execution context, refer to [[How to assign an internal peripheral to a runtime context]] article for guidelines on peripheral assignment and configuration. |
||
== DT bindings documentation == |
== DT bindings documentation == |
||
Line 22: | Line 15: | ||
===DT configuration (STM32 level) === |
===DT configuration (STM32 level) === |
||
− | The RNG node is declared in |
+ | The RNG node is declared in stm32mp151.dtsi<ref>{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp151.dtsi | STM32MP151 device tree}}</ref>. It describes the hardware register address, clock and reset. |
rng1: rng@54003000 { {{highlight| Comments}} |
rng1: rng@54003000 { {{highlight| Comments}} |
||
compatible = "st,stm32-rng"; |
compatible = "st,stm32-rng"; |
||
reg = <0x54003000 0x400>; {{highlight|--> Register location and length}} |
reg = <0x54003000 0x400>; {{highlight|--> Register location and length}} |
||
− | clocks = <& |
+ | clocks = <&scmi0_clk CK_SCMI0_RNG1>; |
− | resets = <& |
+ | resets = <&scmi0_reset RST_SCMI0_RNG1>; |
status = "disabled"; |
status = "disabled"; |
||
}; |
}; |
||
Line 52: | Line 45: | ||
<references/> |
<references/> |
||
+ | |||
+ | <noinclude> |
||
+ | {{ArticleBasedOnModel|Peripheral or framework device tree configuration model}} |
||
+ | {{PublicationRequestId | 8900 | 2018-10-08 | AlainF}} |
||
+ | [[Category:Device tree configuration]] |
||
+ | [[Category:Security]] |
||
+ | </noinclude> |