Last edited 3 years ago

PWM overview

The printable version is no longer supported and may have rendering errors. Please update your browser bookmarks and please use the default browser print function instead.

This article gives information about the Linux® PWM framework.
It explains how to activate the PWM interface and, based on examples, how to use it.

1 Framework purpose[edit source]

PWM (Pulse Width Modulation) framework offers a unified interface for the users to:

  • control PWM output(s) such as period, duty cycle and polarity.
  • capture a PWM signal and report its period and duty cycle (e.g. input).

The interface can be used from:

  • user space (sysfs)
  • kernel space (API)

PWMs can be used in various use cases, as mentioned in How to use the framework to control LEDs, beepers, vibrators or fans...

2 System overview[edit source]

PWM sysfs interfacePWM kernel interfaceSTM32 TIM Linux driverSTM32 LPTIM Linux driverSTM32 TIM internal peripheralSTM32 LPTIM internal peripheral
PWM Implementation architecture

2.1 Component description[edit source]

  • PWM user (User space)

The user can use PWM sysfs interface, from a user terminal or a custom application, to control PWM device(s) from user space.

  • PWM user (Kernel space)

User drivers can use PWM API to control PWM external device(s) from kernel space (such as back-light, vibrator, LED or fan drivers).

  • PWM framework (Kernel space)

The PWM core provides sysfs interface and PWM API. They can be used to implement PWM user and PWM controller drivers.

  • PWM drivers (Kernel space)

Provider drivers such as STM32 TIM Linux driver and STM32 LPTIM Linux driver that expose PWM controller(s) to the core.

  • PWM hardware

PWM controller(s) such as TIM internal peripheral[1] and LPTIM internal peripheral[2] used to drive external PWM controlled devices.

2.2 API description[edit source]

Documentation on PWM interface can be found under kernel Documentation/driver-api/pwm.rst[3]

2.2.1 Kernel PWM API[edit source]

The main useful user API are the following:

  • devm_pwm_get() or pwm_get() / pwm_put(): this API is used to look up, request, then free a PWM device.
  • pwm_init_state(), pwm_get_state(), pwm_apply_state(): this API is used to initialize, retrieve and apply the current PWM device state.
  • pwm_config(): this API updates the PWM device configuration (period and duty cycle).
  • ...

2.2.2 Sysfs interface[edit source]

In addition to Documentation/driver-api/pwm.rst[3], details on ABI are available in Documentation/ABI/testing/sysfs-class-pwm[4].

3 Configuration[edit source]

3.1 Kernel configuration[edit source]

Activate PWM framework in the kernel configuration through the Linux menuconfig tool, Menuconfig or how to configure kernel (CONFIG_PWM=y):

Device Drivers  --->
   [*] Pulse-Width Modulation (PWM) Support  --->

Activate PWM drivers for STM32 PWM drivers: STM32 TIM Linux driver and/or STM32 LPTIM Linux driver

3.2 Device tree configuration[edit source]

  • PWM generic DT bindings:

PWM DT bindings documentation[5] describes device tree properties related to standard PWM user nodes and PWM controller nodes.

  • Detailed DT configuration for STM32 internal peripherals:

TIM device tree configuration and/or LPTIM device tree configuration

4 How to use the framework[edit source]

PWM can be used either from the user or the kernel space.

4.1 How to use PWM with sysfs interface[edit source]

The available PWM controllers are listed in sysfs:

 ls /sys/class/pwm
pwmchip0

The number of channels per controller can be read in npwm (read-only)

 cd /sys/class/pwm/pwmchip0
 cat npwm
4

Each channel is exported (requested for sysfs activation) by writing the corresponding number in 'export'.

Info white.png Information
TIMx_CH1 is exported as "pwm0", TIMx_CH2 as "pwm1", and so on:
  • PWM channels are numbered from 0 to 'npwm' - 1
  • TIM[1] channels are numbered from 1 to 'npwm'.

As an example, proceed as follows to export the first channel (TIMx_CH1, e.g. channel 0):

 echo 0 > export
 ls
device  export  npwm  power  pwm0  subsystem  uevent  unexport

The period and duty cycle must be configured before enabling any channel.

As an example, proceed as follows to set a period of 100 ms with a duty cycle of 60% on channel 0:

 echo 100000000 > pwm0/period
 echo 60000000 > pwm0/duty_cycle
 echo 1 > pwm0/enable

The polarity can be inverted or set to normal by using the polarity entry:

 echo "inversed" > pwm0/polarity
 cat pwm0/polarity
inversed

 echo "normal" > pwm0/polarity
 cat pwm0/polarity
normal

4.2 How to use PWM capture with sysfs interface[edit source]

PWM capture is available on some PWM controllers such as TIM internal peripheral[1] (see TIM configured in PWM input capture mode ).

Info white.png Information
PWM output and capture mode are mutually exclusive on a TIM instance
# First export a channel (e.g. 0), then capture PWM input on it:
 cd /sys/class/pwm/pwmchip0
 echo 0 > export

 cd pwm0
 ls
capture  duty_cycle  enable  period  polarity  power  uevent

 cat capture
10000 1002               # capture result is in nano-seconds, e.g.: 100KHz, 10% duty cycle

4.3 Example of PWM usage with kernel PWM API[edit source]

Several in-kernel drivers use kernel PWM API. Below a few examples:

5 How to trace and debug the framework[edit source]

5.1 How to monitor with debugfs[edit source]

PWM usage can be monitored from debugfs 'pwm' entry. For example:

 cd /sys/kernel/debug/
 cat pwm
platform/44000000.timer:pwm, 4 PWM devices                                                               <-- One timer instance exposes 4 PWM channels.
 pwm-0   (sysfs               ): requested enabled period: 1000000 ns duty: 500000 ns polarity: normal   <-- Channel 0 has been exported, enabled and configured via sysfs
 pwm-1   ((null)              ): period: 0 ns duty: 0 ns polarity: normal
 pwm-2   ((null)              ): period: 0 ns duty: 0 ns polarity: normal                                <-- Other channels aren't used currently
 pwm-3   ((null)              ): period: 0 ns duty: 0 ns polarity: normal

5.2 Troubleshooting PWM capture[edit source]

Here are some clues on how to debug possible errors in PWM capture mode.
See How to use PWM capture with sysfs interface as a pre-requisite.

 cat capture 
cat: capture: Connection timed out

This may be due to:

  • the input signal isn't recognized as a PWM input (or there's no input signal to capture).
  • a wrong alternate function number is used for the input pin configuration in the device-tree.
    See "TIM configured in PWM input capture mode" for further details.
 cat capture 
cat: capture: Device or resource busy

This may be due to:

  • a PWM channel on the same TIM instance is already running (in capture or output mode)
 cat capture 
cat: capture: No such device

This may be due to:

 cat capture
cat: capture: Function not implemented

This may be due to:

  • a wrong TIM instance is being used (e.g. "/sys/class/pwm/pwmchip/pwmchipN"), and it doesn't support capture (like LPTIM)
  • the DMA support isn't enabled (CONFIG_DMA_ENGINE)

6 References[edit source]

  1. 1.0 1.1 1.2 TIM internal peripheral
  2. LPTIM internal peripheral
  3. 3.0 3.1 Documentation/driver-api/pwm.rst , Pulse Width Modulation interface
  4. Documentation/ABI/testing/sysfs-class-pwm , Pulse Width Modulation ABI
  5. Documentation/devicetree/bindings/pwm/pwm.txt , PWM DT bindings documentation
  6. drivers/input/misc/pwm-beeper.c , Example to use kernel PWM API
  7. drivers/input/misc/pwm-vibra.c , Example to use kernel PWM API