- Last edited 4 years ago ago
Linux Mailbox framework overview
Template:ArticleMainWriter
Template:ArticleApprovedVersion
SUMMARY
This article gives information about the Linux® mailbox framework. The mailbox framework is involved in interprocessor communication in heterogeneous multicore systems.
Contents
1 Framework purpose[edit]
The mailbox is used in interprocessor communication to exchange messages or signals between the host and the coprocessor cores. The mailbox framework is based on:
- A mailbox controller that is platform dependent:
- It is in charge of configuring and handling IRQ from the IPCC peripheral.
- It provides a generic API to the mailbox client.
- A mailbox client that is in charge of the message to send or receive.
A general presentation of the mailbox framework is available in the Linux mailbox documentation [1].
2 System overview[edit]
2.1 Component description[edit]
- Mailbox controller
- The mailbox controller is the stm32_ipcc. It configures and controls the IPCC peripheral
- Mailbox client
- The user can define his own mailbox client.
- For example, the RPMsg framework uses mailbox for the interprocessor communication.
- In this case the mailbox client is the remoteproc driver that forwards services from/to the RPMsg framework.
2.2 API description[edit]
The APIs are described in the Linux documentation:
3 Configuration[edit]
Activate stm32 IPCC mailbox in kernel configuration using the Linux Menuconfig tool: Menuconfig or how to configure kernel
Device drivers --->
-*- Mailbox Hardware Support --->
<*> STM32 IPCC Mailbox
4 Device tree configuration[edit]
The mailbox device node must be declared and enabled in the Linux kernel device tree. Here is an extract of the STM32MP1 evaluation board device tree:
ipcc: mailbox@4c001000 { compatible = "st,stm32-ipcc"; #mbox-cells = <1>; reg = <0x4c001000 0x400>; interrupts-extended = <&intc GIC_SPI 100 IRQ_TYPE_NONE>, <&intc GIC_SPI 101 IRQ_TYPE_NONE>, <&exti 62 1>; interrupt-names = "rx", "tx", "wakeup"; clocks = <&rcc_clk IPCC>; wakeup-source; Status = "Okay"; };
Then client has to reserve channels. Here is an example of channel allocation for the remoteproc node:
&m4_rproc { memory-region = <&ipc_share>; mboxes = <&ipcc 0>, <&ipcc 1>, <&ipcc 2>; mbox-names = "vq0", "vq1", "init_shdn"; status = "okay"; };
5 How to trace and debug the framework[edit]
5.1 How to trace[edit]
Dynamic debug traces can be added using the following commands:
echo -n 'file stm32-ipcc.c +p' > /sys/kernel/debug/dynamic_debug/control echo -n 'file mailbox.c +p' > /sys/kernel/debug/dynamic_debug/control