Difference between revisions of "How to use the kernel dynamic debug"
[quality revision] | [quality revision] |
m
|
m
|
Contents
1 Introduction[edit]
As prerequisite to reading this article, please refer to the Dmesg and Linux kernel log page.
"Dynamic debug is designed to allow you to dynamically enable/disable kernel code to obtain additional kernel information. Currently, if CONFIG_DYNAMIC_DEBUG is set, all pr_debug()/dev_dbg() calls can be dynamically enabled per-callsite." extracted from the Linux kernel documentation[1].
The related debugfs entry is usually:
/sys/kernel/debug/dynamic_debug/control
Note that the verbose dev_vdbg() calls cannot be dynamically activated.
When the dynamic debug traces are activated, the trace results are printed in dmesg (or /proc/kmsg), and in the console if console loglevel is set to 8.
2 More technical information[edit]
The dynamic debug trace configuration is done through a control file in the debugfs filesystem: <debugfs>/dynamic_debug/control
The command includes keywords and flag elements (for details see the Linux kernel documentation[1]).
- Keywords
Possible keywords are:
func : function name file : source filename module : module name format : format string line : line number (including ranges of line numbers)
- The colored keywords above are illustrated by examples in the next chapter.
- Flags
The flag specification comprises a change operation followed by one or more flag characters. The change operation is one of the characters:
- : remove the given flags + : add the given flags = : set the flags to the given flags
Possible flags are:
f : Include the function name in the printed message l : Include line number in the printed message m : Include module name in the printed message p : Causes a printk() message to be emitted to dmesg t : Include thread ID in messages not generated from interrupt context
3 Examples[edit]
- Track all dev_*dbg/pr_debug() in a file (you can add several files if necessary):
mount -t debugfs none /sys/kernel/debug
echo "file stm32-adc.c +p" > /sys/kernel/debug/dynamic_debug/control
Note that just the file name or full file path can be given, here stm32-adc.c or drivers/iio/adc/stm32-adc.c
- Track only one line with dev_dbg() in a file (you can add several files and several lines if necessary, please use the last line number of the function call):
echo "file stm32-adc.c line 1438 +p" > /sys/kernel/debug/dynamic_debug/control
- For an entire "module (module means ~.ko, so not applicable for a statically linked driver)":
echo "module cfg80211 +p" > /sys/kernel/debug/dynamic_debug/control
- If you want to list all available traces (warning: it is a long file so you may need to use "tee" or another solution to save it):
cat /sys/kernel/debug/dynamic_debug/control | tee /tmp/dynamic_log.log
- For instance, if you are looking for a particular file to find a particular line:
cat /sys/kernel/debug/dynamic_debug/control | grep adc drivers/iio/adc/stm32-adc.c:1515 [stm32_adc]stm32_adc_conf_scan_seq =p "%s chan %d to %s%d\012" drivers/iio/adc/stm32-adc.c:1438 [stm32_adc]stm32_adc_awd_set =p "%s chan%d htr:%d ltr:%d\012" drivers/iio/adc/stm32-adc.c:2182 [stm32_adc]stm32_adc_dma_start =p "%s size=%d watermark=%d\012" drivers/iio/adc/stm32-adc.c:2304 [stm32_adc]stm32_adc_trigger_handler =p "%s bufi=%d\012" drivers/iio/adc/stm32-adc.c:2443 [stm32_adc]stm32_adc_chan_of_init =p "Configured to use injected\012" drivers/iio/adc/stm32-adc.c:2364 [stm32_adc]stm32_adc_of_get_resolution =p "Using %u bits resolution\012"
- Multiple commands can be written together, separated by ';' or '\n'.
echo "file stm32-adc.c +p; file stm32-adc-core.c +p" > /sys/kernel/debug/dynamic_debug/control
- A another method is to use a wildcard. The match rule supports * (matches zero or more characters) and ? (matches exactly one character). For example, you can match all USB drivers:
echo "file drivers/usb/* +p" > /sys/kernel/debug/dynamic_debug/control
4 Synchronous tracing on the console[edit]
In the case of a crash, or impossibility to call dmesg, it is sometimes useful to have traces synchronously emitted on the console.
Only error, warning and informational traces are emitted synchronously on the console (that is, loglevel=5), so if you need to see the lower level traces too, you need to change the console loglevel to "8".
<enable the conditional traces> echo 8 > /proc/sys/kernel/printk or dmesg -n 8 or dmesg -n debug
Please follow this article to get a serial console for the target: How to get Terminal
5 Debug messages during boot process[edit]
In order to activate debug messages during the boot process, even before userspace and debugfs exist, use the kernel's command-line parameter: dyndbg
For instance, the kernel bootargs can be modified in the following ways:
- Mount a boot partition from the Linux kernel console, and then update the extlinux.conf file using the vi editor (see man page[2], or introduction page[3] ). For example:
mount /dev/mmcblk0p4 /boot vi /boot/mmc0_stm32mp157c-ev1_extlinux/extlinux.conf
or
- Edit the extlinux.conf file by using UMS (USB Mass Storage): see How to use USB mass storage in U-Boot for details.
To mount partitions (mmc 0:microSD card / mmc 1: eMMC):
- - Press any key to stop at U-Boot execution when booting the board.
... Hit any key to stop autoboot: 0 STM32MP>
- - Then
STM32MP> ums 0 mmc 0
- - Check for the boot partition mounted on your host PC (/media/$USER/bootfs)
- - Edit the extlinux file corresponding to your setup (/media/$USER/bootfs/mmc0_stm32mp157cextlinux/stm32mp157f-ev2dk2_extlinux/extlinux.conf
- Update the kernel command line, adding the dyndbg parameter:
root=/dev/mmcblk0p5PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=ttyS3ttySTM0,115200 dyndbg="file drivers/usb/core/hub.c +p"
Save and quit file update, and then reboot the board.
Note: to display these debug messages in the console, in addition to the dmesg, add loglevel=8 in the kernel command line.
- Reboot the board and check for a kernel command-line, and that debug messages are present in the dmesg output
6 References[edit]
- Useful external links
Document link | Document Type | Description |
---|---|---|
The dynamic debugging interface (lwn.net) | User guide | http://lwn.net |
Documentation/dynamic-debug-howto.txt (lwn.txt) | User guide | http://lwn.net |
Dynamic debug howto (kernel.org) | Standard | http://www.kernel.org |
== Introduction == As prerequisite to reading this article, please refer to the [[Dmesg and Linux kernel log]] page. "Dynamic debug is designed to allow you to dynamically enable/disable kernel code to obtain additional kernel information. Currently, if '''CONFIG_DYNAMIC_DEBUG''' is set, all {{Highlight|'''pr_debug()/dev_dbg()'''}} calls can be dynamically enabled per-callsite." extracted from the Linux kernel documentation<ref name="dynamic-debug-howto.rst">{{CodeSource | Linux kernel | Documentation/admin-guide/dynamic-debug-howto.rst}}</ref>. The related debugfs entry is usually: /sys/kernel/debug/{{highlight|dynamic_debug/control}} Note that the verbose '''{{Highlight|dev_vdbg()}}''' calls cannot be dynamically activated. When the dynamic debug traces are activated, the trace results are printed in '''dmesg (or /proc/kmsg)''', and in the console if console loglevel is set to 8. == More technical information == The dynamic debug trace configuration is done through a '''control''' file in the '''debugfs''' filesystem: ''{{HighlightParam|<debugfs>}}{{highlight|/dynamic_debug/control}}'' The command includes keywords and flag elements (for details see the Linux kernel documentation<ref name="dynamic-debug-howto.rst"/>). *Keywords Possible keywords are: '''func''' '': function name''<span style="color: green;">{{Green|'''file'''</span>}} '': source filename''<span style="color: blue;">{{STDarkBlue|'''module'''</span>}} '': module name'' '''format''' '': format string''<span style="color: orange;">{{Orange|'''line'''</span>}} '': line number (including ranges of line numbers)'' :The colored keywords above are illustrated by examples in the next chapter. *Flags The flag specification comprises a change operation followed by one or more flag characters. The change operation is one of the characters: - '': remove the given flags'' '''+''' '': add the given flags'' = '': set the flags to the given flags'' Possible flags are: f '': Include the function name in the printed message'' l '': Include line number in the printed message'' m '': Include module name in the printed message'' '''p''' '': Causes a printk() message to be emitted to dmesg'' t '': Include thread ID in messages not generated from interrupt context'' ==Examples== * Track all dev_*dbg/pr_debug() in a <span style="color: green;">{{Green|'''file'''</span>}} (you can add several files if necessary): {{Board$}} mount -t debugfs none /sys/kernel/debug {{Board$}} echo "<span style="color: green;">{{Green|'''file'''</span>}} stm32-adc.c '''+p'''" > /sys/kernel/debug/dynamic_debug/control Note that just the file name or full file path can be given, here ''stm32-adc.c'' or ''drivers/iio/adc/stm32-adc.c'' * Track only one <span style="color: orange;">{{Orange|'''line'''</span>}} with dev_dbg() in a <span style="color: green;">{{Green|'''file'''</span>}} (you can add several files and several lines if necessary, please use the last line number of the function call): {{Board$}} echo "<span style="color: green;">{{Green|'''file'''</span>}} stm32-adc.c <span style="color: orange;">{{Orange|'''line'''</span>}} 1438 '''+p'''" > /sys/kernel/debug/dynamic_debug/control * For an entire "<span style="color: blue;">{{STDarkBlue|'''module'''</span>}} (module means ~.ko, so not applicable for a statically linked driver)": {{Board$}} echo "<span style="color: blue;">{{STDarkBlue|'''module'''</span>}} cfg80211 '''+p'''" > /sys/kernel/debug/dynamic_debug/control * If you want to list all available traces {{Grey|''(warning: it is a long file so you may need to use "tee" or another solution to save it)''}}: {{Board$}} cat /sys/kernel/debug/dynamic_debug/control {{Grey|''| tee /tmp/dynamic_log.log''}} * For instance, if you are looking for a particular <span style="color: green;">{{Green|'''file'''</span>}} to find a particular <span style="color: orange;">{{Orange|'''line'''</span>}}: {{Board$}} cat /sys/kernel/debug/dynamic_debug/control | grep adc<span style="color: green;">{{Green|drivers/iio/adc/stm32-adc.c</span>:<span style="color: orange;">1515</span>}}:{{Orange|1515}} [stm32_adc]stm32_adc_conf_scan_seq =p "%s chan %d to %s%d\012"<span style="color: green;">{{Green|drivers/iio/adc/stm32-adc.c</span>:<span style="color: orange;">1438</span>}}:{{Orange|1438}} [stm32_adc]stm32_adc_awd_set =p "%s chan%d htr:%d ltr:%d\012"<span style="color: green;">{{Green|drivers/iio/adc/stm32-adc.c</span>:<span style="color: orange;">2182</span>}}:{{Orange|2182}} [stm32_adc]stm32_adc_dma_start =p "%s size=%d watermark=%d\012"<span style="color: green;">{{Green|drivers/iio/adc/stm32-adc.c</span>:<span style="color: orange;">2304</span>}}:{{Orange|2304}} [stm32_adc]stm32_adc_trigger_handler =p "%s bufi=%d\012"<span style="color: green;">{{Green|drivers/iio/adc/stm32-adc.c</span>:<span style="color: orange;">2443</span>}}:{{Orange|2443}} [stm32_adc]stm32_adc_chan_of_init =p "Configured to use injected\012"<span style="color: green;">{{Green|drivers/iio/adc/stm32-adc.c</span>:<span style="color: orange;">2364</span>}}:{{Orange|2364}} [stm32_adc]stm32_adc_of_get_resolution =p "Using %u bits resolution\012" * Multiple commands can be written together, separated by ';' or '\n'. {{Board$}} echo "<span style="color: green;">{{Green|'''file'''</span>}} stm32-adc.c '''+p'''; <span style="color: green;">{{Green|'''file'''</span>}} stm32-adc-core.c '''+p'''" > /sys/kernel/debug/dynamic_debug/control * A another method is to use a wildcard. The match rule supports * (matches zero or more characters) and ? (matches exactly one character). For example, you can match all USB drivers: {{Board$}} echo "<span style="color: green;">{{Green|'''file'''</span>}} drivers/usb/* '''+p'''" > /sys/kernel/debug/dynamic_debug/control == Synchronous tracing on the console == In the case of a crash, or impossibility to call dmesg, it is sometimes useful to have traces synchronously emitted on the console.<br> Only error, warning and informational traces are emitted synchronously on the console (that is, loglevel=5), so if you need to see the lower level traces too, you need to change the console loglevel to "8". <enable the conditional traces> {{Board$}} echo 8 > /proc/sys/kernel/printk or {{Board$}} dmesg -n 8 or {{Board$}} dmesg -n debug Please follow this article to get a serial console for the target: [[How to get Terminal]] {{Warning |As all traces are now synchronously emitted, real-time is affected<br/> If you want to return to the default console log level, you have to get this default value from the procfs entry ''/proc/sys/kernel/printk'':<br/> {{Board$}} cat /proc/sys/kernel/printk 8 4 1 {{highlight|'''7'''}} {{Board$}} dmesg -n {{highlight|'''7'''}} {{Board$}} cat /proc/sys/kernel/printk {{highlight|'''7'''}} 4 1 7 }} ==Debug messages during boot process== In order to activate debug messages during the boot process, even before userspace and debugfs exist, use the kernel's command-line parameter: {{Highlight|'''dyndbg'''}} For instance, the kernel ''bootargs'' can be modified in the following ways:<br> * Mount a boot partition from the Linux kernel console, and then update the extlinux.conf file using the vi editor (see man page<ref>http://ex-vi.sourceforge.net/vi.html</ref>, or introduction page<ref>http://ex-vi.sourceforge.net/viin/paper.html</ref> ). For example: {{Board$}} mount /dev/mmcblk0p4 /boot {{Board$}} vi /boot/mmc0_stm32mp157c-ev1_extlinux/extlinux.conf or * Edit the extlinux.conf file by using UMS (USB Mass Storage): see [[How to use USB mass storage in U-Boot]] for details. To mount partitions (mmc 0:microSD card / mmc 1: eMMC): :- Press any key to stop at U-Boot execution when booting the board. {{Board$}} ... {{Board$}} Hit any key to stop autoboot: 0 {{Board$}} STM32MP> :- Then STM32MP> ums 0 mmc 0 :- Check for the boot partition mounted on your host PC (/media/''$USER''/bootfs)<br> :- Edit the extlinux file corresponding to your setup (/media/''$USER''/bootfs/mmc0_stm32mp157c-ev2extlinux/stm32mp157f-dk2_extlinux/extlinux.conf<br> * Update the kernel command line, adding the dyndbg parameter: root=/dev/mmcblk0p5 rootwait rw console=ttyS3,115200 '''dyndbg="<span style="color: green;">file</span>PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=ttySTM0,115200 '''dyndbg="{{Green|file}} drivers/usb/core/hub.c +p"''' Save and quit file update, and then reboot the board. '''Note''': to display these debug messages in the console, in addition to the dmesg, add '''loglevel=8''' in the kernel command line. * Reboot the board and check for a kernel command-line, and that debug messages are present in the dmesg output<br> == References ==<references /> * Useful external links {| ! scope=col | Document link ! scope=col | Document Type ! scope=col | Description |- | [http://lwn.net/Articles/434833/ The dynamic debugging interface (lwn.net)] | User guide | http://lwn.net |- | [http://lwn.net/Articles/434856/ Documentation/dynamic-debug-howto.txt (lwn.txt)] | User guide | http://lwn.net |- | [https://www.kernel.org/doc/html/latest/{{DocSource | domain=Linux kernel | path=admin-guide/dynamic-debug-howto.html | text=Dynamic debug howto (kernel.org)]}} | Standard | http://www.kernel.org |} <noinclude> {{PublicationRequestId | 9237 | 2018-11-05 | PhilipS}} [[Category:How to trace and debug]]</noinclude>
(5 intermediate revisions by 2 users not shown) | |||
Line 19: | Line 19: | ||
Possible keywords are: |
Possible keywords are: |
||
'''func''' '': function name'' |
'''func''' '': function name'' |
||
− | + | {{Green|'''file'''}} '': source filename'' |
|
− | + | {{STDarkBlue|'''module'''}} '': module name'' |
|
'''format''' '': format string'' |
'''format''' '': format string'' |
||
− | + | {{Orange|'''line'''}} '': line number (including ranges of line numbers)'' |
|
:The colored keywords above are illustrated by examples in the next chapter. |
:The colored keywords above are illustrated by examples in the next chapter. |
||
Line 39: | Line 39: | ||
==Examples== |
==Examples== |
||
− | * Track all dev_*dbg/pr_debug() in a |
+ | * Track all dev_*dbg/pr_debug() in a {{Green|'''file'''}} (you can add several files if necessary): |
{{Board$}} mount -t debugfs none /sys/kernel/debug |
{{Board$}} mount -t debugfs none /sys/kernel/debug |
||
− | {{Board$}} echo " |
+ | {{Board$}} echo "{{Green|'''file'''}} stm32-adc.c '''+p'''" > /sys/kernel/debug/dynamic_debug/control |
Note that just the file name or full file path can be given, here ''stm32-adc.c'' or ''drivers/iio/adc/stm32-adc.c'' |
Note that just the file name or full file path can be given, here ''stm32-adc.c'' or ''drivers/iio/adc/stm32-adc.c'' |
||
− | * Track only one |
+ | * Track only one {{Orange|'''line'''}} with dev_dbg() in a {{Green|'''file'''}} (you can add several files and several lines if necessary, please use the last line number of the function call): |
− | {{Board$}} echo " |
+ | {{Board$}} echo "{{Green|'''file'''}} stm32-adc.c {{Orange|'''line'''}} 1438 '''+p'''" > /sys/kernel/debug/dynamic_debug/control |
− | * For an entire " |
+ | * For an entire "{{STDarkBlue|'''module'''}} (module means ~.ko, so not applicable for a statically linked driver)": |
− | {{Board$}} echo " |
+ | {{Board$}} echo "{{STDarkBlue|'''module'''}} cfg80211 '''+p'''" > /sys/kernel/debug/dynamic_debug/control |
* If you want to list all available traces {{Grey|''(warning: it is a long file so you may need to use "tee" or another solution to save it)''}}: |
* If you want to list all available traces {{Grey|''(warning: it is a long file so you may need to use "tee" or another solution to save it)''}}: |
||
{{Board$}} cat /sys/kernel/debug/dynamic_debug/control {{Grey|''| tee /tmp/dynamic_log.log''}} |
{{Board$}} cat /sys/kernel/debug/dynamic_debug/control {{Grey|''| tee /tmp/dynamic_log.log''}} |
||
− | * For instance, if you are looking for a particular |
+ | * For instance, if you are looking for a particular {{Green|'''file'''}} to find a particular {{Orange|'''line'''}}: |
{{Board$}} cat /sys/kernel/debug/dynamic_debug/control | grep adc |
{{Board$}} cat /sys/kernel/debug/dynamic_debug/control | grep adc |
||
− | + | {{Green|drivers/iio/adc/stm32-adc.c}}:{{Orange|1515}} [stm32_adc]stm32_adc_conf_scan_seq =p "%s chan %d to %s%d\012" |
|
− | + | {{Green|drivers/iio/adc/stm32-adc.c}}:{{Orange|1438}} [stm32_adc]stm32_adc_awd_set =p "%s chan%d htr:%d ltr:%d\012" |
|
− | + | {{Green|drivers/iio/adc/stm32-adc.c}}:{{Orange|2182}} [stm32_adc]stm32_adc_dma_start =p "%s size=%d watermark=%d\012" |
|
− | + | {{Green|drivers/iio/adc/stm32-adc.c}}:{{Orange|2304}} [stm32_adc]stm32_adc_trigger_handler =p "%s bufi=%d\012" |
|
− | + | {{Green|drivers/iio/adc/stm32-adc.c}}:{{Orange|2443}} [stm32_adc]stm32_adc_chan_of_init =p "Configured to use injected\012" |
|
− | + | {{Green|drivers/iio/adc/stm32-adc.c}}:{{Orange|2364}} [stm32_adc]stm32_adc_of_get_resolution =p "Using %u bits resolution\012" |
|
* Multiple commands can be written together, separated by ';' or '\n'. |
* Multiple commands can be written together, separated by ';' or '\n'. |
||
− | {{Board$}} echo " |
+ | {{Board$}} echo "{{Green|'''file'''}} stm32-adc.c '''+p'''; {{Green|'''file'''}} stm32-adc-core.c '''+p'''" > /sys/kernel/debug/dynamic_debug/control |
* A another method is to use a wildcard. The match rule supports * (matches zero or more characters) and ? (matches exactly one character). For example, you can match all USB drivers: |
* A another method is to use a wildcard. The match rule supports * (matches zero or more characters) and ? (matches exactly one character). For example, you can match all USB drivers: |
||
− | {{Board$}} echo " |
+ | {{Board$}} echo "{{Green|'''file'''}} drivers/usb/* '''+p'''" > /sys/kernel/debug/dynamic_debug/control |
== Synchronous tracing on the console == |
== Synchronous tracing on the console == |
||
Line 110: | Line 110: | ||
:- Check for the boot partition mounted on your host PC (/media/''$USER''/bootfs)<br> |
:- Check for the boot partition mounted on your host PC (/media/''$USER''/bootfs)<br> |
||
− | :- Edit the extlinux file corresponding to your setup (/media/''$USER''/bootfs/ |
+ | :- Edit the extlinux file corresponding to your setup (/media/''$USER''/bootfs/mmc0_extlinux/stm32mp157f-dk2_extlinux.conf<br> |
* Update the kernel command line, adding the dyndbg parameter: |
* Update the kernel command line, adding the dyndbg parameter: |
||
− | root= |
+ | root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw console=ttySTM0,115200 '''dyndbg="{{Green|file}} drivers/usb/core/hub.c +p"''' |
Save and quit file update, and then reboot the board. |
Save and quit file update, and then reboot the board. |
||
Line 138: | Line 138: | ||
| http://lwn.net |
| http://lwn.net |
||
|- |
|- |
||
− | | |
+ | | {{DocSource | domain=Linux kernel | path=admin-guide/dynamic-debug-howto.html | text=Dynamic debug howto (kernel.org)}}
|
| Standard |
| Standard |
||
| http://www.kernel.org |
| http://www.kernel.org |