- Last edited 3 years ago ago
How to use coprocessor service for Android
This article explains how to use the CoproService which is a SystemService embedded in the Android framework, allowing to use a serial connection to communicate with the Arm® Cortex®-M processor embedded in a compatible hardware board.
See STM32MPU Embedded Software for Android architecture overview to get more information on compatible hardware boards.
Contents
1 Prerequisites[edit]
The environment must be installed using the Developer Package adapted to your selected microprocessor device. See the list of Android Developer Package.
The firmware built for the Arm® Cortex®-M processor has to use RemoteProc and RPMSG, and has to instantiate a /dev/ttyRPMSG
unit during its initialization.
2 CoproService[edit]
CoproService is composed of two parts: Firmware management and TTY management.
2.1 Firmware management[edit]
The Arm® Cortex®-M processor can be used to offload real time algorithms (such as MotorControl), support connectivity mediums (like LORA), etc.
The users develop their firmwares thanks to the STM32CubeMX and SW4STM32 tools.
The firmware is embedded in the Android vendor partition in the /vendor/firmware/copro/
directory.
The CoproService looks at the contents of /vendor/firmware/copro/
to get the list of available firmwares. It then loads the requested firmware at the user's/application's request.
2.2 TTY management[edit]
When the firmware is loaded and running, a /dev/ttyRPMSG0
driver is available to communicate with the Arm® Cortex®-M processor.
It is up to the users to define and write their own protocol on top of ttyRPMSG0
.
Application is then able to:
- open
ttyRPMSG0
- write to
ttyRPMSG0
- read from
ttyRPMSG0
- close
ttyRPMSG0
3 API[edit]
3.1 CoproManager API[edit]
The CoproManager API gives access to the Firmware management.
CoproManager getInstance()
: Gets the instance of the availableCoproManager
to start using it.FirmwareInfo[] getFirmwareList()
: Returns the list of available firmwares present in/vendor/firmware/copro/
FirmwareInfo getFirmwareByName(String name)
: Looks up a firmware by its name in the/vendor/firmware/copro/
folder and returns all useful information about it, otherwise returnsnull
.boolean isFirmwareRunning(int id)
: Returnstrue
if the firmware of identifierid
is running, otherwise returnsfalse
.void startFirmware(int id)
: Starts the firmware defined by its identifierid
.void stopFirmware()
: Stops any running firmwareCoproSerialPort getSerialPort()
: Gets access toCoproSerialPort
to interact with the firmware. See below for more info.
3.2 FirmwareInfo API[edit]
The FirmwareInfo API gives information about firmwares.
int getId()
: get the ID given by the CoproService to this firmwareString getName()
: get the file name of this firmwareboolean getState()
: returns the state of the firmware at the moment of the call: running (true
) or stopped (false
).
3.3 CoproSerialPort API[edit]
The CoproSerialPort API gives access to the /dev/ttyRPMSG0
driver available when a firmware is running. It allows the application to open and close the interface and also to send and receive data.
void open(int mode)
: opens a file descriptor to/dev/ttyRPMSG0
with the given mode : 0 for normal mode, 1 for raw modevoid close()
: closes the file descriptor to/dev/ttyRPMSG0
String read()
: reads available string if the file descriptor is open, otherwise an empty string is returned.byte[] readB()
: reads available bytes if the file descriptor is open, otherwise "-1" is returned.void write(String command)
: writes the given string to the file descriptor.void writeB(byte[] command)
: writes the given bytes to the file descriptor.
4 Develop an application using the coprocessor service[edit]
In order to build the application, make sure you are using the appropriate Android SDK including CoproService (refer to How to build and install an SDK for Android).
In Android Studio create a new application.
Then, do not forget to select the right API level in the application Manifest, in order to be sure that CoproService is available.
To use the CoproService you need to get the instance to the CoproManager, then you will be able to use the CoproManager API defined above:
CoproManager mCoproManager = CoproManager.getInstance();
To be able to communicate with the running firmware you need to get a CoproSerialPort from CoproManager, then you will be available to use the CoproSerialPort API defined above :
ICoproSerialPort mCoproSerialPort = mCoproManager.getSerialPort();
The serial communication is possible only if a firmware is running. Make sure to close the serial communication when you stop a firmware and open it when you start one.