Difference between revisions of "How to update U-Boot"
[quality revision] | [quality revision] |
m
|
m
|
This page explains how to manually update the U-Boot binaries on an SD card or on the e•MMC.
Contents
1 To update an SD card with the Linux dd command[edit]
When a Linux console has access to the SD card device partitions:
- on a Linux PC
- with a card reader of this PC
- through a USB connection to the target and the
ums
command executed on a U-Boot console
- on target, with Linux console.
The 3 first GPT partitions on the SD card are:
- FSBL1
- FSBL2
- SSBL
See Boot_chainschain_overview for the bootloader definitions.
You can use the Linux dd
command to copy the FSBL and SSBL directly to the correct partition:
dd if=<file> of=/dev/<dev> conv=fdatasync
<dev> is:
- mmcblk<X>p<n>: PC-embedded card reader case or target Linux console
- sd<X><n>: USB-connected SD card reader case
where <X> is the ID of the device, and <n> the ID of the partition.
Note: the dd option conv=fdatasync is used to force synchronous copying.
1.1 U-Boot environment[edit]
The U-Boot environment is saved at the end of the U-Boot partition, named "ssbl": ID = 3.
To clear this environment, erase the U-Boot partition before any update; for example, by writing 0 to this partition:
dd if=/dev/zero of=/dev/mmcblk<X>p3 conv=fdatasync
dd if=/dev/zero of=sd<X>3 conv=fdatasync
1.2 SD card update example[edit]
The internal card reader is /dev/mmcblk0 or for a target Linux console, GPT partition <n> is /dev/mmcblk0p<n>:
dd if=tf-a.stm32 of=/dev/mmcblk0p1 conv=fdatasync dd if=tf-a.stm32 of=/dev/mmcblk0p2 conv=fdatasync dd if=/dev/zero of=/dev/mmcblk0p3 conv=fdatasync dd if=u-boot.stm32 of=/dev/mmcblk0p3 conv=fdatasync
Alternatively, with U-Boot console, dev = 0 (SD card device on ST Microelectronics board), GPT partition <n> is /dev/sda<n>:
mmc dev 0 ums 0 mmc 0 dd if=tf-a.stm32 of=/dev/sda1 conv=fdatasync dd if=tf-a.stm32 of=/dev/sda2 conv=fdatasync dd if=/dev/zero of=/dev/sda3 conv=fdatasync dd if=u-boot.stm32 of=/dev/sda3 conv=fdatasync
1.3 SD card update example with SPL as FSBL[edit]
The USB card reader is /dev/sdb, GPT partition <n> is /dev/sdb<n>:
dd if=u-boot-spl.stm32 of=/dev/sdb1 conv=fdatasync dd if=u-boot-spl.stm32 of=/dev/sdb2 conv=fdatasync dd if=/dev/zero of=/dev/sdb3 conv=fdatasync dd if=u-boot.img of=/dev/sdb3 conv=fdatasync
2 Update of e•MMC with the Linux dd command[edit]
The same command, dd
, can be used to update e•MMC memory mapping:
- SSBL U-Boot is the first GPT partition in the e•MMC user area
- FSBL = TF-A (or SPL) is saved at the beginning of the e•MMC boot partition
The user needs to select the e•MMC hardware partition to update: user data, boot1, or boot2.
2.1 On a Linux console[edit]
If dev = mmcblk1 for e•MMC device (default on ST Microelectronics board)
The boot partitions are available in /dev/mmcblk1boot0 and /dev/mmcblk1boot1 [1].
The user perhaps needs to allow access, for example with:
echo 0 > /sys/class/block/mmcblk1boot0/force_ro
The mmc tools allow the boot partition to be selected [2].
The STM32MP15x ROM code requires:
- <send_ack> =1
- the eMMC boot configuration is: 1 wire configuration and 25 MHz, it is done with the command:
mmc bootbus set single_backward x1 x1 dev/mmcblk1
To update TF-A in boot1 and select this boot partition:
dd if=tf-a.stm32 of=/dev/mmcblk1boot0 conv=fdatasync mmc bootpart enable 1 1 /dev/mmcblk1
To update TF-A in boot2 and select this boot partition:
dd if=tf-a.stm32 of=/dev/mmcblk1boot1 conv=fdatasync mmc bootpart enable 2 1 /dev/mmcblk1
To update U-Boot in the first GPT partition:
dd if=/dev/zero of=/dev/mmcblk1p1 conv=fdatasync dd if=u-boot.stm32 of=/dev/mmcblk1p1 conv=fdatasync
See also [3].
2.2 On a U-Boot console[edit]
The e•MMC update is done with the ums
command and the targeted e•MMC HW partition is selected in U-Boot by the third parameter partition_access of command mmc partconf
:
- 0: user data partition
- 1: boot partition 1
- 2: boot partition 2
help mmc
...
mmc bootbus dev boot_bus_width reset_boot_bus_width boot_mode
- Set the BOOT_BUS_WIDTH field of the specified device
mmc bootpart-resize <dev> <boot part size MB> <RPMB part size MB>
- Change sizes of boot and RPMB partitions of specified device
mmc partconf dev [boot_ack boot_partition partition_access]
- Show or change the bits of the PARTITION_CONFIG field of the specified device
For example:
* dev = 1 (e•MMC device on ST Microelectronics board) * boot_ack=1 (Boot Acknowledge is needed by ROM code) * boot_partition = 1 (Boot partition 1 enabled for boot) * partition_access = 0 (No access to boot partition - default) * or partition_access = 1 (R/W boot partition 1)
And on a PC, the mass storage is mounted as /dev/sda
To update FSBL=TF-A, select the boot1 HW partition and come back to the user area at the end.
mmc dev 1 mmc partconf 1 1 1 1 ums 0 mmc 1 dd if=tf-a.stm32 of=/dev/sda conv=fdatasync mmc partconf 1 1 1 0
To update SSBL = U-Boot in the first GPT partition in the user partition
mmc dev 1 ums 0 mmc 1 dd if=u-boot.stm32 of=/dev/sda1 conv=fdatasync
Before the first boot, select the e•MMC correct boot configuration (1 wire, 25 MHz) with the command:
mmc bootbus 1 0 0 0
3 References[edit]
Please refer to the following links for additional information:
This page explains how to manually update the [[U-Boot_overview|U-Boot]] binaries on an SD card or on the ''e''•MMC. == To update an SD card with the Linux dd command == When a Linux console has access to the SD card device partitions: * on a Linux PC ** with a card reader of this PC ** through a USB connection to the target and the [[How to use USB mass storage in U-Boot|<code>ums</code> command]] executed on a U-Boot console * on target, with Linux console. [[STM32MP15_Flash_mapping#SD_card_memory_mapping|The 3 first GPT partitions on the SD card]] are: # FSBL1 # FSBL2 # SSBL See [[Boot_chainschain_overview]] for the bootloader definitions. You can use the Linux <code>dd</code> command to copy the FSBL and SSBL directly to the correct partition: {{PC$}} dd if={{HighlightParam|<file>}} of=/dev/{{HighlightParam|<dev>}} conv={{HighlightParam|fdatasync}} {{HighlightParam|<dev>}} is: * mmcblk{{Highlight|<X>}}p{{Highlight|<n>}}: PC-embedded card reader case or target Linux console * sd{{Highlight|<X>}}{{Highlight|<n>}}: USB-connected SD card reader case where {{Highlight|<X>}} is the ID of the device, and {{Highlight|<n>}} the ID of the partition. Note: the dd option {{HighlightParam|conv}}={{HighlightParam|fdatasync}} is used to force synchronous copying. === U-Boot environment === The U-Boot environment is saved at the end of the U-Boot partition, named "ssbl": ID = {{HighlightParam|3}}. To clear this environment, erase the U-Boot partition before any update; for example, by writing 0 to this partition: {{PC$}} dd if=/dev/zero of=/dev/mmcblk{{Highlight|<X>}}p{{HighlightParam|3}} conv=fdatasync {{PC$}} dd if=/dev/zero of=sd{{Highlight|<X>}}{{HighlightParam|3}} conv=fdatasync === SD card update example === The internal card reader is /dev/mmcblk0 or for a target Linux console, GPT partition <n> is {{HighlightParam|/dev/mmcblk0}}p<n>: {{PC$}} dd if={{HighlightParam|tf-a.stm32}} of={{HighlightParam|/dev/mmcblk0}}p1 conv=fdatasync {{PC$}} dd if={{HighlightParam|tf-a.stm32}} of={{HighlightParam|/dev/mmcblk0}}p2 conv=fdatasync {{PC$}} dd if=/dev/zero of={{HighlightParam|/dev/mmcblk0}}p3 conv=fdatasync {{PC$}} dd if={{HighlightParam|u-boot.stm32}} of={{HighlightParam|/dev/mmcblk0}}p3 conv=fdatasync Alternatively, with U-Boot console, dev = {{Highlight|0}} (SD card device on ST Microelectronics board), GPT partition <n> is {{HighlightParam|/dev/sda}}<n>: {{Board$}} mmc dev {{Highlight|0}} {{Board$}} ums 0 mmc {{Highlight|0}} {{PC$}} dd if={{HighlightParam|tf-a.stm32}} of={{HighlightParam|/dev/sda}}1 conv=fdatasync {{PC$}} dd if={{HighlightParam|tf-a.stm32}} of={{HighlightParam|/dev/sda}}2 conv=fdatasync {{PC$}} dd if=/dev/zero of={{HighlightParam|/dev/sda}}3 conv=fdatasync {{PC$}} dd if={{HighlightParam|u-boot.stm32}} of={{HighlightParam|/dev/sda}}3 conv=fdatasync === SD card update example with SPL as FSBL === The USB card reader is /dev/sdb, GPT partition <n> is {{HighlightParam|/dev/sdb<n>}}: {{PC$}} dd if={{HighlightParam|u-boot-spl.stm32}} of={{HighlightParam|/dev/sdb1}} conv=fdatasync {{PC$}} dd if={{HighlightParam|u-boot-spl.stm32}} of={{HighlightParam|/dev/sdb2}} conv=fdatasync {{PC$}} dd if=/dev/zero of={{HighlightParam|/dev/sdb3}} conv=fdatasync {{PC$}} dd if={{HighlightParam|u-boot.img}} of={{HighlightParam|/dev/sdb3}} conv=fdatasync == Update of ''e''•MMC with the Linux dd command == The same command, <code>dd</code>, can be used to update [[STM32MP15_Flash_mapping#eMMC_memory_mapping|''e''•MMC memory mapping]]: * SSBL U-Boot is the first GPT partition in the ''e''•MMC user area * FSBL = TF-A (or SPL) is saved at the beginning of the ''e''•MMC boot partition The user needs to select the ''e''•MMC hardware partition to update: user data, boot1, or boot2. === On a Linux console === If dev = {{Highlight|mmcblk1}} for ''e''•MMC device (default on ST Microelectronics board) The boot partitions are available in /dev/{{Highlight|mmcblk1}}{{HighlightParam|boot0}} and /dev/{{Highlight|mmcblk1}}{{HighlightParam|boot1}} <ref>https://www.kernel.org/doc/Documentation/mmc/mmc-dev-parts.txt</ref>. The user perhaps needs to allow access, for example with: {{Board$}} echo 0 > /sys/class/block/{{Highlight|mmcblk1}}{{HighlightParam|boot0}}/force_ro The mmc tools allow the boot partition to be selected <ref>https://manpages.debian.org/buster/mmc-utils/mmc.1.en.html</ref>. The STM32MP15x ROM code requires: * <send_ack> =1 * the eMMC boot configuration is: 1 wire configuration and 25 MHz, it is done with the command: {{Board$}} mmc bootbus set single_backward x1 x1 dev/{{Highlight|mmcblk1}} To update TF-A in boot1 and select this boot partition: {{Board$}} dd if={{HighlightParam|tf-a.stm32}} of=/dev/{{Highlight|mmcblk1}}{{HighlightParam|boot0}} conv=fdatasync {{Board$}} mmc bootpart enable {{HighlightParam|1}} 1 /dev/{{Highlight|mmcblk1}} To update TF-A in boot2 and select this boot partition: {{Board$}} dd if={{HighlightParam|tf-a.stm32}} of=/dev/{{Highlight|mmcblk1}}{{HighlightParam|boot1}} conv=fdatasync {{Board$}} mmc bootpart enable {{HighlightParam|2}} 1 /dev/{{Highlight|mmcblk1}} To update U-Boot in the first GPT partition: {{Board$}} dd if=/dev/zero of=/dev/{{Highlight|mmcblk1}}{{HighlightParam|p1}} conv=fdatasync {{Board$}} dd if={{HighlightParam|u-boot.stm32}} of=/dev/{{Highlight|mmcblk1}}{{HighlightParam|p1}} conv=fdatasync See also <ref>https://www.emcraft.com/som/stm32mp1/booting-linux-from-emmc</ref>. === On a U-Boot console === The ''e''•MMC update is done with the [[How to use USB mass storage in U-Boot|<code>ums</code> command]] and the targeted ''e''•MMC HW partition is selected in U-Boot by the third parameter {{HighlightParam|partition_access}} of command <code>{{Highlight|mmc partconf}}</code>: * {{HighlightParam|0}}: user data partition * {{HighlightParam|1}}: boot partition 1 * {{HighlightParam|2}}: boot partition 2 {{Board$}} help mmc ... mmc bootbus dev boot_bus_width reset_boot_bus_width boot_mode - Set the BOOT_BUS_WIDTH field of the specified device mmc bootpart-resize <dev> <boot part size MB> <RPMB part size MB> - Change sizes of boot and RPMB partitions of specified device mmc partconf dev [boot_ack boot_partition {{HighlightParam|partition_access}}] - Show or change the bits of the PARTITION_CONFIG field of the specified device For example: * dev = {{Highlight|1}} (''e''•MMC device on ST Microelectronics board) * boot_ack=1 (Boot Acknowledge is needed by ROM code) * boot_partition = 1 (Boot partition 1 enabled for boot) * {{HighlightParam|partition_access}} = {{HighlightParam|0}} (No access to boot partition - default) * or {{HighlightParam|partition_access}} = {{HighlightParam|1}} (R/W boot partition 1) And on a PC, the mass storage is mounted as {{HighlightParam|/dev/sda}} To update FSBL=TF-A, select the boot1 HW partition and come back to the user area at the end. {{Board$}} mmc dev {{Highlight|1}} {{Board$}} mmc partconf {{Highlight|1}} 1 1 {{HighlightParam|1}} {{Board$}} ums 0 mmc {{Highlight|1}} {{PC$}} dd if=tf-a.stm32 of={{HighlightParam|/dev/sda}} conv=fdatasync {{Board$}} mmc partconf {{Highlight|1}} 1 1 {{HighlightParam|0}} To update SSBL = U-Boot in the first GPT partition in the user partition {{Board$}} mmc dev {{Highlight|1}} {{Board$}} ums 0 mmc {{Highlight|1}} {{PC$}} dd if={{HighlightParam|u-boot.stm32}} of={{HighlightParam|/dev/sda}}1 conv=fdatasync Before the first boot, select the ''e''•MMC correct boot configuration (1 wire, 25 MHz) with the command: {{Board$}} mmc bootbus {{HighlightParam|1}} 0 0 0 ==References== Please refer to the following links for additional information: <references /> <noinclude> [[Category:How to populate boards]] {{PublicationRequestId | 16075 | 2020-05-12}}</noinclude>
Line 14: | Line 14: | ||
# SSBL |
# SSBL |
||
− | See [[ |
+ | See [[Boot_chain_overview]] for the bootloader definitions. |
You can use the Linux <code>dd</code> command to copy the FSBL and SSBL directly to the correct partition: |
You can use the Linux <code>dd</code> command to copy the FSBL and SSBL directly to the correct partition: |