Last edited 3 years ago

How to set up proxy and P2P Ethernet connection with STM32CubeIDE

The printable version is no longer supported and may have rendering errors. Please update your browser bookmarks and please use the default browser print function instead.

1 Introduction[edit source]

This article explain how to set up a Point-to-Point connection to the STM32 MPU board, especially in case of a proxy is also setup on the PC for accessing the Internet.

2 Setting up network[edit source]

To set up the connection

  • go to Windows -> Preferences -> General -> Network Connections
  • select "Manual" in the Active Provider field, and:
    • adjust your proxy setup with Edit... in Proxy entries
    • configure a new Proxy bypass with Add Host... giving the IP address of the STM32 MPUtarget.


Network Setting in STM32CubeIDE