Difference between revisions of "How to install JAVA JDK"
[checked revision] | [quality revision] |
m (→The yoctoproject meta-java)
|
m (→The yoctoproject meta-java)
|
The goal of this page is to describe the OpenJDK installation procedure on your STM32 MPU board and (native) desktop, in a Distribution Package environment. It is the "Open Standard Edition Java Development Kit" installation process. According to the OpenstLinux Weston software architecture, XWayland is used for all Java applications based on X11, which means AWT/SWING Java display/graphical applications. By default the Java Development Kit is installed on the rootfs partition of the target.
Contents
1 Prerequisites[edit]
1.1 Hardware prerequisites[edit]
- STM32MP157x-DKx Discovery kit
Or aSTM32MP157x-EV1 Evaluation board
- a keyboard and a mouse connected to the board
1.2 Software prerequisites[edit]
The STM32MP1 Distribution Package must be installed on your host. To do this, follow the procedure described in the Install the STM32MP1 OpenSTLinux distribution article.
![]() |
The Host OS Ubuntu release 18.04 and next is required |
2 The yoctoproject meta-java[edit]
JAVA for Linux-based embedded systems is available as metadata in the Yocto project.
- Clone the following git repository into [your STM32MP1 Distribution path]/layers/meta-st/
cd [your STM32MP1 Distribution path]/layers git clone git://git.yoctoproject.org/meta-java
Depending on the Yocto release, select the right branch. (for example, branch dunfell for the ecosystem release v2.0.0 )
![]() |
The last commit tested is cf9604a4789801d9dfb0cb8ca134ff04b42ae161 : openjdk-8: remove -Werror |
cd meta-java git checkout remotes/origin/dunfell
You can see the list of available Yocto branches with the following command:
cd meta-java git branch -a master remotes/origin/HEAD -> origin/master remotes/origin/dora remotes/origin/dunfell remotes/origin/g0hl1n/jdk14 remotes/origin/krogoth remotes/origin/master remotes/origin/master-next remotes/origin/morty remotes/origin/pyro remotes/origin/rocko remotes/origin/sumo remotes/origin/thud remotes/origin/warrior remotes/origin/zeus
- If not already done, set up your build environment
cd [your STM32MP1 Distribution path] source layers/meta-st/scripts/envsetup.sh (Select for the DISTRO openstlinux-weston and for MACHINE stm32mp1)
- Add the meta layer in your Yocto environment
cd [your STM32MP1 Distribution path]/build-openstlinuxweston-stm32mp1 bitbake-layers add-layer [your STM32MP1 Distribution path]/meta-st/meta-java
- Define at least the following variables in your local.conf file
([your STM32MP1 Distribution path]/build-openstlinuxweston-stm32mp1/conf/local.conf) #Possible provider: cacao-initial-native and jamvm-initial-native PREFERRED_PROVIDER_virtual/java-initial-native = "cacao-initial-native" #Possible provider: cacao-native and jamvm-native PREFERRED_PROVIDER_virtual/java-native = "jamvm-native" #Optional since there is only one provider for now PREFERRED_PROVIDER_virtual/javac-native = "ecj-bootstrap-native"
- Include in your image the openjdk-8 component
cd [your STM32MP1 Distribution path]/meta-st/meta-st-openstlinux/recipes-st/images
- Edit the file st-image-weston.bb and add the following line under CORE_IMAGE_EXTRA_INSTALL
openjdk-8 \ openjdk-8-demo \
- Build the image
cd [your STM32MP1 Distribution path]/build-openstlinuxweston-stm32mp1 bitbake st-image-weston
3 Compilation and execution of some JAVA demos[edit]
- forkjoin benchmark Java application
cd /usr/lib/jvm/openjdk-8/sample/forkjoin/mergesort javac MergeDemo.java java MergeDemo 200 100 3 1 1 3 Running with parameters: 200 100 3 1 1 3 Time in milliseconds. Y-axis: number of elements. X-axis parallelism used. 1 2 3 200: 10 7 8 300: 17 12 12 400: 20 14 14 Total: 47 33 34
- SampleTree Java application
Read the README.txt file for details. To execute in a Linux Weston console on the board, with a keyboard and a mouse.
cd /usr/lib/jvm/openjdk-8/demo/jfc/SampleTree java -jar SampleTree.jar
The goal of this page is to describe the OpenJDK installation procedure on your STM32 MPU board and (native) desktop, in a Distribution Package environment. It is the "Open Standard Edition Java Development Kit" installation process. According to the OpenstLinux Weston software architecture, '''XWayland''' is used for all Java applications based on '''X11''', which means '''AWT/SWING''' Java display/graphical applications. By default the Java Development Kit is installed on the rootfs partition of the target. ==Prerequisites== ===Hardware prerequisites=== *{{Board | type=157x-DKx}} Or a{{Board | type=157x-EV1}} * a keyboard and a mouse connected to the board ===Software prerequisites=== The STM32MP1 Distribution Package must be installed on your host. To do this, follow the procedure described in the [[STM32MP1 Distribution Package - OpenSTLinux distribution#Download|Install the STM32MP1 OpenSTLinux distribution]] article. {{Info|The Host OS Ubuntu release 18.04 and next is required}} ==The yoctoproject meta-java == JAVA for Linux-based embedded systems is available as metadata in the Yocto project. * Clone the following git repository into [your STM32MP1 Distribution path]/layers/meta-st/ {{PC$}}cd [your STM32MP1 Distribution path]/layers {{PC$}}git clone git://git.yoctoproject.org/meta-java Depending on the Yocto release, select the right branch. (for example, branch dunfell for the {{EcosystemRelease | revision=2.0.0}}) {{Info|The last commit tested is cf9604a4789801d9dfb0cb8ca134ff04b42ae161 : openjdk-8: remove -Werror}} {{PC$}}cd meta-java {{PC$}}git checkout remotes/origin/dunfell You can see the list of available Yocto branches with the following command: {{PC$}}cd meta-java {{PC$}}git branch -a master remotes/origin/HEAD -> origin/master remotes/origin/dora remotes/origin/dunfell remotes/origin/g0hl1n/jdk14 remotes/origin/krogoth remotes/origin/master remotes/origin/master-next remotes/origin/morty remotes/origin/pyro remotes/origin/rocko remotes/origin/sumo remotes/origin/thud remotes/origin/warrior remotes/origin/zeus</pre> * If not already done, set up your build environment {{PC$}} cd [your STM32MP1 Distribution path] {{PC$}} source layers/meta-st/scripts/envsetup.sh (Select for the DISTRO openstlinux-weston and for MACHINE stm32mp1) * Add the meta layer in your Yocto environment {{PC$}} cd [your STM32MP1 Distribution path]/build-openstlinuxweston-stm32mp1 {{PC$}} bitbake-layers add-layer [your STM32MP1 Distribution path]/meta-st/meta-java * Define at least the following variables in your local.conf file ([your STM32MP1 Distribution path]/build-openstlinuxweston-stm32mp1/conf/local.conf) #Possible provider: cacao-initial-native and jamvm-initial-native PREFERRED_PROVIDER_virtual/java-initial-native = "cacao-initial-native" #Possible provider: cacao-native and jamvm-native PREFERRED_PROVIDER_virtual/java-native = "jamvm-native" #Optional since there is only one provider for now PREFERRED_PROVIDER_virtual/javac-native = "ecj-bootstrap-native" * Include in your image the '''openjdk-8''' component {{PC$}} cd [your STM32MP1 Distribution path]/meta-st/meta-st-openstlinux/recipes-st/images * Edit the file st-image-weston.bb and add the following line under CORE_IMAGE_EXTRA_INSTALL<pre> openjdk-8 \ openjdk-8-demo \</pre> * Build the image {{PC$}} cd [your STM32MP1 Distribution path]/build-openstlinuxweston-stm32mp1 {{PC$}} bitbake st-image-weston ==Compilation and execution of some JAVA demos== * '''forkjoin''' benchmark Java application {{Board$}} cd /usr/lib/jvm/openjdk-8/sample/forkjoin/mergesort {{Board$}} javac MergeDemo.java {{Board$}} java MergeDemo 200 100 3 1 1 3 Running with parameters: 200 100 3 1 1 3 Time in milliseconds. Y-axis: number of elements. X-axis parallelism used. 1 2 3 200: 10 7 8 300: 17 12 12 400: 20 14 14 Total: 47 33 34 * '''SampleTree''' Java application Read the README.txt file for details. To execute in a Linux Weston console on the board, with a keyboard and a mouse. {{Board$}} cd /usr/lib/jvm/openjdk-8/demo/jfc/SampleTree {{Board$}} java -jar SampleTree.jar [[File:Sampletree.png|link=]] <noinclude> [[Category:How to run use cases with expansions]] {{PublicationRequestId | 17583 | 2020-10-02 | Philip Sage}}</noinclude>
Line 16: | Line 16: | ||
JAVA for Linux-based embedded systems is available as metadata in the Yocto project. |
JAVA for Linux-based embedded systems is available as metadata in the Yocto project. |
||
− | * Clone the following git repository into [your STM32MP1 Distribution path]/layers |
+ | * Clone the following git repository into [your STM32MP1 Distribution path]/layers |
{{PC$}}cd [your STM32MP1 Distribution path]/layers |
{{PC$}}cd [your STM32MP1 Distribution path]/layers |
||
{{PC$}}git clone git://git.yoctoproject.org/meta-java |
{{PC$}}git clone git://git.yoctoproject.org/meta-java |