Approved version. Approved on: 16:04, 6 November 2020
You are viewing an old version of this page. Return to the latest version.
- Last edited one year ago ago
How to diagnose a boot failure
Revision as of 09:29, 25 September 2020 by Jean Christophe Trotin (talk | contribs)
1 Introduction[edit]
The blue and red LEDs on STM32MP15 boards are used to notify the user in case of boot failure during the boot chain execution and at runtime.
2 Description and debug[edit]
The statuses of blue and red LEDs allow to see at which stage the execution failed: the diagram below shows how each boot component uses these LEDs while the table gives more information on the way to interpret the LED statuses when the boot fails. Among the boot components, the FSBL can be TF-A or U-Boot SPL and the SSBL is U-Boot, as explained in the boot chain overview.
Blue LED | Red LED | System state | Action |
---|---|---|---|
Off | Blinking | The execution failed during ROM code execution | Check that:
|
On | Blinking | The execution failed during the second stage bootloader (SSBL) | See U-Boot - How to debug to investigate the failure |
Off | Off | The execution may have failed:
|
|
Off or on | Off | The execution may have failed during Linux® kernel execution between two heartbeat pulses (blue LED): a fatal error leading to a kernel panic might have occurred... | See How to debug a Linux kernel crash to investigate the failure |
Blinking | Off | Your platform is alive | Enjoy ! |