<noinclude>
{{ArticleMainWriter | GeraldB}}
{{ArticleApprovedVersion| GeraldB | PatrickD, PatriceC, YannG, Jean-PhilippeR, LoicP | No previous approved version | AnneJ - 21Sep'18 - 8902 | 12Sep'18}}
[[Category:How to trace and debug]]</noinclude>
== Introduction ==
The blue and red [[LEDs and buttons on STM32 MPU boards|LEDs on STM32MP15 boards]] are used to notify the user in case of boot failure during the [[Boot chains overview|boot chain]] execution and at runtime.<br />
== Description and debug ==
The statuses of blue and red LEDs allow to see at which stage the execution failed: the diagram below shows how each boot component uses these LEDs while the table gives more information on the way to interpret the LED statuses when the boot fails. Among the boot components, the FSBL can be TF-A or U-Boot SPL and the SSBL is U-Boot, as explained in the [[Boot chains overview|boot chains overview]].<br /><br />
[[File:How_to_diagnose_a_boot_failure.png|center]]<br />
{|
! Blue LED
! Red LED
! System state
! Action
|-
| Off
| Blinking
| The execution failed during [[STM32MP15 ROM code overview|ROM code]] execution
| Check that:<br />
* your microSD card is properly inserted in the board
* the [[STM32MP15_ROM_code_overview#Boot device selection via the boot pins and OTP|boot pins]] configuration selects the boot device
* your boot memory was well programmed with [[STM32CubeProgrammer]]
|-
| On
| Blinking
| The execution failed during the second stage bootloader (SSBL)
| See [[U-Boot - How to debug]] to investigate the failure
|-
| Off
| Off
| The execution may have failed:<br />
# In FSBL execution
# After the SSBL execution but before the heartbeat (blue LED) started
| <br />
# See [[TF-A - How to debug]] to investigate the failure
# See [[U-Boot - How to debug]] and [[:Category:How_to_trace_and_debug|how to trace and debug]] to investigate the failure
|-
| Off or on
| Off
| The execution may have failed during Linux<sup>®</sup> kernel execution between two heartbeat pulses (blue LED): a fatal error leading to a kernel panic might have occurred...
| See [[How to debug a Linux kernel crash]] to investigate the failure
|-
| Blinking
| Off
| Your platform is alive
| Enjoy !
|}
<noinclude>
[[Category:How to trace and debug]]
{{PublicationRequestId | 8902 | 2018-09-21 | AnneJ}}</noinclude>