Difference between revisions of "How to cross-compile with the Distribution Package"
[quality revision] | [quality revision] |
Denis Humeau (talk | contribs)
m (→Modifying the TF-A)
|
m
|
Template:ArticleMainWriter Template:ArticleApprovedVersion
Contents
1 Article purpose[edit]
This article provides simple examples for the Distribution Package of the OpenSTLinux distribution, that illustrate the cross-compilation with the devtool and BitBake tools:
- modification with Linux® Kernel (configuration, device tree, driver, ...)
- modification of an external in-tree Linux Kernel module
- modification of U-Boot
- modification of TF-A
- addition of software
These examples also show how to deploy the results of the cross-compilation on the target, through a network connection to the host machine.
![]() |
All the examples described on this page use devtool and/or bitbake from OpenEmbededded, see OpenEmbedded - devtool for more information. |
2 Prerequisites[edit]
The prerequisites from Installing the OpenSTLinux distribution must be executed.
The board and the host machine are connected through an Ethernet link, and a remote terminal program is started on the host machine: see How to get Terminal.
The target is started, and its IP address (<board ip address>) is known.
3 Modification with kernel[edit]
3.1 Preamble[edit]
To start modification with a module, you need to initialize your Distribution Package environment.
cd <working directory path of distribution> DISTRO=openstlinux-weston MACHINE=stm32mp1 source layers/meta-st/scripts/envsetup.sh
You are now in the build directory, identified by <build dir> in the following paragraphs.
Initialize devtool for kernel component:
devtool modify virtual/kernel NOTE: Starting bitbake server... NOTE: Creating workspace layer in /mnt/internal_storage/oetest/oe_openstlinux_rocko/build-openstlinuxweston-stm32mp1/workspace NOTE: Enabling workspace layer in bblayers.conf Parsing recipes: 100% |########################################################################################| Time: 0:00:54 Parsing of 2401 .bb files complete (0 cached, 2401 parsed). 3282 targets, 88 skipped, 0 masked, 0 errors. NOTE: Mapping virtual/kernel to linux-stm32mp NOTE: Resolving any missing task queue dependencies ...
![]() |
The source code of kernel is located on <build dir>/workspace/sources. You can change the path where the source code is extracted by customizing the devtool modify command |
![]() |
For all the work around the kernel, we strongly encourage some usage for deploying the binaries on board
The difference of usage comes from the number of files to deploy on board. When there is only one or two files to put on board, the easiest way to do it is to deploy only the desired files . |
3.2 Modifying kernel configuration[edit]
This simple example modifies the kernel configuration via menuconfig for the CMA size.
- Get the current value of the CMA size (128 Mbytes here) through the analysis of the target boot log
dmesg | grep -i cma [ 0.000000] cma: Reserved 128 MiB at 0xf0000000
- Start the Linux kernel configuration menu: see Menuconfig or how to configure kernel
- Navigate to "Device Drivers - Generic Driver Options"
- select "Size in Megabytes"
- modify its value to 256
- exit and save the new configuration
- Check that the configuration file (.config) has been modified
grep -i CONFIG_CMA_SIZE_MBYTES <build dir>/workspace/sources/<name of kernel recipe>/.config.new CONFIG_CMA_SIZE_MBYTES=256
- Cross-compile the Linux kernel: see Menuconfig or how to configure kernel
- Update the Linux kernel image on board: see Menuconfig or how to configure kernel
- Reboot the board: see Menuconfig or how to configure kernel
- Get the new value of the CMA size (256 Mbytes) through the analysis of the target boot log
dmesg | grep -i cma
[ 0.000000] cma: Reserved 256 MiB at 0xe0000000
3.3 Modifying the Linux kernel device tree[edit]
This simple example modifies the default status of a user LED.
- With the board started; check that the user LED (LD3) is disabled
- Go to the <build dir>/workspace/sources/<name of kernel recipe>/ directory
cd <build dir>/workspace/sources/<name of kernel recipe>/
- Edit the arch/arm/boot/dts/stm32mp157c-ed1.dts Device Tree Source file for evaluation board or
Edit the arch/arm/boot/dts/stm32mp157c-dk2.dts Device Tree Source file for discovery board or
- Change the status of the "stm32mp:green:user" led to "okay", and set its default state to "on"
led { compatible = "gpio-leds"; status = "okay"; red { label = "stm32mp:red:status"; gpios = <&gpioa 13 GPIO_ACTIVE_LOW>; status = "disabled"; }; green { label = "stm32mp:green:user"; gpios = <&gpioa 14 GPIO_ACTIVE_LOW>; default-state = "on"; status = "okay"; }; };
- Go to the build directory
cd <build dir>
If this update is accepted, then to report in other paragraph of this page}}
- Generate the device tree blobs (*.dtb)
bitbake virtual/kernel -C compile
- Update the device tree blobs on the board
scp <build dir>/tmp-glibc/deploy/images/<machine name>/*.dtb root@<board ip address>:/boot
![]() |
If the /boot mounting point doesn't exist yet, please see how to create a mounting point |
- Reboot the board
cd /boot; sync; systemctl reboot
- Check that the user LED (LD3) is enabled (green)
3.4 Modifying a built-in Linux kernel device driver[edit]
This simple example adds unconditional log information when the display driver is probed.
- Check that there is no log information when the display driver is probed
dmesg | grep -i stm_drm_platform_probe
- Go to the <build dir>/workspace/sources/<name of kernel recipe>/
cd <build dir>/workspace/sources/<name of kernel recipe>/
- Edit the ./drivers/gpu/drm/stm/drv.c source file
- Add a log information in the stm_drm_platform_probe function
static int stm_drm_platform_probe(struct platform_device *pdev)
{
struct device *dev = &pdev->dev;
struct drm_device *ddev;
int ret;
[...]
DRM_INFO("Simple example - %s\n", __func__);
return 0;
[...]
}
- Go to the build directory
cd <build dir>
- Cross-compile the Linux kernel
bitbake virtual/kernel -C compile
- Update the Linux kernel image on board
scp <build dir>/tmp-glibc/deploy/images/<machine name>/uImage root@<board ip address>:/boot
![]() |
If the /boot mounting point doesn't exist yet, please see how to create a mounting point |
- Reboot the board
cd /boot; sync; systemctl reboot
- Check that there is now log information when the display driver is probed
dmesg | grep -i stm_drm_platform_probe
[ 5.005833] [drm] Simple example - stm_drm_platform_probe
3.5 Modifying/adding an external Linux kernel module[edit]
Most device drivers (modules) in the Linux kernel can be compiled either into the kernel itself (built-in/internal module) or as Loadable Kernel Modules (LKM/external module) that need to be placed in the root file system under the /lib/modules directory. An external module can be in-tree (in the kernel tree structure), or out-of-tree (outside the kernel tree structure).
This simple example adds an unconditional log information when the virtual video test driver (vivid) kernel module is probed or removed.
- Go to the <build dir>/workspace/sources/<name of kernel recipe>/
cd <build dir>/workspace/sources/<name of kernel recipe>/
- Edit the ./drivers/media/platform/vivid/vivid-core.c source file
- Add log information in the vivid_probe and vivid_remove functions
static int vivid_probe(struct platform_device *pdev)
{
const struct font_desc *font = find_font("VGA8x16");
int ret = 0, i;
[...]
/* n_devs will reflect the actual number of allocated devices */
n_devs = i;
pr_info("Simple example - %s\n", __func__);
return ret;
}
static int vivid_remove(struct platform_device *pdev)
{
struct vivid_dev *dev;
unsigned int i, j;
[...]
pr_info("Simple example - %s\n", __func__);
return 0;
}
- Go to the build directory
cd <build dir>
- Cross-compile the Linux kernel modules
bitbake virtual/kernel -C compile
- Update the vivid kernel module on the board
devtool deploy-target -Ss <name of kernel recipe> root@<board ip address>:/
- Update dependency descriptions for loadable kernel modules, and synchronize the data on disk with memory
/sbin/depmod -a sync
- Insert the vivid kernel module into the Linux kernel
modprobe vivid
[...]
[ 3412.784638] Simple example - vivid_probe
- Remove the vivid kernel module from the Linux kernel
rmmod vivid
[...]
[ 3423.708517] Simple example - vivid_remove
4 Adding an external out-of-tree Linux kernel module[edit]
This simple example adds a "Hello World" external out-of-tree Linux kernel module to the Linux kernel.
- Create a directory for this kernel module example
mkdir kernel_module_example cd kernel_module_example
- Create the source code file for this kernel module example: kernel_module_example.c
// SPDX-identifier: GPL-2.0
/*
* Copyright (C) STMicroelectronics SA 2018
*
* Authors: Jean-Christophe Trotin <jean-christophe.trotin@st.com>
*
*/
#include <linux/module.h> /* for all kernel modules */
#include <linux/kernel.h> /* for KERN_INFO */
#include <linux/init.h> /* for __init and __exit macros */
static int __init kernel_module_example_init(void)
{
printk(KERN_INFO "Kernel module example: hello world from STMicroelectronics\n");
return 0;
}
static void __exit kernel_module_example_exit(void)
{
printk(KERN_INFO "Kernel module example: goodbye from STMicroelectronics\n");
}
module_init(kernel_module_example_init);
module_exit(kernel_module_example_exit);
MODULE_DESCRIPTION("STMicroelectronics simple external out-of-tree Linux kernel module example");
MODULE_AUTHOR("Jean-Christophe Trotin <jean-christophe.trotin@st.com>");
MODULE_LICENSE("GPL v2");
- Create the makefile for this kernel module example: Makefile
![]() |
All the indentations in a makefile are tabulations |
# Makefile for simple external out-of-tree Linux kernel module example # Object file(s) to be built obj-m := kernel_module_example.o # Path to the directory that contains the Linux kernel source code # and the configuration file (.config) KERNEL_DIR ?= <Linux kernel path> # Path to the directory that contains the source file(s) to compile PWD := $(shell pwd) default: $(MAKE) -C $(KERNEL_DIR) M=$(PWD) modules clean: $(MAKE) -C $(KERNEL_DIR) M=$(PWD) clean
- Add a new recipe to the workspace
cd <build dir> devtool add mymodule kernel_module_example/
- Adapt recipe to kernel module build
devtool edit-recipe mymodule
- Modify the recipe according the following changes (see highlighted lines)
1 # Recipe created by recipetool
2 # This is the basis of a recipe and may need further editing in order to be fully functional.
3 # (Feel free to remove these comments when editing.)
4
5 # Unable to find any files that looked like license statements. Check the accompanying
6 # documentation and source headers and set LICENSE and LIC_FILES_CHKSUM accordingly.
7 #
8 # NOTE: LICENSE is being set to "CLOSED" to allow you to at least start building - if
9 # this is not accurate with respect to the licensing of the software being built (it
10 # will not be in most cases) you must specify the correct value before using this
11 # recipe for anything other than initial testing/development!
12 LICENSE = "CLOSED"
13 LIC_FILES_CHKSUM = ""
14
15 # No information for SRC_URI yet (only an external source tree was specified)
16 SRC_URI = ""
17
18 # NOTE: this is a Makefile-only piece of software, so we cannot generate much of the
19 # recipe automatically - you will need to examine the Makefile yourself and ensure
20 # that the appropriate arguments are passed in.
21 DEPENDS = "virtual/kernel"
22 inherit module
23
24 EXTRA_OEMAKE = "ARCH=arm"
25 EXTRA_OEMAKE += "KERNEL_DIR=${STAGING_KERNEL_BUILDDIR}"
26
27 S = "${WORKDIR}"
28
29 do_configure () {
30 # Specify any needed configure commands here
31 :
32 }
33
34 do_compile () {
35 # You will almost certainly need to add additional arguments here
36 oe_runmake
37 }
38
39 do_install () {
40 # NOTE: unable to determine what to put here - there is a Makefile but no
41 # target named "install", so you will need to define this yourself
42 install -d ${D}/lib/modules/${KERNEL_VERSION}
43 install -m 0755 ${B}/kernel_module_example.ko ${D}/lib/modules/${KERNEL_VERSION}/
44 }
- Go to the build directory
cd <build dir>
- Generated kernel module example
devtool build mymodule
- Push this kernel module example on board
devtool deploy-target -Ss mymodule root@<board ip address>
- Update dependency descriptions for loadable kernel modules, and synchronize the data on disk with memory
/sbin/depmod -a sync
- Insert the kernel module example into the Linux kernel
modprobe kernel_module_example
[18167.821725] Kernel module example: hello world from STMicroelectronics
- Remove the kernel module example from the Linux kernel
rmmod kernel_module_example
[18180.086722] Kernel module example: goodbye from STMicroelectronics
5 Modifying the U-Boot[edit]
This simple example adds unconditional log information when U-Boot starts. Within the scope of the trusted boot chain, U-Boot is used as second stage boot loader (SSBL).
- Have a look at the U-Boot log information when the board reboots
reboot [...] U-Boot <U-Boot version> CPU: STM32MP1 rev1.0 Model: STMicroelectronics STM32MP157C [...] Board: stm32mp1 in trusted mode [...]
- Go to the build directory
cd <build dir>
- Search U-boot recipe
devtool search u-boot* u-boot-stm32mp-extlinux Generate 'extlinux.conf' file for U-boot u-boot-stm32mp Universal Boot Loader for embedded devices for stm32mp
On this example, the recipe name is u-boot-stm32mp
- Start to work with u-boot
devtool modify u-boot-stm32mp
Example: cd <build dir>/workspace/sources/u-boot-stm32mp
- Edit the ./board/st/stm32mp1/stm32mp1.c source file
- Add a log information in the checkboard function
int checkboard(void)
{
char *mode;
[...]
printf("Board: stm32mp1 in %s mode\n", mode);
printf("U-Boot simple example\n");
return 0;
}
- Cross-compile the U-Boot: trusted boot
devtool build u-boot-stm32mp bitbake u-boot-stm32mp -c deploy
- Go to the directory in which the compilation results are stored
cd <build dir>/tmp-glibc/deploy/images/<machine name>/
- Reboot the board, and hit any key to stop in the U-boot shell
reboot [...] Hit any key to stop autoboot: 0 STM32MP>
- Connect a USB cable between the host machine and the board via the USB OTG ports
- In the U-Boot shell, call the USB mass storage function
STM32MP> ums 0 mmc 0
![]() |
for more information about the usage of U-Boot UMS functionality, see How to use USB mass storage in U-Boot |
- On the host machine, check the partition associated with the secondary stage boot loader (ssbl): sdc3 here
ls -l /dev/disk/by-partlabel/
total 0
lrwxrwxrwx 1 root root 10 Jan 17 18:05 bootfs -> ../../sdc4
lrwxrwxrwx 1 root root 10 Jan 17 18:05 fsbl1 -> ../../sdc1
lrwxrwxrwx 1 root root 10 Jan 17 18:05 fsbl2 -> ../../sdc2
lrwxrwxrwx 1 root root 10 Jan 17 18:05 rootfs -> ../../sdc5
lrwxrwxrwx 1 root root 10 Jan 17 18:05 ssbl -> ../../sdc3
lrwxrwxrwx 1 root root 10 Jan 17 18:05 userfs -> ../../sdc6
- Copy the binary (u-boot.stm32) to the dedicated partition
dd if=u-boot-<board name>-trusted.stm32 of=/dev/sdc3 bs=1M conv=fdatasync
(here u-boot-stm32mp157c-ev1-trusted.stm32 or u-boot-stm32mp157c-dk2-trusted.stm32)
- Reset the U-Boot shell
STM32MP> reset
- Have a look at the new U-Boot log information when the board reboots
[...]
U-Boot <U-Boot version>
CPU: STM32MP1 rev1.0
Model: STMicroelectronics STM32MP157C [...]
Board: stm32mp1 in trusted mode
U-Boot simple example
[...]
6 Modifying the TF-A[edit]
This simple example adds unconditional log information when the TF-A starts. Within the scope of the trusted boot chain, TF-A is used as first stage boot loader (FSBL).
- Have a look at the TF-A log information when the board reboots
reboot [...] INFO: System reset generated by MPU (MPSYSRST) INFO: Using SDMMC [...]
- Go to the build directory
cd <build dir>
- Search TF-A recipe
devtool search tf-a*
babeltrace Babeltrace - Trace Format Babel Tower
libunistring Library for manipulating C and Unicode strings
lttng-tools Linux Trace Toolkit Control
gettext Utilities and libraries for producing multi-lingual messages
glibc GLIBC (GNU C Library)
tf-a-stm32mp Trusted Firmware-A for STM32MP1
gnutls GNU Transport Layer Security Library
gstreamer1.0 GStreamer 1.0 multimedia framework
harfbuzz Text shaping library
glibc-locale Locale data from glibc
kbd Keytable files and keyboard utilities
On this example, the recipe name is tf-a-stm32mp
- Start to work with tf-a
devtool modify tf-a-stm32mp
- Go to <build dir>/workspace/sources/tf-a-stm32mp
cd <build dir>/workspace/sources/tf-a-stm32mp
- Edit the ./plat/st/stm32mp1/bl2_io_storage.c source file
- Add a log information in the stm32mp1_io_setup function
void stm32mp1_io_setup(void) { int io_result; [...] /* Add a trace about reset reason */ print_reset_reason(); INFO("TF-A simple example"); [...] }
- Cross-compile the TF-A
devtool build tf-a-stm32mp bitbake tf-a-stm32mp -c deploy
- Go to the directory in which the compilation results are stored
cd <build dir>/tmp-glibc/deploy/images/<machine name>/
- Reboot the board, and hit any key to stop in the U-boot shell
reboot [...] Hit any key to stop autoboot: 0 STM32MP>
- Connect a USB cable between the host machine and the board via the USB OTG ports
- In the U-Boot shell, call the USB mass storage function
STM32MP> ums 0 mmc 0
![]() |
for more information about the usage of U-boot ums functionality see How to use USB mass storage in U-Boot |
- On the host machine, check the partition associated with the first stage boot loader (fsbl1 and fsbl2 as backup): sdc1 and sdc2 (as backup) here
ls -l /dev/disk/by-partlabel/ total 0 lrwxrwxrwx 1 root root 10 Jan 17 18:05 bootfs -> ../../sdc4 lrwxrwxrwx 1 root root 10 Jan 17 18:05 sfsbl1 -> ../../sdc1 lrwxrwxrwx 1 root root 10 Jan 17 18:05 sfsbl2 -> ../../sdc2 lrwxrwxrwx 1 root root 10 Jan 17 18:05 rootfs -> ../../sdc5 lrwxrwxrwx 1 root root 10 Jan 17 18:05 ssbl -> ../../sdc3 lrwxrwxrwx 1 root root 10 Jan 17 18:05 userfs -> ../../sdc6
- Copy the binary (tf-a-stm32mp157c-ev1-trusted.stm32) to the dedicated partition; to test the new TF-A binary, it might be useful to keep the old TF-A binary in the backup FSBL (fsbl2)
dd if=tf-a-<board name>-trusted.stm32 of=/dev/sdc1 bs=1M conv=fdatasync
(here tf-a-stm32mp157c-ev1-trusted.stm32 or tf-a-stm32mp157c-dk2-trusted.stm32)
- Reset the U-Boot shell
STM32MP> reset
- Have a look at the new TF-A log information when the board reboots
[...]
INFO: System reset generated by MPU (MPSYSRST)
INFO: TF-A simple example
INFO: Using SDMMC
[...]
7 Adding a "hello world" user space example[edit]
This chapter shows how to compile and execute a simple "hello world" example.
- Create a directory for this user space example
mkdir hello_world_example cd hello_world_example
- Create the source code file for this user space example: hello_world_example.c
// SPDX-identifier: GPL-2.0
/*
* Copyright (C) STMicroelectronics SA 2018
*
* Authors: Jean-Christophe Trotin <jean-christophe.trotin@st.com>
*
*/
#include <stdio.h>
#include <unistd.h>
int main(int argc, char **argv)
{
int i =11;
printf("\
nUser space example: hello world from STMicroelectronics\n");
setbuf(stdout,NULL);
while (i--) {
printf("%i ", i);
sleep(1);
}
printf("\
nUser space example: goodbye from STMicroelectronics\n");
return(0);
}
- Add a new recipe to the workspace
cd <build dir> devtool add myhelloword hello_world_example/
- Adapt recipe
devtool edit-recipe myhelloword
- Modify the recipe according the following changes (see highlighted lines)
1 # Recipe created by recipetool
2 # This is the basis of a recipe and may need further editing in order to be fully functional.
3 # (Feel free to remove these comments when editing.)
4
5 # Unable to find any files that looked like license statements. Check the accompanying
6 # documentation and source headers and set LICENSE and LIC_FILES_CHKSUM accordingly.
7 #
8 # NOTE: LICENSE is being set to "CLOSED" to allow you to at least start building - if
9 # this is not accurate with respect to the licensing of the software being built (it
10 # will not be in most cases) you must specify the correct value before using this
11 # recipe for anything other than initial testing/development!
12 LICENSE = "CLOSED"
13 LIC_FILES_CHKSUM = ""
14
15 # No information for SRC_URI yet (only an external source tree was specified)
16 SRC_URI = ""
17
18 # NOTE: no Makefile found, unable to determine what needs to be done
19
20 do_configure () {
21 # Specify any needed configure commands here
22 :
23 }
24
25 do_compile () {
26 # Specify compilation commands here
27 cd ${S}
28 ${CC} hello_world_example.c -o hello_word_example
29 }
30
31 do_install () {
32 # Specify install commands here
33 install -d ${D}${bindir}
34 install -m 755 ${S}/hello_word_example ${D}${bindir}/
35 }
- Compile binary
devtool build myhelloword
- Push this binary on board
devtool deploy-target -s myhelloword root@<board ip address>
- Execute this user space example
/usr/bin/hello_world_example User space example: hello world from STMicroelectronics 10 9 8 7 6 5 4 3 2 1 0 User space example: goodbye from STMicroelectronics
8 Tips[edit]
8.1 Creating a mounting point[edit]
The objective is to create a mounting point for the boot file system (bootfs partition)
- Find the partition label associated with the boot file system
ls -l /dev/disk/by-partlabel/
total 0
lrwxrwxrwx 1 root root 15 Dec 13 12:31 bootfs -> ../../mmcblk0p4
lrwxrwxrwx 1 root root 15 Dec 13 12:31 fsbl1 -> ../../mmcblk0p1
lrwxrwxrwx 1 root root 15 Dec 13 12:31 fsbl2 -> ../../mmcblk0p2
lrwxrwxrwx 1 root root 15 Dec 13 12:31 rootfs -> ../../mmcblk0p5
lrwxrwxrwx 1 root root 15 Dec 13 12:31 ssbl -> ../../mmcblk0p3
lrwxrwxrwx 1 root root 15 Dec 13 12:31 userfs -> ../../mmcblk0p6
- Attach the boot file system found under /dev/mmcblk0p4 in the directory /boot
mount /dev/mmcblk0p4 /boot
<noinclude> {{ArticleMainWriter | ChristopheP}} {{ ArticleApprovedVersion | ChristopheP | NathalieS (Not Done), BernardP (PASS, 28June'18), ChristopheM (Pass, 10Jul'18), SebastienG (Not Done), RomualdJ (Not Done), Jean-ChristopheT (Passed with some comments, 27Jun'18), DenisH (25Jun'18, Done with comments) | No previous approved version | AlainF - 10439 - 24Jan'19 | 25Jan'19}} [[Category:How to build software]] [[Category:Distribution Package]] {{UpdateNeededForNewRelease|Please check regularly that the commands work fine}}</noinclude> {{ReviewsComments|JCT W826: general remark: * sometimes, you use "devtool build" to cross-compile, and sometimes, you use "bitbake <name of recipe> -C compile". * sometimes, you use "devtool deploy-target" to deploy, and sometimes, you use "bitbake <name of kernel recipe> -c deploy" It might be interesting to explain the reasons why different methods are used if there are such reasons. If there's no special reason (it's just that there are several methods possible, it might be interesting to indicate it}} ==Article purpose== This article provides simple examples for the Distribution Package of the OpenSTLinux distribution, that illustrate the cross-compilation with the [[OpenEmbedded - devtool|devtool]] and [[BitBake cheat sheet|BitBake]] tools: * modification with Linux<sup>®</sup> Kernel (configuration, device tree, driver, ...) * modification of an external in-tree Linux Kernel module * modification of U-Boot * modification of TF-A * addition of software These examples also show how to deploy the results of the cross-compilation on the target, through a network connection to the host machine. <br/> {{info|All the examples described on this page use devtool and/or bitbake from OpenEmbededded, see [[OpenEmbedded - devtool]] for more information.}} {{ReviewsComments|BPU W826: an article exists on bitbake in the wiki, it may be interesting to reference it here: BitBake_cheat_sheet }} {{info|There are many ways to achieve the same result; this article aims to provide at least one solution per example. You have the liberty to explore other methods that are better adapted to your development constraints.}} ==Prerequisites== The prerequisites from [[STM32MP1 Distribution Package#Installing the OpenSTLinux distribution|Installing the OpenSTLinux distribution]] must be executed. The board and the host machine are connected through an Ethernet link, and a remote terminal program is started on the host machine: see [[How to get Terminal]]. The target is started, and its IP address (<board ip address>) is known. ==Modification with kernel == ===Preamble=== To start modification with a module, you need to initialize your Distribution Package environment. {{PC$}} cd <working directory path of distribution> {{PC$}} DISTRO=openstlinux-weston MACHINE=stm32mp1 source layers/meta-st/scripts/envsetup.sh You are now in the build directory, identified by <build dir> in the following paragraphs. Initialize devtool for kernel component: {{PC$}} devtool modify virtual/kernel NOTE: Starting bitbake server... NOTE: Creating workspace layer in /mnt/internal_storage/oetest/oe_openstlinux_rocko/build-openstlinuxweston-stm32mp1/workspace NOTE: Enabling workspace layer in bblayers.conf Parsing recipes: 100% |########################################################################################| Time: 0:00:54 Parsing of 2401 .bb files complete (0 cached, 2401 parsed). 3282 targets, 88 skipped, 0 masked, 0 errors. NOTE: '''Mapping virtual/kernel to linux-stm32mp''' NOTE: Resolving any missing task queue dependencies ... {{Info| For the case of virtual/<something> component, you need to get the name of mapping between virtual component and associated recipe. In this example, the name of kernel recipe is indicated in the trace, but you can also get it by calling '''devtool status''' A minority of devtool command supports the virtual/<something> component, like devtool modify, it is why you need to get the recipe name associated to virtual/component. <br/> In this example, the name of kernel recipe is indicated in the trace (''linux-stm32mp'')}} {{Info| The source code of kernel is located on <build dir>/workspace/sources. You can change the path where the source code is extracted by customizing the devtool modify command }} {{Info| For all the work around the kernel, we strongly encourage some usage for deploying the binaries on board * Kernel image, device tree: use bitbake deploy command and scp (see [[#modifying kernel configuration]] )) * Kernel module: use devtool deploy-target by passing by a temporary directory (see [[#Modifying/adding an external Linux kernel module]]) The difference of usage comes from the number of files to deploy on board. When there is only one or two files to put on board, the easiest way to do it is to deploy only the desired files .}} ===Modifying kernel configuration=== This simple example modifies the kernel configuration via menuconfig for the CMA size. * Get the current value of the CMA size (128 Mbytes here) through the analysis of the target boot log {{Board$}} dmesg | grep -i cma [ 0.000000] cma: Reserved 128 MiB at 0xf0000000 * Start the Linux kernel configuration menu: see [[Menuconfig or how to configure kernel#Menuconfig and Distribution Package|Menuconfig or how to configure kernel]] * Navigate to "Device Drivers - Generic Driver Options" ** select "Size in Megabytes" ** modify its value to 256 ** exit and save the new configuration * Check that the configuration file (''.config'') has been modified {{PC$}} grep -i CONFIG_CMA_SIZE_MBYTES <build dir>/workspace/sources/<name of kernel recipe>/.config.new CONFIG_CMA_SIZE_MBYTES=256 * Cross-compile the Linux kernel: see [[Menuconfig or how to configure kernel#Menuconfig and Distribution Package|Menuconfig or how to configure kernel]] * Update the Linux kernel image on board: see [[Menuconfig or how to configure kernel#Menuconfig and Distribution Package|Menuconfig or how to configure kernel]] * Reboot the board: see [[Menuconfig or how to configure kernel#Menuconfig and Distribution Package|Menuconfig or how to configure kernel]] * Get the new value of the CMA size (256 Mbytes) through the analysis of the target boot log {{Board$}} dmesg | grep -i cma [ 0.000000] cma: Reserved {{Highlight|256}} MiB at 0xe0000000 ===Modifying the Linux kernel device tree=== This simple example modifies the default status of a user LED. * With the board started; check that the user LED (LD3) is disabled * Go to the <build dir>/workspace/sources/<name of kernel recipe>/ directory {{PC$}} cd <build dir>/workspace/sources/<name of kernel recipe>/ * Edit the ''arch/arm/boot/dts/stm32mp157c-ed1.dts'' Device Tree Source file for evaluation board or Edit the ''arch/arm/boot/dts/stm32mp157c-dk2.dts'' Device Tree Source file for discovery board or * Change the status of the "stm32mp:green:user" led to "okay", and set its default state to "on" led { compatible = "gpio-leds"; status = "{{Highlight|okay}}"; red { label = "stm32mp:red:status"; gpios = <&gpioa 13 GPIO_ACTIVE_LOW>; status = "disabled"; }; green { label = "stm32mp:green:user"; gpios = <&gpioa 14 GPIO_ACTIVE_LOW>; {{Highlight|default-state {{=}} "on";}} status = "{{Highlight|okay}}"; }; }; {{ReviewsComments|mcc W906: why not create a patch on kernel configuration as described : http://intranet.lme.st.com:8000/php-bin/ug_mcdmpu/index.php/How_to_customize_the_Linux_kernel seems better method to compile the kernel modification please can you refer to this wiki page and following section 3.2 Adding kernel driver or device tree modifications <br/>W2015: CPR: the goal of this page are not to integrate some change but to cross compile some changes and test it.)}} * Go to the build directory {{PC$}} cd <build dir> If this update is accepted, then to report in other paragraph of this page}} {{ReviewsComments|BPU W826: Why we do not do like before (build + deploy) ? It may need some explanation here (diff should be limited but interesting to learn)}} * Generate the device tree blobs (''*.dtb'') {{PC$}} bitbake virtual/kernel -C compile * Generate the device tree blobs (''*.dtb'') {{PC$}} bitbake virtual/kernel -C compile {{Info|we use here bitbake command instead of '''devtool build''' because the '''build''' makes '''compile''', '''compile_kernemodules''' and '''install''' commands whereas we only need only '''compile''' command to generate the kernel image and the device tree }}* Update the device tree blobs on the board {{PC$}} scp <build dir>/tmp-glibc/deploy/images/<machine name>/*.dtb root@<board ip address>:/boot {{Info|If the ''/boot'' mounting point doesn't exist yet, please see [[#Creating a mounting point|how to create a mounting point]]}} * Reboot the board {{Board$}} cd /boot; sync; systemctl reboot * Check that the user LED (LD3) is {{Highlight|enabled}} (green) ===Modifying a built-in Linux kernel device driver=== This simple example adds unconditional log information when the display driver is probed.<br><br> * Check that there is no log information when the display driver is probed {{Board$}} dmesg | grep -i stm_drm_platform_probe {{Board$}} * Go to the <build dir>/workspace/sources/<name of kernel recipe>/ {{PC$}} cd <build dir>/workspace/sources/<name of kernel recipe>/ * Edit the ''./drivers/gpu/drm/stm/drv.c'' source file * Add a log information in the ''stm_drm_platform_probe'' function static int stm_drm_platform_probe(struct platform_device *pdev) { struct device *dev = &pdev->dev; struct drm_device *ddev; int ret; [...] {{Highlight|DRM_INFO("Simple example - %s\n", __func__);}} return 0; [...] } * Go to the build directory {{PC$}} cd <build dir> * Cross-compile the Linux kernel {{PC$}} bitbake virtual/kernel -C compile * Update the Linux kernel image on board {{PC$}} scp <build dir>/tmp-glibc/deploy/images/<machine name>/uImage root@<board ip address>:/boot {{Info|If the ''/boot'' mounting point doesn't exist yet, please see [[#Creating a mounting point|how to create a mounting point]]}} * Reboot the board {{Board$}} cd /boot; sync; systemctl reboot * Check that there is now log information when the display driver is probed {{Board$}} dmesg | grep -i stm_drm_platform_probe [ 5.005833] [drm] {{Highlight|Simple example}} - stm_drm_platform_probe ===Modifying/adding an external Linux kernel module=== Most device drivers (modules) in the Linux kernel can be compiled either into the kernel itself (built-in/internal module) or as Loadable Kernel Modules (LKM/external module) that need to be placed in the root file system under the /lib/modules directory. An external module can be in-tree (in the kernel tree structure), or out-of-tree (outside the kernel tree structure). This simple example adds an unconditional log information when the virtual video test driver (vivid) kernel module is probed or removed.<br><br> * Go to the <build dir>/workspace/sources/<name of kernel recipe>/ {{PC$}} cd <build dir>/workspace/sources/<name of kernel recipe>/ * Edit the ''./drivers/media/platform/vivid/vivid-core.c'' source file * Add log information in the ''vivid_probe'' and ''vivid_remove'' functions static int vivid_probe(struct platform_device *pdev) { const struct font_desc *font = find_font("VGA8x16"); int ret = 0, i; [...] /* n_devs will reflect the actual number of allocated devices */ n_devs = i; {{Highlight|pr_info("Simple example - %s\n", __func__)}}; return ret; } static int vivid_remove(struct platform_device *pdev) { struct vivid_dev *dev; unsigned int i, j; [...] {{Highlight|pr_info("Simple example - %s\n", __func__)}}; return 0; } * Go to the build directory {{PC$}} cd <build dir> * Cross-compile the Linux kernel modules {{PC$}} bitbake virtual/kernel -C compile * Update the vivid kernel module on the board {{PC$}} devtool deploy-target -Ss <name of kernel recipe> root@<board ip address>:/ {{ReviewsComments|YCO W908: the command failed with my config (openstlinux-4.19-thud-mp1-19-02-20)<br> it seems to be link to the strip option, the error displayed is : <br> TypeError: strip_execs() missing 1 required positional argument: 'd' }} * Update dependency descriptions for loadable kernel modules, and synchronize the data on disk with memory {{Board$}} /sbin/depmod -a {{Board$}} sync * Insert the vivid kernel module into the Linux kernel {{Board$}} modprobe vivid [...] [ 3412.784638] {{Highlight|Simple example}} - vivid_probe * Remove the vivid kernel module from the Linux kernel {{Board$}} rmmod vivid [...] [ 3423.708517] {{Highlight|Simple example}} - vivid_remove ==Adding an external out-of-tree Linux kernel module== This simple example adds a "Hello World" external out-of-tree Linux kernel module to the Linux kernel.<br><br> * Create a directory for this kernel module example {{PC$}} mkdir kernel_module_example {{PC$}} cd kernel_module_example * Create the source code file for this kernel module example: ''kernel_module_example.c''<pre><syntaxhighlight lang="c"> // SPDX-identifier: GPL-2.0 /* * Copyright (C) STMicroelectronics SA 2018 * * Authors: Jean-Christophe Trotin <jean-christophe.trotin@st.com> * */ #include <linux/module.h> /* for all kernel modules */ #include <linux/kernel.h> /* for KERN_INFO */ #include <linux/init.h> /* for __init and __exit macros */ static int __init kernel_module_example_init(void) { printk(KERN_INFO "Kernel module example: hello world from STMicroelectronics\n"); return 0; } static void __exit kernel_module_example_exit(void) { printk(KERN_INFO "Kernel module example: goodbye from STMicroelectronics\n"); } module_init(kernel_module_example_init); module_exit(kernel_module_example_exit); MODULE_DESCRIPTION("STMicroelectronics simple external out-of-tree Linux kernel module example"); MODULE_AUTHOR("Jean-Christophe Trotin <jean-christophe.trotin@st.com>"); MODULE_LICENSE("GPL v2");</pre></syntaxhighlight> * Create the makefile for this kernel module example: ''Makefile'' {{info|All the indentations in a makefile are tabulations}}<pre> # Makefile for simple external out-of-tree Linux kernel module example # Object file(s) to be built obj-m := kernel_module_example.o # Path to the directory that contains the Linux kernel source code # and the configuration file (.config) KERNEL_DIR ?= <Linux kernel path> # Path to the directory that contains the source file(s) to compile PWD := $(shell pwd) default: $(MAKE) -C $(KERNEL_DIR) M=$(PWD) modules clean: $(MAKE) -C $(KERNEL_DIR) M=$(PWD) clean</pre> * Add a new recipe to the workspace {{PC$}} cd <build dir> {{PC$}} devtool add mymodule kernel_module_example/ * Adapt recipe to kernel module build {{PC$}} devtool edit-recipe mymodule :Modify the recipe according the following changes (see highlighted lines){{ReviewsComments|YCO W908: no highlighted lines in the text below <br>So we dont know what we have to add to the template created by devtool, perhaps this template has changed since previous devtool !! <br> To compile I needed to delete "\</font\>" in do_install function }}<pre class="brush:c; gutter:true; highlight: [21,22,24,25,27,40,41];"> <syntaxhighlight lang="c" line highlight="21-22,24-25,27,40-41"> # Recipe created by recipetool # This is the basis of a recipe and may need further editing in order to be fully functional. # (Feel free to remove these comments when editing.) # Unable to find any files that looked like license statements. Check the accompanying # documentation and source headers and set LICENSE and LIC_FILES_CHKSUM accordingly. # # NOTE: LICENSE is being set to "CLOSED" to allow you to at least start building - if # this is not accurate with respect to the licensing of the software being built (it # will not be in most cases) you must specify the correct value before using this # recipe for anything other than initial testing/development! LICENSE = "CLOSED" LIC_FILES_CHKSUM = "" # No information for SRC_URI yet (only an external source tree was specified) SRC_URI = "" # NOTE: this is a Makefile-only piece of software, so we cannot generate much of the # recipe automatically - you will need to examine the Makefile yourself and ensure # that the appropriate arguments are passed in. DEPENDS = "virtual/kernel" inherit module EXTRA_OEMAKE = "ARCH=arm" EXTRA_OEMAKE += "KERNEL_DIR=${STAGING_KERNEL_BUILDDIR}" S = "${WORKDIR}" do_configure () { # Specify any needed configure commands here : } do_compile () { # You will almost certainly need to add additional arguments here oe_runmake } do_install () { # NOTE: unable to determine what to put here - there is a Makefile but no # target named "install", so you will need to define this yourself install -d ${D}/lib/modules/${KERNEL_VERSION}</font> install -m 0755 ${B}/kernel_module_example.ko ${D}/lib/modules/${KERNEL_VERSION}/</font> }</pre> }</syntaxhighlight> * Go to the build directory {{PC$}} cd <build dir> * Generated kernel module example {{PC$}} devtool build mymodule * Push this kernel module example on board {{PC$}} devtool deploy-target -Ss mymodule root@<board ip address> * Update dependency descriptions for loadable kernel modules, and synchronize the data on disk with memory {{Board$}} /sbin/depmod -a {{Board$}} sync * Insert the kernel module example into the Linux kernel {{Board$}} modprobe kernel_module_example [18167.821725] {{Highlight|Kernel module example}}: hello world from STMicroelectronics * Remove the kernel module example from the Linux kernel {{Board$}} rmmod kernel_module_example [18180.086722] {{Highlight|Kernel module example}}: goodbye from STMicroelectronics ==Modifying the U-Boot== This simple example adds unconditional log information when U-Boot starts. Within the scope of the [[Boot chainschain overview|trusted boot chain]], U-Boot is used as second stage boot loader (SSBL). * Have a look at the U-Boot log information when the board reboots {{Board$}} reboot [...] U-Boot <U-Boot version> CPU: STM32MP1 rev1.0 Model: STMicroelectronics STM32MP157C [...] Board: stm32mp1 in trusted mode [...] * Go to the build directory {{PC$}} cd <build dir> * Search U-boot recipe {{PC$}} devtool search u-boot* u-boot-stm32mp-extlinux Generate 'extlinux.conf' file for U-boot u-boot-stm32mp Universal Boot Loader for embedded devices for stm32mp On this example, the recipe name is '''u-boot-stm32mp''' * Start to work with u-boot {{PC$}} devtool modify u-boot-stm32mp Example: {{PC$}} cd <build dir>/workspace/sources/u-boot-stm32mp * Edit the ''./board/st/stm32mp1/stm32mp1.c'' source file * Add a log information in the ''checkboard'' function int checkboard(void) { char *mode; [...] printf("Board: stm32mp1 in %s mode\n", mode); {{Highlight|printf("U-Boot simple example\n");}} return 0; } * Cross-compile the U-Boot: trusted boot {{PC$}} devtool build u-boot-stm32mp {{PC$}} bitbake u-boot-stm32mp -c deploy * Go to the directory in which the compilation results are stored {{PC$}} cd <build dir>/tmp-glibc/deploy/images/<machine name>/ * Reboot the board, and hit any key to stop in the U-boot shell {{Board$}} reboot [...] Hit any key to stop autoboot: 0 STM32MP> * Connect a USB cable between the host machine and the board via the USB OTG ports * In the U-Boot shell, call the USB mass storage function STM32MP> ums 0 mmc 0 {{Info|for more information about the usage of U-Boot UMS functionality, see [[How to use USB mass storage in U-Boot]]}} * On the host machine, check the partition associated with the secondary stage boot loader (''ssbl''): ''sdc3'' here {{PC$}} ls -l /dev/disk/by-partlabel/ total 0 lrwxrwxrwx 1 root root 10 Jan 17 18:05 bootfs -> ../../sdc4 lrwxrwxrwx 1 root root 10 Jan 17 18:05 fsbl1 -> ../../sdc1 lrwxrwxrwx 1 root root 10 Jan 17 18:05 fsbl2 -> ../../sdc2 lrwxrwxrwx 1 root root 10 Jan 17 18:05 rootfs -> ../../sdc5 lrwxrwxrwx 1 root root 10 Jan 17 18:05 {{Highlight|ssbl -> ../../sdc3}} lrwxrwxrwx 1 root root 10 Jan 17 18:05 userfs -> ../../sdc6 * Copy the binary (u-boot.stm32) to the dedicated partition {{PC$}} dd if=u-boot-<board name>-trusted.stm32 of=/dev/sdc3 bs=1M conv=fdatasync (here u-boot-stm32mp157c-ev1-trusted.stm32 or u-boot-stm32mp157c-dk2-trusted.stm32) * Reset the U-Boot shell STM32MP> reset * Have a look at the new U-Boot log information when the board reboots [...] U-Boot <U-Boot version> CPU: STM32MP1 rev1.0 Model: STMicroelectronics STM32MP157C [...] Board: stm32mp1 in trusted mode {{Highlight|U-Boot simple example}} [...] ==Modifying the TF-A== This simple example adds unconditional log information when the TF-A starts. Within the scope of the [[Boot chainschain overview|trusted boot chain]], TF-A is used as first stage boot loader (FSBL). * Have a look at the TF-A log information when the board reboots {{Board$}} reboot [...] INFO: System reset generated by MPU (MPSYSRST) INFO: Using SDMMC [...] * Go to the build directory {{PC$}} cd <build dir> * Search TF-A recipe {{PC$}} devtool search tf-a* babeltrace Babeltrace - Trace Format Babel Tower libunistring Library for manipulating C and Unicode strings lttng-tools Linux Trace Toolkit Control gettext Utilities and libraries for producing multi-lingual messages glibc GLIBC (GNU C Library) {{Highlight|tf-a-stm32mp }} Trusted Firmware-A for STM32MP1 gnutls GNU Transport Layer Security Library gstreamer1.0 GStreamer 1.0 multimedia framework harfbuzz Text shaping library glibc-locale Locale data from glibc kbd Keytable files and keyboard utilities On this example, the recipe name is '''tf-a-stm32mp''' * Start to work with tf-a {{PC$}} devtool modify tf-a-stm32mp * Go to <build dir>/workspace/sources/tf-a-stm32mp {{PC$}} cd <build dir>/workspace/sources/tf-a-stm32mp * Edit the ''./plat/st/stm32mp1/bl2_io_storage.c'' source file * Add a log information in the ''stm32mp1_io_setup'' function void stm32mp1_io_setup(void) { int io_result; [...] /* Add a trace about reset reason */ print_reset_reason(); INFO("TF-A simple example"); [...] } * Cross-compile the TF-A {{PC$}} devtool build tf-a-stm32mp {{PC$}} bitbake tf-a-stm32mp -c deploy * Go to the directory in which the compilation results are stored {{PC$}} cd <build dir>/tmp-glibc/deploy/images/<machine name>/ * Reboot the board, and hit any key to stop in the U-boot shell {{Board$}} reboot [...] Hit any key to stop autoboot: 0 STM32MP> * Connect a USB cable between the host machine and the board via the USB OTG ports * In the U-Boot shell, call the USB mass storage function STM32MP> ums 0 mmc 0 {{Info|for more information about the usage of U-boot ums functionality see [[How to use USB mass storage in U-Boot]]}} * On the host machine, check the partition associated with the first stage boot loader (''fsbl1'' and ''fsbl2'' as backup): ''sdc1'' and ''sdc2'' (as backup) here {{PC$}} ls -l /dev/disk/by-partlabel/ total 0 lrwxrwxrwx 1 root root 10 Jan 17 18:05 bootfs -> ../../sdc4 lrwxrwxrwx 1 root root 10 Jan 17 18:05 {{Highlight|sfsbl1 -> ../../sdc1}} lrwxrwxrwx 1 root root 10 Jan 17 18:05 {{Highlight|sfsbl2 -> ../../sdc2}} lrwxrwxrwx 1 root root 10 Jan 17 18:05 rootfs -> ../../sdc5 lrwxrwxrwx 1 root root 10 Jan 17 18:05 ssbl -> ../../sdc3 lrwxrwxrwx 1 root root 10 Jan 17 18:05 userfs -> ../../sdc6 * Copy the binary (tf-a-stm32mp157c-ev1-trusted.stm32) to the dedicated partition; to test the new TF-A binary, it might be useful to keep the old TF-A binary in the backup FSBL (''fsbl2'') {{PC$}} dd if=tf-a-<board name>-trusted.stm32 of=/dev/sdc1 bs=1M conv=fdatasync (here tf-a-stm32mp157c-ev1-trusted.stm32 or tf-a-stm32mp157c-dk2-trusted.stm32) * Reset the U-Boot shell STM32MP> reset * Have a look at the new TF-A log information when the board reboots [...] INFO: System reset generated by MPU (MPSYSRST) INFO: {{Highlight|TF-A simple example}} INFO: Using SDMMC [...] ==Adding a "hello world" user space example== This chapter shows how to compile and execute a simple "hello world" example. * Create a directory for this user space example {{PC$}} mkdir hello_world_example {{PC$}} cd hello_world_example * Create the source code file for this user space example: ''hello_world_example.c''<pre><syntaxhighlight lang="c"> // SPDX-identifier: GPL-2.0 /* * Copyright (C) STMicroelectronics SA 2018 * * Authors: Jean-Christophe Trotin <jean-christophe.trotin@st.com> * */ #include <stdio.h> #include <unistd.h> int main(int argc, char **argv) { int i =11; printf("\nUser space example: hello world from STMicroelectronics\n"); setbuf(stdout,NULL); while (i--) { printf("%i ", i); sleep(1); } printf("\nUser space example: goodbye from STMicroelectronics\n"); return(0); }</pre></syntaxhighlight> * Add a new recipe to the workspace {{PC$}} cd <build dir> {{PC$}} devtool add myhelloword hello_world_example/ * Adapt recipe {{PC$}} devtool edit-recipe myhelloword :Modify the recipe according the following changes (see highlighted lines)<pre class="brush:c; gutter:true; highlight: [27,28,33,34];"><syntaxhighlight lang="c" line highlight="27-28,33-34"> # Recipe created by recipetool # This is the basis of a recipe and may need further editing in order to be fully functional. # (Feel free to remove these comments when editing.) # Unable to find any files that looked like license statements. Check the accompanying # documentation and source headers and set LICENSE and LIC_FILES_CHKSUM accordingly. # # NOTE: LICENSE is being set to "CLOSED" to allow you to at least start building - if # this is not accurate with respect to the licensing of the software being built (it # will not be in most cases) you must specify the correct value before using this # recipe for anything other than initial testing/development! LICENSE = "CLOSED" LIC_FILES_CHKSUM = "" # No information for SRC_URI yet (only an external source tree was specified) SRC_URI = "" # NOTE: no Makefile found, unable to determine what needs to be done do_configure () { # Specify any needed configure commands here : } do_compile () { # Specify compilation commands here cd ${S} ${CC} hello_world_example.c -o hello_word_example } do_install () { # Specify install commands here install -d ${D}${bindir} install -m 755 ${S}/hello_word_example ${D}${bindir}/ }</pre> {{ReviewsComments|YCO W908: build step is missing : devtool build myhelloworld}}</syntaxhighlight> * Compile binary {{PC$}} devtool build myhelloword * Push this binary on board {{PC$}} devtool deploy-target -s myhelloword root@<board ip address> * Execute this user space example {{Board$}} /usr/bin/hello_world_example {{Highlight|User space example}}: hello world from STMicroelectronics 10 9 8 7 6 5 4 3 2 1 0 {{Highlight|User space example}}: goodbye from STMicroelectronics ==Tips== ===Creating a mounting point=== The objective is to create a mounting point for the boot file system (bootfs partition) * Find the partition label associated with the boot file system {{Board$}} ls -l /dev/disk/by-partlabel/ total 0 lrwxrwxrwx 1 root root 15 Dec 13 12:31 {{Highlight|bootfs -> ../../mmcblk0p4}} lrwxrwxrwx 1 root root 15 Dec 13 12:31 fsbl1 -> ../../mmcblk0p1 lrwxrwxrwx 1 root root 15 Dec 13 12:31 fsbl2 -> ../../mmcblk0p2 lrwxrwxrwx 1 root root 15 Dec 13 12:31 rootfs -> ../../mmcblk0p5 lrwxrwxrwx 1 root root 15 Dec 13 12:31 ssbl -> ../../mmcblk0p3 lrwxrwxrwx 1 root root 15 Dec 13 12:31 userfs -> ../../mmcblk0p6 * Attach the boot file system found under ''/dev/mmcblk0p4'' in the directory ''/boot'' {{Board$}} mount /dev/mmcblk0p4 /boot <noinclude> [[Category:How to build software]] [[Category:Distribution Package]] {{PublicationRequestId | 10439 | 2019-01-24 | AlainF}} {{UpdateNeededForNewRelease|Please check regularly that the commands work fine}} {{ReviewsComments|JCT W826: general remark: * sometimes, you use "devtool build" to cross-compile, and sometimes, you use "bitbake <name of recipe> -C compile". * sometimes, you use "devtool deploy-target" to deploy, and sometimes, you use "bitbake <name of kernel recipe> -c deploy" It might be interesting to explain the reasons why different methods are used if there are such reasons. If there's no special reason (it's just that there are several methods possible, it might be interesting to indicate it}}</noinclude>
(3 intermediate revisions by 3 users not shown) | |||
Line 1: | Line 1: | ||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
==Article purpose== |
==Article purpose== |
||
This article provides simple examples for the Distribution Package of the OpenSTLinux distribution, that illustrate the cross-compilation with the [[OpenEmbedded - devtool|devtool]] and [[BitBake cheat sheet|BitBake]] tools: |
This article provides simple examples for the Distribution Package of the OpenSTLinux distribution, that illustrate the cross-compilation with the [[OpenEmbedded - devtool|devtool]] and [[BitBake cheat sheet|BitBake]] tools: |
||
Line 128: | Line 116: | ||
please can you refer to this wiki page and following section |
please can you refer to this wiki page and following section |
||
3.2 Adding kernel driver or device tree modifications |
3.2 Adding kernel driver or device tree modifications |
||
− | + | <br/>W2015: CPR: the goal of this page are not to integrate some change but to cross compile some changes and test it. |
|
)}} |
)}} |
||
Line 136: | Line 124: | ||
If this update is accepted, then to report in other paragraph of this page}} |
If this update is accepted, then to report in other paragraph of this page}} |
||
− | |||
* Generate the device tree blobs (''*.dtb'') |
* Generate the device tree blobs (''*.dtb'') |
||
{{PC$}} bitbake virtual/kernel -C compile |
{{PC$}} bitbake virtual/kernel -C compile |
||
− | + | {{Info|we use here bitbake command instead of '''devtool build''' because the '''build''' makes '''compile''', '''compile_kernemodules''' and '''install''' commands whereas we only need only '''compile''' command to generate the kernel image and the device tree }} |
|
* Update the device tree blobs on the board |
* Update the device tree blobs on the board |
||
{{PC$}} scp <build dir>/tmp-glibc/deploy/images/<machine name>/*.dtb root@<board ip address>:/boot |
{{PC$}} scp <build dir>/tmp-glibc/deploy/images/<machine name>/*.dtb root@<board ip address>:/boot |
||
Line 262: | Line 249: | ||
* Create the source code file for this kernel module example: ''kernel_module_example.c'' |
* Create the source code file for this kernel module example: ''kernel_module_example.c'' |
||
− | < |
+ | <syntaxhighlight lang="c"> |
// SPDX-identifier: GPL-2.0 |
// SPDX-identifier: GPL-2.0 |
||
/* |
/* |
||
Line 292: | Line 279: | ||
MODULE_AUTHOR("Jean-Christophe Trotin <jean-christophe.trotin@st.com>"); |
MODULE_AUTHOR("Jean-Christophe Trotin <jean-christophe.trotin@st.com>"); |
||
MODULE_LICENSE("GPL v2"); |
MODULE_LICENSE("GPL v2"); |
||
− | </ |
+ | </syntaxhighlight > |
* Create the makefile for this kernel module example: ''Makefile'' |
* Create the makefile for this kernel module example: ''Makefile'' |
||
Line 323: | Line 310: | ||
{{PC$}} devtool edit-recipe mymodule |
{{PC$}} devtool edit-recipe mymodule |
||
:Modify the recipe according the following changes (see highlighted lines) |
:Modify the recipe according the following changes (see highlighted lines) |
||
− | + | ||
− | + | <syntaxhighlight lang="c" line highlight="21-22,24-25,27,40-41"> |
|
− | |||
# Recipe created by recipetool |
# Recipe created by recipetool |
||
# This is the basis of a recipe and may need further editing in order to be fully functional. |
# This is the basis of a recipe and may need further editing in order to be fully functional. |
||
Line 367: | Line 353: | ||
# NOTE: unable to determine what to put here - there is a Makefile but no |
# NOTE: unable to determine what to put here - there is a Makefile but no |
||
# target named "install", so you will need to define this yourself |
# target named "install", so you will need to define this yourself |
||
− | install -d ${D}/lib/modules/${KERNEL_VERSION} |
+ | install -d ${D}/lib/modules/${KERNEL_VERSION} |
− | install -m 0755 ${B}/kernel_module_example.ko ${D}/lib/modules/${KERNEL_VERSION}/ |
+ | install -m 0755 ${B}/kernel_module_example.ko ${D}/lib/modules/${KERNEL_VERSION}/ |
} |
} |
||
− | </ |
+ | </syntaxhighlight > |
* Go to the build directory |
* Go to the build directory |
||
Line 395: | Line 381: | ||
==Modifying the U-Boot== |
==Modifying the U-Boot== |
||
− | This simple example adds unconditional log information when U-Boot starts. Within the scope of the [[Boot |
+ | This simple example adds unconditional log information when U-Boot starts. Within the scope of the [[Boot chain overview|trusted boot chain]], U-Boot is used as second stage boot loader (SSBL). |
* Have a look at the U-Boot log information when the board reboots |
* Have a look at the U-Boot log information when the board reboots |
||
Line 481: | Line 467: | ||
==Modifying the TF-A== |
==Modifying the TF-A== |
||
− | This simple example adds unconditional log information when the TF-A starts. Within the scope of the [[Boot |
+ | This simple example adds unconditional log information when the TF-A starts. Within the scope of the [[Boot chain overview|trusted boot chain]], TF-A is used as first stage boot loader (FSBL). |
* Have a look at the TF-A log information when the board reboots |
* Have a look at the TF-A log information when the board reboots |
||
Line 579: | Line 565: | ||
* Create the source code file for this user space example: ''hello_world_example.c'' |
* Create the source code file for this user space example: ''hello_world_example.c'' |
||
− | < |
+ | <syntaxhighlight lang="c"> |
// SPDX-identifier: GPL-2.0 |
// SPDX-identifier: GPL-2.0 |
||
/* |
/* |
||
Line 605: | Line 591: | ||
return(0); |
return(0); |
||
} |
} |
||
− | </ |
+ | </syntaxhighlight> |
* Add a new recipe to the workspace |
* Add a new recipe to the workspace |
||
Line 614: | Line 600: | ||
{{PC$}} devtool edit-recipe myhelloword |
{{PC$}} devtool edit-recipe myhelloword |
||
:Modify the recipe according the following changes (see highlighted lines) |
:Modify the recipe according the following changes (see highlighted lines) |
||
− | < |
+ | <syntaxhighlight lang="c" line highlight="27-28,33-34"> |
# Recipe created by recipetool |
# Recipe created by recipetool |
||
# This is the basis of a recipe and may need further editing in order to be fully functional. |
# This is the basis of a recipe and may need further editing in order to be fully functional. |
||
Line 650: | Line 636: | ||
install -m 755 ${S}/hello_word_example ${D}${bindir}/ |
install -m 755 ${S}/hello_word_example ${D}${bindir}/ |
||
} |
} |
||
− | </ |
+ | </syntaxhighlight> |
+ | |||
+ | * Compile binary |
||
+ | {{PC$}} devtool build myhelloword |
||
− | |||
* Push this binary on board |
* Push this binary on board |
||
{{PC$}} devtool deploy-target -s myhelloword root@<board ip address> |
{{PC$}} devtool deploy-target -s myhelloword root@<board ip address> |
||
Line 677: | Line 665: | ||
* Attach the boot file system found under ''/dev/mmcblk0p4'' in the directory ''/boot'' |
* Attach the boot file system found under ''/dev/mmcblk0p4'' in the directory ''/boot'' |
||
{{Board$}} mount /dev/mmcblk0p4 /boot |
{{Board$}} mount /dev/mmcblk0p4 /boot |
||
+ | |||
+ | <noinclude> |
||
+ | [[Category:How to build software]] |
||
+ | [[Category:Distribution Package]] |
||
+ | {{PublicationRequestId | 10439 | 2019-01-24 | AlainF}} |
||
+ | {{UpdateNeededForNewRelease|Please check regularly that the commands work fine}} |
||
+ | {{ReviewsComments|JCT W826: general remark: |
||
+ | * sometimes, you use "devtool build" to cross-compile, and sometimes, you use "bitbake <name of recipe> -C compile". |
||
+ | * sometimes, you use "devtool deploy-target" to deploy, and sometimes, you use "bitbake <name of kernel recipe> -c deploy" |
||
+ | It might be interesting to explain the reasons why different methods are used if there are such reasons. If there's no special reason (it's just that there are several methods possible, it might be interesting to indicate it}} |
||
+ | </noinclude> |