This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1 Configure a wlan interface on hotspot mode[edit source]
- Configure the wlan interface for systemd/netword
Add the following rule on /lib/systemd/network/
cat /lib/systemd/network/hostapd.network [Match] Name=wlan0 [Network] Address=192.168.72.1/24 DHCPServer=yes IPForward=ipv4 IPMasquerade=yes
192.168.72.1/24: ip address affected to the hotspot device.
This configuration supports dhcpserver, ip forward and ip masquerade for this wlan interface: wlan0.
- Create the hotspot configuration by replacing /etc/hostapd.config content by the following lines
cat /etc/hostapd.conf interface=wlan0 driver=nl80211 # mode Wi-Fi (a = IEEE 802.11a, b = IEEE 802.11b, g = IEEE 802.11g) hw_mode=g ssid=STExampleNetwork channel=7 wmm_enabled=0 macaddr_acl=0 # Wi-Fi closed, need an authentication auth_algs=1 ignore_broadcast_ssid=0 wpa=2 wpa_passphrase=ExamplePassphareNetwork wpa_key_mgmt=WPA-PSK wpa_pairwise=TKIP rsn_pairwise=CCMP
STExampleNetwork is the visible name of the new wlan hotspot (SSID).
ExamplePassphareNetwork is the passphare associated to the wlan hotspot (SSID).
- Correct one issue with systemd-networkd.service which does not enable the wifi link by default
Add the highlighted line in /lib/systemd/system/hostapd.service file
cat /lib/systemd/system/hostapd.service [Service] ExecStartPre=/sbin/ip link set wlan0 up ExecStart=/usr/sbin/hostapd /etc/hostapd.conf -P /run/hostapd.pid -B
- Enable systemd service
systemctl enable hostapd
2 How to configure a gateway configuration[edit source]
For this example of configuration, the setup is:
- wlan0: wireless interface connected to SSID_NETWORK with DHCP
- eth0: ethernet interface with static IP which also have a DHCPserver on it
- forward of packet are activated between the two network interfaces.
2.1 Configure wireless interface[edit source]
cat /lib/systemd/network/wlan0.network
[Match]
Name=wlan0
[Network]
DHCP=ipv4
IPForward=ipv4
- IPForward
- permit to forward all network packet from wireless network to other network.
Configure wireless interface for SSID_NETWORK network:
mkdir -p /etc/wpa_supplicant/ echo "ctrl_interface=/var/run/wpa_supplicant" > /etc/wpa_supplicant/wpa_supplicant-wlan0.conf echo "eapol_version=1" >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf echo "ap_scan=1" >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf echo "fast_reauth=1" >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf echo "" >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf wpa_passphrase SSID_NETWORK PASSWORD_NETWORK >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf or wpa_passphrase SSID_NETWORK >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf
Where SSID_NETWORK PASSWORD_NETWORK correspond to the SSID and password of wireless network.
Enable the wireless configuration (to be take into account after reboot):
systemctl enable wpa_supplicant@wlan0.service systemctl restart systemd-networkd.service systemctl restart wpa_supplicant@wlan0.service