Difference between revisions of "How to build and use an SDK for QT"

[checked revision] [quality revision]
m
m (remove diff-style line change)
 

The OpenSTLinux distribution enables the generation of example images based on the QT framework (st-example-image-qt and, for ecosystem release ≥ v2.1.0 More info.png , st-example-image-qtwayland) for demonstration purposes, not for developing products.

This article provides information on how to create the SDK for building QT applications based on the above example images.

1 Prerequisites[edit]

Be able to rebuild an OpenSTLinux image

2 OpenSTLinux QT images and SDK[edit]

OpenSTLinux distribution provides two examples of images based on the QT framework:

  • st-example-image-qtwayland (requires 'openstlinux-weston' distro and ecosystem release ≥ v2.1.0 More info.png ): thanks to weston window management, QT applications are displayed in independent windows and can coexist on the same screen with other non-QT applications;

To build the images and the associated SDK, first install the OpenSTLinux distribution by following the procedure described in chapter Installing the OpenSTLinux distribution.

2.1 QT image and SDK with weston/wayland[edit]

The QT image and SDK use QTwayland back-end to run QT applications in independent windows managed by weston. This requires ecosystem release ≥ v2.1.0 More info.png .

Initialize the OpenEmbedded build environment for the openstlinux-weston distro:

 DISTRO=openstlinux-weston MACHINE=stm32mp1 source layers/meta-st/scripts/envsetup.sh

Read and accept EULA. Refer to Initializing the OpenEmbedded build environment for further details.

Then build the image and the SDK:

 bitbake st-example-image-qtwayland
 bitbake st-example-image-qtwayland -c populate_sdk

Refer to Generating your own Starter and Developer Packages and How to create an SDK for OpenSTLinux distribution for further details.

Note: the legacy command bitbake meta-toolchain-qt5 is not recommended because the resulting SDK would miss some target packages.

The image can be flashed on the target board as in Flashing the built image.

The generated SDK is available in the tmp-glibc/deploy/sdk/ folder. It can be installed as described in Run the SDK installation script, using the following command:

 ./tmp-glibc/deploy/sdk/st-example-image-qtwayland-openstlinux-weston-stm32mp1-x86_64-toolchain-3.1-snapshot.sh -y -d <working directory absolute path>/Developer-Package/SDK

2.2 QT image and SDK with EGLFS[edit]

The QT image and SDK use QT back-end to run single QT applications in full-screen mode.

Initialize the OpenEmbedded build environment for the openstlinux-eglfs distro:

 DISTRO=openstlinux-eglfs MACHINE=stm32mp1 source layers/meta-st/scripts/envsetup.sh

Read and accept EULA. Refer to Initializing the OpenEmbedded build environment for further details.

Then build the image and the SDK:

 bitbake st-example-image-qt
 bitbake st-example-image-qt -c populate_sdk

Refer to Generating your own Starter and Developer Packages and How to create an SDK for OpenSTLinux distribution for further details.

Note: the legacy command bitbake meta-toolchain-qt5 is not recommended because the resulting SDK would miss some target packages.

The image can be flashed on the target board as in Flashing the built image.

The generated SDK is available in the tmp-glibc/deploy/sdk/ folder. It can be installed as described in Run the SDK installation script, using the following command:

 ./tmp-glibc/deploy/sdk/st-example-image-qt-openstlinux-eglfs-stm32mp1-x86_64-toolchain-3.1-snapshot.sh -y -d <working directory absolute path>/Developer-Package/SDK

2.2.1 Selecting the display resolution and size in EGLFS[edit]

When using a display that accepts multiple resolutions, the preferred resolution can be specified by editing the board file /usr/share/qt5/cursor.json. For example, for an HDMI display, change the line

{ "name": "HDMI1", "mode": "1280x720" },

and enter one of the valid resolutions reported by the command

 modetest

If the current display resolution is higher than the resolution requested by the QT application, QT expands the application to run it in full screen. This can produce blurred images on the display and can impact the system performance.

The QT framework can be configured to use only one part of the overall display. For example, to use only an area of 400x300 pixels, add:

{ "name": "HDMI1", "mode": "1280x720", "size": "400x300" },

3 Configuring the QT framework[edit]

By default, QT internal data use 64 bits per pixel (16 bits for each R, G, B and A component). The performance can be slightly improved by forcing the QT framework to use 32 bits per pixel (8 bits for each component). This can be achieved by editing the file layers/meta-st/meta-st-openstlinux/recipes-qt/qt5/qtbase_git.bbappend before the build and replacing the line

-QT_CONFIG_FLAGS += " -no-sse2 -no-opengles3"
+

with

QT_CONFIG_FLAGS += " -no-sse2 -no-opengles3 -no-feature-raster-64bit"

Note: the above setup can produce visible artefacts and has to be evaluated on a case by case basis.

4 Building a QT application[edit]

Open the folder that contains the application, enable the QT SDK and compile the application:

 cd <path_of_app>
 . <install_path_sdk>/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
 qmake && make


The OpenSTLinux distribution enables the generation of example images based on the [[QT overview|QT framework]] ([[OpenSTLinux distribution#Images|st-example-image-qt]] and, for {{EcosystemRelease | revision=2.1.0 | range=and after}}, [[OpenSTLinux distribution#Images|st-example-image-qtwayland]]) for demonstration purposes, not for developing products.

This article provides information on how to create the [[SDK for OpenSTLinux distribution|SDK]] for building QT applications based on the above example images.

== Prerequisites ==

Be able to rebuild an OpenSTLinux image

== OpenSTLinux QT images and SDK ==

OpenSTLinux distribution provides two examples of images based on the [[QT overview|QT framework]]:

* [[OpenSTLinux distribution#Images|st-example-image-qtwayland]] (requires '[[OpenSTLinux distribution#Distros|openstlinux-weston]]' distro and {{EcosystemRelease | revision=2.1.0 | range=and after}}): thanks to weston window management, QT applications are displayed in independent windows and can coexist on the same screen with other non-QT applications;

* [[OpenSTLinux distribution#Images|st-example-image-qt]] (requires '[[OpenSTLinux distribution#Distros|openstlinux-eglfs]]' distro): only one QT application can access the screen. It is displayed in full-screen mode.

To build the images and the associated SDK, first install the OpenSTLinux distribution by following the procedure described in chapter [[STM32MP1 Distribution Package#Installing the OpenSTLinux distribution|Installing the OpenSTLinux distribution]].

=== QT image and SDK with weston/wayland ===

The QT image and SDK use QTwayland back-end to run QT applications in independent windows managed by weston. This requires {{EcosystemRelease | revision=2.1.0 | range=and after}}.

Initialize the OpenEmbedded build environment for the [[OpenSTLinux distribution#Distros|openstlinux-weston]] distro:

 {{PC$}} DISTRO=openstlinux-weston MACHINE=stm32mp1 source layers/meta-st/scripts/envsetup.sh

Read and accept EULA. Refer to [[STM32MP1 Distribution Package#Initializing the OpenEmbedded build environment|Initializing the OpenEmbedded build environment]] for further details.

Then build the image and the SDK:
 {{PC$}} bitbake st-example-image-qtwayland
 {{PC$}} bitbake st-example-image-qtwayland -c populate_sdk

Refer to [[STM32MP1 Distribution Package#Generating your own Starter and Developer Packages|Generating your own Starter and Developer Packages]] and [[How to create an SDK for OpenSTLinux distribution]] for further details.

'''Note:''' the legacy command '''bitbake meta-toolchain-qt5''' is not recommended because the resulting SDK would miss some target packages.

The image can be flashed on the target board as in [[STM32MP1 Distribution Package#Flashing the built image|Flashing the built image]].

The generated SDK is available in the '''tmp-glibc/deploy/sdk/''' folder. It can be installed as described in [[Install the SDK#Run the SDK installation script|Run the SDK installation script]], using the following command:

 {{PC$}} ./tmp-glibc/deploy/sdk/st-example-image-qtwayland-openstlinux-weston-stm32mp1-x86_64-toolchain-{{EcosystemRelease/Component | revision=2.0.0 | component=OpenEmbedded | name=short}}-snapshot.sh -y -d <working directory absolute path>/Developer-Package/SDK

=== QT image and SDK with EGLFS ===

The QT image and SDK use QT back-end to run single QT applications in full-screen mode.

Initialize the OpenEmbedded build environment for the [[OpenSTLinux distribution#Distros|openstlinux-eglfs]] distro:

 {{PC$}} DISTRO=openstlinux-eglfs MACHINE=stm32mp1 source layers/meta-st/scripts/envsetup.sh

Read and accept EULA. Refer to [[STM32MP1 Distribution Package#Initializing the OpenEmbedded build environment|Initializing the OpenEmbedded build environment]] for further details.

Then build the image and the SDK:
 {{PC$}} bitbake st-example-image-qt
 {{PC$}} bitbake st-example-image-qt -c populate_sdk

Refer to [[STM32MP1 Distribution Package#Generating your own Starter and Developer Packages|Generating your own Starter and Developer Packages]] and [[How to create an SDK for OpenSTLinux distribution]] for further details.

'''Note:''' the legacy command '''bitbake meta-toolchain-qt5''' is not recommended because the resulting SDK would miss some target packages.

The image can be flashed on the target board as in [[STM32MP1 Distribution Package#Flashing the built image|Flashing the built image]].

The generated SDK is available in the '''tmp-glibc/deploy/sdk/''' folder. It can be installed as described in [[Install the SDK#Run the SDK installation script|Run the SDK installation script]], using the following command:

 {{PC$}} ./tmp-glibc/deploy/sdk/st-example-image-qt-openstlinux-eglfs-stm32mp1-x86_64-toolchain-{{EcosystemRelease/Component | revision=2.0.0 | component=OpenEmbedded | name=short}}-snapshot.sh -y -d <working directory absolute path>/Developer-Package/SDK

==== Selecting the display resolution and size in EGLFS ====

When using a display that accepts multiple resolutions, the preferred resolution can be specified by editing the board file '''/usr/share/qt5/cursor.json'''.
For example, for an HDMI display, change the line
 { "name": "HDMI1", "mode": "1280x720" },
and enter one of the valid resolutions reported by the command
 {{Board$}} modetest

If the current display resolution is higher than the resolution requested by the QT application, QT expands the application to run it in full screen. This can produce blurred images on the display and can impact the system performance.

The QT framework can be configured to use only one part of the overall display. For example, to use only an area of 400x300 pixels, add:
 { "name": "HDMI1", "mode": "1280x720"{{HighlightParam|, "size": "400x300"}} },

== Configuring the QT framework ==

By default, QT internal data use 64 bits per pixel (16 bits for each R, G, B and A component).
The performance can be slightly improved by forcing the QT framework to use 32 bits per pixel (8 bits for each component).
This can be achieved by editing the file '''layers/meta-st/meta-st-openstlinux/recipes-qt/qt5/qtbase_git.bbappend''' before the build  -and replacing the lineQT_CONFIG_FLAGS += " -no-sse2 -no-opengles3" +withQT_CONFIG_FLAGS += " -no-sse2 -no-opengles3 {{HighlightParam|-no-feature-raster-64bit"

{{ReviewsComments|-- [[User:Lionel Vitte|Lionel Vitte]] ([[User talk:Lionel Vitte|talk]]) 17:55, 19November 2020 (CET)<br />You should explain more you are using the "diff" syntax. Afraid the user will try to find lines starting by a - and a + <br> NathalieS : I agree with Lionel}}}}"
'''Note:''' the above setup can produce visible artefacts and has to be evaluated on a case by case basis.

== Building a QT application ==

Open the folder that contains the application, enable the QT SDK and compile the application:

 {{PC$}} cd <path_of_app>

 {{PC$}} . <install_path_sdk>/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
 {{PC$}} qmake && make
<noinclude>

[[Category:QT framework]]
{{PublicationRequestId | 18172 | 2020-11-19|}}</noinclude>
Line 82: Line 82:
 
By default, QT internal data use 64 bits per pixel (16 bits for each R, G, B and A component).
 
By default, QT internal data use 64 bits per pixel (16 bits for each R, G, B and A component).
 
The performance can be slightly improved by forcing the QT framework to use 32 bits per pixel (8 bits for each component).
 
The performance can be slightly improved by forcing the QT framework to use 32 bits per pixel (8 bits for each component).
This can be achieved by editing the file '''layers/meta-st/meta-st-openstlinux/recipes-qt/qt5/qtbase_git.bbappend''' before the build
+
This can be achieved by editing the file '''layers/meta-st/meta-st-openstlinux/recipes-qt/qt5/qtbase_git.bbappend''' before the build and replacing the line
  -QT_CONFIG_FLAGS += " -no-sse2 -no-opengles3"
+
  QT_CONFIG_FLAGS += " -no-sse2 -no-opengles3"
  +QT_CONFIG_FLAGS += " -no-sse2 -no-opengles3 -no-feature-raster-64bit"
+
with
  +
  QT_CONFIG_FLAGS += " -no-sse2 -no-opengles3 {{HighlightParam|-no-feature-raster-64bit}}"
   
{{ReviewsComments|-- [[User:Lionel Vitte|Lionel Vitte]] ([[User talk:Lionel Vitte|talk]]) 17:55, 19November 2020 (CET)<br />You should explain more you are using the "diff" syntax. Afraid the user will try to find lines starting by a - and a + <br> NathalieS : I agree with Lionel}}
 
 
'''Note:''' the above setup can produce visible artefacts and has to be evaluated on a case by case basis.
 
'''Note:''' the above setup can produce visible artefacts and has to be evaluated on a case by case basis.