Last edited 3 years ago

FMC device tree configuration


Template:ArticleMainWriter Template:ArticleApprovedVersion


1 Article purpose[edit source]

This article explains how to configure the FMC internal peripheral when it is assigned to the Linux® OS. In that case, it is controlled by the MTD framework.

The configuration is performed using the device tree mechanism that provides a hardware description of the FMC peripheral, used by the STM32 FMC Linux driver and by the MTD framework.

2 DT bindings documentation[edit source]

The FMC device tree bindings are composed of:

  • generic MTD nand bindings [1].
  • FMC driver bindings documented in Documentation/devicetree/bindings/mtd/stm32-fmc2-nand.txt.

3 DT configuration[edit source]

This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device tree file split.

STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.

3.1 DT configuration (STM32 level)[edit source]

The FMC peripheral node is located in stm32mp157c.dtsi[2] file.

   fmc: nand-controller@58002000 {                           Comments
       compatible = "st,stm32mp15-fmc2";
       reg = <0x58002000 0x1000>,                            --> First region contains the register location
             <0x80000000 0x1000>,                            --> Régions 2 to 4 respectively contain the data, command and address space for CS0
             <0x88010000 0x1000>,                            
             <0x88020000 0x1000>,                            
             <0x81000000 0x1000>,                            --> Régions 5 to 7 contain the same areas for CS1
             <0x89010000 0x1000>,                            
             <0x89020000 0x1000>;                            
       interrupts = <GIC_SPI 48 IRQ_TYPE_LEVEL_HIGH>;        --> The interrupt number used
       dmas = <&mdma1 20 0x10 0x12000A02 0x0 0x0 0>,         --> DMA specifiers [3]
              <&mdma1 20 0x10 0x12000A08 0x0 0x0 0>,
              <&mdma1 21 0x10 0x12000A0A 0x0 0x0 0>;
       dma-names = "tx", "rx", "ecc";
       clocks = <&rcc FMC_K>;                  
       resets = <&rcc FMC_R>;                           
       status = "disabled";
   };
Warning white.png Warning
This device tree part related to the STM32 should be kept as is, customer should not modify it.

3.2 DT configuration (board level)[edit source]

The FMC peripheral may connect to one SLC NAND Flash memory (with a maximum of 2 dies per package).

   &fmc {                                                    Comments     
       pinctrl-names = "default", "sleep";                   --> For pinctrl configuration, please refer to Pinctrl device tree configuration
       pinctrl-0 = <&fmc2_pins_a>;
       pinctrl-1 = <&fmc2_sleep_pins_a>;
       status = "okay";                                      --> Enable the node
       #address-cells = <1>;
       #size-cells = <0>;
nand: nand@0 { reg = <0>; --> Describe the CS line assigned to the NAND chip nand-on-flash-bbt; --> Store the bad block table on NAND Flash memory nand-ecc-strength = <8>; --> Number of bits to correct per ECC step nand-ecc-step-size = <512>; --> Number of data bytes that are covered by a single ECC step #address-cells = <1>; #size-cells = <1>; }; };

The supported ECC strength and step size are:

  • nand-ecc-strength = <1>, nand-ecc-step-size = <512> (HAMMING).
  • nand-ecc-strength = <4>, nand-ecc-step-size = <512> (BCH4).
  • nand-ecc-strength = <8>, nand-ecc-step-size = <512> (BCH8).

3.3 DT configuration examples[edit source]

The below example shows how to configure the FMC controller when a SLC 8-bit NAND Flash memory device is connected (ECC requirement: 8 bits / 512 bytes).

   &fmc {                                              
       pinctrl-names = "default", "sleep";                  
       pinctrl-0 = <&fmc2_pins_a>;
       pinctrl-1 = <&fmc2_sleep_pins_a>;
       status = "okay";                                      
       #address-cells = <1>;
       #size-cells = <0>;
nand: nand@0 { reg = <0>; nand-on-flash-bbt; #address-cells = <1>; #size-cells = <1>;
partition@0 { ... }; }; };

The below example shows how to configure the FMC controller when a SLC 8-bit NAND Flash memory device is connected (ECC requirement: 4 bits / 512 bytes).

   &fmc {                        
       pinctrl-names = "default", "sleep";            
       pinctrl-0 = <&fmc2_pins_a>;
       pinctrl-1 = <&fmc2_sleep_pins_a>;
       status = "okay";                                      
       #address-cells = <1>;
       #size-cells = <0>;
nand: nand@0 { reg = <0>; nand-on-flash-bbt; nand-ecc-strength = <4>; nand-ecc-step-size = <512>; #address-cells = <1>; #size-cells = <1>;
partition@0 { ... }; }; };

4 How to configure the DT using STM32CubeMX[edit source]

The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.

5 References[edit source]

Please refer to the following links for full description: