Difference between revisions of "FMC device tree configuration"
[checked revision] | [quality revision] |
m
|
m
|
Contents
1 For ecosystem release ≥ v2.1.0
[edit]
1.1 Article purpose[edit]
This article explains how to configure the FMC internal peripheral when it is assigned to the Linux® OS. In that case, the FMC NAND Flash controller is controlled by the MTD framework.
The configuration is performed using the device tree mechanism that provides a hardware description of the FMC peripheral, used by the STM32 FMC Linux drivers and by the MTD framework.
1.2 DT bindings documentation[edit]
The FMC device tree bindings are composed of:
- generic MTD NAND bindings [1].
- FMC NAND Flash controller driver bindings [2].
- FMC external bus interface driver bindings [3].
1.3 DT configuration[edit]
This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device tree file split.
STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.
1.3.1 DT configuration (STM32 level)[edit]
The FMC peripheral node is located in stm32mp151.dtsi[4] file.
fmc: memory-controller@58002000 { Comments #address-cells = <2>; #size-cells = <1>; compatible = "st,stm32mp1-fmc2-ebi"; reg = <0x58002000 0x1000>; --> This region contains the register location clocks = <&rcc FMC_K>; resets = <&rcc FMC_R>; status = "disabled";
ranges = <0 0 0x60000000 0x04000000>, /* EBI CS 1 */ --> External bus interface region is used to address up to four external devices <1 0 0x64000000 0x04000000>, /* EBI CS 2 */ <2 0 0x68000000 0x04000000>, /* EBI CS 3 */ <3 0 0x6c000000 0x04000000>, /* EBI CS 4 */ <4 0 0x80000000 0x10000000>; /* NAND */ --> NAND Flash controller region is used to address NAND Flash memory devices
nand-controller@4,0 { #address-cells = <1>; #size-cells = <0>; compatible = "st,stm32mp1-fmc2-nfc"; reg = <4 0x00000000 0x1000>, --> Regions 1 to 3 respectively contain the data, command and address space for CS0 <4 0x08010000 0x1000>, <4 0x08020000 0x1000>, <4 0x01000000 0x1000>, --> Regions 4 to 6 contain the same areas for CS1 <4 0x09010000 0x1000>, <4 0x09020000 0x1000>; interrupts = <GIC_SPI 48 IRQ_TYPE_LEVEL_HIGH>; --> The interrupt number used dmas = <&mdma1 20 0x2 0x12000a02 0x0 0x0 0x0>, --> DMA specifiers [5] <&mdma1 20 0x2 0x12000a08 0x0 0x0 0x0>, <&mdma1 21 0x2 0x12000a0a 0x0 0x0 0x0>; dma-names = "tx", "rx", "ecc"; status = "disabled"; }; };
![]() |
This device tree part related to the STM32 should be kept as is, customer should not modify it. |
1.3.2 DT configuration of the external bus interface controller (board level)[edit]
The FMC external bus interface controller may connect up to four external devices.
&fmc { Comments pinctrl-names = "default", "sleep"; --> For pinctrl configuration, please refer to Pinctrl device tree configuration pinctrl-0 = <&fmc2_pins_b>; pinctrl-1 = <&fmc2_sleep_pins_b>; status = "okay"; --> Enable the node
ksz8851: ks8851mll@1,0 { compatible = "micrel,ks8851-mll"; --> Configure the external device reg = <1 0x0 0x2>, <1 0x2 0x20000>; interrupt-parent = <&gpioc>; interrupts = <3 IRQ_TYPE_LEVEL_LOW>; bank-width = <2>;
st,fmc2-ebi-cs-mux-enable; --> Configure the transactions with the external device st,fmc2-ebi-cs-transaction-type = <4>; st,fmc2-ebi-cs-buswidth = <16>; st,fmc2-ebi-cs-address-setup-ns = <5>; st,fmc2-ebi-cs-address-hold-ns = <5>; st,fmc2-ebi-cs-bus-turnaround-ns = <5>; st,fmc2-ebi-cs-data-setup-ns = <45>; st,fmc2-ebi-cs-data-hold-ns = <1>; }; };
1.3.3 DT configuration of the NAND Flash controller (board level)[edit]
The FMC NAND Flash controller may connect to one SLC NAND Flash memory (with a maximum of 2 dies per package).
&fmc { Comments pinctrl-names = "default", "sleep"; --> For pinctrl configuration, please refer to Pinctrl device tree configuration pinctrl-0 = <&fmc2_pins_a>; pinctrl-1 = <&fmc2_sleep_pins_a>; status = "okay"; --> Enable the node
nand-controller@4,0 { status = "okay"; --> Enable the NAND controller node
nand@0 { reg = <0>; --> Describe the CS line assigned to the NAND chip nand-on-flash-bbt; --> Store the bad block table on NAND Flash memory nand-ecc-strength = <8>; --> Number of bits to correct per ECC step nand-ecc-step-size = <512>; --> Number of data bytes that are covered by a single ECC step #address-cells = <1>; #size-cells = <1>; }; }; };
The supported ECC strength and step size are:
- nand-ecc-strength = <1>, nand-ecc-step-size = <512> (HAMMING).
- nand-ecc-strength = <4>, nand-ecc-step-size = <512> (BCH4).
- nand-ecc-strength = <8>, nand-ecc-step-size = <512> (BCH8).
1.3.4 DT configuration examples[edit]
The below example shows how to configure the FMC NAND Flash controller when a SLC 8-bit NAND Flash memory device is connected (ECC requirement: 8 bits / 512 bytes).
&fmc { pinctrl-names = "default", "sleep"; pinctrl-0 = <&fmc2_pins_a>; pinctrl-1 = <&fmc2_sleep_pins_a>; status = "okay";
nand-controller@4,0 { status = "okay";
nand: nand@0 { reg = <0>; nand-on-flash-bbt; #address-cells = <1>; #size-cells = <1>;
partition@0 { ... }; }; }; };
The below example shows how to configure the FMC NAND Flash controller when a SLC 8-bit NAND Flash memory device is connected (ECC requirement: 4 bits / 512 bytes).
&fmc { pinctrl-names = "default", "sleep"; pinctrl-0 = <&fmc2_pins_a>; pinctrl-1 = <&fmc2_sleep_pins_a>; status = "okay";
nand-controller@4,0 { status = "okay";
nand: nand@0 { reg = <0>; nand-on-flash-bbt; nand-ecc-strength = <4>; nand-ecc-step-size = <512>; #address-cells = <1>; #size-cells = <1>;
partition@0 { ... }; }; }; };
1.4 How to configure the DT using STM32CubeMX[edit]
The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.
1.5 References[edit]
Please refer to the following links for full description:
- ↑ Documentation/devicetree/bindings/mtd/nand-controller.yaml (v5.4-stm32mp-r2)
- ↑ Documentation/devicetree/bindings/mtd/st,stm32-fmc2-nand.yaml (v5.4-stm32mp-r2)
- ↑ Documentation/devicetree/bindings/memory-controllers/st,stm32-fmc2-ebi.yaml (v5.4-stm32mp-r2)
- ↑ arch/arm/boot/dts/stm32mp151.dtsi (v5.4-stm32mp-r2)
- ↑ Documentation/devicetree/bindings/dma/stm32-mdma.txt (v5.4-stm32mp-r2)
2 For ecosystem release v2.0.0
[edit]
2.1 Article purpose[edit]
This article explains how to configure the FMC internal peripheral when it is assigned to the Linux® OS. In that case, it is controlled by the MTD framework.
The configuration is performed using the device tree mechanism that provides a hardware description of the FMC peripheral, used by the STM32 FMC Linux driver and by the MTD framework.
2.2 DT bindings documentation[edit]
The FMC device tree bindings are composed of:
- generic MTD nand bindings [1].
- FMC driver bindings [2].
2.3 DT configuration[edit]
This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device tree file split.
STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.
2.3.1 DT configuration (STM32 level)[edit]
The FMC peripheral node is located in stm32mp151.dtsi[3] file.
fmc: nand-controller@58002000 { Comments compatible = "st,stm32mp15-fmc2"; reg = <0x58002000 0x1000>, --> First region contains the register location <0x80000000 0x1000>, --> Regions 2 to 4 respectively contain the data, command and address space for CS0 <0x88010000 0x1000>, <0x88020000 0x1000>, <0x81000000 0x1000>, --> Regions 5 to 7 contain the same areas for CS1 <0x89010000 0x1000>, <0x89020000 0x1000>; interrupts = <GIC_SPI 48 IRQ_TYPE_LEVEL_HIGH>; --> The interrupt number used dmas = <&mdma1 20 0x10 0x12000A02 0x0 0x0 0>, --> DMA specifiers [4] <&mdma1 20 0x10 0x12000A08 0x0 0x0 0>, <&mdma1 21 0x10 0x12000A0A 0x0 0x0 0>; dma-names = "tx", "rx", "ecc"; clocks = <&rcc FMC_K>; resets = <&rcc FMC_R>; status = "disabled"; };
![]() |
This device tree part related to the STM32 should be kept as is, customer should not modify it. |
2.3.2 DT configuration (board level)[edit]
The FMC peripheral may connect to one SLC NAND Flash memory (with a maximum of 2 dies per package).
&fmc { Comments pinctrl-names = "default", "sleep"; --> For pinctrl configuration, please refer to Pinctrl device tree configuration pinctrl-0 = <&fmc2_pins_a>; pinctrl-1 = <&fmc2_sleep_pins_a>; status = "okay"; --> Enable the node #address-cells = <1>; #size-cells = <0>;
nand: nand@0 { reg = <0>; --> Describe the CS line assigned to the NAND chip nand-on-flash-bbt; --> Store the bad block table on NAND Flash memory nand-ecc-strength = <8>; --> Number of bits to correct per ECC step nand-ecc-step-size = <512>; --> Number of data bytes that are covered by a single ECC step #address-cells = <1>; #size-cells = <1>; }; };
The supported ECC strength and step size are:
- nand-ecc-strength = <1>, nand-ecc-step-size = <512> (HAMMING).
- nand-ecc-strength = <4>, nand-ecc-step-size = <512> (BCH4).
- nand-ecc-strength = <8>, nand-ecc-step-size = <512> (BCH8).
2.3.3 DT configuration examples[edit]
The below example shows how to configure the FMC controller when a SLC 8-bit NAND Flash memory device is connected (ECC requirement: 8 bits / 512 bytes).
&fmc { pinctrl-names = "default", "sleep"; pinctrl-0 = <&fmc2_pins_a>; pinctrl-1 = <&fmc2_sleep_pins_a>; status = "okay"; #address-cells = <1>; #size-cells = <0>;
nand: nand@0 { reg = <0>; nand-on-flash-bbt; #address-cells = <1>; #size-cells = <1>;
partition@0 { ... }; }; };
The below example shows how to configure the FMC controller when a SLC 8-bit NAND Flash memory device is connected (ECC requirement: 4 bits / 512 bytes).
&fmc { pinctrl-names = "default", "sleep"; pinctrl-0 = <&fmc2_pins_a>; pinctrl-1 = <&fmc2_sleep_pins_a>; status = "okay"; #address-cells = <1>; #size-cells = <0>;
nand: nand@0 { reg = <0>; nand-on-flash-bbt; nand-ecc-strength = <4>; nand-ecc-step-size = <512>; #address-cells = <1>; #size-cells = <1>;
partition@0 { ... }; }; };
2.4 How to configure the DT using STM32CubeMX[edit]
The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.
2.5 References[edit]
Please refer to the following links for full description:
==For {{EcosystemRelease | revision=2.1.0 | range=and after}}= == Article purpose === === Article purpose === This article explains how to configure the [[FMC internal peripheral|'''FMC''' internal peripheral]] when it is assigned to the Linux<sup>®</sup> OS. In that case, the FMC NAND Flash controller is controlled by the [[MTD overview|MTD framework]]. The configuration is performed using the [[Device tree|device tree]] mechanism that provides a hardware description of the FMC peripheral, used by the STM32 FMC Linux drivers and by the MTD framework. === DT bindings documentation === The FMC device tree bindings are composed of: * generic MTD NAND bindings <ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/mtd/nand-controller.yaml | | 5.4-stm32mp-r2}}</ref>. * FMC NAND Flash controller driver bindings <ref> {{CodeSource | Linux kernel | Documentation/devicetree/bindings/mtd/st,stm32-fmc2-nand.yaml | | 5.4-stm32mp-r2}} </ref>. * FMC external bus interface driver bindings <ref> {{CodeSource | Linux kernel | Documentation/devicetree/bindings/memory-controllers/st,stm32-fmc2-ebi.yaml | | 5.4-stm32mp-r2}} </ref>. === DT configuration === This hardware description is a combination of the '''STM32 microprocessor''' device tree files (''.dtsi'' extension) and '''board''' device tree files (''.dts'' extension). See the [[Device tree]] for an explanation of the device tree file split. '''STM32CubeMX''' can be used to generate the board device tree. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX|How to configure the DT using STM32CubeMX]] for more details. ====DT configuration (STM32 level) ==== The FMC peripheral node is located in ''stm32mp151.dtsi''<ref>{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp151.dtsi | | 5.4-stm32mp-r2}}</ref> file. fmc: memory-controller@58002000 { {{highlight|Comments}} #address-cells = <2>; #size-cells = <1>; compatible = "st,stm32mp1-fmc2-ebi"; reg = <0x58002000 0x1000>; {{highlight|--> This region contains the register location}} clocks = <&rcc FMC_K>; resets = <&rcc FMC_R>; status = "disabled";<br> ranges = <0 0 0x60000000 0x04000000>, /* EBI CS 1 */ {{highlight|--> External bus interface region is used to address up to four external devices}}<1 0 0x64000000 0x04000000>, /* EBI CS 2 */<2 0 0x68000000 0x04000000>, /* EBI CS 3 */<3 0 0x6c000000 0x04000000>, /* EBI CS 4 */<4 0 0x80000000 0x10000000>; /* NAND */ {{highlight|--> NAND Flash controller region is used to address NAND Flash memory devices}}<br> nand-controller@4,0 { #address-cells = <1>; #size-cells = <0>; compatible = "st,stm32mp1-fmc2-nfc"; reg = <4 0x00000000 0x1000>, {{highlight|--> Regions 1 to 3 respectively contain the data, command and address space for CS0}}<4 0x08010000 0x1000>,<4 0x08020000 0x1000>,<4 0x01000000 0x1000>, {{highlight|--> Regions 4 to 6 contain the same areas for CS1}}<4 0x09010000 0x1000>,<4 0x09020000 0x1000>; interrupts = <GIC_SPI 48 IRQ_TYPE_LEVEL_HIGH>; {{highlight|--> The interrupt number used}} dmas = <&mdma1 20 0x2 0x12000a02 0x0 0x0 0x0>, {{highlight|--> DMA specifiers <ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/dma/stm32-mdma.txt | | 5.4-stm32mp-r2}}</ref>}}<&mdma1 20 0x2 0x12000a08 0x0 0x0 0x0>,<&mdma1 21 0x2 0x12000a0a 0x0 0x0 0x0>; dma-names = "tx", "rx", "ecc"; status = "disabled"; }; }; {{Warning|This device tree part related to the STM32 should be kept as is, customer should not modify it.}} ==== DT configuration of the external bus interface controller (board level) ==== The FMC external bus interface controller may connect up to four external devices. &fmc { {{highlight|Comments}} pinctrl-names = "default", "sleep"; {{highlight|--> For pinctrl configuration, please refer to [[Pinctrl device tree configuration]]}} pinctrl-0 = <&fmc2_pins_b>; pinctrl-1 = <&fmc2_sleep_pins_b>; status = "okay"; {{highlight|--> Enable the node}}<br> ksz8851: ks8851mll@1,0 { compatible = "micrel,ks8851-mll"; {{highlight|--> Configure the external device}} reg = <1 0x0 0x2>, <1 0x2 0x20000>; interrupt-parent = <&gpioc>; interrupts = <3 IRQ_TYPE_LEVEL_LOW>; bank-width = <2>;<br> st,fmc2-ebi-cs-mux-enable; {{highlight|--> Configure the transactions with the external device}} st,fmc2-ebi-cs-transaction-type = <4>; st,fmc2-ebi-cs-buswidth = <16>; st,fmc2-ebi-cs-address-setup-ns = <5>; st,fmc2-ebi-cs-address-hold-ns = <5>; st,fmc2-ebi-cs-bus-turnaround-ns = <5>; st,fmc2-ebi-cs-data-setup-ns = <45>; st,fmc2-ebi-cs-data-hold-ns = <1>; }; }; ==== DT configuration of the NAND Flash controller (board level) ==== The FMC NAND Flash controller may connect to one SLC NAND Flash memory (with a maximum of 2 dies per package). &fmc { {{highlight|Comments}} pinctrl-names = "default", "sleep"; {{highlight|--> For pinctrl configuration, please refer to [[Pinctrl device tree configuration]]}} pinctrl-0 = <&fmc2_pins_a>; pinctrl-1 = <&fmc2_sleep_pins_a>; status = "okay"; {{highlight|--> Enable the node}}<br> nand-controller@4,0 { status = "okay"; {{highlight|--> Enable the NAND controller node}}<br> nand@0 { reg = <0>; {{highlight|--> Describe the CS line assigned to the NAND chip}} nand-on-flash-bbt; {{highlight|--> Store the bad block table on NAND Flash memory}} nand-ecc-strength = <8>; {{highlight|--> Number of bits to correct per ECC step}} nand-ecc-step-size = <512>; {{highlight|--> Number of data bytes that are covered by a single ECC step}} #address-cells = <1>; #size-cells = <1>; }; }; }; The supported ECC strength and step size are: * nand-ecc-strength = <1>, nand-ecc-step-size = <512> (HAMMING). * nand-ecc-strength = <4>, nand-ecc-step-size = <512> (BCH4). * nand-ecc-strength = <8>, nand-ecc-step-size = <512> (BCH8). ==== DT configuration examples ==== The below example shows how to configure the FMC NAND Flash controller when a SLC 8-bit NAND Flash memory device is connected (ECC requirement: 8 bits / 512 bytes). &fmc { pinctrl-names = "default", "sleep"; pinctrl-0 = <&fmc2_pins_a>; pinctrl-1 = <&fmc2_sleep_pins_a>; status = "okay"; <br> nand-controller@4,0 { status = "okay"; <br> nand: nand@0 { reg = <0>; nand-on-flash-bbt; #address-cells = <1>; #size-cells = <1>;<br> partition@0 { ... }; }; }; }; The below example shows how to configure the FMC NAND Flash controller when a SLC 8-bit NAND Flash memory device is connected (ECC requirement: 4 bits / 512 bytes). &fmc { pinctrl-names = "default", "sleep"; pinctrl-0 = <&fmc2_pins_a>; pinctrl-1 = <&fmc2_sleep_pins_a>; status = "okay";<br> nand-controller@4,0 { status = "okay"; <br> nand: nand@0 { reg = <0>; nand-on-flash-bbt; nand-ecc-strength = <4>; nand-ecc-step-size = <512>; #address-cells = <1>; #size-cells = <1>;<br> partition@0 { ... }; }; }; }; ===How to configure the DT using STM32CubeMX=== The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree#STM32|platform configuration device tree]] files.<br /> The STM32CubeMX may not support all the properties described in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to [[STM32CubeMX]] user manual for further information. ===References=== Please refer to the following links for full description: <references /> <div class="mw-collapsible mw-collapsed"> ==For {{EcosystemRelease | revision=2.0.0}}== <div class="mw-collapsible-content"> === Article purpose === This article explains how to configure the [[FMC internal peripheral|'''FMC''' internal peripheral]] when it is assigned to the Linux<sup>®</sup> OS. In that case, it is controlled by the [[MTD overview|MTD framework]]. The configuration is performed using the [[Device tree|device tree]] mechanism that provides a hardware description of the FMC peripheral, used by the STM32 FMC Linux driver and by the MTD framework. === DT bindings documentation === The FMC device tree bindings are composed of: * generic MTD nand bindings <ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/mtd/nand-controller.yaml | | 5.4-stm32mp-r1}}</ref>. * FMC driver bindings <ref> {{CodeSource | Linux kernel | Documentation/devicetree/bindings/mtd/stm32-fmc2-nand.txt | | 5.4-stm32mp-r1}} </ref>. === DT configuration === This hardware description is a combination of the '''STM32 microprocessor''' device tree files (''.dtsi'' extension) and '''board''' device tree files (''.dts'' extension). See the [[Device tree]] for an explanation of the device tree file split. '''STM32CubeMX''' can be used to generate the board device tree. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX|How to configure the DT using STM32CubeMX]] for more details. ====DT configuration (STM32 level) ==== The FMC peripheral node is located in ''stm32mp151.dtsi''<ref>{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp151.dtsi | | 5.4-stm32mp-r1}}</ref> file. fmc: nand-controller@58002000 { {{highlight|Comments}} compatible = "st,stm32mp15-fmc2"; reg = <0x58002000 0x1000>, {{highlight|--> First region contains the register location}}<0x80000000 0x1000>, {{highlight|--> Regions 2 to 4 respectively contain the data, command and address space for CS0}}<0x88010000 0x1000>, <0x88020000 0x1000>, <0x81000000 0x1000>, {{highlight|--> Regions 5 to 7 contain the same areas for CS1}}<0x89010000 0x1000>, <0x89020000 0x1000>; interrupts = <GIC_SPI 48 IRQ_TYPE_LEVEL_HIGH>; {{highlight|--> The interrupt number used}} dmas = <&mdma1 20 0x10 0x12000A02 0x0 0x0 0>, {{highlight|--> DMA specifiers <ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/dma/stm32-mdma.txt | | 5.4-stm32mp-r1}}</ref>}}<&mdma1 20 0x10 0x12000A08 0x0 0x0 0>,<&mdma1 21 0x10 0x12000A0A 0x0 0x0 0>; dma-names = "tx", "rx", "ecc"; clocks = <&rcc FMC_K>; resets = <&rcc FMC_R>; status = "disabled"; }; {{Warning|This device tree part related to the STM32 should be kept as is, customer should not modify it.}} ==== DT configuration (board level) ==== The FMC peripheral may connect to one SLC NAND Flash memory (with a maximum of 2 dies per package). &fmc { {{highlight|Comments}} pinctrl-names = "default", "sleep"; {{highlight|--> For pinctrl configuration, please refer to [[Pinctrl device tree configuration]]}} pinctrl-0 = <&fmc2_pins_a>; pinctrl-1 = <&fmc2_sleep_pins_a>; status = "okay"; {{highlight|--> Enable the node}} #address-cells = <1>; #size-cells = <0>;<br> nand: nand@0 { reg = <0>; {{highlight|--> Describe the CS line assigned to the NAND chip}} nand-on-flash-bbt; {{highlight|--> Store the bad block table on NAND Flash memory}} nand-ecc-strength = <8>; {{highlight|--> Number of bits to correct per ECC step}} nand-ecc-step-size = <512>; {{highlight|--> Number of data bytes that are covered by a single ECC step}} #address-cells = <1>; #size-cells = <1>; }; }; The supported ECC strength and step size are: * nand-ecc-strength = <1>, nand-ecc-step-size = <512> (HAMMING). * nand-ecc-strength = <4>, nand-ecc-step-size = <512> (BCH4). * nand-ecc-strength = <8>, nand-ecc-step-size = <512> (BCH8). ==== DT configuration examples ==== The below example shows how to configure the FMC controller when a SLC 8-bit NAND Flash memory device is connected (ECC requirement: 8 bits / 512 bytes). &fmc { pinctrl-names = "default", "sleep"; pinctrl-0 = <&fmc2_pins_a>; pinctrl-1 = <&fmc2_sleep_pins_a>; status = "okay"; #address-cells = <1>; #size-cells = <0>;<br> nand: nand@0 { reg = <0>; nand-on-flash-bbt; #address-cells = <1>; #size-cells = <1>;<br> partition@0 { ... }; }; }; The below example shows how to configure the FMC controller when a SLC 8-bit NAND Flash memory device is connected (ECC requirement: 4 bits / 512 bytes). &fmc { pinctrl-names = "default", "sleep"; pinctrl-0 = <&fmc2_pins_a>; pinctrl-1 = <&fmc2_sleep_pins_a>; status = "okay"; #address-cells = <1>; #size-cells = <0>;<br> nand: nand@0 { reg = <0>; nand-on-flash-bbt; nand-ecc-strength = <4>; nand-ecc-step-size = <512>; #address-cells = <1>; #size-cells = <1>;<br> partition@0 { ... }; }; }; ===How to configure the DT using STM32CubeMX=== The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree#STM32|platform configuration device tree]] files.<br /> The STM32CubeMX may not support all the properties described in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to [[STM32CubeMX]] user manual for further information. ===References=== Please refer to the following links for full description: <references /> </div></div> <noinclude> {{ArticleBasedOnModel | Peripheral or framework device tree configuration model}} [[Category:Device tree configuration]] [[Category:Mass storage]]</noinclude>
Line 1: | Line 1: | ||
− | =For {{EcosystemRelease | revision=2.1.0 | range=and after}}= |
+ |
==For {{EcosystemRelease | revision=2.1.0 | range=and after}}== |
− | == Article purpose == |
+ |
=== Article purpose === |
This article explains how to configure the [[FMC internal peripheral|'''FMC''' internal peripheral]] when it is assigned to the Linux<sup>®</sup> OS. In that case, the FMC NAND Flash controller is controlled by the [[MTD overview|MTD framework]]. |
This article explains how to configure the [[FMC internal peripheral|'''FMC''' internal peripheral]] when it is assigned to the Linux<sup>®</sup> OS. In that case, the FMC NAND Flash controller is controlled by the [[MTD overview|MTD framework]]. |
||
The configuration is performed using the [[Device tree|device tree]] mechanism that provides a hardware description of the FMC peripheral, used by the STM32 FMC Linux drivers and by the MTD framework. |
The configuration is performed using the [[Device tree|device tree]] mechanism that provides a hardware description of the FMC peripheral, used by the STM32 FMC Linux drivers and by the MTD framework. |
||
− | == DT bindings documentation == |
+ |
=== DT bindings documentation === |
The FMC device tree bindings are composed of: |
The FMC device tree bindings are composed of: |
||
Line 15: | Line 15: | ||
* FMC external bus interface driver bindings <ref> {{CodeSource | Linux kernel | Documentation/devicetree/bindings/memory-controllers/st,stm32-fmc2-ebi.yaml | | 5.4-stm32mp-r2}} </ref>. |
* FMC external bus interface driver bindings <ref> {{CodeSource | Linux kernel | Documentation/devicetree/bindings/memory-controllers/st,stm32-fmc2-ebi.yaml | | 5.4-stm32mp-r2}} </ref>. |
||
− | == DT configuration == |
+ |
=== DT configuration === |
This hardware description is a combination of the '''STM32 microprocessor''' device tree files (''.dtsi'' extension) and '''board''' device tree files (''.dts'' extension). See the [[Device tree]] for an explanation of the device tree file split. |
This hardware description is a combination of the '''STM32 microprocessor''' device tree files (''.dtsi'' extension) and '''board''' device tree files (''.dts'' extension). See the [[Device tree]] for an explanation of the device tree file split. |
||
'''STM32CubeMX''' can be used to generate the board device tree. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX|How to configure the DT using STM32CubeMX]] for more details. |
'''STM32CubeMX''' can be used to generate the board device tree. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX|How to configure the DT using STM32CubeMX]] for more details. |
||
− | ===DT configuration (STM32 level) === |
+ |
====DT configuration (STM32 level) ==== |
The FMC peripheral node is located in ''stm32mp151.dtsi''<ref>{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp151.dtsi | | 5.4-stm32mp-r2}}</ref> file. |
The FMC peripheral node is located in ''stm32mp151.dtsi''<ref>{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp151.dtsi | | 5.4-stm32mp-r2}}</ref> file. |
||
Line 57: | Line 57: | ||
{{Warning|This device tree part related to the STM32 should be kept as is, customer should not modify it.}} |
{{Warning|This device tree part related to the STM32 should be kept as is, customer should not modify it.}} |
||
− | === DT configuration of the external bus interface controller (board level) === |
+ |
==== DT configuration of the external bus interface controller (board level) ==== |
The FMC external bus interface controller may connect up to four external devices. |
The FMC external bus interface controller may connect up to four external devices. |
||
Line 82: | Line 82: | ||
}; |
}; |
||
− | === DT configuration of the NAND Flash controller (board level) === |
+ |
==== DT configuration of the NAND Flash controller (board level) ==== |
The FMC NAND Flash controller may connect to one SLC NAND Flash memory (with a maximum of 2 dies per package). |
The FMC NAND Flash controller may connect to one SLC NAND Flash memory (with a maximum of 2 dies per package). |
||
Line 108: | Line 108: | ||
* nand-ecc-strength = <8>, nand-ecc-step-size = <512> (BCH8). |
* nand-ecc-strength = <8>, nand-ecc-step-size = <512> (BCH8). |
||
− | === DT configuration examples === |
+ |
==== DT configuration examples ==== |
The below example shows how to configure the FMC NAND Flash controller when a SLC 8-bit NAND Flash memory device is connected (ECC requirement: 8 bits / 512 bytes). |
The below example shows how to configure the FMC NAND Flash controller when a SLC 8-bit NAND Flash memory device is connected (ECC requirement: 8 bits / 512 bytes). |
||
Line 153: | Line 153: | ||
}; |
}; |
||
− | ==How to configure the DT using STM32CubeMX== |
+ |
===How to configure the DT using STM32CubeMX=== |
The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree#STM32|platform configuration device tree]] files.<br /> |
The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree#STM32|platform configuration device tree]] files.<br /> |
||
The STM32CubeMX may not support all the properties described in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to [[STM32CubeMX]] user manual for further information. |
The STM32CubeMX may not support all the properties described in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to [[STM32CubeMX]] user manual for further information. |
||
− | ==References== |
+ |
===References=== |
Please refer to the following links for full description: |
Please refer to the following links for full description: |
||
Line 164: | Line 164: | ||
<div class="mw-collapsible mw-collapsed"> |
<div class="mw-collapsible mw-collapsed"> |
||
− | =For {{EcosystemRelease | revision=2.0.0}}= |
+ |
==For {{EcosystemRelease | revision=2.0.0}}== |
<div class="mw-collapsible-content"> |
<div class="mw-collapsible-content"> |
||
− | == Article purpose == |
+ |
=== Article purpose === |
This article explains how to configure the [[FMC internal peripheral|'''FMC''' internal peripheral]] when it is assigned to the Linux<sup>®</sup> OS. In that case, it is controlled by the [[MTD overview|MTD framework]]. |
This article explains how to configure the [[FMC internal peripheral|'''FMC''' internal peripheral]] when it is assigned to the Linux<sup>®</sup> OS. In that case, it is controlled by the [[MTD overview|MTD framework]]. |
||
The configuration is performed using the [[Device tree|device tree]] mechanism that provides a hardware description of the FMC peripheral, used by the STM32 FMC Linux driver and by the MTD framework. |
The configuration is performed using the [[Device tree|device tree]] mechanism that provides a hardware description of the FMC peripheral, used by the STM32 FMC Linux driver and by the MTD framework. |
||
− | == DT bindings documentation == |
+ |
=== DT bindings documentation === |
The FMC device tree bindings are composed of: |
The FMC device tree bindings are composed of: |
||
Line 179: | Line 179: | ||
* FMC driver bindings <ref> {{CodeSource | Linux kernel | Documentation/devicetree/bindings/mtd/stm32-fmc2-nand.txt | | 5.4-stm32mp-r1}} </ref>. |
* FMC driver bindings <ref> {{CodeSource | Linux kernel | Documentation/devicetree/bindings/mtd/stm32-fmc2-nand.txt | | 5.4-stm32mp-r1}} </ref>. |
||
− | == DT configuration == |
+ |
=== DT configuration === |
This hardware description is a combination of the '''STM32 microprocessor''' device tree files (''.dtsi'' extension) and '''board''' device tree files (''.dts'' extension). See the [[Device tree]] for an explanation of the device tree file split. |
This hardware description is a combination of the '''STM32 microprocessor''' device tree files (''.dtsi'' extension) and '''board''' device tree files (''.dts'' extension). See the [[Device tree]] for an explanation of the device tree file split. |
||
'''STM32CubeMX''' can be used to generate the board device tree. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX|How to configure the DT using STM32CubeMX]] for more details. |
'''STM32CubeMX''' can be used to generate the board device tree. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX|How to configure the DT using STM32CubeMX]] for more details. |
||
− | ===DT configuration (STM32 level) === |
+ |
====DT configuration (STM32 level) ==== |
The FMC peripheral node is located in ''stm32mp151.dtsi''<ref>{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp151.dtsi | | 5.4-stm32mp-r1}}</ref> file. |
The FMC peripheral node is located in ''stm32mp151.dtsi''<ref>{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp151.dtsi | | 5.4-stm32mp-r1}}</ref> file. |
||
Line 208: | Line 208: | ||
{{Warning|This device tree part related to the STM32 should be kept as is, customer should not modify it.}} |
{{Warning|This device tree part related to the STM32 should be kept as is, customer should not modify it.}} |
||
− | === DT configuration (board level) === |
+ |
==== DT configuration (board level) ==== |
The FMC peripheral may connect to one SLC NAND Flash memory (with a maximum of 2 dies per package). |
The FMC peripheral may connect to one SLC NAND Flash memory (with a maximum of 2 dies per package). |
||
Line 233: | Line 233: | ||
* nand-ecc-strength = <8>, nand-ecc-step-size = <512> (BCH8). |
* nand-ecc-strength = <8>, nand-ecc-step-size = <512> (BCH8). |
||
− | === DT configuration examples === |
+ |
==== DT configuration examples ==== |
The below example shows how to configure the FMC controller when a SLC 8-bit NAND Flash memory device is connected (ECC requirement: 8 bits / 512 bytes). |
The below example shows how to configure the FMC controller when a SLC 8-bit NAND Flash memory device is connected (ECC requirement: 8 bits / 512 bytes). |
||
Line 276: | Line 276: | ||
}; |
}; |
||
− | ==How to configure the DT using STM32CubeMX== |
+ |
===How to configure the DT using STM32CubeMX=== |
The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree#STM32|platform configuration device tree]] files.<br /> |
The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree#STM32|platform configuration device tree]] files.<br /> |
||
The STM32CubeMX may not support all the properties described in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to [[STM32CubeMX]] user manual for further information. |
The STM32CubeMX may not support all the properties described in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to [[STM32CubeMX]] user manual for further information. |
||
− | ==References== |
+ |
===References=== |
Please refer to the following links for full description: |
Please refer to the following links for full description: |
||