Difference between revisions of "Dmesg and Linux kernel log"

[unchecked revision] [quality revision]
m (Linux kernel configuration)
m


1 Article purpose[edit]

The purpose of this article is to provide information about the Linux® kernel log including configuration, and to detail usage of dmesg command.

2 Introduction[edit]

Linux kernel is able to print log and trace messages, which are by default stored in a ring buffer.

The same messages can also be displayed, applying filter, on uart/console using serial port. This is defined in the kernel command-line, with the "console" parameter. See [1] for detail.

dmesg is a shell command on the kernel console, which also displays the content of the ring buffer, with filter or not (default).

3 printk function[edit]

The simplest way to get some debug information from the kernel code is by printing out various information with the kernel's equivalent of printf - the printk function and its derivatives.

printk("My Debugger is Printk\n");

See elinux.org[2] for reference. This information will be sent to the console, and also stored in a ring buffer.

You can also check to the printk-format.txt[3] document provided in the Linux kernel package to get detail about syntax and formatting.

4 Linux kernel ring buffer[edit]

The Linux kernel also manages a ring buffer to store log and trace messages.

The size of the buffer cannot be modified in runtime, and its default size value is 2^CONFIG_LOG_BUF_SHIFT bytes.

To change it, there are 3 possibles ways:

  • Modify CONFIG_LOG_BUF_SHIFT value in defconfig file or use the config fragment file:
In example for 64K : CONFIG_LOG_BUF_SHIFT=16
 Location:
   -> General setup
     -> Kernel log buffer size (16 => 64KB, 17 => 128KB)
  • Or modify kernel arguments[4] in kernel command-line (via bootargs value in device tree, or directly in extlinux uboot config file)
bootargs = "root=/dev/mmcblk0p5 rootwait rw console=ttySTM0,115200 log_buf_len=65536";

This ring buffer can be displayed using dmesg command (see dmesg).

5 Loglevels[edit]

As reference, please see elinux.org[5].

The log level is used by the kernel to determine the importance of a message and to decide whether it should be presented to the user immediately, by printing it to the current console.

For this, the kernel compares the log level of the message to the console_loglevel (a kernel variable) and if the priority is higher (i.e. a lower value) than the console_loglevel, the message will be printed to the current console. As example, if console_loglevel=5, all messages with log level 0 to 4 will be displayed.

Please note that all messages with loglevel lower or equal to KERN_INFO level are stored in the ring buffer.

5.1 loglevels values[edit]

"Loglevels table"
Name String Meaning alias functions dev alias function
KERN_EMERG "0" Emergency messages, system is about to crash or is unstable pr_emerg dev_emerg
KERN_ALERT "1" Something bad happened and action must be taken immediately pr_alert dev_alert
KERN_CRIT "2" A critical condition occurred like a serious hardware/software failure pr_crit dev_crit
KERN_ERR "3" An error condition, often used by drivers to indicate difficulties with the hardware pr_err dev_err
KERN_WARNING "4" A warning, meaning nothing serious by itself but might indicate problems pr_warning dev_warn
KERN_NOTICE "5" Nothing serious, but notably nevertheless. Often used to report security events pr_notice dev_notice
KERN_INFO "6" Informational message e.g. startup information at driver initialization pr_info dev_info
KERN_DEBUG "7" Debug messages pr_debug, pr_devel if DEBUG is defined dev_dbg

Important: please note that Higher priority message is loglevel 0

5.2 Set loglevel filter value for console[edit]

5.2.1 Default values[edit]

To determine your current console_loglevel on the target you can verifiy with the following command:

 cat /proc/sys/kernel/printk
7       4           1       7
current default_msg minimum default_console

The first integer shows you the current console_loglevel; the second the default log level, see Use loglevel in the kernel source for log and trace.

This is defined at compilation:

- Current console loglevel via CONFIG_CONSOLE_LOGLEVEL_DEFAULT=7 (defined in file lib/Kconfig.debug)
- Default message loglevel via CONFIG_MESSAGE_LOGLEVEL_DEFAULT=4 (defined in file lib/Kconfig.debug)
- Minimum console loglevel via #define CONSOLE_LOGLEVEL_MIN 1 (defined in file include/linux/printk.h)
- Default console loglevel is equal to CONFIG_CONSOLE_LOGLEVEL_DEFAULT

5.2.2 Using kernel command-line[edit]

The console loglevel can be also set via a kernel command-line parameter if you want to use a different value than one specify by CONFIG_CONSOLE_LOGLEVEL_DEFAULT.
For example:

root=/dev/mmcblk0p5 rootwait rw console=ttySTM0,115200 loglevel=4

In that case only messages with a higher priority than KERN_WARNING (means < 4, KERN_EMERG to KERN_ERR ) will be displayed on the console.

2 ways to add this command-line parameter which is set in the extlinux.conf file of boot partition:

  • If using SD card, this is possible to edit the file on host PC:
Insert SD card on host PC
Check for mounting boot partition (i.e. /media/$USER/bootfs)
Check for your HW config (i.e. booting on mmc0 (SD Card) with ev1 board)
 cd /media/$USER/bootfs/mmc0_stm32mp157c-ev1_extlinux/
 gedit extlinux.conf
Add loglevel=8 at the end of APPEND line
Save and insert SD card on the board
  • If using SD Card or eMMC, this is possible to edit the file directly on the board side:
When software is boot
Mount boot partition
 mount /dev/mmcblk0p4 /boot (if not already done)
Update the kernel command line
 cd /boot
 cd mmc0_stm32mp157c-ev1_extlinux (case SD card on ev1 board)
Modify extlinux.conf to add loglevel=8 at the end of APPEND line by using ‘vi’ editor
Save and reboot the board

5.2.3 Using sysfs in runtime[edit]

To change your current console_loglevel simply write to this file:

 echo <loglevel> > /proc/sys/kernel/printk

or using dmesg command.

As example:

 echo 8 > /proc/sys/kernel/printk         # Temporary increase loglevel to display messages up to loglevel 8

In that case, every kernel messages will appear on your console, as all priority higher than 8 (lower loglevel values) will be displayed.

Please note that after reboot, this configuration is reset.

5.2.4 Using menuconfig before compilation[edit]

As values are defined first at compilation step, this is also possible to set them (CONFIG_CONSOLE_LOGLEVEL_DEFAULT and CONFIG_MESSAGE_LOGLEVEL_DEFAULT) using the Linux kernel Menuconfig tool (Menuconfig or how to configure kernel):

Symbol: CONSOLE_LOGLEVEL_DEFAULT [=7]
Location:
  Kernel hacking --->
    printk and dmesg options --->
      (7) Default console loglevel (1-15)

Symbol: MESSAGE_LOGLEVEL_DEFAULT [=4]
Location:
  Kernel hacking --->
    printk and dmesg options --->
      (4) Default message log level (1-7)

5.3 Use loglevel in kernel source for log and trace[edit]

5.3.1 Using printk[edit]

A loglevel information can be added in the printk function call, with the following syntax.

printk(KERN_ERR "something went wrong, return code: %d\n",ret);

When not present, default loglevel value is given by CONFIG_MESSAGE_LOGLEVEL_DEFAULT (usually "4"=KERN_WARNING)

5.3.2 Using dedicated functions[edit]

In the loglevels table above, there are some alias functions pr_ and dev_.

These functions are defined to replace printk + loglevel info inside, in order to simplify syntax.

pr_err("something went wrong, return code: %d\n",ret);

dev_ functions are taken one more parameter to provide more information about current device or driver where message is coming from.

  • Example for pr_info
pr_info("%s%s%s at %s (irq = %d, base_baud = %d) is a %s\n",
        port->dev ? dev_name(port->dev) : "",
        port->dev ? ": " : "",
        port->name,
        address, port->irq, port->uartclk / 16, uart_type(port));

will display information below:

[ 0.919488] 40010000.serial: ttySTM0 at MMIO 0x40010000 (irq = 41, base_baud = 6046875) is a stm32-usart
  • Example for dev_info
dev_info(&pdev->dev, "interrupt mode used for rx (no dma)\n");

will display information below, including device reference automatically:

[    1.046700] stm32-usart 40010000.serial: interrupt mode used for rx (no dma)

6 earlyprintk[edit]

earlyprintk is a Linux kernel debug feature useful to get traces for kernel issues which happen before the normal console is initialized.

6.1 Linux kernel configuration[edit]


In order to enable earlyprintk feature, the Linux kernel configuration must activate CONFIG_DEBUG_LL, CONFIG_STM32MP1_DEBUG_UART and CONFIG_EARLY_PRINTK using the Linux kernel Menuconfig tool (Menuconfig or how to configure kernel):

Symbol: DEBUG_LL
Location:
  Kernel hacking --->
    [*] Kernel low-level debugging functions

Symbol: STM32MP1_DEBUG_UART
Location:
  Kernel hacking --->
    [*] Kernel low-level debugging functions
      [*] Kernel low-level debugging port
      (X) Use STM32MP1 UART for low-level debug

Symbol: EARLY_PRINTK
Location:
  Kernel hacking --->
    [*] Early printk

6.2 Serial port configuration[edit]

When enabling the Linux kernel configuration CONFIG_STM32MP1_DEBUG_UART, it configures the addresses of the UART registers to be used.

By default, on STM32MP1 boards, UART4 is used for console for Linux kernel and by extension at all boot stages.

In case the UART port is different on a new board, you must apply the following changes:

  • Update value for CONFIG_DEBUG_UART_PHYS, to select the UART port for the debug console
Symbol: DEBUG_UART_PHYS [=0x40010000]
Location:
  Kernel hacking --->
    [*] Kernel low-level debugging port (Use STM32MP1 UART4 for low-level debug)
    (0x40010000)  Physical base address of debug UART

  • Update value for CONFIG_DEBUG_UART_VIRT, to define the associated virtual address to be used
Symbol: DEBUG_UART_VIRT [=0xFE010000]
Location:
  Kernel hacking --->
    [*] Kernel low-level debugging port (Use STM32MP1 UART4 for low-level debug)
    (0xFE010000)  Virtual base address of debug UART

Following rules to be respected for defining the virtual address:
- The 20 low weight bits (21 in case LPAE is enabled) must be kept in order to align region size of 1MB (2MB in LPAE is enabled).
- It must be mapped at the upper address of the vmalloc area, in order to not be overwritten by kernel which is stating from lower addresses: i.e here we select 0xFE0xxxxx
CONFIG_DEBUG_UART_PHYS: 0x40010000 /* UART4 */
CONFIG_DEBUG_UART_VIRT: 0xFE010000

  • Please find below table for USART/UART of STMP32MP1:
Name Physical base address Virtual base address
USART1 5c000000 FE000000
USART2 4000e000 FE00e000
USART3 4000f000 FE00f000
UART4 40010000 FE010000
UART5 40011000 FE011000
USART6 44003000 FE003000
UART7 40018000 FE018000
UART8 40019000 FE019000
Warning white.png Warning
Note that the UART port used for console must be aligned for all components of the boot chain: FSBL(TF-A), SSBL-U-Boot) and Linux kernel

Especially because the Linux kernel do not configure all the setting registers for the UART port, as this is done by SSBL (U-Boot - How to debug)
See also TF-A - How to debug for FSBL changes)

6.3 Linux kernel boot command configuration[edit]

The Linux kernel boot command must contain the command-line parameter earlyprintk.

For instance, the kernel bootargs can be modified in the following ways:

  • Mount a boot partition from the Linux kernel console, and then update the extlinux.conf file using the vi editor (see man page[6], or introduction page[7] ). For example:
 mount /dev/mmcblk0p4 /boot
 vi /boot/mmc0_stm32mp157c-ev1_extlinux/extlinux.conf

or

To mount partitions (mmc 0:microSD card / mmc 1: eMMC):

- Press any key to stop at U-Boot execution when booting the board.
 ...
 Hit any key to stop autoboot:  0
 STM32MP>
- Then
STM32MP> ums 0 mmc 0
- Check for the boot partition mounted on your host PC (/media/$USER/bootfs)
- Edit the extlinux file corresponding to your setup (/media/$USER/bootfs/mmc0_stm32mp157c-ev2_extlinux/extlinux.conf
  • Update the kernel command line by adding the earlyprintk parameter:
root=/dev/mmcblk0p6 rootwait rw earlyprintk console=ttySTM0,115200

Save and quit file update, and then reboot the board.

6.4 Get trace[edit]

Earlyprintk traces are pushed automatically to the serial console defined as seen previously, and also added to the kernel ring log buffer.

7 dmesg command[edit]

As reference, please see man page[8].

The Kernel ring buffer can be displayed using dmesg command. It will display on the console all the content of the ring buffer.

  • It is possible to filter messages following the loglevels:
 dmesg -n <loglevel>

In that case, only messages with a value lower (not lower equal) than the console_loglevel will be printed.

Here, <loglevel> can be a numeric value, but also a string:

Supported log levels (priorities):
  emerg (0)
  alert (1)
   crit (2)
    err (3)
   warn (4)
 notice (5)
   info (6)
  debug (7)
As example:
 dmesg -n 8         # Temporary change loglevel to display messages up to debug level
or
 dmesg -n debug 

In that case, every kernel messages will appear on your console, as all priority higher than 8 (lower loglevel values) will be displayed.
  • It is possible to clear the dmesg buffer
 dmesg -c        # Display the full content of dmesg ring buffer, and then clear it
 dmesg -C        # Clear the dmesg ring buffer

8 /var/log/messages file system entry[edit]

An other way to display the content of the Linux kernel log is to look at the content of the file /var/log/messages.

It contains general system activity messages from the start-up. It also provides useful information about origin of the message, and log level.

9 Dynamic debug message[edit]

These messages are using the loglevel 7 (KERN_DEBUG).

Please see How to use the kernel dynamic debug article.

10 References[edit]



<noinclude>

{{ClonedFrom | stm32mpu}}</noinclude>

== Article purpose ==
The purpose of this article is to provide information about the Linux<sup>&reg;</sup> kernel log including configuration, and to detail usage of dmesg command.

== Introduction ==
Linux kernel is able to print log and trace messages, which are by default stored in a ring buffer.

The same messages can also be displayed, applying filter, on uart/console using serial port. This is defined in the kernel command-line, with the "console" parameter. See <ref>https://www.kernel.org/doc/html/latest/{{DocSource | domain=Linux kernel | path=admin-guide/serial-console.html | text=Linux Serial Console}}</ref> for detail.

dmesg is a shell command on the kernel console, which also displays the content of the ring buffer, with filter or not (default).

== printk function ==
The simplest way to get some debug information from the kernel code is by printing out various information with the kernel's equivalent of printf - the printk function and its derivatives.
 printk("My Debugger is Printk\n");
See elinux.org<ref>https://elinux.org/Debugging_by_printing</ref> for reference.
This information will be sent to the console, and also stored in a ring buffer.

You can also check to the printk-format.txt<ref>https://www.kernel.org/doc/Documentation/printk-formats.txt</ref> document provided in the Linux kernel package to get detail about syntax and formatting.

== Linux kernel ring buffer ==
The Linux kernel also manages a ring buffer to store log and trace messages.

The size of the buffer cannot be modified in runtime, and its default size value is 2^CONFIG_LOG_BUF_SHIFT bytes.

To change it, there are 3 possibles ways:

* Modify CONFIG_LOG_BUF_SHIFT value in defconfig file or use the config fragment file:
 In example for 64K : CONFIG_LOG_BUF_SHIFT=16

* or use the Linux kernel [[Menuconfig or how to configure kernel|menuconfig update]]
  Location:
    -> General setup
      -> Kernel log buffer size (16 => 64KB, 17 => 128KB)

* Or modify kernel arguments<ref>https://www.kernel.org/doc/html/latest/{{DocSource | domain=Linux kernel | path=admin-guide/kernel-parameters.html | text=The kernel’s command-line parameters}}</ref> in kernel command-line (via bootargs value in device tree, or directly in extlinux uboot config file)
 bootargs = "root=/dev/mmcblk0p5 rootwait rw console=ttySTM0,115200 {{highlight|log_buf_len&#61;65536}}";

This ring buffer can be displayed using ''dmesg'' command (see [[#dmesg command|dmesg]]).

== Loglevels ==
As reference, please see elinux.org<ref>https://elinux.org/Debugging_by_printing#Log_Levels</ref>.

The log level is used by the kernel to determine the importance of a message and to decide whether it should be presented to the user immediately, by printing it to the current console.

For this, the kernel compares the log level of the message to the console_loglevel (a kernel variable) and if the priority is higher (i.e. a lower value) than the console_loglevel, the message will be printed to the current console. As example, if console_loglevel&#61;5, all messages with log level 0 to 4 will be displayed.

Please note that all messages with loglevel lower or equal to KERN_INFO level are stored in the ring buffer.

=== loglevels values ===
{| class="st-table"
|+ "Loglevels table"
|-
!  Name !! String !!  Meaning !! alias functions !! dev alias function
|- 
| KERN_EMERG || "0" || Emergency messages, system is about to crash or is unstable || pr_emerg || dev_emerg
|-
| KERN_ALERT  || "1" || Something bad happened and action must be taken immediately || pr_alert  || dev_alert
|-
| KERN_CRIT  || "2" || A critical condition occurred like a serious hardware/software failure || pr_crit  || dev_crit
|-
| KERN_ERR  || "3" || An error condition, often used by drivers to indicate difficulties with the hardware || pr_err || dev_err
|-
| KERN_WARNING  || "4" || A warning, meaning nothing serious by itself but might indicate problems || pr_warning || dev_warn
|-
| KERN_NOTICE  || "5" || Nothing serious, but notably nevertheless. Often used to report security events || pr_notice  || dev_notice
|-
| KERN_INFO  || "6" || Informational message e.g. startup information at driver initialization || pr_info || dev_info
|-
| KERN_DEBUG  || "7" || Debug messages || pr_debug, pr_devel if DEBUG is defined || dev_dbg
|}

{{Highlight|'''Important''': please note that Higher priority message is loglevel 0}}

=== Set loglevel filter value for console ===
==== Default values ====
To determine your current console_loglevel on the target you can verifiy with the following command:
 {{Board$}} cat /proc/sys/kernel/printk
 {{green|'''7'''}}       {{Orange|'''4'''}}           {{STPurple|'''1'''}}       {{highlight|'''7'''}}
 {{green|'''current'''}} {{Orange|'''default_msg'''}} {{STPurple|'''minimum'''}} {{highlight|'''default_console'''}}

The first integer shows you the current console_loglevel; the second the default log level, see [[#Use_loglevel_in_kernel_source_for_log_and_trace|Use loglevel in the kernel source for log and trace]].

This is defined at compilation:<br>

:- {{green|Current console}} loglevel via {{green|CONFIG_CONSOLE_LOGLEVEL_DEFAULT&#61;7}} (defined in file ''lib/Kconfig.debug'')<br>

:- {{Orange|Default message}} loglevel via {{Orange|CONFIG_MESSAGE_LOGLEVEL_DEFAULT&#61;4}} (defined in file ''lib/Kconfig.debug'')<br>

:- {{STPurple|Minimum console}} loglevel via {{STPurple|#define CONSOLE_LOGLEVEL_MIN 1}} (defined in file ''include/linux/printk.h'')<br>

:- {{highlight|Default console}} loglevel is {{highlight|equal to CONFIG_CONSOLE_LOGLEVEL_DEFAULT}}<br>


==== Using kernel command-line ====
The console loglevel can be also set via a kernel command-line parameter if you want to use a different value than one specify by CONFIG_CONSOLE_LOGLEVEL_DEFAULT.<br>

For example:
 root=/dev/mmcblk0p5 rootwait rw console=ttySTM0,115200 {{highlight|loglevel&#61;4}}
In that case only messages with a higher priority than KERN_WARNING (means < 4, KERN_EMERG to KERN_ERR ) will be displayed on the console.

2 ways to add this command-line parameter which is set in the extlinux.conf file of boot partition:
* If using SD card, this is possible to edit the file on host PC:
 Insert SD card on host PC
 Check for mounting boot partition (i.e. /media/$USER/bootfs)
 Check for your HW config (i.e. booting on mmc0 (SD Card) with ev1 board)
 {{PC$}} cd /media/$USER/bootfs/mmc0_stm32mp157c-ev1_extlinux/
 {{PC$}} gedit extlinux.conf
 Add '''loglevel=8''' at the end of APPEND line
 Save and insert SD card on the board
* If using SD Card or eMMC, this is possible to edit the file directly on the board side:
 When software is boot
 Mount boot partition
 {{Board$}} mount /dev/mmcblk0p4 /boot (if not already done)
 Update the kernel command line
 {{Board$}} cd /boot
 {{Board$}} cd mmc0_stm32mp157c-ev1_extlinux (''case SD card on ev1 board'')
 Modify extlinux.conf to add '''loglevel=8''' at the end of APPEND line by using ‘vi’ editor
 Save and reboot the board

==== Using sysfs in runtime ====
To change your current console_loglevel simply write to this file: 
 {{Board$}} echo {{HighlightParam|<''loglevel''>}} > /proc/sys/kernel/printk

or using [[#dmesg command|dmesg command]].

As example:
 {{Board$}} echo {{highlight|8}} > /proc/sys/kernel/printk         ''# Temporary increase loglevel to display messages up to loglevel 8''
:In that case, every kernel messages will appear on your console, as {{highlight|all priority higher than 8 (lower loglevel values)}} will be displayed.
'''Please note that after reboot, this configuration is reset.'''

==== Using menuconfig before compilation ====
As values are defined first at compilation step, this is also possible to set them ('''CONFIG_CONSOLE_LOGLEVEL_DEFAULT''' and '''CONFIG_MESSAGE_LOGLEVEL_DEFAULT''') using the Linux kernel Menuconfig tool ([[Menuconfig or how to configure kernel]]):
 Symbol: '''CONSOLE_LOGLEVEL_DEFAULT''' [={{green|7}}]
 Location:
   Kernel hacking --->
     printk and dmesg options --->
       {{highlight|(7) Default console loglevel (1-15)}}

 Symbol: '''MESSAGE_LOGLEVEL_DEFAULT''' [={{green|4}}]
 Location:
   Kernel hacking --->
     printk and dmesg options --->
       {{highlight|(4) Default message log level (1-7)}}

=== Use loglevel in kernel source for log and trace ===
==== Using printk ====
A loglevel information can be added in the printk function call, with the following syntax.
 printk(KERN_ERR "something went wrong, return code: %d\n",ret);
When not present, default loglevel value is given by CONFIG_MESSAGE_LOGLEVEL_DEFAULT (usually "4"=KERN_WARNING)

==== Using dedicated functions ====
In the loglevels table above, there are some alias functions ''pr_'' and ''dev_''.

These functions are defined to replace ''printk + loglevel info inside'', in order to simplify syntax.

 pr_err("something went wrong, return code: %d\n",ret);
''dev_'' functions are taken one more parameter to provide more information about current device or driver where message is coming from.

* Example for ''pr_info''
 pr_info("%s%s%s at %s (irq = %d, base_baud = %d) is a %s\n",
         port->dev ? dev_name(port->dev) : "",
         port->dev ? ": " : "",
         port->name,
         address, port->irq, port->uartclk / 16, uart_type(port));
will display information below:
 [ 0.919488] 40010000.serial: ttySTM0 at MMIO 0x40010000 (irq = 41, base_baud = 6046875) is a stm32-usart

* Example for ''dev_info''
 dev_info(&pdev->dev, "interrupt mode used for rx (no dma)\n");
will display information below, including device reference automatically:
 [    1.046700] {{highlight|stm32-usart 40010000.serial}}: interrupt mode used for rx (no dma)

== earlyprintk ==
'''earlyprintk''' is a Linux kernel debug feature useful to get traces for kernel issues which happen before the normal console is initialized.
=== Linux kernel configuration ===

{{ReviewsComments | [[User:Erwan Le Ray|Erwan Le Ray]] ([[User talk:Erwan Le Ray|talk]]) 10:50, 29 January 2020 (CET) - Path has changed in kernel v5.5: those symbols are now located in Kernel hacking ---> arm Debugging<br>

[[User:Jean-philippe Romain|Jean-Philippe Romain]]: v5.5 not for v2.x stream, keep this comment for future}}

In order to enable earlyprintk feature, the Linux kernel configuration must activate '''CONFIG_DEBUG_LL''', '''CONFIG_STM32MP1_DEBUG_UART''' and '''CONFIG_EARLY_PRINTK''' using the Linux kernel Menuconfig tool ([[Menuconfig or how to configure kernel]]):
 Symbol: '''DEBUG_LL'''
 Location:
   Kernel hacking --->
     {{highlight|[*] Kernel low-level debugging functions}}

 Symbol: '''STM32MP1_DEBUG_UART'''
 Location:
   Kernel hacking --->
     [*] Kernel low-level debugging functions
       [*] Kernel low-level debugging port
       {{highlight|(X) Use STM32MP1 UART for low-level debug}}

 Symbol: '''EARLY_PRINTK'''
 Location:
   Kernel hacking --->
     {{highlight|[*] Early printk}}

=== Serial port configuration ===
When enabling the Linux kernel configuration '''CONFIG_STM32MP1_DEBUG_UART''', it configures the addresses of the UART registers to be used.

By default, on STM32MP1 boards, UART4 is used for console for Linux kernel and by extension at all boot stages.

In case the UART port is different on a new board, you must apply the following changes:
:* Update value for '''CONFIG_DEBUG_UART_PHYS''', to select the UART port for the debug console
 Symbol: '''DEBUG_UART_PHYS''' [=0x40010000]
 Location:
   Kernel hacking --->
     [*] Kernel low-level debugging port (Use STM32MP1 UART4 for low-level debug)
     {{highlight|(0x40010000)  Physical base address of debug UART}}

:* Update value for '''CONFIG_DEBUG_UART_VIRT''', to define the associated virtual address to be used
 Symbol: '''DEBUG_UART_VIRT''' [=0xFE010000]
 Location:
   Kernel hacking --->
     [*] Kernel low-level debugging port (Use STM32MP1 UART4 for low-level debug)
     {{highlight|(0xFE010000)  Virtual base address of debug UART}}
:{{highlight|Following rules to be respected for defining the virtual address}}:
::- The 20 low weight bits (21 in case LPAE is enabled) must be kept in order to align region size of 1MB (2MB in LPAE is enabled).
::- It must be mapped at the upper address of the vmalloc area, in order to not be overwritten by kernel which is stating from lower addresses: i.e here we select 0x{{highlight|'''FE0'''}}xxxxx
 CONFIG_DEBUG_UART_PHYS: 0x400{{green|'''10000'''}} /* UART4 */
 CONFIG_DEBUG_UART_VIRT: 0x{{highlight|'''FE0'''}}{{green|'''10000'''}}

::*Please find below table for USART/UART of STMP32MP1:
:{| class="st-table"
|-
! '''Name''' !! '''Physical base address'''!! '''Virtual base address'''
|-
| USART1
| style="text-align:center;" | 5c000000
| style="text-align:center;" | '''FE0'''00000
|-
| USART2
| style="text-align:center;" | 4000e000
| style="text-align:center;" | '''FE0'''0e000
|-
| USART3
| style="text-align:center;" | 4000f000
| style="text-align:center;" | '''FE0'''0f000
|-
| UART4
| style="text-align:center;" | 40010000
| style="text-align:center;" | '''FE0'''10000
|-
| UART5
| style="text-align:center;" | 40011000
| style="text-align:center;" | '''FE0'''11000
|-
| USART6
| style="text-align:center;" | 44003000
| style="text-align:center;" | '''FE0'''03000
|-
| UART7
| style="text-align:center;" | 40018000
| style="text-align:center;" | '''FE0'''18000
|-
| UART8
| style="text-align:center;" | 40019000
| style="text-align:center;" | '''FE0'''19000
|}

{{Warning|Note that the UART port used for console must be aligned for all components of the boot chain: FSBL(TF-A), SSBL-U-Boot) and Linux kernel<br/>

Especially because the Linux kernel do not configure all the setting registers for the UART port, as this is done by SSBL ([[U-Boot_-_How_to_debug#Debug_with_console|U-Boot - How to debug]])<br/>

See also [[TF-A - How to debug#Debug_with_Traces|TF-A - How to debug]] for FSBL changes)
}}

=== Linux kernel boot command configuration ===
The Linux kernel boot command must contain the command-line parameter '''earlyprintk'''.

For instance, the kernel ''bootargs'' can be modified in the following ways:<br>

* Mount a boot partition from the Linux kernel console, and then update the extlinux.conf file using the vi editor (see man page<ref>http://ex-vi.sourceforge.net/vi.html</ref>, or introduction page<ref>http://ex-vi.sourceforge.net/viin/paper.html</ref> ). For example:
 {{Board$}} mount /dev/mmcblk0p4 /boot
 {{Board$}} vi /boot/mmc0_stm32mp157c-ev1_extlinux/extlinux.conf

or
* Edit the extlinux.conf file by using UMS (USB Mass Storage): see [[How to use USB mass storage in U-Boot]] for details.

To mount partitions (mmc 0:microSD card / mmc 1: eMMC):
:- Press any key to stop at U-Boot execution when booting the board.
 {{Board$}} ...
 {{Board$}} Hit any key to stop autoboot:  0
 {{Board$}} STM32MP>

:- Then
 STM32MP> ums 0 mmc 0

:- Check for the boot partition mounted on your host PC (/media/''$USER''/bootfs)<br>

:- Edit the extlinux file corresponding to your setup (/media/''$USER''/bootfs/mmc0_stm32mp157c-ev2_extlinux/extlinux.conf<br>


* Update the kernel command line by adding the '''earlyprintk''' parameter:
 root=/dev/mmcblk0p6 rootwait rw '''earlyprintk''' console=ttySTM0,115200
Save and quit file update, and then reboot the board.

=== Get trace ===
Earlyprintk traces are pushed automatically to the serial console defined as seen previously, and also added to the kernel ring log buffer.

== dmesg command ==
As reference, please see man page<ref>http://man7.org/linux/man-pages/man1/dmesg.1.html</ref>.

The Kernel ring buffer can be displayed using ''dmesg'' command.
It will display on the console all the content of the ring buffer.

* It is possible to filter messages following the loglevels:
 {{Board$}} dmesg -n {{HighlightParam|<''loglevel''>}}
In that case, only messages with a value lower ('''not lower equal''') than the console_loglevel will be printed.

Here, {{HighlightParam|<''loglevel''>}} can be a numeric value, but also a string:
 Supported log levels (priorities):
   emerg (0)
   alert (1)
    crit (2)
     err (3)
    warn (4)
  notice (5)
    info (6)
   debug (7)

:As example:
 {{Board$}} dmesg -n {{highlight|8 }}        ''# Temporary change loglevel to display messages up to debug level''
 or
 {{Board$}} dmesg -n {{highlight|debug }}
:In that case, every kernel messages will appear on your console, as {{highlight|all priority higher than 8 (lower loglevel values)}} will be displayed.

* It is possible to clear the dmesg buffer
 {{Board$}} dmesg {{highlight|-c}}        ''# Display the full content of dmesg ring buffer, and then clear it''
 {{Board$}} dmesg {{highlight|-C}}        ''# Clear the dmesg ring buffer''

== /var/log/messages file system entry ==
An other way to display the content of the Linux kernel log is to look at the content of the file /var/log/messages.

It contains general system activity messages from the start-up. It also provides useful information about origin of the message, and log level.

== Dynamic debug message ==
These messages are using the loglevel 7 (KERN_DEBUG).

Please see [[How to use the kernel dynamic debug]] article.

==References==<references />

<noinclude>

{{PublicationRequestId | 9567 | 2018-11-15 | AlainF}}
[[Category:Linux tracing tools]]</noinclude>
Line 8: Line 8:
 
Linux kernel is able to print log and trace messages, which are by default stored in a ring buffer.
 
Linux kernel is able to print log and trace messages, which are by default stored in a ring buffer.
   
The same messages can also be displayed, applying filter, on uart/console using serial port. This is defined in the kernel command-line, with the "console" parameter. See <ref>https://www.kernel.org/doc/html/latest/admin-guide/serial-console.html</ref> for detail.
+
The same messages can also be displayed, applying filter, on uart/console using serial port. This is defined in the kernel command-line, with the "console" parameter. See <ref>{{DocSource | domain=Linux kernel | path=admin-guide/serial-console.html | text=Linux Serial Console}}</ref> for detail.
   
 
dmesg is a shell command on the kernel console, which also displays the content of the ring buffer, with filter or not (default).
 
dmesg is a shell command on the kernel console, which also displays the content of the ring buffer, with filter or not (default).
Line 35: Line 35:
 
       -> Kernel log buffer size (16 => 64KB, 17 => 128KB)
 
       -> Kernel log buffer size (16 => 64KB, 17 => 128KB)
   
* Or modify kernel arguments<ref>https://www.kernel.org/doc/html/latest/admin-guide/kernel-parameters.html</ref> in kernel command-line (via bootargs value in device tree, or directly in extlinux uboot config file)
+
* Or modify kernel arguments<ref>{{DocSource | domain=Linux kernel | path=admin-guide/kernel-parameters.html | text=The kernel’s command-line parameters}}</ref> in kernel command-line (via bootargs value in device tree, or directly in extlinux uboot config file)
 
  bootargs = "root=/dev/mmcblk0p5 rootwait rw console=ttySTM0,115200 {{highlight|log_buf_len&#61;65536}}";
 
  bootargs = "root=/dev/mmcblk0p5 rootwait rw console=ttySTM0,115200 {{highlight|log_buf_len&#61;65536}}";