Difference between revisions of "DSI internal peripheral"

[checked revision] [quality revision]
(Overview)
(Peripheral usage and associated software)
 

1 Article purpose[edit]

The purpose of this article is to:

  • Introduce the DSI peripheral and its main features,
  • Indicate the level of security supported by this hardware block,
  • Explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components,
  • Explain, where necessary, how to configure the DSI peripheral.

2 Peripheral overview[edit]

The DSI peripheral implements all the protocol functions defined in the MIPI® Display Serial Interface (MIPI® DSI) specification. It provides an interface to communicate with a DSI-compliant display. The MIPI® DSI is part of a group of communication protocols defined by the MIPI® Alliance [1].

2.1 Features[edit]

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to see which features are implemented.

2.2 Security support[edit]

The DSI is a non-secure peripheral.

3 Peripheral usage and associated software[edit]

Even if some MIPI DSI modes are supported by the DSI internal peripheral, in practice:

  • software frameworks like U-Boot or Linux® kernel do not support all the possible modes.
  • hardware integration constraints such as support for all the clock values or the pll configurations make it difficult to use all possible modes.


Select a MIPI DSI panel or bridge supporting the DSI video burst mode [2] because this mode is supported by all software frameworks and is easier to fine tune. Please consider the following recommendations when selecting a MIPI DSI panel or bridge for your project:

  • Pixel data transmission
    • in DSI command mode: use the DSI video mode as it is not supported by neither U-Boot nor Linux® kernels kernel, use instead the DSI video burst mode.
    • in DSI video mode:
      • burst mode: supported
      • non-burst mode with sync events or pulses: supported with clock constraints to be considered [2].
  • Command transmission (initialization sequence, backlight...)
    • in DSI command mode: supported
    • in DSI video mode:
      • burst mode: supported if there is enough time to send commands before or/and after pixel data [2].
      • non-burst mode with sync events or pulses: supported but there are timing constraints to be considered [2].

3.1 Boot time[edit]

The DSI is used at boot time for displaying a splash screen through the U-Boot framework [3].

3.2 Runtime[edit]

3.2.1 Overview[edit]

The DSI internal peripheral runs on the Arm® Cortex®-A7 non-secure core to be controlled by the Linux® DRM/KMS framework.

Chapter Peripheral assignment describes which peripheral instance can be assigned to which context.

3.2.2 Software frameworks[edit]

Domain Peripheral Software frameworks Comment
Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Visual DSI DRM/KMS framework

3.2.3 Peripheral configuration[edit]

The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the STM32CubeMX tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article or for Linux® in the DSI device tree configuration article.

3.2.4 Peripheral assignment[edit]

Internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned () to the given runtime context.
  • is used for system peripherals that cannot be unchecked because they are statically connected in the device.

Refer to How to assign an internal peripheral to a runtime context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Visual DSI DSI

4 How to go further[edit]

Refer to the STM32 DSI application note (AN4860) [2] for a detailed description of the DSI peripheral and applicable use-cases.

Even if this application note is related to STM32 microcontrollers, it also applies to STM32 MPUs.

5 References[edit]



==Article purpose==
The purpose of this article is to:
* Introduce the DSI peripheral and its main features,
* Indicate the level of security supported by this hardware block,
* Explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components,
* Explain, where necessary, how to configure the DSI peripheral.

==Peripheral overview==
The DSI peripheral implements all the protocol functions defined in the MIPI<sup>&reg;</sup> Display Serial Interface (MIPI<sup>&reg;</sup> DSI) specification. It provides an interface to communicate with a DSI-compliant display. The MIPI<sup>&reg;</sup> DSI is part of a group of communication protocols defined by the MIPI<sup>&reg;</sup> Alliance <ref>https://www.mipi.org MIPI<sup>&reg;</sup> Alliance</ref>. 

===Features===
Refer to the [[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]] for the complete list of features, and to the software components, introduced below, to see which features are implemented.

===Security support===
The DSI is a '''non-secure''' peripheral.

==Peripheral usage and associated software==
Even if some MIPI DSI modes are supported by the DSI internal peripheral, in practice:
* software frameworks like U-Boot or Linux<sup>&reg;</sup> kernel do not support all the possible modes.
* hardware integration constraints such as support for all the clock values or the pll configurations make it difficult to use all possible modes.

Select a MIPI DSI panel or bridge supporting the '''DSI video burst mode''' <ref name="AN4860"/> because this mode is supported by all software frameworks and is easier to fine tune. Please consider the following recommendations when selecting a MIPI DSI panel or bridge for your project:
* '''Pixel data transmission'''
** in DSI command mode: use the DSI video mode as it is not supported by neither U-Boot nor Linux<sup>&reg;</sup> kernelskernel, use instead the DSI video burst mode.
** in DSI video mode:
*** burst mode: supported
*** non-burst mode with sync events or pulses: supported with clock constraints to be considered <ref name="AN4860"/>.

* '''Command transmission''' (initialization sequence, backlight...)
** in DSI command mode: supported
** in DSI video mode:
***burst mode: supported if there is enough time to send commands before or/and after pixel data <ref name="AN4860"/>.
***non-burst mode with sync events or pulses: supported but there are timing constraints to be considered <ref name="AN4860"/>.

===Boot time===
The DSI is used at boot time for displaying a splash screen through the U-Boot framework <ref>[[U-Boot overview | U-Boot framework]]</ref>.

===Runtime===

====Overview====
The DSI internal peripheral runs on the Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-A7 non-secure core to be controlled by the Linux<sup>&reg;</sup>[[DRM KMS overview | DRM/KMS framework]].

Chapter [[#Peripheral assignment|Peripheral assignment]] describes which peripheral instance can be assigned to which context.

====Software frameworks====
{{:Internal_peripherals_software_table_template}}
 | Visual
 | [[DSI internal peripheral|DSI]]
 | 
 | [[DRM KMS overview | DRM/KMS framework]]
 | 
 |
 |-
 |}

====Peripheral configuration====
The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the [[STM32CubeMX]] tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article or for Linux<sup>&reg;</sup> in the [[DSI device tree configuration]] article.

====Peripheral assignment====
{{:Internal_peripherals_assignment_table_template}}<onlyinclude>

 | rowspan="1" | Visual
 | rowspan="1" | [[DSI internal peripheral|DSI]]
 | DSI
 | 
 | <span title="assignable peripheral" style="font-size:21px"></span>

 |
 |
 |-</onlyinclude>

 |}

==How to go further==
Refer to the STM32 DSI application note (AN4860) <ref name="AN4860">[[STM32MP15 resources#AN4860 | DSI host on STM32 MCUs Application Note (AN4860)]]</ref> for a detailed description of the DSI peripheral and applicable use-cases.

Even if this application note is related to STM32 microcontrollers, it also applies to STM32 MPUs.

==References==<references/>

<noinclude>

{{ArticleBasedOnModel | Internal peripheral article model}}
{{PublicationRequestId | 14297 (9174 v1) | 2019-12-10 | AnneJ}}
[[Category:Visual peripherals]]</noinclude>
Line 23: Line 23:
 
Select a MIPI DSI panel or bridge supporting the '''DSI video burst mode''' <ref name="AN4860"/> because this mode is supported by all software frameworks and is easier to fine tune. Please consider the following recommendations when selecting a MIPI DSI panel or bridge for your project:
 
Select a MIPI DSI panel or bridge supporting the '''DSI video burst mode''' <ref name="AN4860"/> because this mode is supported by all software frameworks and is easier to fine tune. Please consider the following recommendations when selecting a MIPI DSI panel or bridge for your project:
 
* '''Pixel data transmission'''
 
* '''Pixel data transmission'''
** in DSI command mode: use the DSI video mode as it is not supported by neither U-Boot nor Linux<sup>&reg;</sup> kernels.
+
** in DSI command mode: not supported by neither U-Boot nor Linux<sup>&reg;</sup> kernel, use instead the DSI video burst mode.
 
** in DSI video mode:
 
** in DSI video mode:
 
*** burst mode: supported
 
*** burst mode: supported