- Last edited 2 years ago ago
DDRCTRL and DDRPHYC device tree configuration
Contents
1 Article purpose[edit]
This article explains how to configure the DDRCTRL and DDRPHYC internal peripherals from the first stage bootloader.
The configuration is performed using the device tree mechanism that provides a hardware description of the DDR subsystem (DDR controler and DDR PHY peripheral), and embeds the configuration used by the first stage bootloader to initialize the DDR before loading the second stage bootloader.
The DDR settings are only used in the device tree of the boot chain FSBL, that is, in the TF-A device tree for OpenSTLinux official delivery (or in SPL only for the DDR tuning tool).
Even if the DDR node information is also present in the U-Boot device tree, only st,mem-size is used by this SSBL.
2 DT bindings documentation[edit]
The DDR subsystem is a 'memory-controller' device represented by the device tree bindings documented below:
- TF-A: docs/devicetree/bindings/memory-controllers/st,stm32mp1-ddr.txt"[1]
- U-Boot: doc/device-tree-bindings/memory-controllers/st,stm32mp1-ddr.txt"[2]
3 DT configuration[edit]
This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device-tree file split.
STM32CubeMX can be used to generate this DDR board device tree. Refer to How to configure the DT using STM32CubeMX for more details.
3.1 DT configuration (STM32 level)[edit]
The STM32MP1 DDR node is located in stm32mp15-ddr.dtsi[3] (see Device tree for further explanation).
/ { ... soc { ... ddr: ddr@5a003000{ compatible = "st,stm32mp1-ddr"; reg = <0x5A003000 0x550 0x5A004000 0x234>; clocks = <&rcc_clk AXIDCG>, <&rcc_clk DDRC1>, <&rcc_clk DDRC2>, <&rcc_clk DDRPHYC>, <&rcc_clk DDRCAPB>, <&rcc_clk DDRPHYCAPB>; clock-names = "axidcg", "ddrc1", "ddrc2", "ddrphyc", "ddrcapb", "ddrphycapb"; status = "okay"; }; }; };
3.2 DT configuration (board level)[edit]
The next attributes provide the DDR information and DDR settings; the values used by the FSBL to initialize the registers of the DDR subsystem (the DDR controller and the DDR PHY).
These value are generated by DDR tools included in STM32CubeMX.
The board configuration defines each configuration needed (DDR_...) and includes the STM32-level device tree.
3.2.1 info[edit]
- st,mem-name: name for the DDR configuration, a simple string for information
- st,mem-speed: DDR expected speed in kHz
- st,mem-size: DDR mem size in bytes (used in SSBL and FSBL)
3.2.2 Controller register values[edit]
- st,ctl-reg: controller values depending on the DDR type (DDR3/LPDDR2/LPDDR3):
- st,ctl-timing: controller values depending on the DDR frequency and timing parameters:
- st,ctl-map: controller values depending on the address mapping:
- st,ctl-perf: controller values depending on performance and scheduling:
3.2.3 phy register values[edit]
- st,phy-reg: phy values depending on the DDR type: (DDR3/LPDDR2/LPDDR3):
- st,phy-timing: phy values depending on the DDR frequency and timing parameters:
- st,phy-cal: phy cal depending on the DDR calibration or tuning. This parameter is optional: when it is absent, the built-in PHY calibration is done (see the next chapter for details); when it is present:
3.2.3.1 st,phy-cal value and DDR tuning[edit]
By default, the st,phy-cal property is absent in device tree and the built-in PHY calibration is executed by the DDR driver to determine DXnDQTR and DXnDQSTR register values (with n = byte id, 0 to 3).
When st,phy-cal is present in device tree (e.g. when DDR_PHY_CAL_SKIP is defined), the built-in PHY calibration is skipped and the driver use the DXnDQTR and DXnDQSTR values defined in the device tree: they described the fine step delays used for DQ/DQS pin deskew and for eye centering. These optimal values are determined by the STM32CubeMX DDR Tuning Tool calibration result.
This DDR tuning is expected only during the bring-up of a new design and only when the build-in calibration is not enough to determine the optimal values for the above registers; the following procedure may be used:
- run multiple tunings on the same board (with power ON/OFF cycle or reset), the DQ/DQS line delays are expected to be stable (1step max), otherwise a noise issue on PCB may be suspected.
- run the DDR tuning on multiple boards to determine the best values, board to board variations are expected to be low (1 step in typical case, 2 steps in worst cases)
Then the best values are saved in the device tree and will be applied to all boards.
See #How to configure the DT using STM32CubeMX and the dedicated application note[4] for further information.
3.3 DT configuration examples[edit]
3.3.1 Simple example[edit]
You can add the DDR configuration node with :
1 / {
2 ...
3 soc {
4 ddr: ddr@5a003000{
5 compatible = "st,stm32mp1-ddr";
6
7 reg = <0x5A003000 0x550
8 0x5A004000 0x234>;
9
10 clocks = <&rcc_clk AXIDCG>,
11 <&rcc_clk DDRC1>,
12 <&rcc_clk DDRC2>,
13 <&rcc_clk DDRPHYC>,
14 <&rcc_clk DDRCAPB>,
15 <&rcc_clk DDRPHYCAPB>;
16
17 clock-names = "axidcg",
18 "ddrc1",
19 "ddrc2",
20 "ddrphyc",
21 "ddrcapb",
22 "ddrphycapb";
23
24 st,mem-name = "DDR3 2x4Gb 533MHz";
25 st,mem-speed = <533000>;
26 st,mem-size = <0x40000000>;
27
28 st,ctl-reg = <
29 0x00040401 /*MSTR*/
30 0x00000010 /*MRCTRL0*/
31 0x00000000 /*MRCTRL1*/
32 0x00000000 /*DERATEEN*/
33 0x00800000 /*DERATEINT*/
34 0x00000000 /*PWRCTL*/
35 0x00400010 /*PWRTMG*/
36 0x00000000 /*HWLPCTL*/
37 0x00210000 /*RFSHCTL0*/
38 0x00000000 /*RFSHCTL3*/
39 0x00000000 /*CRCPARCTL0*/
40 0xC2000040 /*ZQCTL0*/
41 0x02050105 /*DFITMG0*/
42 0x00000202 /*DFITMG1*/
43 0x07000000 /*DFILPCFG0*/
44 0xC0400003 /*DFIUPD0*/
45 0x00000000 /*DFIUPD1*/
46 0x00000000 /*DFIUPD2*/
47 0x00000000 /*DFIPHYMSTR*/
48 0x00000001 /*ODTMAP*/
49 0x00000000 /*DBG0*/
50 0x00000000 /*DBG1*/
51 0x00000000 /*DBGCMD*/
52 0x00000000 /*POISONCFG*/
53 0x00000010 /*PCCFG*/
54 >;
55
56 st,ctl-timing = <
57 0x0080008A /*RFSHTMG*/
58 0x121B2414 /*DRAMTMG0*/
59 0x000D041B /*DRAMTMG1*/
60 0x0607080E /*DRAMTMG2*/
61 0x0050400C /*DRAMTMG3*/
62 0x07040407 /*DRAMTMG4*/
63 0x06060303 /*DRAMTMG5*/
64 0x02020002 /*DRAMTMG6*/
65 0x00000202 /*DRAMTMG7*/
66 0x00001005 /*DRAMTMG8*/
67 0x000D041B /*DRAMTMG14*/
68 0x06000600 /*ODTCFG*/
69 >;
70
71 st,ctl-map = <
72 0x00080808 /*ADDRMAP1*/
73 0x00000000 /*ADDRMAP2*/
74 0x00000000 /*ADDRMAP3*/
75 0x00001F1F /*ADDRMAP4*/
76 0x07070707 /*ADDRMAP5*/
77 0x0F070707 /*ADDRMAP6*/
78 0x00000000 /*ADDRMAP9*/
79 0x00000000 /*ADDRMAP10*/
80 0x00000000 /*ADDRMAP11*/
81 >;
82
83 st,ctl-perf = <
84 0x00001201 /*SCHED*/
85 0x00001201 /*SCHED*/1
86 0x01000001 /*PERFHPR1*/
87 0x08000200 /*PERFLPR1*/
88 0x08000400 /*PERFWR1*/
89 0x00010000 /*PCFGR_0*/
90 0x00000000 /*PCFGW_0*/
91 0x02100B03 /*PCFGQOS0_0*/
92 0x00800100 /*PCFGQOS1_0*/
93 0x01100B03 /*PCFGWQOS0_0*/
94 0x01000200 /*PCFGWQOS1_0*/
95 0x00010000 /*PCFGR_1*/
96 0x00000000 /*PCFGW_1*/
97 0x02100B03 /*PCFGQOS0_1*/
98 0x00800000 /*PCFGQOS1_1*/
99 0x01100B03 /*PCFGWQOS0_1*/
100 0x01000200 /*PCFGWQOS1_1*/
101 >;
102
103 st,phy-reg = <
104 0x01442E02 /*PGCR*/
105 0x10400812 /*ACIOCR*/
106 0x00000C40 /*DXCCR*/
107 0xF200001F /*DSGCR*/
108 0x0000000B /*DCR*/
109 0x00010000 /*ODTCR*/
110 0x0000007B /*ZQ0CR1*/
111 0x0000CE81 /*DX0GCR*/
112 0x0000CE81 /*DX1GCR*/
113 0x0000CE81 /*DX2GCR*/
114 0x0000CE81 /*DX3GCR*/
115 >;
116
117 st,phy-timing = <
118 0x0022A41B /*PTR0*/
119 0x047C0740 /*PTR1*/
120 0x042D9C80 /*PTR2*/
121 0x369477D0 /*DTPR0*/
122 0x098A00D8 /*DTPR1*/
123 0x10023600 /*DTPR2*/
124 0x00000830 /*MR0*/
125 0x00000000 /*MR1*/
126 0x00000208 /*MR2*/
127 0x00000000 /*MR3*/
128 >;
129
130 status = "okay";
131 };
The optional node st,phy-cal allows to use a calibration result when it is present, for example:
1 / {
2 ...
3 soc {
4 ddr: ddr@5a003000{
5 compatible = "st,stm32mp1-ddr";
6 ...
7 st,phy-cal = <
8 0x40000000 /*DX0DLLCR*/
9 0xFFFFFFFF /*DX0DQTR*/
10 0x3DB02000 /*DX0DQSTR*/
11 0x40000000 /*DX1DLLCR*/
12 0xFFFFFFFF /*DX1DQTR*/
13 0x3DB02000 /*DX1DQSTR*/
14 0x40000000 /*DX2DLLCR*/
15 0xFFFFFFFF /*DX2DQTR*/
16 0x3DB02000 /*DX2DQSTR*/
17 0x40000000 /*DX3DLLCR*/
18 0xFFFFFFFF /*DX3DQTR*/
19 0x3DB02000 /*DX3DQSTR*/
20 >;
21 ...
22 };
3.3.2 STM32CubeMX configuration file[edit]
STM32CubeMX generates a .dtsi file with the needed values as defines (named DDR_...), and includes the #Generic DDR dtsi file "stm32mp15-ddr.dtsi"[3]: as this dtsi file is preprocessed during FSBL compilation, it generates a correct device tree.
For example the file fdts/stm32mp15-ddr3-1x4Gb-1066-binG.dtsi is:
/ SPDX-License-Identifier: GPL-2.0+ OR BSD-3-Clause
/*
* File generated by STMicroelectronics STM32CubeMX DDR Tool for MPUs
* DDR type: DDR3 / DDR3L
* DDR width: 16bits
* DDR density: 4Gb
* System frequency: 533000Khz
* Relaxed Timing Mode: false
* Address mapping type: RBC
*
* Save Date: 2020.02.20, save Time: 18:45:20
*/
#define DDR_MEM_NAME "DDR3-DDR3L 16bits 533000Khz"
#define DDR_MEM_SPEED 533000
#define DDR_MEM_SIZE 0x20000000
#define DDR_MSTR 0x00041401
#define DDR_MRCTRL0 0x00000010
#define DDR_MRCTRL1 0x00000000
#define DDR_DERATEEN 0x00000000
#define DDR_DERATEINT 0x00800000
.....
#define DDR_DX2DQSTR 0x3DB02000
#define DDR_DX3GCR 0x0000CE80
#define DDR_DX3DLLCR 0x40000000
#define DDR_DX3DQTR 0xFFFFFFFF
#define DDR_DX3DQSTR 0x3DB02000
#include "stm32mp15-ddr.dtsi"
NB: the calibration values (DXnDLLCR, DXnDQTR, DXnDQSTR, with n in 1...3) are not used when DDR_PHY_CAL_SKIP is not defined
3.3.3 Generic DDR dtsi file[edit]
The dtsi file used with DDR_ defines for STM32MP15x lines is stm32mp15-ddr.dtsi
1 // SPDX-License-Identifier: GPL-2.0+ OR BSD-3-Clause
2 /*
3 * Copyright (C) 2018, STMicroelectronics - All Rights Reserved
4 */
5
6 / {
7 soc {
8 ddr: ddr@5a003000{
9
10 compatible = "st,stm32mp1-ddr";
11
12 reg = <0x5A003000 0x550
13 0x5A004000 0x234>;
14
15 clocks = <&rcc AXIDCG>,
16 <&rcc DDRC1>,
17 <&rcc DDRC2>,
18 <&rcc DDRPHYC>,
19 <&rcc DDRCAPB>,
20 <&rcc DDRPHYCAPB>;
21
22 clock-names = "axidcg",
23 "ddrc1",
24 "ddrc2",
25 "ddrphyc",
26 "ddrcapb",
27 "ddrphycapb";
28
29 st,mem-name = DDR_MEM_NAME;
30 st,mem-speed = <DDR_MEM_SPEED>;
31 st,mem-size = <DDR_MEM_SIZE>;
32
33 st,ctl-reg = <
34 DDR_MSTR
35 DDR_MRCTRL0
36 DDR_MRCTRL1
37 DDR_DERATEEN
38 DDR_DERATEINT
39 DDR_PWRCTL
40 DDR_PWRTMG
41 DDR_HWLPCTL
42 DDR_RFSHCTL0
43 DDR_RFSHCTL3
44 DDR_CRCPARCTL0
45 DDR_ZQCTL0
46 DDR_DFITMG0
47 DDR_DFITMG1
48 DDR_DFILPCFG0
49 DDR_DFIUPD0
50 DDR_DFIUPD1
51 DDR_DFIUPD2
52 DDR_DFIPHYMSTR
53 DDR_ODTMAP
54 DDR_DBG0
55 DDR_DBG1
56 DDR_DBGCMD
57 DDR_POISONCFG
58 DDR_PCCFG
59 >;
60
61 st,ctl-timing = <
62 DDR_RFSHTMG
63 DDR_DRAMTMG0
64 DDR_DRAMTMG1
65 DDR_DRAMTMG2
66 DDR_DRAMTMG3
67 DDR_DRAMTMG4
68 DDR_DRAMTMG5
69 DDR_DRAMTMG6
70 DDR_DRAMTMG7
71 DDR_DRAMTMG8
72 DDR_DRAMTMG14
73 DDR_ODTCFG
74 >;
75
76 st,ctl-map = <
77 DDR_ADDRMAP1
78 DDR_ADDRMAP2
79 DDR_ADDRMAP3
80 DDR_ADDRMAP4
81 DDR_ADDRMAP5
82 DDR_ADDRMAP6
83 DDR_ADDRMAP9
84 DDR_ADDRMAP10
85 DDR_ADDRMAP11
86 >;
87
88 st,ctl-perf = <
89 DDR_SCHED
90 DDR_SCHED1
91 DDR_PERFHPR1
92 DDR_PERFLPR1
93 DDR_PERFWR1
94 DDR_PCFGR_0
95 DDR_PCFGW_0
96 DDR_PCFGQOS0_0
97 DDR_PCFGQOS1_0
98 DDR_PCFGWQOS0_0
99 DDR_PCFGWQOS1_0
100 DDR_PCFGR_1
101 DDR_PCFGW_1
102 DDR_PCFGQOS0_1
103 DDR_PCFGQOS1_1
104 DDR_PCFGWQOS0_1
105 DDR_PCFGWQOS1_1
106 >;
107
108 st,phy-reg = <
109 DDR_PGCR
110 DDR_ACIOCR
111 DDR_DXCCR
112 DDR_DSGCR
113 DDR_DCR
114 DDR_ODTCR
115 DDR_ZQ0CR1
116 DDR_DX0GCR
117 DDR_DX1GCR
118 DDR_DX2GCR
119 DDR_DX3GCR
120 >;
121
122 st,phy-timing = <
123 DDR_PTR0
124 DDR_PTR1
125 DDR_PTR2
126 DDR_DTPR0
127 DDR_DTPR1
128 DDR_DTPR2
129 DDR_MR0
130 DDR_MR1
131 DDR_MR2
132 DDR_MR3
133 >;
134
135 #ifdef DDR_PHY_CAL_SKIP
136 st,phy-cal = <
137 DDR_DX0DLLCR
138 DDR_DX0DQTR
139 DDR_DX0DQSTR
140 DDR_DX1DLLCR
141 DDR_DX1DQTR
142 DDR_DX1DQSTR
143 DDR_DX2DLLCR
144 DDR_DX2DQTR
145 DDR_DX2DQSTR
146 DDR_DX3DLLCR
147 DDR_DX3DQTR
148 DDR_DX3DQSTR
149 >;
150 #endif
151
152 status = "okay";
153 };
154 };
155 };
4 How to configure the DT using STM32CubeMX[edit]
The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX supports all the defines described in the above DT bindings documentation paragraph with a generated included file "stm32mp15-mx.dtsi"; it is included in the mx dts file before the #Generic DDR dtsi file . Refer to the STM32CubeMX user manual and the dedicated application note[5] for further information.
See also How_to_create_your_board_device_tree#DDR configuration with STM32CubeMX DDR Tuning Tool.
If you want to use the STM32CubeMX DDR Tuning Tool calibration result, add in the generated files "stm32mp15-mx.dtsi" the line:
#define DDR_PHY_CAL_SKIP
5 References[edit]
Please refer to the following links for additional information:
- ↑ docs/devicetree/bindings/memory-controllers/st,stm32mp1-ddr.txt TF-A DDR binding information file
- ↑ doc/device-tree-bindings/memory-controllers/st,stm32mp1-ddr.txt U-Boot DDR binding information file
- ↑ 3.03.1 fdts/stm32mp15-ddr.dtsi (for TF-A): STM32MP157C device tree files
- ↑ Cite error: Invalid
<ref>
tag; no text was provided for refs namedAN5168
- ↑ AN5168 - DDR configuration on STM32MP1 Series MPU