Difference between revisions of "Category:Hardware components"

[unchecked revision] [quality revision]
m
m
 
This category groups together all articles and subcategories related to the hardware components used on the STM32 MPU boards, and for which additional software information is needed.

A hardware component is either soldered on a STM32 MPU board (e.g. the Cirrus cs42l51 audio codec for the STM32MP157x_DKx Discovery kits), or plugged into a STM32MPU board via a hardware port (such as the OmniVision OV5640 camera sensor for the STM32MP157C-EV1 Evaluation board).

A hardware component is natively managed by the STM32MPU Embedded Software distributions.

Be careful not to confuse a hardware component with an internal peripheral (a.k.a. hardware block ) which is embedded inside a STM32 MPU microprocessor device.

Hardware components



{| class="st-table" style="border-style: hidden;"
| This category groups together all articles and subcategories related to the hardware components used on the STM32 MPU boards, and for which additional software information is needed.

A hardware component is either soldered on a STM32 MPU board (e.g. the Cirrus cs42l51 audio codec for the STM32MP157x_DKx Discovery kits), or plugged into a STM32MPU board via a hardware port (such as the OmniVision OV5640 camera sensor for the STM32MP157C-EV1 Evaluation board).

A hardware component is natively managed by the STM32MPU Embedded Software distributions.

Be careful not to confuse a hardware component with an [[:Category:Peripherals_-_Hardware_blocks|internal peripheral]] (a.k.a. hardware block ) which is embedded inside a STM32 MPU microprocessor device.
| style="border-style: hidden;" | [[File:Hardware_components.png|150px|link=|Hardware components]]
|}
<noinclude>

{{PublicationRequestId | Auto |  | Automatic approval based on the “Category model” article}}
[[Category:Getting started with ST boardsHardware|03]]</noinclude>
Line 12: Line 12:
 
<noinclude>
 
<noinclude>
 
{{PublicationRequestId | Auto |  | Automatic approval based on the “Category model” article}}
 
{{PublicationRequestId | Auto |  | Automatic approval based on the “Category model” article}}
[[Category:Getting started with ST boards]]
+
[[Category:Hardware|03]]
 
</noinclude>
 
</noinclude>

Subcategories

This category has the following 5 subcategories, out of 5 total.