Difference between revisions of "ADC Linux driver"

[quality revision] [quality revision]
 
m
 
Template:ArticleMainWriter Template:ReviewersList Template:ArticleApprovedVersion

1 Article purpose[edit]

This article introduces the Linux® driver for the ADC[1] internal peripheral:

  • Which ADC features are supported by the driver
  • How to configure, use and debug the driver
  • What is the driver structure, and where the source code can be found.

2 Short description[edit]

The ADC Linux® driver (kernel space) is based on the IIO framework. It supports two modes:

  1. IIO direct mode: single capture on a channel (using interrupts)
  2. IIO triggered buffer mode: capture on one or more channels (preferably using DMA).
    It uses the hardware triggers available in IIO. See TIM Linux driver and LPTIM Linux driver.

3 Configuration[edit]

3.1 Kernel configuration[edit]

Activate the ADC[1] Linux® driver in the kernel configuration using the Linux Menuconfig tool: Menuconfig or how to configure kernel (enable both CONFIG_STM32_ADC_CORE and CONFIG_STM32_ADC).

Device Drivers  --->
   <*> Industrial I/O support  --->
      Analog to digital converters  --->
         <*> STMicroelectronics STM32 adc core
         <*>   STMicroelectronics STM32 adc

3.2 Device tree[edit]

Refer to the ADC device tree configuration article when configuring the ADC Linux kernel driver.

4 How to use[edit]

In "IIO direct mode", the conversion result can be read directly from sysfs (refer to How to do a simple ADC conversion using the sysfs interface).

In "IIO triggered buffer mode", the configuration must be performed using sysfs first. Then, character device (/dev/iio:deviceX) is used to read data (refer to Convert one or more channels using triggered buffer mode).

5 How to trace and debug[edit]

Refer to How to trace with dynamic debug for how to enable the debug logs in the driver and in the framework.

Refer to How to debug with debugfs for how to access the ADC registers.

The ADC has system wide dependencies towards other key resources:

  • runtime power management can be disabled, for example it may be forced on via power/control sysfs entry:
 cd /sys/devices/platform/soc/48003000.adc/48003000.adc:adc@0
 cat power/autosuspend_delay_ms
2000
 cat power/control
auto                                     # kernel is allowed to automatically suspend the ADC device after autosuspend_delay_ms
 echo on > power/control         # force the kernel to resume the ADC device (e.g. keep clocks and regulators enabled)
Info white.png Information
It might be useful to disable runtime power management, in order to dump registers by any means or to check clock and regulator usage (see example below).
  • clock[2] usage can be verified by reading clk_summary:
 cat /sys/kernel/debug/clk/clk_summary | grep adc
         adc12_k                     1        1        0    24000000          0 0
                  adc12              1        1        0   196607910          0 0
  • regulator[3] tree and usage can be verified (e.g. use count, open count or regulator reference voltage) as follows:
 cat /sys/kernel/debug/regulator/regulator_summary
 regulator                      use open bypass voltage current     min     max
-------------------------------------------------------------------------------
    v3v3                          4    5      0  3300mV     0mA  3300mV  3300mV
       vdda                       1    2      0  2900mV     0mA  2900mV  2900mV 
          40017000.dac                                              0mV     0mV
          48003000.adc                                              0mV     0mV
  • pinctrl[4] usage can be verified by reading pinmux-pins:
 cd /sys/kernel/debug/pinctrl/soc\:pin-controller@50002000/
 cat pinmux-pins | grep adc
pin 92 (PF12): device 48003000.adc function analog group PF12   # check pin is assigned to ADC and is configured as "analog"
  • interrupts can be verified by reading "interrupts":
 cat /proc/interrupts
           CPU0       CPU1
 56:          2          0     dummy   0 Edge      48003000.adc:adc@0

6 Source code location[edit]

The ADC source code is composed of:

  • stm32-adc-core driver to handle common resources such as clock (selection, prescaler), regulator used as reference voltage, interrupt and common registers.
  • stm32-adc driver to handle the resources available for each ADC such as channel configuration and buffer handling.

7 References[edit]


<noinclude>

{{ArticleBasedOnModel | [[Linux driver article model]]}}
{{ArticleMainWriter | FabriceG}}
{{ReviewersList | ArnaudP, OlivierM}}
{{ArticleApprovedVersion | FabriceG | OlivierM, ArnaudP | No previous approved version | AnneJ - 23Oct'18 - 9337 | 05Nov'18}}
[[Category:IIO]]</noinclude>

== Article purpose ==
This article introduces the Linux<sup>&reg;</sup> driver for the ADC<ref name="ADC internal peripheral">[[ADC internal peripheral]]</ref> internal peripheral:
* Which ADC features are supported by the driver
* How to configure, use and debug the driver 
* What is the driver structure, and where the source code can be found.

== Short description ==
The ADC Linux<sup>&reg;</sup> driver (kernel space) is based on the [[IIO overview|IIO]] framework.
It supports two modes:
# '''IIO direct mode''': single capture on a channel (using interrupts)
# '''IIO triggered buffer mode''': capture on one or more channels (preferably using DMA).<br/>It uses the hardware triggers available in IIO. See [[TIM Linux driver]] and [[LPTIM Linux driver]].

== Configuration ==
=== Kernel configuration ===
Activate the ADC<ref name="ADC internal peripheral"/> Linux<sup>&reg;</sup> driver in the kernel configuration using the Linux Menuconfig tool: [[Menuconfig or how to configure kernel]] (enable both CONFIG_STM32_ADC_CORE and CONFIG_STM32_ADC).<pre>

Device Drivers  ---><*> Industrial I/O support  --->
      Analog to digital converters  ---><*> STMicroelectronics STM32 adc core<*>   STMicroelectronics STM32 adc</pre>


=== Device tree ===
Refer to the [[ADC device tree configuration]] article when configuring the ADC Linux kernel driver.

== How to use ==
In "'''IIO direct mode'''", the conversion result can be read directly from '''sysfs''' (refer to
[[How to use the IIO user space interface#How to do a simple ADC conversion using the sysfs interface|How to do a simple ADC conversion using the sysfs interface]]).

In "'''IIO triggered buffer mode'''", the configuration must be performed using '''sysfs''' first. Then, '''character device''' (/dev/iio:deviceX) is used to read data (refer to [[How to use the IIO user space interface#Convert one or more channels using triggered buffer mode|Convert one or more channels using triggered buffer mode]]).

== How to trace and debug ==
Refer to [[IIO_overview#How_to_trace_with_dynamic_debug|How to trace with dynamic debug]] for how to '''enable the debug logs''' in the driver and in the framework.

Refer to [[IIO_overview#How_to_debug_with_debugfs|How to debug with debugfs]] for how to '''access the ADC registers'''.

The ADC has system wide dependencies towards other key resources:
* '''runtime power management''' can be disabled, for example it may be forced '''on''' via ''power/control'' sysfs entry:
 {{Board$}} cd /sys/devices/platform/soc/48003000.adc/48003000.adc:adc@0
 {{Board$}} cat power/autosuspend_delay_ms
 2000
 {{Board$}} cat power/control
 auto                                     # kernel is allowed to automatically suspend the ADC device after autosuspend_delay_ms
 {{Board$}} {{highlight|echo on > power/control}}         # force the kernel to resume the ADC device (e.g. keep clocks and regulators enabled)
{{Info| It might be useful to disable runtime power management, in order to dump registers by any means or to check clock and regulator usage (see example below).}}

* '''clock'''<ref name="Clock overview">[[Clock overview]]</ref> usage can be verified by reading ''clk_summary'':
 {{Board$}} {{highlight|cat /sys/kernel/debug/clk/clk_summary}} | grep adc
          adc12_k                     1        1        0    24000000          0 0
                   adc12              1        1        0   196607910          0 0

* '''regulator'''<ref name="Regulator overview">[[Regulator overview]]</ref> tree and usage can be verified (e.g. use count, open count or regulator reference voltage) as follows:
 {{Board$}} {{highlight|cat /sys/kernel/debug/regulator/regulator_summary}}
  regulator                      use open bypass voltage current     min     max
 -------------------------------------------------------------------------------
     v3v3                          4    5      0  3300mV     0mA  3300mV  3300mV
        vdda                       1    2      0  2900mV     0mA  2900mV  2900mV 
           40017000.dac                                              0mV     0mV
           48003000.adc                                              0mV     0mV

* '''pinctrl'''<ref name="Pinctrl_overview">[[Pinctrl overview]]</ref> usage can be verified by reading ''pinmux-pins'':
 {{Board$}} cd /sys/kernel/debug/pinctrl/soc\:pin-controller@50002000/
 {{Board$}} {{highlight|cat pinmux-pins}} | grep adc
 pin 92 (PF12): device 48003000.adc function {{highlight|analog}} group PF12   # check pin is assigned to ADC and is configured as "analog"

* '''interrupts''' can be verified by reading "interrupts":
 {{Board$}} {{highlight|cat /proc/interrupts}}
            CPU0       CPU1
  56:          2          0     dummy   0 Edge      48003000.adc:adc@0

== Source code location ==
The ADC source code is composed of:
* {{CodeSource | Linux kernel | drivers/iio/adc/stm32-adc-core.c | stm32-adc-core driver}} to handle common resources such as clock (selection, prescaler), [[Regulator overview|regulator]] used as reference voltage, interrupt and common registers.
* {{CodeSource | Linux kernel | drivers/iio/adc/stm32-adc.c | stm32-adc driver}} to handle the resources available for each ADC such as  channel configuration and buffer handling.

==References==<references />

<noinclude>

[[Category:IIO]]
{{PublicationRequestId | 9337 | 2018-10-23 | AnneJ}}
{{ArticleBasedOnModel | Linux driver article model}}</noinclude>
(2 intermediate revisions by 2 users not shown)
Line 1: Line 1:
<noinclude>
 
{{ArticleBasedOnModel | [[Linux driver article model]]}}
 
{{ArticleMainWriter | FabriceG}}
 
{{ReviewersList | ArnaudP, OlivierM}}
 
{{ArticleApprovedVersion | FabriceG | OlivierM, ArnaudP | No previous approved version | AnneJ - 23Oct'18 - 9337 | 05Nov'18}}
 
[[Category:IIO]]
 
</noinclude>
 
 
 
== Article purpose ==
 
== Article purpose ==
 
This article introduces the Linux<sup>&reg;</sup> driver for the ADC<ref name="ADC internal peripheral">[[ADC internal peripheral]]</ref> internal peripheral:
 
This article introduces the Linux<sup>&reg;</sup> driver for the ADC<ref name="ADC internal peripheral">[[ADC internal peripheral]]</ref> internal peripheral:
Line 85: Line 77:
 
==References==
 
==References==
 
<references />
 
<references />
  +
  +
<noinclude>
  +
[[Category:IIO]]
  +
{{PublicationRequestId | 9337 | 2018-10-23 | AnneJ}}
  +
{{ArticleBasedOnModel | Linux driver article model}}
  +
</noinclude>