Difference between revisions of "STM32MP157x-DKx - board assembly"

[quality revision] [quality revision]
m
 

Template:ArticleApprovedVersion This article explains how to assemble the STM32MP157x-DKx Discovery kits. It is valid both for the STM32MP157A-DK1 and STM32MP157C-DK2 Discovery kits: the part numbers are specified in the STM32MP15 microprocessor part numbers article.

Warning white.png Warning
To successfully start the board, it is recommended to go through the corresponding Starter Package article: Category:Starter Package


The STM32MP157x-DKx Discovery kits packages (STM32MP157A-DK1 and STM32MP157C-DK2) are delivered assembled, and contain the items listed below. A USB Type-C cable is also included.

Please note that;

  • the STM32MP157A-DK1 Discovery kit neither includes the "WLAN + Bluetooth" component (muRata LBEE5KL1DX), nor the MB1407 daughterboard DSI display
  • the STM32MP157C-DK2 Discovery kit includes the "WLAN + Bluetooth" component (muRata LBEE5KL1DX), and the MB1407 daughterboard DSI display
Position Description
1 MB1272 motherboard ("WLAN + Bluetooth" component included only for the STM32MP157C-DK2 Discovery kit)
2 MB1407 daughterboard DSI display (480x800 pixels): only for the STM32MP157C-DK2 Discovery kit
3 microSD card


STM32MP157x-DKx Discovery kit assembled
STM32MP157C-DK2 shown here (picture not contractual)
(for the STM32MP157A-DK1, the element 2 is not present)


<noinclude>
{{ArticleApprovedVersion | Jean-ChristopheT | BernardP, GeraldB | No previous approved version | AnneJ - 07Aug'18 - 8427 | 09Aug'18}}
[[Category:Sub-articles]]This article explains how to assemble the '''STM32MP157x-DKx''' Discovery kits. It is valid both for the STM32MP157A-DK1 and STM32MP157C-DK2 Discovery kits: the part numbers are specified in the [[STM32MP15 microprocessor#Part number codification|STM32MP15 microprocessor part numbers]] article.
{{Warning|To successfully start the board, it is recommended to go through the corresponding Starter Package article: [[:Category:Starter Package]]}}</noinclude>


The STM32MP157x-DKx Discovery kits packages (STM32MP157A-DK1 and STM32MP157C-DK2) are delivered assembled, and contain the items listed below. A USB Type-C<sup>&trade;</sup> cable is also included.

Please note that;
* the '''STM32MP157A-DK1''' Discovery kit neither includes the  "WLAN + Bluetooth" component (muRata LBEE5KL1DX), nor the MB1407 daughterboard DSI display
* the '''STM32MP157C-DK2''' Discovery kit includes the  "WLAN + Bluetooth" component (muRata LBEE5KL1DX), and the MB1407 daughterboard DSI display

{|
|+ 
! Position !! Description                                               
|-
| 1 || [[MB1272]] motherboard ("WLAN + Bluetooth" component included only for the '''STM32MP157C-DK2''' Discovery kit)
|-
| 2 || [[MB1407]] daughterboard DSI display (480x800 pixels): only for the '''STM32MP157C-DK2''' Discovery kit
|-
| 3 || microSD card
|}<br clear=all>

[[File: STM32MP157x-DKx_assembled.png | thumb | upright=4 | center | link= | STM32MP157x-DKx Discovery kit assembled <br> '''STM32MP157C-DK2''' shown here (picture not contractual) <br> (for the STM32MP157A-DK1, the element 2 is not present)]]

<noinclude>

[[Category:Sub-articles]]
{{PublicationRequestId | 8427 | 2018-08-07 | AnneJ}}</noinclude>
Line 1: Line 1:
 
<noinclude>
 
<noinclude>
{{ArticleApprovedVersion | Jean-ChristopheT | BernardP, GeraldB | No previous approved version | AnneJ - 07Aug'18 - 8427 | 09Aug'18}}
 
[[Category:Sub-articles]]
 
 
This article explains how to assemble the '''STM32MP157x-DKx''' Discovery kits. It is valid both for the STM32MP157A-DK1 and STM32MP157C-DK2 Discovery kits: the part numbers are specified in the [[STM32MP15 microprocessor#Part number codification|STM32MP15 microprocessor part numbers]] article.
 
This article explains how to assemble the '''STM32MP157x-DKx''' Discovery kits. It is valid both for the STM32MP157A-DK1 and STM32MP157C-DK2 Discovery kits: the part numbers are specified in the [[STM32MP15 microprocessor#Part number codification|STM32MP15 microprocessor part numbers]] article.
 
{{Warning|To successfully start the board, it is recommended to go through the corresponding Starter Package article: [[:Category:Starter Package]]}}
 
{{Warning|To successfully start the board, it is recommended to go through the corresponding Starter Package article: [[:Category:Starter Package]]}}
Line 24: Line 22:
 
<br clear=all>
 
<br clear=all>
 
[[File: STM32MP157x-DKx_assembled.png | thumb | upright=4 | center | link= | STM32MP157x-DKx Discovery kit assembled <br> '''STM32MP157C-DK2''' shown here (picture not contractual) <br> (for the STM32MP157A-DK1, the element 2 is not present)]]
 
[[File: STM32MP157x-DKx_assembled.png | thumb | upright=4 | center | link= | STM32MP157x-DKx Discovery kit assembled <br> '''STM32MP157C-DK2''' shown here (picture not contractual) <br> (for the STM32MP157A-DK1, the element 2 is not present)]]
  +
  +
<noinclude>
  +
[[Category:Sub-articles]]
  +
{{PublicationRequestId | 8427 | 2018-08-07 | AnneJ}}
  +
</noinclude>