This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1 System Workbench for STM32 - STM32-CoPro-MPU Plugin[edit source]
1.1 Overview[edit source]
In order to support the STM32 MPU Family, ST provides STM32-CoPro-MPU plugin which completes SystemWorkbench for STM32 from Ac6.
This plugin is delivered in SW4STM32 from version 2.9.0.
This plugin addresses the Cortex®-M located inside the STM32MP1 Series. It provides:
- Target Status Widget
- Console Management
- Cortex®-M Project Creation, Compilation and Debug in two modes:
- Engineering Mode, with Cortex®-M firmware download via JTAG/SWD
- Production Mode, with Cortex®-M firmware download :
- via Ethernet Link to the LAN or Point-to-Point
- via Ethernet-over-USB for point-to-point connection
- Support of STM32CubeMX generated projects
- Remote Target Path project property (for Production Mode)
- Remote System Explorer configuration
It is available on Linux® and Windows® platforms.
1.2 Perspectives[edit source]
1.2.1 C/C++ Perspective[edit source]
C/C++ Perspective allows to build a Cortex-M project for STM32MP1 boards (STM32MP157C-EV1 and STM32MP157C-DK2)
1.2.2 Debug Configuration[edit source]
Debug Configuration allows to select Production or Engineering modes.
1.3 Documentation[edit source]
- The STM32-CoPro-MPU plugin is delivered with SystemWorkbench for STM32 available on OpenSTM32 Community site
- The Help > Help Contents available inside the Eclipse IDE includes a dedicated section STM32 MCU User Guide > Micro Processor Unit (MPU) Family - MCU support
- Project creation
- Build configuration
- Target management
- Debug an MCU application
- Remote System Explorer
- Tips and tricks