Last edited 5 years ago

MB1272

The printable version is no longer supported and may have rendering errors. Please update your browser bookmarks and please use the default browser print function instead.

MB1272 board overview.

1. Board overview[edit source]

MB1272 motherboard STM32MP157x 12x12 with PMIC and DDR3, revision C-0.1: part of the STM32MP157x-DKx Discovery kit

Note that:

  • MB1272 for STM32MP157A-DK1 Discovery kit doesn't include the "WLAN + Bluetooth" component (muRata LBEE5KL1DX)
  • MB1272 for STM32MP157C-DK2 Discovery kit includes the "WLAN + Bluetooth" component (Murata LBEE5KL1DX)


GPIO expansionWLAN + Bluetooth (muRata LBEE5KL1DX): only for STM32MP157C-DK2 Discovery kitBackup battery connectorDSI LCD connectorPMIC (STPMIC1A)DDR3L 16 bitsUSB type A LED (red LD1)4 x USB type A (host)USB type C (power 5V-3A)Power LED (green LD2)STM32MP157x 12x12HDMIUSB type C (DRP)EthernetEthernet LED (green LD3)Wakeup buttonAudio codec headsetAudio codec (Cirrus CS42L51)Reset buttonUser LED (green LD5)User button (USER1)User LED (red LD6)User button (USER2)User LED (orange LD7)User LED (blue LD8)USB micro-B (ST-LINK/V2-1)ST-LINK/V2-1 LED (bicolor LD4)ST-LINK/V2-1 DFUHDMI connector
MB1272 front side (picture not contractual)


Details of some LEDs:

  • LD1: red if USB type A connection established
  • LD2: green if power connection established
  • LD3: green flashing the Ethernet connection established
  • LD4: red flashing if ST-LINK/V2-1 connection not established, else green
  • LD5, LD6, LD7, LD8: some user LEDs are used to reflect the system activity, whereas the others are left free and can be directly used by the application, as explained in the LEDs and buttons on STM32 MPU boards article


Arduino Uno connector (part 1)Arduino LED (green LD9)MicroSD 3.0 cardBoot mode selectionArduino Uno connector (part 2)
MB1272 back side (picture is not contractual)

2. Links[edit source]

MB1272 schematics