Difference between revisions of "Latest wiki"

[quality revision] [quality revision]
m
m
 

This page aims to provide link to the flagship/latest wiki.
Each ecosystem releases flow has its corresponding wiki.

An ecosystem release flow designates all the ecosystem releases which are based on the same versions of the major software components (e.g. Linux® kernel) of the OpenSTLinux distribution (see details in the below table).
Each vx flow groups together all the vx.y.z ecosystem releases, and has its own wiki.

The most recent flow is associated with the flagship/latest wiki (whose URL is "https://wiki.st.com/stm32mpu"), while the previous flows are associated with archived wikis (whose URLs are "https://wiki.st.com/stm32mpu-ecosystem-vx").

This current wiki is a wiki archived for the v1 flow (v1.y.z ecosystem releases): if you need information about this ecosystem releases flow, continue browsing this wiki.

However, if you discover the STM32 Arm® Cortex®-based MPUs, it is highly recommended to browse the flagship/latest wiki that contains the latest major ecosystem release:

STM32 MPU wiki by ST.png
STM32 MPU flagship/latest wiki for the v3.y.z ecosystem releases


Wikis and software components
Wiki Major ecosystem releases Major software components (OpenSTLinux distribution)
Wiki for the v2 flow

v2.1.0
v2.0.0

Linux® kernel v5.4 (LTS)
U-Boot v2020.01
TF-A v2.2
OP-TEE v3.9.0
OpenEmbedded v3.1 (Dunfell)

This wiki - Wiki for the v1 flow

v1.2.0
v1.1.0
v1.0.0

Linux® kernel v4.19 (LTS)
U-Boot v2018.11
TF-A v2.0
OP-TEE v3.3.0
OpenEmbedded v2.6 (Thud)


This page aims to provide link to the flagship/latest wiki.<br>

Each ecosystem releases flow has its corresponding wiki.

An '''ecosystem release flow''' designates all the '''ecosystem releases''' which are based on the '''same versions of the major software components''' (e.g. Linux<sup>&reg;</sup> kernel) of the OpenSTLinux distribution (see details in the below table).<br>

Each '''v''x''''' flow groups together all the '''v''x''.''y''.''z''''' ecosystem releases, and has '''its own wiki'''.

The most recent flow is associated with the '''flagship/latest wiki''' (whose URL is "<nowiki>https:</nowiki>//wiki.st.com/stm32mpu"), while the previous flows are associated with '''archived wikis''' (whose URLs are "<nowiki>https:</nowiki>//wiki.st.com/stm32mpu-ecosystem-v''x''").

{{Highlight|This current wiki is a wiki archived for the '''v1''' flow ('''v1.''y''.''z''''' ecosystem releases)}}: if you need information about this ecosystem releases flow, continue browsing this wiki.{{ReviewsComments|-- [[User:Jean Christophe Trotin|Jean Christophe Trotin]] ([[User talk:Jean Christophe Trotin|talk]]) 09:55, 2 April 2021 (CEST)<br />Useless to have 2 interwiki links "stm32mpu" and "stm32mpuMain". In [[Special:InterWikiLinks]], all the interwiki links are in lowercase, and have no special characters such as "_", so I propose that the interwiki link towards the main wiki is named "stm32mpumain".}}

However, {{Highlight|if you discover the STM32 Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-based MPUs, it is highly recommended to browse the flagship/latest wiki}} that contains the [[stm32mpu:STM32MP15 ecosystem release note|latest major ecosystem release]]:
{| class="st-table"
|-
| [[File:STM32_MPU_wiki_by_ST.png|center|200px|link=stm32mpu:Main Page]]
| STM32 MPU flagship/latest wiki for the {{Highlight|v3.''y''.''z''}} ecosystem releases
|}


{| class="st-table"
|+ Wikis and software components
! Wiki !! Major ecosystem releases !! Major software components (OpenSTLinux distribution)
|-
| [[stm32mpuv2:Main Page|Wiki for the v2 flow]]
|
v2.1.0<br>

v2.0.0
|
Linux<sup>&reg;</sup> kernel v5.4 (LTS)<br>

U-Boot v2020.01<br>

TF-A v2.2<br>

OP-TEE v3.9.0<br>

OpenEmbedded v3.1 (Dunfell)
|-
| [[Main_Page|This wiki - Wiki for the v1 flow]]
|
v1.2.0<br>

v1.1.0<br>

v1.0.0
|
Linux<sup>&reg;</sup> kernel v4.19 (LTS)<br>

U-Boot v2018.11<br>

TF-A v2.0<br>

OP-TEE v3.3.0<br>

OpenEmbedded v2.6 (Thud)
|}
<noinclude>

[[Category:MainMenuTab2]]
{{PublicationRequestId}}</noinclude>
Line 8: Line 8:
   
 
{{Highlight|This current wiki is a wiki archived for the '''v1''' flow ('''v1.''y''.''z''''' ecosystem releases)}}: if you need information about this ecosystem releases flow, continue browsing this wiki.
 
{{Highlight|This current wiki is a wiki archived for the '''v1''' flow ('''v1.''y''.''z''''' ecosystem releases)}}: if you need information about this ecosystem releases flow, continue browsing this wiki.
{{ReviewsComments|-- [[User:Jean Christophe Trotin|Jean Christophe Trotin]] ([[User talk:Jean Christophe Trotin|talk]]) 09:55, 2 April 2021 (CEST)<br />Useless to have 2 interwiki links "stm32mpu" and "stm32mpuMain". In [[Special:InterWikiLinks]], all the interwiki links are in lowercase, and have no special characters such as "_", so I propose that the interwiki link towards the main wiki is named "stm32mpumain".}}
 
   
 
However, {{Highlight|if you discover the STM32 Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-based MPUs, it is highly recommended to browse the flagship/latest wiki}} that contains the [[stm32mpu:STM32MP15 ecosystem release note|latest major ecosystem release]]:
 
However, {{Highlight|if you discover the STM32 Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-based MPUs, it is highly recommended to browse the flagship/latest wiki}} that contains the [[stm32mpu:STM32MP15 ecosystem release note|latest major ecosystem release]]: