Difference between revisions of "LPTIM device tree configuration"

[quality revision] [unchecked revision]
m
m (Article purpose)

1 Article purpose[edit]

The purpose of this article is to explain how to configure the low-power timer (LPTIM)[1] when the peripheral is assigned to Linux® OS, and in particular:

  • how to configure the LPTIM peripheral to enable PWM, trigger, event counter and quadrature encoder
  • how to configure the board, e.g. LPTIM input/output pins

The configuration is performed using the device tree mechanism[2].

It is used by the LPTIM Linux driver that registers relevant information in PWM and IIO frameworks.

If the peripheral is assigned to another execution context, refer to How to assign an internal peripheral to a runtime context article for guidelines on peripheral assignment and configuration.

2 DT bindings documentation[edit]

The LPTIM[1] is a multifunction device (MFD).

Each function is represented by a separate binding document:

  • STM32 LPTIM MFD device tree bindings[3] deals with core resources (e.g. registers, clock)
  • STM32 LPTIM PWM device tree bindings[4] deals with PWM interface resources (e.g. PWM pins)
  • STM32 LPTIM trigger device tree bindings[5] deals with LPTIM triggers resources (e.g. trigger output connected to other STM32 internal peripherals)
  • STM32 LPTIM counter device tree bindings[6] deals with LPTIM counter and quadrature encoder resources (e.g. counter/encoder IN[1..2] pins)

3 DT configuration[edit]

This hardware description is a combination of STM32 microprocessor and board device tree files. See Device tree for more explanations on device tree file split.

The STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.

LPTIM configured as event counter and quadrature encoder LPTIM configured as PWM and trigger source LPTIM configured as PWM and trigger source
LPTIM DT configuration

3.1 DT configuration (STM32 level)[edit]

LPTIM nodes are declared in stm32mp157c.dtsi[7].

DT root node (aka lptimer1, ..., lptimer5) and DT child nodes describe the LPTIM features such as:

  • PWM
  • trigger
  • event counter and quadrature encoder.

They also describe hardware parameters such as register addresses and clock.

lptimer1: timer@40009000 {
	compatible = "st,stm32-lptimer";                      /* lptimer's common resources */
	...
	pwm {
		compatible = "st,stm32-pwm-lp";               /* PWM part of LPTIM */
	};
	trigger@0 {
		compatible = "st,stm32-lptimer-trigger";      /* trigger part of LPTIM */
		reg = <0>;                                    /* trigger identifier (e.g. 0 for LPTIM1 trigger, 1 for LPTIM2... */
	};
	counter {
		compatible = "st,stm32-lptimer-counter";      /* quadrature encoder & event counter part of LPTIM */
	};
};
Warning white.png Warning
This device tree part is related to STM32 microprocessors. It should be kept as is, without being modified by the end-user.

3.2 DT configuration (board level)[edit]

Follow the below sequence to configure and enable the LPTIM on your board STM32MP15 microprocessor:

  • Enable DT root node for the LPTIM instance in use (e.g lptimer1, ..., lptimer5), with status = "okay";
  • Enable DT child node(s) for the feature(s) in use (PWM output, trigger, event counter and quadrature encoder), with status = "okay";
  • Configure the pins in use via pinctrl, with pinctrl-0, pinctrl-1 and pinctrl-names.

3.3 DT configuration examples[edit]

3.3.1 LPTIM1 configured as PWM and trigger source[edit]

The example below shows how to configure LPTIM1 to act as:

lppwm1_pins_a: lppwm1-0 {
 	pins {
		pinmux = <STM32_PINMUX('G', 13, AF1)>;    /* configure 'PG13' as alternate 1 for LPTIM1_OUT mode of operation */
		bias-pull-down;
		drive-push-pull;
		slew-rate = <0>;
 	};
};
lppwm1_sleep_pins_a: lppwm1-sleep-0 {
	pins {
		pinmux = <STM32_PINMUX('G', 13, ANALOG)>; /* configure 'PG13' as analog for low power mode */
	};
};
&lptimer1 {
	status = "okay";
	pwm {
		pinctrl-0 = <&lppwm1_pins_a>;             /* configure PWM on LPTIM1_OUT */
		pinctrl-1 = <&lppwm1_sleep_pins_a>;
		pinctrl-names = "default", "sleep";
		status = "okay";                          /* enable PWM on LPTIM1 */
	};
	trigger@0 {
		status = "okay";                          /* enable LPTIM1_OUT trigger source */
	};
};

3.3.2 LPTIM2 configured as counter and quadrature encoder[edit]

The example below shows how to configure LPTIM2 to act as counter and/or quadrature encoder, with LPTIM2_IN1 and LPTIM2_IN2 pins configured as inputs on PD12 and PD11, respectively (See pinctrl device tree configuration and GPIO internal peripheral)

# part of pin-controller dt node
lptim2_in_pins_a: lptim2-in-pins-0 {
	pins {
		pinmux = <STM32_PINMUX('D', 12, AF3)>, /* LPTIM2_IN1 */
			 <STM32_PINMUX('D', 11, AF3)>; /* LPTIM2_IN2 */
		bias-disabled;
	};
};
lptim2_sleep_in_pins_a: lptim2-sleep-in-pins-0 {
	pins {
		pinmux = <STM32_PINMUX('D', 12, ANALOG)>, /* LPTIM2_IN1 */
			 <STM32_PINMUX('D', 11, ANALOG)>; /* LPTIM2_IN2 */
	};
};
&lptimer2 {
	status = "okay";
	counter {
		pinctrl-0 = <&lptim2_in_pins_a>;          /* configure LPTIM2 counter/encoder pins */
		pinctrl-1 = <&lptim2_sleep_in_pins_a>;
		pinctrl-names = "default", "sleep";
		status = "okay";                          /* enable counter/encoder on LPTIM2 */
	};
};

4 How to configure the DT using STM32CubeMX[edit]

The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.

5 References[edit]

For additional information, refer to the following links:




== Article purpose ==
The purpose of this article is to explain how to configure the low-power timer (''LPTIM'')<ref name="LPTIM internal peripheral"> [[LPTIM internal peripheral]]</ref> ''' when the peripheral is assigned to Linux<sup>&reg;</sup> OS''', and in particular:
* how to configure the LPTIM '''peripheral''' to enable PWM, trigger, event counter and quadrature encoder
* how to configure the '''board''', e.g. LPTIM input/output pins
The configuration is performed using the '''device tree mechanism'''<ref> [[Device tree]]</ref>.

It is used by the [[LPTIM Linux driver]] that registers relevant information in [[PWM overview|PWM]] and [[IIO overview|IIO]] frameworks.
If the peripheral is assigned to another execution context, refer to [[How to assign an internal peripheral to a runtime context]] article for guidelines on peripheral assignment and configuration.
== DT bindings documentation ==

The LPTIM<ref name="LPTIM internal peripheral"/> is a multifunction device (MFD).

Each function is represented by a separate binding document:
* ''STM32 LPTIM MFD device tree bindings''<ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/mfd/stm32-lptimer.txt | Documentation/devicetree/bindings/mfd/stm32-lptimer.txt}}, STM32 LPTIM MFD device tree bindings</ref> deals with core resources (e.g. registers, clock)

* ''STM32 LPTIM PWM device tree bindings''<ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/pwm/pwm-stm32-lp.txt | Documentation/devicetree/bindings/pwm/pwm-stm32-lp.txt}}, STM32 LPTIM PWM device tree bindings</ref> deals with '''PWM''' interface resources (e.g. PWM pins)

* ''STM32 LPTIM trigger device tree bindings''<ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/iio/timer/stm32-lptimer-trigger.txt | Documentation/devicetree/bindings/iio/timer/stm32-lptimer-trigger.txt}}, STM32 LPTIM trigger device tree bindings</ref> deals with '''LPTIM triggers''' resources (e.g. trigger output connected to other STM32 internal peripherals)

* ''STM32 LPTIM counter device tree bindings''<ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/iio/counter/stm32-lptimer-cnt.txt | Documentation/devicetree/bindings/iio/counter/stm32-lptimer-cnt.txt}}, STM32 LPTIM counter/encoder device tree bindings</ref> deals with '''LPTIM counter and quadrature encoder''' resources (e.g. counter/encoder IN[1..2] pins)

== DT configuration ==
This hardware description is a combination of STM32 microprocessor and board device tree files. See [[Device tree]] for more explanations on device tree file split.

The '''STM32CubeMX''' can be used to generate the board device tree. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX|How to configure the DT using STM32CubeMX]] for more details.
{{
ImageMap|Image:LPTIM DT configuration.png {{!}} thumb {{!}} 800px {{!}} center{{!}} LPTIM DT configuration
rect 376 238 524 295 [[#LPTIM2_configured_as_counter_and_quadrature_encoder|LPTIM configured as event counter and quadrature encoder]]
rect 556 238 704 295 [[#LPTIM1_configured_as_PWM_and_trigger_source|LPTIM configured as PWM and trigger source]]
rect 737 238 885 295 [[#LPTIM1_configured_as_PWM_and_trigger_source|LPTIM configured as PWM and trigger source]]
}}

=== DT configuration (STM32 level) ===

LPTIM nodes are declared in stm32mp157c.dtsi<ref name="stm32mp157c_dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp157c.dtsi | STM32MP157C device tree file}}</ref>.

'''DT root node''' (aka lptimer1, ..., lptimer5) and '''DT child nodes'''  describe the [[LPTIM internal peripheral#Features|LPTIM features]] such as:
* PWM
* trigger
* event counter and quadrature encoder.

They also describe hardware parameters such as register addresses and clock.
 lptimer1: timer@40009000 {
 	compatible = "st,stm32-lptimer";                      {{highlight|/* lptimer's common resources */}}
 	...
 	pwm {
 		compatible = "st,stm32-pwm-lp";               {{highlight|/* PWM part of LPTIM */}}
 	};
 	trigger@'''0''' {
 		compatible = "st,stm32-lptimer-trigger";      {{highlight|/* trigger part of LPTIM */}}
 		reg = <'''0'''>;                                    {{highlight|/* trigger identifier (e.g. 0 for LPTIM1 trigger, 1 for LPTIM2... */}}
 	};
 	counter {
 		compatible = "st,stm32-lptimer-counter";      {{highlight|/* quadrature encoder & event counter part of LPTIM */}}
 	};
 };
{{Warning|This device tree part is related to STM32 microprocessors. It should be kept as is, without being modified by the end-user.}}

=== DT configuration (board level) ===

Follow the below sequence to configure and enable the LPTIM on your board STM32MP15 microprocessor:
* Enable '''DT root node''' for the LPTIM instance in use (e.g lptimer1, ..., lptimer5), with '''status = "okay";'''
* Enable '''DT child node(s)''' for the feature(s) in use (PWM output, trigger, event counter and quadrature encoder), with '''status = "okay";'''
* Configure the pins in use via [[Pinctrl overview|pinctrl]], with '''pinctrl-0''', '''pinctrl-1''' and '''pinctrl-names'''.

=== DT configuration examples ===
==== LPTIM1 configured as PWM and trigger source ====
The example below shows how to configure LPTIM1 to act as:
* PWM output on PG13 ([[Pinctrl_device_tree_configuration|See pinctrl device tree configuration]] and [[GPIO internal peripheral]])
* trigger source (in Synchronous mode with PWM) for other internal peripherals such as ADC<ref name="adc_internal">[[ADC internal peripheral]]</ref>, DAC<ref name="dac_internal">[[DAC internal peripheral]]</ref>, and DFSDM<ref name="dfsdm_internal">[[DFSDM internal peripheral]]</ref>


 lppwm1_pins_a: lppwm1-0 {
  	pins {
 		pinmux = <STM32_PINMUX('G', 13, AF1)>;    {{highlight|/* configure 'PG13' as alternate 1 for LPTIM1_OUT mode of operation */}}
 		bias-pull-down;
 		drive-push-pull;
 		slew-rate = <0>;
  	};
 };
 lppwm1_sleep_pins_a: lppwm1-sleep-0 {
 	pins {
 		pinmux = <STM32_PINMUX('G', 13, ANALOG)>; {{highlight|/* configure 'PG13' as analog for low power mode */}}
 	};
 };

 &lptimer1 {
 	status = "{{highlight|okay}}";
 	pwm {
 		pinctrl-0 = <&lppwm1_pins_a>;             {{highlight|/* configure PWM on LPTIM1_OUT */}}
 		pinctrl-1 = <&lppwm1_sleep_pins_a>;
 		pinctrl-names = "default", "sleep";
 		status = "{{highlight|okay}}";                          {{highlight|/* enable PWM on LPTIM1 */}}
 	};
 	trigger@0 {
 		status = "{{highlight|okay}}";                          {{highlight|/* enable LPTIM1_OUT trigger source */}}
 	};
 };

==== LPTIM2 configured as counter and quadrature encoder ====
The example below shows how to configure LPTIM2 to act as counter and/or quadrature encoder, with LPTIM2_IN1 and LPTIM2_IN2 pins configured as inputs on PD12 and PD11, respectively ([[Pinctrl_device_tree_configuration|See pinctrl device tree configuration]] and [[GPIO internal peripheral]])
 # part of pin-controller dt node
 lptim2_in_pins_a: lptim2-in-pins-0 {
 	pins {
 		pinmux = <STM32_PINMUX('D', 12, AF3)>, /* LPTIM2_IN1 */<STM32_PINMUX('D', 11, AF3)>; /* LPTIM2_IN2 */
 		bias-disabled;
 	};
 };
 lptim2_sleep_in_pins_a: lptim2-sleep-in-pins-0 {
 	pins {
 		pinmux = <STM32_PINMUX('D', 12, ANALOG)>, /* LPTIM2_IN1 */<STM32_PINMUX('D', 11, ANALOG)>; /* LPTIM2_IN2 */
 	};
 };

 &lptimer2 {
 	status = "{{highlight|okay}}";
 	counter {
 		pinctrl-0 = <&lptim2_in_pins_a>;          {{highlight|/* configure LPTIM2 counter/encoder pins */}}
 		pinctrl-1 = <&lptim2_sleep_in_pins_a>;
 		pinctrl-names = "default", "sleep";
 		status = "{{highlight|okay}}";                          {{highlight|/* enable counter/encoder on LPTIM2 */}}
 	};
 };

==How to configure the DT using STM32CubeMX==
The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree#STM32|platform configuration device tree]] files.<br />

The STM32CubeMX may not support all the properties described in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to [[STM32CubeMX]] user manual for further information.

==References==
For additional information, refer to the following links:
<references />

<noinclude>

{{ArticleBasedOnModel | Peripheral or framework device tree configuration model}}
{{PublicationRequestId | 8438 | 2018-08-02 | AnneJ}}
[[Category:Device tree configuration]]
[[Category:IIO]]
[[Category:Timers]]
{{ReviewsComments|JCT 1840: alignment needed with the last version of the model [[Peripheral or framework device tree configuration model]]<br>

[[Category:ToBeAlignedWithModel]]
}}</noinclude>
Line 6: Line 6:
   
 
It is used by the [[LPTIM Linux driver]] that registers relevant information in [[PWM overview|PWM]] and [[IIO overview|IIO]] frameworks.
 
It is used by the [[LPTIM Linux driver]] that registers relevant information in [[PWM overview|PWM]] and [[IIO overview|IIO]] frameworks.
  +
  +
If the peripheral is assigned to another execution context, refer to [[How to assign an internal peripheral to a runtime context]] article for guidelines on peripheral assignment and configuration.
   
 
== DT bindings documentation ==
 
== DT bindings documentation ==