Last edited 4 years ago

How to launch Khronos OpenGLES conformance tests

The printable version is no longer supported and may have rendering errors. Please update your browser bookmarks and please use the default browser print function instead.

1 Introduction[edit source]

The purpose of this article is to describe how to build and execute the Khronos OpenGL ES 2.0 Conformance Tests.

These tests are provided by the Khronos Group [1]. They are available as open source from the Khronos CTS GitHub source repo [2].

For a detailed description of the Khronos OpenGL ES2.0 CTS, please refer to the openglcts README.md [3] file.

2 How to install khronos-cts[edit source]

2.1 Building khronos-cts[edit source]

Execute the following command in the OpenSTLinux build environment:

 bitbake khronos-cts

2.2 Installing kronos-cts on the target board[edit source]

Execute the following command in the OpenSTLinux build environment:

 scp tmp*/deploy/deb/*neon*/khronos-cts_opengl-cts-<CTS Release>.deb root@<IPBOARD>:<SomewhereInTheBoard>
Info white.png Information
But default dpkg will extract within /home/root/.

This debian package is rather huge. For instance opengl-cts-4.6.0 is around 115MB. If rootfs space is at sake this is better to unpack the debian somewhere else by appending instdir=<SomewhereElse> to the above command

3 How to execute khronos-cts[edit source]

3.1 Running test suite[edit source]

Execute the following commands on the target board:

 cd /home/root
 ./cts-runner --type=es2 1>results.txt
[     1] EGL: enable default configs for conformance test
...
Info white.png Information
The test execution can take several hours.
Warning white.png Warning
The *free* system RAM amount required to complete this test suite in around 500MB. Under out of memory occurs.
Khronos gles cts1.png

3.2 Running a single/group of test(s)[edit source]

 cd /home/root
 glcts.exe --deqp-case=dEQP-EGL.functional.*

4 Testing verdict example[edit source]


...
Test run totals:
  Passed:        13786/13957 (98.8%)
  Failed:        11/13957 (0.1%)
  Not supported: 131/13957 (0.9%)
  Warnings:      29/13957 (0.2%)
219/220 sessions passed, conformance test FAILED

In order to interpret result, please look at "Understanding the result"[4]

Even more there are several tools available to process those test logs[5]

5 References[edit source]