1. Usage
The InternalInfo template is used to store, in a page, information that are restricted to STMicroelectronics employees (and therefore useless for any other reader): configurations specific to the STMicroelectronics network, links to internal resources (e.g. video files) etc.
It puts a message box with a "dark blue be.ST" icon in the page.
Only logged-in users who have writing permissions, can see this box. However, do not put any confidential information in the parameters of this template.
<message>}}Usage: {{InternalInfo |
Where <message> is the mandatory internal info message.
2. Basic examples
You type | You get |
---|---|
Internal info
{{InternalInfo | When connecting to the STMicroelectronics network, you have to execute these additional commands: ...}}
|
3. More examples
You type | You get |
---|---|
No message supplied
{{InternalInfo}}
|
|
Message supplied with a long sentence
{{InternalInfo | The message is a long sentence. Lorem ipsum: isdem diebus Apollinaris Domitiani gener, paulo ante agens palatii Caesaris curam, ad Mesopotamiam missus a socero per militares numeros immodice scrutabatur, an quaedam altiora meditantis iam Galli.}}
|
|
Check that the spaces before and after the message
BEFORE{{InternalInfo | Check spaces}}AFTER<br>
BEFORE
{{InternalInfo | Check spaces}}
AFTER
|
BEFOREAFTER AFTER |
4. Maintenance
This template is a template common to all ST wikis.
Modifications must be done into the WikiModel. They must be reviewed by all ST wikis maintainers.
When approved, the template can be pushed/merged towards all ST wikis.