Last edited 5 months ago

ArticleToDelete

1. Usage

The ArticleToDelete template is used to request the deletion of a page. It should be added as the very first line on the page that you believe should be deleted from the wiki.

It puts a message box with a "pink garbage can" icon in the page, and adds this page to the Candidates for deletion category.

Only logged-in users who have writing permissions, can see this box. However, do not put any confidential information in the parameters of this template.

Wiki maintainers periodically have a look at this category, and delete the pages that belong to it.

Usage:  {{ArticleToDelete | <reason> | <signature>}}

Where <reason> and <signature> are mandatory parameters:

  • <reason> is the reason supplied for the deletion
  • <signature> is the signature of the requester. It is recommended to use ~~~~ wiki markup to sign the request

2. Basic examples

You type You get
Deletion requested: reason and signature supplied
{{ArticleToDelete | This is the reason for this request | ~~~~}}

3. More examples

You type You get
Deletion requested: no reason supplied, no signature supplied
{{ArticleToDelete}}
Deletion requested: reason supplied with few words, no signature supplied
{{ArticleToDelete | This is the reason for this request}}
Deletion requested: no reason supplied, signature supplied
{{ArticleToDelete | | ~~~~}}
Deletion requested: reason supplied with a long sentence, signature supplied
{{ArticleToDelete | The reason is a long sentence. Lorem ipsum: isdem diebus Apollinaris Domitiani gener, paulo ante agens palatii Caesaris curam, ad Mesopotamiam missus a socero per militares numeros immodice scrutabatur, an quaedam altiora meditantis iam Galli. | ~~~~}}
Check that the spaces before and after the message
BEFORE{{ArticleToDelete | Check spaces | ~~~~}}AFTER<br>
BEFORE
{{ArticleToDelete | Check spaces | ~~~~}}
AFTER

BEFOREAFTER
BEFORE

AFTER

4. Maintenance

This template is a template common to all ST wikis.
Modifications must be done into the WikiModel. They must be reviewed by all ST wikis maintainers.
When approved, the template can be pushed/merged towards all ST wikis.


5. Code

No categories assignedEdit