STLightBlue

Revision as of 14:12, 7 October 2021 by Registered User (Merge articles)
(diff) ← Older revision | Latest revision (diff) | Newer revision → (diff)

1 Usage

The STLightBlue template is used to color text in pages, with the STMicroelectronics corporate primary color shade of light blue (█).

Usage:  {{STLightBlue|<text to color>|tint=<tint>}}

Where:

  • <text to color> is the text to format in light blue. If this template is called with no text, the hexadecimal code of the color is returned.
  • <tint> is the tint of the color expressed in percentage. If tint is not set then the original color is used (tint = 100%). The possible value are:
    • 75: 75% of the original color tint
    • 50: 50% of the original color tint
    • 25: 25% of the original color tint

2 Basic examples

You type You get
Coloring text in light blue
This is a {{STLightBlue|STMicroelectronics corporate color: shade of light blue: █}}

This is a STMicroelectronics corporate color: shade of light blue: █

Coloring text in 75% tint of light blue
This is a {{STLightBlue|STMicroelectronics corporate color: 75% tint of light blue: █ | tint=75}}

This is a STMicroelectronics corporate color: 75% tint of light blue: █

Coloring text in 50% tint of light blue
This is a {{STLightBlue|STMicroelectronics corporate color: 50% tint of light blue: █ | tint=50}}

This is a STMicroelectronics corporate color: 50% tint of light blue: █

Coloring text in 25% tint of light blue
This is a {{STLightBlue|STMicroelectronics corporate color: 25% tint of light blue: █ | tint=25}}

This is a STMicroelectronics corporate color: 25% tint of light blue: █

Getting the hexadecimal code of the color
{{STLightBlue}} is the hexadecimal code of STMicroelectronics light blue.

#3CB4E6 is the hexadecimal code of STMicroelectronics light blue.

Getting the hexadecimal code of the 75% tint of the color
{{STLightBlue | tint=75}} is the hexadecimal code of STMicroelectronics 75% tint of light blue.

#6DC7EC is the hexadecimal code of STMicroelectronics 75% tint of light blue.

Getting the hexadecimal code of the 50% tint of the color
{{STLightBlue | tint=50}} is the hexadecimal code of STMicroelectronics 50% tint of light blue.

#9DD9F2 is the hexadecimal code of STMicroelectronics 50% tint of light blue.

Getting the hexadecimal code of the 25% tint of the color
{{STLightBlue | tint=25}} is the hexadecimal code of STMicroelectronics 25% tint of light blue.

#CEECF9 is the hexadecimal code of STMicroelectronics 25% tint of light blue.

3 More examples

You type You get
light blue and bold
This is a {{STLightBlue|'''STMicroelectronics'''}} corporate color: '''{{STLightBlue|shade of light blue: █}}'''

This is a STMicroelectronics corporate color: shade of light blue: █

light blue and italic
This is a {{STLightBlue|''STMicroelectronics''}} corporate color: ''{{STLightBlue|shade of light blue: █}}''

This is a STMicroelectronics corporate color: shade of light blue: █

4 Maintenance

This template is a template common to all ST wikis.
Modifications must be done into the WikiModel. They must be reviewed by all ST wikis maintainers.
When approved, the template can be pushed/merged towards all ST wikis.

5 Code

#3CB4E6