This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.
1 Single shunt phase shift overview
In the context of a single shunt topology, the purpose of the phase-shifting is to shift one or two duty cycles to be able to sample the current signal in the boundary zones instead of inserting a distortion window.
The benefits are:
- Fewer commutations
- Less switching losses
2 Phase shift principle
Boundary zone 1:
- The firmware shifts on the right the smallest duty cycle by TMIN (minimum window time for sampling)
Boundary zone 2:
- The firmware shifts on the right the most middle duty cycle by TMIN (minimum window time for sampling)
Boundary zone 3:
- The firmware shifts on the right the smallest duty cycle and on the left the highest duty cycle by TMIN (minimum window time for sampling)
3 Peripheral usage
Phase-shifting needs the following peripherals to create the shifting. According to the advanced timer capabilities, one or two DMA channels will be used
MCU | TIM | DMA | IRQ |
---|---|---|---|
F0 | TIM1 | DMA1_Ch5 DMA1_Ch4 | DMA1_Ch5 HT and TC |
G0 | TIM1 | DMA1_Ch4 | DMA1_Ch4 HT and TC |
F3 | TIM1 | DMA1_Ch4 | DMA1_Ch4 HT and TC |
TIM8 | DMA1_Ch2 | DMA1_Ch2 HT and TC | |
F4 | TIM1 | DMA2_stream4 DMA2_stream5 | DMA_stream5 HT and TC |
TIM8 | DMA2_stream7 DMA2_stream1 | DMA_Stream1 HT and TC | |
G4 | TIM1 | DMA1_Ch1 | DMA1_Ch1 HT and TC |
TIM8 | DMA2_Ch1 | DMA2_Ch4 HT and TC | |
L4 | TIM1 | DMA1_Ch4 | DMA1_Ch4 HT and TC |
TIM8 | DMA2_Ch2 | DMA2_Ch2 HT and TC | |
F7 | TIM1 | DMA2_stream4 | DMA2_Stream4 HT and TC |
TIM8 | DMA2_stream7 | DMA2_Stream7 HT and TC |
4 Single shunt phase shift scheduling example
6 channels advanced timer and execution rate = 1 (G0,G4,F3,L4,F7)
5 Single shunt phase shift in the STM32 MC SDK
Single shunt is implemented by r1_ps_pwm_fdbk.c (and .h) processed when the STM32 MC project uses a MCU.