Approved version. Approved on: 17:17, 26 April 2021
You are viewing an old version of this page. Return to the latest version.
Difference between revisions of "STM32MotorControl:How To manually configure the motor parameters"
[checked revision] | [quality revision] |
m
|
m
|
Contents
1 Max Rated Speed, Nominal Current and Nominal DC Voltage parameters[edit]
- Set the Max Rated Speed to the maximum motor speed according to the application specifications.
- Set the Nominal Current to the maximum peak current provided to each of the motor phases according to the motor specifications.
- Set the Nominal DC Voltage to the value of the DC bus provided to the inverter or the rectified value of AC input.
2 Pole pair (number) parameter[edit]
- The number of pole pairs is usually provided by the motor supplier, but in case it’s not or if you’d like to double-check it:
- Connect a DC power supply between two (of the three) motor phases and provide up to 5% of the expected nominal DC bus voltage. (You may also set the current protection to the nominal motor current.)
- Rotate the motor with your hands, you should notice a little resistance, otherwise:
- If you are not able to rotate the motor, decrease the applied voltage.
- If the motor does not generate any resistance, gradually increase the applied voltage.
- The number of rotor stable positions in one mechanical turn represents the number of pole pairs.
3 Stator resistance and inductance parameters[edit]
- Using the multimeter, measure the DC stator resistance phase-to-phase (Rs) and divide it by two.
- Connect the DC voltage between two motor phases.
- Connect the oscilloscope voltage and current probes as shown in the figure.
- Increase the voltage up to the value where the current equals the nominal value, so the rotor aligns with the generated flux.
- Don’t move the rotor anymore.
- Disable the current protection of the DC voltage source.
- Unplug one terminal of the voltage source cable without switching it off.
- Plug the voltage source rapidly and monitor on the scope the voltage and current waveform until you get something like the one shown in the figure.
- The measurement is good if the voltage can be assimilated to a step and the current increase such as I∞ * (1-e- t *L/R).
- Measure the time required for the current waveform to rise to 63%.
- This time is Ld/Rs constant. Multiply it by Rs and you’ll get the Ld value.
4 Back EMF constant Ke[edit]
- The Back-EMF constant represents the proportionality constant between the mechanical motor speed and the amplitude of the B-EMF induced into the motor phases:
- To measure Ke, it usually suffices to turn the motor with your hands (or using a drill or another motor mechanically coupled) and use an oscilloscope to look for the phase-to-phase induced voltage (VBemf )
- Measure the VBemf frequency (fBemf) and the peak-to-peak amplitude (VBemf –A)
- Compute Ke in VRMS / KRPM:
{{DISPLAYTITLE: How To manually configure the motor parameters}} === Max Rated Speed, Nominal Current and Nominal DC Voltage parameters === * Set the '''''Max Rated Speed''''' to the maximum motor speed according to the application specifications. * Set the '''''Nominal Current''''' to the maximum peak current provided to each of the motor phases according to the motor specifications. * Set the '''''Nominal DC Voltage''''' to the value of the DC bus provided to the inverter or the rectified value of AC input. [[file:Setup_motor_parameters_manually-1.png|center]] === Pole pair (number) parameter === * The number of pole pairs is usually provided by the motor supplier, but in case it’s not or if you’d like to double-check it: ** Connect a DC power supply between two (of the three) motor phases and provide up to 5% of the expected nominal DC bus voltage. (You may also set the current protection to the nominal motor current.) ** Rotate the motor with your hands, you should notice a little resistance, otherwise: *** If you are not able to rotate the motor, decrease the applied voltage. *** If the motor does not generate any resistance, gradually increase the applied voltage. ** The number of rotor stable positions in one mechanical turn represents the number of pole pairs. [[file:Setup_motor_parameters_manually-2.png|center]] === Stator resistance and inductance parameters === * Using the multimeter, measure the DC stator resistance phase-to-phase (Rs) and divide it by two. * Connect the DC voltage between two motor phases. * Connect the oscilloscope voltage and current probes as shown in the figure. * Increase the voltage up to the value where the current equals the nominal value, so the rotor aligns with the generated flux. * Don’t move the rotor anymore. [[file:Setup_motor_parameters_manually-3.png|center]] * Disable the current protection of the DC voltage source. * Unplug one terminal of the voltage source cable without switching it off. * Plug the voltage source rapidly and monitor on the scope the voltage and current waveform until you get something like the one shown in the figure. * The measurement is good if the voltage can be assimilated to a step and the current increase such as I∞ * (1-e- t *L/R). * Measure the time required for the current waveform to rise to 63%. * This time is Ld/Rs constant. Multiply it by Rs and you’ll get the Ld value. [[file:Setup_motor_parameters_manually-4.png|center]] === Back EMF constant Ke === * The Back-EMF constant represents the proportionality constant between the mechanical motor speed and the amplitude of the B-EMF induced into the motor phases: [[file:Setup_motor_parameters_manually-5.png|center]] * To measure Ke, it usually suffices to turn the motor with your hands (or using a drill or another motor mechanically coupled) and use an oscilloscope to look for the phase-to-phase induced voltage (VBemf ) [[file:Setup_motor_parameters_manually-6.png|center]] * Measure the VBemf frequency (fBemf) and the peak-to-peak amplitude (VBemf –A) * Compute Ke in VRMS / KRPM: [[file:Setup_motor_parameters_manually-7.png|center]] [[file:Setup_motor_parameters_manually-8.png|center]] <noinclude> <!-- [[Category:Motor Control]] --> [[Category:STM32 MC Under ConstructionMotor Control]] {{PublicationRequestId|19726| 4/23/2021| JM LAGOUTTE}}</noinclude> <!-- Internal source: "Set up motor parameters manually.ppt" -->
Line 49: | Line 49: | ||
<noinclude> |
<noinclude> |
||
− | + | ||
[[Category:Motor Control]] |
[[Category:Motor Control]] |
||
− | |||
− | |||
{{PublicationRequestId|19726| 4/23/2021| JM LAGOUTTE}} |
{{PublicationRequestId|19726| 4/23/2021| JM LAGOUTTE}} |
||
</noinclude> |
</noinclude> |