Revision as of 09:07, 4 April 2022 by Registered User
1 Fixed issues
ID |
Summary
|
63212 |
Editor hyperlinks sometimes jump to declaration instead of definition.
|
83159[1] |
After updating STM32CubeIDE to a new version, the post-update restart fails on Linux® and macOS®. STM32CubeIDE must be restarted manually.
|
100287 |
Bin-files are no longer generated by default to reduce build time and the size of build output.
|
118111 |
Slow debug performance with RTOS proxy, especially on Windows®.
|
109124 |
When creating a debug configuration using ST-LINK GDB server, the SWD frequency must manually be changed from auto to a maximum of 8000 kHz.
|
2 Known issues
The known issues are split into general, OS-specific, and target-specific issues.
2.1 General issues
ID |
Summary
|
59435 |
Having a space or non-ASCII character in the project/workspace path or installation path is not fully supported.
|
63624 |
Some STM32CubeMX pop-up dialogs are not opened in front of the STM32CubeIDE workbench on all OS's.
|
68184 |
Hierarchical projects cannot be imported with the option Copy into workspace.
|
68440 |
Hierarchical projects cannot be renamed.
|
74251 |
SWV Exception Trace log data tab displays a peripheral column, which is always empty.
|
89454 |
Restart configuration only works for flash memory projects and not for RAM projects. Program Counter register is not set correctly. Manual work-around: In Restart configuration, manually set PC to the ResetHandler() in RAM: set $pc = 0x20000xxx.
|
101005 [1] |
New JRE™ bundling does not automatically import private certificate authorities, that are needed for secure connections. See the following knowledge article for a solution here.
|
109764 |
FreeRTOS™ kernel-aware debugging: Full stack traces off all tasks do not work if configUSE_PORT_OPTIMISED_TASK_SELECTION 1
|
115928 |
Editing live expressions while target is running does not work with SEGGER J-Link.
|
124062 |
GCC-10 is more strict with respect to declaration of global variables in header files. Read the GCC-10 porting guide.
|
2.2 OS-specific issues
2.2.1 macOS®
ID |
Summary
|
85064 |
Some macOS® versions report installation image corruption or that the image cannot be opened because the developer cannot be verified. The work-around is to execute the following command: xattr -c /Applications/STM32CubeIDE.app
|
2.3 Target-specific issues
2.3.1 STM32H7
ID |
Summary
|
73552 |
Serial Wire Viewer configuration is not reset for STM32H7 devices on the next launch if it was terminated with record active when using ST-LINK GDB server.
|
79658 |
ST-LINK GDB server reports being suspended on address: 0x05F0001 when debugging STM32H7 dual-core devices and the core under debug goes to sleep.
|
81763 |
OpenOCD does not support debugging STM32H7 dual-core devices when the core under debug goes to sleep.
|
2.3.2 STM32MP1
ID |
Summary
|
73456 |
The SFRs view is not aware of the device tree configuration and consequently shows all peripherals regardless if they are managed by the Cortex®-M or not.
|
73895 |
Debugging in production mode requires a network connection. If STM32CubeIDE is configured to use a network proxy, then the IP address of the STM32MP1 board needs to be added to the "Proxy bypass" list.
|
73896 |
The synchronization check between the IP-address entered in launch configuration and the IP-address of the target does not abort the launch in case of mismatch.
|
2.3.3 STM32WL
ID |
Summary
|
124465 |
STM32CubeIDE 1.9.0 is unable to debug the Cortex®-M0+ core of the STM32WL product. Customers are advised to use STM32CubeIDE 1.8.0.
|