Difference between revisions of "Introduction to NETXDUO"

[unchecked revision] [quality revision]
m
m
 

1 Introduction[edit]

Azure® RTOS NetX Duo is a dual IPv4 and IPv6 TCP/IP network stack designed specifically for deeply embedded, real-time, and IoT applications. It has various sets of features. Alongside the TCP/IP IPv4/IPv6 network stack, it provides a crypto library implementing the standard crypto and hash methods, and a TLS/DTLS library to support secure network connections.

NetX Duo Overview

  • The NetX Duo core offers a full TCP/IP IPv4IPV6 compliant stack with 3 types of API: TCP/IP, UDP/IP and RAW API.
  • The Crypto core implements the common crypto cipher suites and hashing algorithms useful for securing connections and exchanging encrypted data: AES, 3DES, HMAC, RSA, SHA1, SHA224, SHA256, SHA384, SHA512, MD5, HMAC-SHA1, and so on (each algorithm has its own implementation file .c and header file .h, which facilitate the selection and the integration of the required algorithms by applications).
  • The TLS core implements the secure connection API. Based on both the Crypto core and NetX Duo core, it supports the TLS and DTLS protocols with their different variants. (TLS 1.0 TLS 1.2, TLS 1.3).

It also supports the X509 public signed certificates protocol.

  • Addon protocols are a pre-supported set of network applicative protocols that ease the integration of the networking feature in the end user application. The main supported protocols are the following:

DHCP, DNS, mDNS, HTTP, HTTPS, FTP, TELNET, MQTT, SMTP, POP3, SNTP, SNMP, and so on.

Further details are available in the NetX Duo official documentation[1]

NetX Duo folders are organized as described below:

NetX Duo Folders

Info white.png Information
For general questions please visit the general FAQ section in the Introduction _ to Azure RTOS with STM32 article.


2 STM32 Integration[edit]

NetX Duo can run on any networking hardware, such as Ethernet, WiFi modules, cellular modems, and so on. It requires a low-level driver to interact between the physical layer already chosen, and the NetX Duo core requests (initialize, transmit data, receive data).

NetX Duo Low Layer Interfacing

To achieve the interaction between the NetX Duo stack and the required PHY, the software architecture should follow the arborescence below.

NetX Duo Low Layer Files


The following hardware configurations are currently supported:

  • Ethernet: Currently any STM32 board that provides an Ethernet IP, uses the Ethernet PHY microchip LAN874X[2] (driver under Drivers/BSP/Components In the X-CUBE-AZRTOS-H7 package).
Info white.png Information
NetX requires the Zero-copy feature that is currently supported only in the STM32H7 HAL Ethernet driver.

  • nx_stm32_eth_config_template.h: a template config header file to tune the corresponding driver for aspecific STM32 MCU/board. This file should be copied into the application source tree and renamed to nx_stm32_eth_driver.h, then customized according to the driver needs.
  • nx_stm32_*_driver.h: the driver header file containing the driver defines and data structure.
  • nx_stm32_*_driver_config_template.h: an application-level configuration file that allows users to tune some options related to the driver. A template file is provided in the driver source tree for reference.
  • nx_stm32_*_driver.c: this is referenced directly by the application and may be different between STM32 Series depending on the supported features.
NetXDuo_LANConfiguration

This is not the final version. Future versions are planned to add interrupt mode to the currently implemented polling mode.

  • nx_stm32_xxx_driver_template.c/.h: an empty interface that can be used to implement a new custom driver.


  • WiFi: this support focuses specifically on WiFi modules supporting Bypass mode and STM32 boards that provide an MXCHIP EMW3080 module.

To enable this connection mode, the user should configure it with flags in the mx_wifi_conf.h file.

  • "mx_wifi_conf_template.h": this application-level config file should be copied into the application source tree and renamed mx_wifi_conf.h. It is then customized according to the application and driver needs.

The following main configuration flags must be taken into consideration:

       "MX_WIFI_USE_SPI use SPI" - communicate with MXCHIP instead of UART.
       "MX_WIFI_NETWORK_BYPASS_MODE" - use Bypass mode instead of AT commands.
       "MX_WIFI_TX_BUFFER_NO_COPY" - no copy of TX buffer required.
       "WIFI_SSID" - defines the username of the access point. 
       "WIFI_PASSWORD" defines the password of the access point.
  • "Nx_driver_framework.c": the default processing entry point for the NetX Driver used as an interface between NetXDuo core and the EMW3080 Phy liaison.
  • "Nx_driver_framework.h": the driver header file containing the driver defines and data structure.
  • "Nx_driver_emw3080.c": a Phy interface to link commands between the nx_driver_framework and the Mxchip module.
  • "Nx_driver_emw3080.h": the driver header file containing the driver defines and data structure.
  • "Mx_wifi_azure_rtos.c": contains all tx and nx allocations required by mxchip.
NetXDuo_WiFiConfiguration

This architecture is being improved and aligned with other wireless and networking packages.

Info white.png Information
The WiFi driver is not supported in X-CUBE-AZRTOS-H7 (the first integration of the Azure RTOS in the STM32Cube Ecosystem), and is planned for a future release. However, WiFi Bypass mode is supported on the STM32U5 package including Azure RTOS Middleware and applications

After low-level configuration, it is called by the application code when an IP instance is created:

/* Create an IP instance by linking the nx network driver */

/* ETHERNET STM32H7 example:  */
  ret = nx_ip_create(&EthIP, "NetX IP Instance 0", NULL_IP_ADDRESS, NULL_IP_ADDRESS, 
&EthPool, nx_stm32_eth_driver, pointer, IP_MEMORY_SIZE, DEFAULT_PRIORITY);

/* WIFI STM32U5 example: */
ret = nx_ip_create(&IpInstance, "Main IP Instance", NULL_IP_ADDRESS, NULL_IP_ADDRESS, 
& AppPool, nx_driver_emw3080_entry, pointer, MEMORY_SIZE, DEFAULT_PRIORITY);

2.1 Known limitations[edit]

  • The BSD API support is not fully-compliant. This may impact the portability of legacy applications. More details are available in the official NetX Duo documentation[1]

3 How to use NetX Duo[edit]

The main APIs needed to use NetX Duo are described in the table below: (further details and a full API description are available from the NetX Duo official documentation[1] )

Function Name Short Description
nx_tcp_socket_create( ) Create a TCP socket
nx_udp_socket_create( ) Create a UDP socket
nx_tcp_server_socket_listen( ) Set up TCP socket to listen
nx_udp_socket_bind( ) Bind UDP socket to the PORT
nx_tcp_server_socket_accept( ) Accept a TCP remote client socket connection
nx_tcp_socket_receive( ) Receive a packet from a TCP remote client
nx_udp_socket_receive( ) Receive a packet from a UDP remote client
nx_tcp_socket_disconnect( ) Disconnect the TCP server socket
nx_tcp_server_socket_unaccept( ) Reject the TCP server socket
nx_tcp_server_socket_relisten( ) Set up server socket for listening again

The main steps to use NetX Duo are:

  • Define NX_APP_MEM_POOL_SIZE on app_azure_rtos_config.h from MX. For example, 100 Kbytes.
#define NX_APP_MEM_POOL_SIZE           102400


  • Create a Byte Pool “nx_app_byte_pool” with a size of NX_APP_MEM_POOL_SIZE in app_azure_rtos.c
if (tx_byte_pool_create(&tx_app_byte_pool, "Tx App memory pool", tx_byte_pool_buffer, TX_APP_MEM_POOL_SIZE) != TX_SUCCESS)
{}


Then in MX_NetXDuo_Init, the user should follow this routine (allocate, create).

  • Allocate memory from the byte pool:
  /* Allocate the memory for packet_pool.  */
  if (tx_byte_allocate(byte_pool, (VOID **) &pointer, NX_PACKET_POOL_SIZE, TX_NO_WAIT) != TX_SUCCESS)
  {
    return TX_POOL_ERROR;
  }


  • Create a pool AppPool:
    /* Create a packet pool.  */
    status = nx_packet_pool_create(&pool_0, "NetX Main Packet Pool", SAMPLE_PACKET_SIZE,
                                   (UCHAR *)sample_pool_stack , sample_pool_stack_size);


  • Then create and configure an IP instance that belongs to the pool already created.
  • Enable the needed NetX Duo components depending on the target application:
Function Name Short Description
nx_arp_enable( ) Enable the Address Resolution Protocol (AutoIP Protocol need ARP) (Require memory allocation)
nx_icmp_enable( ) Required for Ping
nx_udp_enable( ) Enable UDP traffic (DNS & DHCP need UDP)
nx_tcp_enable( ) Enable TCP traffic



4 Migration to NetX Duo[edit]

In order to migrate a development project from an existing network stack (such as LwIP or others) to NetX Duo, there is no straightforward automatic procedure. However, there are usually some similarities between APIs, and these can be helpful when performing this task. Some comparative examples are provided below.

Action NetXDuo LwIP
DHCP Serice
/* create the DHCP client */
ret = nx_dhcp_create(&DHCPClient, &IpInstance, "DHCP Client");
  
/* Create an IP @ change callback */
ret = nx_ip_address_change_notify(&IpInstance, ip_address_change_notify_callback, NULL);

/* start DHCP client */
ret = nx_dhcp_start(&DhcpClient);

/* Start DHCP process to get IP@*/
dhcp_start(netif);

/* Get Client data */
dhcp = (struct dhcp *)netif_get_client_data(netif, LWIP_NETIF_CLIENT_DATA_INDEX_DHCP);

/* Wait until getting DHCP data */
if (dhcp_supplied_address(netif))
{
  DHCP_state = DHCP_ADDRESS_ASSIGNED;
}

HTTP Service
/* Create the HTTP Server.  */
status = nx_http_server_create(&HTTPServer, "WEB HTTP Server", &IPInstance, &ram_disk, 
                          pointer, SERVER8STQCK, &WebServerPool, NX_NULL, webserver_request_notify_callback);

/* Start the WEB HTTP Server.   */
status = nx_http_server_start(&HTTPServer);

/* Web Server callback when a new request from a web client is triggered */
static UINT webserver_request_notify_callback(NX_WEB_HTTP_SERVER *server_ptr, UINT request_type, CHAR* resource, NX_PACKET *packet_ptr);

/* Extract the client request type from the client request */
nx_web_http_server_type_get(server_ptr, server_ptr->nx_web_http_server_request_resource, temp_string, &string_length);

/* Create a new TCP connection handle */
conn = netconn_new(NETCONN_TCP);

/* Bind to port 80 (HTTP) with default IP address */
err = netconn_bind(conn, NULL, 80);

/* Put the connection into LISTEN state */
netconn_listen(conn);

/* Accept any incoming connection */
accept_err = netconn_accept(conn, &newconn);

/* Read the data from the port, blocking if nothing yet there. 
   We assume the request (the part we care about) is in one netbuf */
recv_err = netconn_recv(conn, &inbuf);

/* Get the data pointer and length in netbuf */
netbuf_data(inbuf, (void**)&buf, &buflen);

5 STM32 NetX Duo applications[edit]

The following figure shows the project architecture and main application files for an STM32H7 example using Ethernet.

NetX Duo Application Files

STM32 Packages provide the following set of applications (the list of supported applications may differ between products and boards):

Application Short Description
Nx_TCP_Echo_Server Demonstrates how to develop a NetX TCP server to communicate with a remote client using the NetX TCP socket API. [3]
Nx_TCP_Echo_Client Demonstrates how to develop a NetX TCP client to communicate with a remote sever using the NetX TCP socket API. [4]
Nx_UDP_Echo_Server Demonstrates how to develop a NetX UDP server to communicate with a remote client using the NetX UDP socket API.[5]
Nx_UDP_Echo_Client Demonstrates how to develop a NetX UDP client to communicate with a remote sever using the NetX UDP socket API.[6]
Nx_WebServer Demonstrates how to develop Web HTTP server based application. It is designed to load files and static/dynamic web pages stored in an SD Card or OCTOSPI memory using a Web HTTP server, the code provides all required features to build a compliant Web HTTP Server.[7]
Nx_MQTT_Client Demonstrates how to exchange data between client and server using MQTT protocol in an encrypted mode supporting TLS v1.2.[8]
Nx_SNTP_Client Demonstrates how to develop a NetX SNTP client and connect with an STNP server to get a time update.[9]

6 References[edit]



=== Introduction ===
Azure<sup>®</sup> RTOS NetX Duo is a dual IPv4 and IPv6 TCP/IP network stack designed specifically for deeply embedded, real-time, and IoT applications. It has various sets of features. Alongside the TCP/IP IPv4/IPv6 network stack, it provides a crypto library implementing the standard crypto and hash methods, and a TLS/DTLS library to support secure network connections.

[[File:NetXDuo Overview.png|frameless|400px|center|NetX Duo Overview]]<br>


* The NetX Duo core offers a full TCP/IP IPv4IPV6 compliant stack with 3 types of API: TCP/IP, UDP/IP and RAW API. 
* The Crypto core implements the common crypto cipher suites and hashing algorithms useful for securing connections and exchanging encrypted data: AES, 3DES, HMAC, RSA, SHA1, SHA224, SHA256, SHA384, SHA512, MD5, HMAC-SHA1, and so on (each algorithm has its own implementation file ''.c'' and header file ''.h'', which facilitate the selection and the integration of the required algorithms by applications).
* The TLS core implements the secure connection API. Based on both the Crypto core and NetX Duo core, it supports the TLS and DTLS protocols with their different variants. (TLS 1.0 TLS 1.2, TLS 1.3).
It also supports the ''X509'' public signed certificates protocol.
* Addon protocols are a pre-supported set of network applicative protocols that ease the integration of the networking feature in the end user application. The main supported protocols are the following:
DHCP, DNS, mDNS, HTTP, HTTPS, FTP, TELNET, MQTT, SMTP, POP3, SNTP, SNMP, and so on.

Further details are available in the NetX Duo official documentation<ref name="OfficialDoc" > [https://docs.microsoft.com/en-us/azure/rtos/netx/ Microsoft official documentation]</ref>


NetX Duo folders are organized as described below:
[[File:NetXDuo Folders.png|frameless|500px|center|NetX Duo Folders]]<br>


{{Info | For general questions please visit the general FAQ section in the [[Introduction_ to Azure RTOS with STM32]] article.}}<br>


=== STM32 Integration===
NetX Duo can run on any networking hardware, such as Ethernet, WiFi modules, cellular modems, and so on. 
It requires a low-level driver to interact between the physical layer already chosen, and the NetX Duo core requests (initialize, transmit data, receive data).

[[File:NetXDuo LowLayerInterfacing.png|frameless|400px|center|NetX Duo Low Layer Interfacing]]

To achieve the interaction between the NetX Duo stack and the required PHY, the software architecture should follow the arborescence below.

[[File:NetXDuo LowLayerFiles.png|frameless|600px|center|NetX Duo Low Layer Files]]<br>


The following hardware configurations are currently supported:<br>


* '''Ethernet''': Currently any STM32 board that provides an Ethernet IP, uses the Ethernet PHY microchip  LAN874X<ref>[https://www.microchip.com/wwwproducts/en/LAN8742 LAN874X]</ref> (driver under ''Drivers/BSP/Components'' In the X-CUBE-AZRTOS-H7 package).

{{Info | NetX requires the ''Zero-copy'' feature that is currently supported only in the STM32H7 HAL Ethernet driver.}}<br>


* ''nx_stm32_eth_config_template.h'': a template config header file to tune the corresponding driver for aspecific STM32 MCU/board. This file should be copied into the application source tree and renamed to ''nx_stm32_eth_driver.h'', then customized according to the driver needs.
* ''nx_stm32_*_driver.h'': the driver header file containing the driver defines and data structure.
* ''nx_stm32_*_driver_config_template.h'': an application-level configuration file that allows users to tune some options related to the driver. A template file is provided in the driver source tree for reference.
* ''nx_stm32_*_driver.c'': this is referenced directly by the application and may be different between STM32 Series depending on the supported features.

[[File:NetXDuo LANconfiguration.png|frameless|600px|center|NetXDuo_LANConfiguration]] <br>

This is not the final version. Future versions are planned to add interrupt mode to the currently implemented polling mode.

* ''nx_stm32_xxx_driver_template.c/.h'': an empty interface that can be used  to implement a new custom driver. <br>


* '''WiFi''': this support focuses specifically on WiFi modules supporting ''Bypass'' mode and STM32 boards that provide an  MXCHIP EMW3080 module.
To enable this connection mode, the user should configure it with flags in the ''mx_wifi_conf.h'' file.

* "mx_wifi_conf_template.h": this application-level config file should be copied into the application source tree and renamed ''mx_wifi_conf.h''. It is then customized according to the application and driver needs.
The following main configuration flags must be taken into consideration:
        "MX_WIFI_USE_SPI use SPI" - communicate with MXCHIP instead of UART.
        "MX_WIFI_NETWORK_BYPASS_MODE" - use Bypass mode instead of AT commands.
        "MX_WIFI_TX_BUFFER_NO_COPY" - no copy of TX buffer required.
        "WIFI_SSID" - defines the username of the access point. 
        "WIFI_PASSWORD" defines the password of the access point.
* "Nx_driver_framework.c": the default processing entry point  for the NetX Driver used as an interface between NetXDuo core and the EMW3080 Phy liaison.
* "Nx_driver_framework.h": the driver header file containing the driver defines and data structure.  
* "Nx_driver_emw3080.c": a Phy interface to link commands between the nx_driver_framework and the Mxchip module.
* "Nx_driver_emw3080.h": the driver header file containing the driver defines and data structure.
* "Mx_wifi_azure_rtos.c": contains all tx and nx allocations required by mxchip.

[[File:NetXDuo WiFiconfiguration.png|frameless|600px|center|NetXDuo_WiFiConfiguration]]

This architecture is being improved and aligned with other wireless and networking packages.

{{Info| The WiFi driver is not supported in X-CUBE-AZRTOS-H7 (the first integration of the Azure RTOS in the STM32Cube Ecosystem), and is planned for a future release. However, WiFi Bypass mode is supported on the STM32U5 package including Azure RTOS Middleware and applications}}<br>


After low-level configuration, it is called by the application code when an IP instance is created:
<syntaxhighlight lang="c">

/* Create an IP instance by linking the nx network driver */

/* ETHERNET STM32H7 example:  */
  ret = nx_ip_create(&EthIP, "NetX IP Instance 0", NULL_IP_ADDRESS, NULL_IP_ADDRESS, 
&EthPool, nx_stm32_eth_driver, pointer, IP_MEMORY_SIZE, DEFAULT_PRIORITY);

/* WIFI STM32U5 example: */
ret = nx_ip_create(&IpInstance, "Main IP Instance", NULL_IP_ADDRESS, NULL_IP_ADDRESS, 
& AppPool, nx_driver_emw3080_entry, pointer, MEMORY_SIZE, DEFAULT_PRIORITY);
</syntaxhighlight>


==== Known limitations ====
* The BSD API  support is not fully-compliant. This may impact the portability of legacy applications. More details are available in the official NetX Duo documentation<ref name="OfficialDoc"  /> 


=== How to use NetX Duo ===
The main APIs needed to use NetX Duo are described in the table below: (further details and a full API description are available from the NetX Duo  official documentation<ref name="OfficialDoc" /> )

{| class="st-table sortable"
|-
! Function Name !! Short Description
|-
| ''nx_tcp_socket_create( )'' || Create a TCP socket
|-
| ''nx_udp_socket_create( )'' || Create a UDP socket
|-
| ''nx_tcp_server_socket_listen( )'' || Set up TCP socket to listen
|-
| ''nx_udp_socket_bind( )'' || Bind UDP socket to the PORT
|-
| ''nx_tcp_server_socket_accept( )'' || Accept a TCP remote client socket connection
|-
| ''nx_tcp_socket_receive( )'' || Receive a packet from a TCP remote client
|-
| ''nx_udp_socket_receive( )'' || Receive a packet from a UDP remote client
|-
| ''nx_tcp_socket_disconnect( )'' || Disconnect the TCP server socket
|-
| ''nx_tcp_server_socket_unaccept( )'' || Reject the TCP server socket
|-
|'' nx_tcp_server_socket_relisten( )'' || Set up server socket for listening again
|}

The main steps to use NetX Duo are:

* Define NX_APP_MEM_POOL_SIZE on app_azure_rtos_config.h from MX. For example, 100 Kbytes. <syntaxhighlight lang="c">

#define NX_APP_MEM_POOL_SIZE           102400</syntaxhighlight>
<br>

* Create a Byte Pool “nx_app_byte_pool” with a size of NX_APP_MEM_POOL_SIZE in app_azure_rtos.c<syntaxhighlight lang="c">

if (tx_byte_pool_create(&tx_app_byte_pool, "Tx App memory pool", tx_byte_pool_buffer, TX_APP_MEM_POOL_SIZE) != TX_SUCCESS)
{}</syntaxhighlight>
<br>


Then in MX_NetXDuo_Init, the user should follow this routine (allocate, create).
* Allocate memory from the byte pool:<syntaxhighlight lang="c">

  /* Allocate the memory for packet_pool.  */
  if (tx_byte_allocate(byte_pool, (VOID **) &pointer, NX_PACKET_POOL_SIZE, TX_NO_WAIT) != TX_SUCCESS)
  {
    return TX_POOL_ERROR;
  }</syntaxhighlight>
<br>


* Create a pool AppPool:<syntaxhighlight lang="c">

    /* Create a packet pool.  */
    status = nx_packet_pool_create(&pool_0, "NetX Main Packet Pool", SAMPLE_PACKET_SIZE,
                                   (UCHAR *)sample_pool_stack , sample_pool_stack_size);</syntaxhighlight>
<br>


* Then create and configure an IP instance that belongs to the pool already created.
* Enable the needed NetX Duo components depending on the target application:
{| class="st-table sortable"
|-
! Function Name !! Short Description
|-
| ''nx_arp_enable( )'' || Enable the Address Resolution Protocol (AutoIP Protocol need ARP) (Require memory allocation)
|-
| ''nx_icmp_enable( )'' || Required for Ping
|-
| ''nx_udp_enable( )'' || Enable UDP traffic (DNS & DHCP need UDP)
|-
| ''nx_tcp_enable( )'' || Enable TCP traffic
|}


=== Migration to NetX Duo ===
In order to migrate a development project from an existing network stack (such as LwIP or others) to NetX Duo, there is no straightforward automatic procedure. However, there are usually some similarities between APIs, and these can be helpful when performing this task. Some comparative examples are provided below.

{| class="st-table sortable"
|-
! Action !! NetXDuo !! LwIP
|-
| DHCP Serice || <syntaxhighlight lang="c">

/* create the DHCP client */
ret = nx_dhcp_create(&DHCPClient, &IpInstance, "DHCP Client");

/* Create an IP @ change callback */
ret = nx_ip_address_change_notify(&IpInstance, ip_address_change_notify_callback, NULL);

/* start DHCP client */
ret = nx_dhcp_start(&DhcpClient);</syntaxhighlight>  || <syntaxhighlight lang="c">

/* Start DHCP process to get IP@*/
dhcp_start(netif);

/* Get Client data */
dhcp = (struct dhcp *)netif_get_client_data(netif, LWIP_NETIF_CLIENT_DATA_INDEX_DHCP);

/* Wait until getting DHCP data */
if (dhcp_supplied_address(netif))
{
  DHCP_state = DHCP_ADDRESS_ASSIGNED;
}</syntaxhighlight>

|-
|HTTP Service || <syntaxhighlight lang="c">

/* Create the HTTP Server.  */
status = nx_http_server_create(&HTTPServer, "WEB HTTP Server", &IPInstance, &ram_disk, 
                          pointer, SERVER8STQCK, &WebServerPool, NX_NULL, webserver_request_notify_callback);

/* Start the WEB HTTP Server.   */
status = nx_http_server_start(&HTTPServer);

/* Web Server callback when a new request from a web client is triggered */
static UINT webserver_request_notify_callback(NX_WEB_HTTP_SERVER *server_ptr, UINT request_type, CHAR* resource, NX_PACKET *packet_ptr);

/* Extract the client request type from the client request */
nx_web_http_server_type_get(server_ptr, server_ptr->nx_web_http_server_request_resource, temp_string, &string_length);</syntaxhighlight> || <syntaxhighlight lang="c">

/* Create a new TCP connection handle */
conn = netconn_new(NETCONN_TCP);

/* Bind to port 80 (HTTP) with default IP address */
err = netconn_bind(conn, NULL, 80);

/* Put the connection into LISTEN state */
netconn_listen(conn);

/* Accept any incoming connection */
accept_err = netconn_accept(conn, &newconn);

/* Read the data from the port, blocking if nothing yet there. 
   We assume the request (the part we care about) is in one netbuf */
recv_err = netconn_recv(conn, &inbuf);

/* Get the data pointer and length in netbuf */
netbuf_data(inbuf, (void**)&buf, &buflen);</syntaxhighlight>

|}

=== STM32 NetX Duo applications ===
The following figure shows the project architecture and main application files for an STM32H7 example using Ethernet.
[[File:NetXDuo ApplicationFiles.png|frameless|center|NetX Duo Application Files]]

STM32 Packages provide the following set of applications (the list of supported applications may differ between products and boards):

{| class="st-table sortable"
|-
! Application !! Short Description
|-
| Nx_TCP_Echo_Server   || Demonstrates how to develop a NetX TCP server to communicate with a remote client using the NetX TCP socket API. <ref>[http://Projects/STM32H735G-DK/Applications/NetXDuo/Nx_UDP_Echo_Client/README.md Demonstrates how to develop a NetX TCP server to communicate with a remote client using the NetX TCP socket API]</ref> 

|-
| Nx_TCP_Echo_Client    || Demonstrates how to develop a NetX TCP client to communicate with a remote sever using the NetX TCP socket API. <ref>[https://github.com/STMicroelectronics/x-cube-azrtos-h7/tree/main/Projects/NUCLEO-H723ZG/Applications/NetXDuo/Nx_TCP_Echo_Client/README.md Demonstrates how to develop a NetX TCP client to communicate with a remote sever using the NetX TCP socket API]</ref>

|-
| Nx_UDP_Echo_Server    || Demonstrates how to develop a NetX UDP server to communicate with a remote client using the NetX UDP socket API.<ref>[https://github.com/STMicroelectronics/x-cube-azrtos-h7/tree/main/Projects/STM32H735G-DK/Applications/NetXDuo/Nx_UDP_Echo_Server/README.mdDemonstrates how to develop a NetX UDP server to communicate with a remote client using the NetX UDP socket API ]</ref>

|-
| Nx_UDP_Echo_Client    || Demonstrates how to develop a NetX UDP client to communicate with a remote sever using the NetX UDP socket API.<ref>[https://github.com/STMicroelectronics/x-cube-azrtos-h7/tree/main/Projects/STM32H735G-DK/Applications/NetXDuo/Nx_UDP_Echo_Client/README.md Demonstrates how to develop a NetX UDP client to communicate with a remote sever using the NetX UDP socket API]</ref>

|-
| Nx_WebServer          || Demonstrates how to develop Web HTTP server based application. It is designed to load files and static/dynamic web pages stored in an SD Card or OCTOSPI memory using a Web HTTP server, the code provides all required features to build a compliant Web HTTP Server.<ref>[https://github.com/STMicroelectronics/x-cube-azrtos-h7/tree/main/Projects/STM32H735G-DK/Applications/NetXDuo/Nx_WebServer/README.md Demonstrates how to develop Web HTTP server based application. It is designed to load files and static/dynamic web pages stored in an SD Card or OCTOSPI memory using a Web HTTP server, the code provides all required features to build a compliant Web HTTP Server]</ref>

|-
| Nx_MQTT_Client          || Demonstrates how to exchange data between client and server using MQTT protocol in an encrypted mode supporting TLS v1.2.<ref>[https://github.com/STMicroelectronics/x-cube-azrtos-h7/tree/main/Projects/STM32H735G-DK/Applications/NetXDuo/Nx_MQTT_Client/README.md Demonstrates how to exchange data between client and server using MQTT protocol in an encrypted mode supporting TLS v1.2]</ref>

|-
| Nx_SNTP_Client          || Demonstrates how to develop a NetX SNTP client and connect with an STNP server to get a time update.<ref> [https://github.com/STMicroelectronics/x-cube-azrtos-h7/tree/main/Projects/STM32H747I-DISCO/Applications/NetXDuo/Nx_SNTP_Client/README.md Demonstrates how to develop a NetX SNTP client and connect with an STNP server to get a time update]</ref>

|}

==References==<references />
<noinclude>

[[Category:STM32 middleware | 20]]
{{ArticleBasedOnModel | Example tech domain article}}
{{PublicationRequestId | 21116 | 2021-14-09 | To assign}}
{{PublicationRequestId | 19009 | 2021-02-17 | Philip SAGE}}</noinclude>
Line 17: Line 17:
 
[[File:NetXDuo Folders.png|frameless|500px|center|NetX Duo Folders]]<br>
 
[[File:NetXDuo Folders.png|frameless|500px|center|NetX Duo Folders]]<br>
   
{{Info | For general questions please visit the general FAQ section in [[Introduction_to Azure RTOS with STM32]] article.}}
+
{{Info | For general questions please visit the general FAQ section in the [[Introduction to Azure RTOS with STM32]] article.}}
 
<br>
 
<br>