Difference between revisions of "Cellular:Cellular X-CUBE-CELLULAR How To"
[quality revision] | [quality revision] |
Philip Sage (talk | contribs)
m
|
m
|
Click here for Cellular overview
Contents
-
1 How To...
- 1.1 Introduction
- 1.2 How to start the delivered binary firmware
- 1.3 How to find the needed delivered binary
- 1.4 How to set up the Teraterm parameters
- 1.5 How to set up list available commands
- 1.6 How to set up APN using command line
- 1.7 How to set the SIM APN by updating the plf_cellular_config.h file
- 1.8 How to use console commands to get the modem and cellular network information
- 1.9 How to configure the modem radio band
- 1.10 How to to select components to include in the cellular firmware
- 1.11 How to change default behavior of the application
- 1.12 How to implement your own application
- 1.13 How to setup iSIM for GMS01Q
- 1.14 How to update APN name table
- 1.15 How to enable Quectel software to change the BG96 modem firmware
- 1.16 How to manage EEprom on B-L462E-CELL1
1 How To...[edit]
1.1 Introduction[edit]
This wiki page is a guideline describing how to perform the main activities with X-CUBE-CELLULAR.
1.2 How to start the delivered binary firmware[edit]
Binary firmware is provided for each supported board. For example to run the STM32L496 binary for the BG96 modem, follow the steps below:
- Insert an activated SIM into the BG96 modem STMod+ board
- Plug the BG96 modem board (module up, SIM down) into the STM32L496 board
- Plug an USB cable (the one near the blue quad-switch) on the STM32L496 board (-> a new volume (DIS_L496ZG) appears on your PC)
- Flash the firmware (drag and drop the .bin onto the newly appearing volume)
- Open a TeraTerm serial terminal and set the right parameters (see below: How to setup Teraterm parameters)
- If needed (by default it is empty), enter the right SIM APN using the command line
See the following list for details
1.3 How to find the needed delivered binary[edit]
All the binaries provided are available here: \Projects\<STM32 board name>\Demonstrations\Cellular\Binaries\
Example: \Projects\32L496GDISCOVERY\Demonstrations\Cellular\Binaries\
Name of the binaries indicate its purpose, <STM32 board>_<modem>_<IP stack>.bin
- l496_bg96_lwip.bin is the binary for the L496 discovery board associated to the BG96 modem and the IP stack selected is the LwIP in the STM32
- l496_bg96_socket.bin is the binary for the L496 discovery board associated to the BG96 modem, and the IP stack selected is in the modem.
1.4 How to set up the Teraterm parameters[edit]
- Terminal
- [New line]
- [Receive]: Auto
- [Transmit]: CR
- [Local echo] selected
- [New line]
- Serial
- [Baud rate]: 115200
- [Data]: 8 bit
- [Parity]: none
- [Stop]: 1 bit
- [Flow control]: none
- [Transmit delay]: 10 ms each
1.5 How to set up list available commands[edit]
Hit "enter" then type "help" then hit "enter" the list of commands is displayed.
Example. List of commands:
-
help: help command
-
trace: trace management
-
comlib: com library commands
-
cst: cellular service task management
-
atcmd: send an at command
-
modem: modem configuration management
-
cellularapp: CellularApp commands
-
echoclient: EchoClient commands
- ping: Ping commands
So to send an AT command to modem just enter: atcmd AT+QIRC
1.6 How to set up APN using command line[edit]
Example: The name of the APN is "em", there is no login or password.
Enter the following commands:
- cst apnconf em
- cst targetstate off
- cst targetstate full
Note: to list all cst command parameter just enter "cst help"
The last 2 commands are used to restart modem to take into account the just defined APN.
If you want to avoid this step, it is easy to modify APN values in the source code and rebuild the firmware. See below for details.
1.7 How to set the SIM APN by updating the plf_cellular_config.h file[edit]
According to the SIM/operator used, the cellular parameters can be updated in the plf_cellular_config.h file that contains all the configurable cellular service parameters.
1.8 How to use console commands to get the modem and cellular network information[edit]
- Open a Tera Term serial terminal and set the right parameters.
- Remove the trace display by typing the commands:
- trace off
- cst poll off
Then type the Cellular Service commands:
- cst
- cst state
- cst info
- cst config
1.9 How to configure the modem radio band[edit]
- Open a Tera Term serial terminal and set the right parameters
- Start the firmware and select Modem power on option in the boot menu
- Type the modem command to get help of the modem configuration.
1.10 How to to select components to include in the cellular firmware[edit]
The firmware can be customized by adding or removing components or applications.
The configuration files under Projects\<board>\Demonstrations\Cellular\STM32_Cellular\Config allows selection of the component to include in the cellular firmware by define/undefine environment variables (if using CellularApp overwrites configuration by changing the define in plf_cellular_app_config.h).
Refer to the user manual document (UM2426) how to customize the software.
1.11 How to change default behavior of the application[edit]
The delivered firmware starts Cellular_App application. The default behavior is that a single echo service is started. This service sends data to an Echo server which replies with the same data. Once an answer from Echo server is received, the echo client resends data to Echo server after a delay. A 2nd instance of the Echo client can be started to test multiple socket configurations. The address of the Echo server can be changed. It is also possible to send a ping command while the Echo client is running. It is also possible to start a perfomance test. To see all the possibilities, type the following in the Tera Term: cellularapp help
1.12 How to implement your own application[edit]
The easiest way to implement your application is to adapt the Cellular_App content to your needs.
Another method is to add a new entry task for this new application and start it from main (do not forget to remove entry task start for Cellular_App to avoid conflicts).
Your application is in charge of initializing and starting the Cellular middleware (for this, copy and paste the required lines from Cellular_App).
1.13 How to setup iSIM for GMS01Q[edit]
There are 2 STMod+ boards with Monarch Sequans modem, one with GM01Q (the default in the X-CUBE-CELLULAR delivery) and one with GMS01Q.
The GMS01Q is a GM01Q with an iSIM.
To use GMS01Q, a small modification must be made in the source code, .h file.
The file to update is Projects\<board>\Demonstrations\Cellular\STM32_Cellular\Config\plf_cellular_config.h
With <board> = B-L4S5I-IOT01A or 32L496GDISCOVERY or STWINKT1 or ... according the STM32 board with which you are working.
Patch the file as below and rebuild the binary.
- define PLF_CELLULAR_SIM_SLOT_NB (1U)
- define PLF_CELLULAR_SIM_INDEX_0 (2U) /*!< SIM SLOT 0 interface */
- define PLF_CELLULAR_SIM_INDEX_1 (99U) /*!< SIM SLOT 1 interface */
- define PLF_CELLULAR_SIM_INDEX_2 (99U) /*!< SIM SLOT 2 interface */
- define PLF_CELLULAR_SIM_INDEX_3 (99U) /*!< SIM SLOT 3 interface */
1.14 How to update APN name table[edit]
For B-L462E-CELL1 the SW embeds a APN name list. In the case of remote SIM provisioning, it is possible find the APN name automatically.
The user can modify the default APN name list and rebuild the firmware to have their own APN list.
1.15 How to enable Quectel software to change the BG96 modem firmware[edit]
To be completed.
1.16 How to manage EEprom on B-L462E-CELL1[edit]
The EEprom is filled at Factory process with some data, main information are extract from modem, however a PSK automatically generated is also added. So in case of needs to write the EEprom, backup the parameters to be able to restore them, specially the PSK before. Here is the EEprom first bytes structure (length is 274 bytes):
// Global parameters
uint8_t Board[20]; //={"B-L462-CELL1"};
uint8_t Version [20]; // Version FG displayed on sticker {"EBL462ECELL1$KU4"};
uint8_t Revision [20]; // Revision displayed on sticker {"MB1508-L462E-C01"};
uint8_t Serial[20]; // Serial number displayed on sticker {"K192700022"};
// Modem Related
uint8_t BaseBoard[20];//={"LBAD0XX1SE"};
uint8_t Brand[16]; //={"MURATA"};
uint8_t Model[16]; //={"ALT125X"}; // returned by AT+GMM
uint8_t ModemSoftRevNumber[30]; //={"RK_02_01_02_00_57"} // returned by AT+GMR
uint8_t IMEI[16]; // returned by AT+CGSN
uint8_t PSK[20]; // Pre shared Key - randomly generated
// eSim related
uint8_t eICCID[24]; // EMBEDDED SIM CHIP, returned by AT%CCID
uint8_t eIMSI[16]; // EMBEDDED SIM CHIP, returned by AT+CIMI
uint8_t EID [32]; ///262//270
uint32_t signature; ///266//274
Note: it is easy to read and write (using HAL services HAL_I2C_Mem_Read / HAL_I2C_Mem_Write) the EEprom after calling the I2C initialization.
Click [[Cellular LTE CatM / NBIoT overview|here]] for Cellular overview<br> == How To... == === Introduction === This wiki page is a guideline describing how to perform the main activities with X-CUBE-CELLULAR. === How to start the delivered binary firmware === Binary firmware is provided for each supported board. For example to run the STM32L496 binary for the BG96 modem, follow the steps below: # Insert an activated SIM into the BG96 modem STMod+ board # Plug the BG96 modem board (module up, SIM down) into the STM32L496 board # Plug an USB cable (the one near the blue quad-switch) on the STM32L496 board (-> a new volume (DIS_L496ZG) appears on your PC) # Flash the firmware (drag and drop the .bin onto the newly appearing volume) # Open a TeraTerm serial terminal and set the right parameters (see below: How to setup Teraterm parameters) # If needed (by default it is empty), enter the right SIM APN using the command line See the following list for details === How to find the needed delivered binary === All the binaries provided are available here: \Projects\<STM32 board name>\Demonstrations\Cellular\Binaries\<br> Example: \Projects\32L496GDISCOVERY\Demonstrations\Cellular\Binaries\<br> Name of the binaries indicate its purpose, <STM32 board>_<modem>_<IP stack>.bin * l496_bg96_lwip.bin is the binary for the L496 discovery board associated to the BG96 modem and the IP stack selected is the LwIP in the STM32 * l496_bg96_socket.bin is the binary for the L496 discovery board associated to the BG96 modem, and the IP stack selected is in the modem. === How to set up the Teraterm parameters === *Terminal ** [New line] *** [Receive]: Auto *** [Transmit]: CR ** [Local echo] selected * Serial ** [Baud rate]: 115200 ** [Data]: 8 bit ** [Parity]: none ** [Stop]: 1 bit ** [Flow control]: none ** [Transmit delay]: 10 ms each === How to set up list available commands === Hit "enter" then type "help" then hit "enter" the list of commands is displayed.<br> Example. List of commands:<br> * '''help''': help command<br> *'''trace''': trace management<br> *'''comlib''': com library commands<br> *'''cst''': cellular service task management<br> *'''atcmd''': send an at command<br> *'''modem''': modem configuration management<br> *'''cellularapp''': CellularApp commands<br> *'''echoclient''': EchoClient commands<br> *'''ping''': Ping commands</code> <br> So to send an AT command to modem just enter: atcmd AT+QIRC === How to set up APN using command line === Example: The name of the APN is "em", there is no login or password.<br>Enter the following commands: * cst apnconf em * cst targetstate off * cst targetstate full Note: to list all cst command parameter just enter "cst help"<br>The last 2 commands are used to restart modem to take into account the just defined APN.<br>If you want to avoid this step, it is easy to modify APN values in the source code and rebuild the firmware. See below for details. === How to set the SIM APN by updating the ''plf_cellular_config.h'' file === According to the SIM/operator used, the cellular parameters can be updated in the ''plf_cellular_config.h'' file that contains all the configurable cellular service parameters. === How to use console commands to get the modem and cellular network information === # Open a '''''Tera Term''''' serial terminal and set the right parameters. # Remove the trace display by typing the commands: *trace off *cst poll off Then type the Cellular Service commands: *cst *cst state *cst info *cst config === How to configure the modem radio band === # Open a '''''Tera Term''''' serial terminal and set the right parameters # Start the firmware and select '''''Modem power on''''' option in the boot menu # Type the '''modem''' command to get help of the modem configuration. === How to to select components to include in the cellular firmware === The firmware can be customized by adding or removing components or applications.<br> The configuration files under Projects\<board>\Demonstrations\Cellular\STM32_Cellular\Config allows selection of the component to include in the cellular firmware by define/undefine environment variables (if using CellularApp overwrites configuration by changing the define in ''plf_cellular_app_config.h'').<br> Refer to the user manual document ([https://www.st.com/content/ccc/resource/technical/document/user_manual/group1/3a/76/d7/0d/39/7d/4d/80/DM00511019/files/DM00511019.pdf/jcr:content/translations/en.DM00511019.pdf UM2426]) how to customize the software. === How to change default behavior of the application === The delivered firmware starts Cellular_App application. The default behavior is that a single echo service is started. This service sends data to an Echo server which replies with the same data. Once an answer from Echo server is received, the echo client resends data to Echo server after a delay. A 2nd instance of the Echo client can be started to test multiple socket configurations. The address of the Echo server can be changed. It is also possible to send a ping command while the Echo client is running. It is also possible to start a perfomance test. To see all the possibilities, type the following in the Tera Term: cellularapp help === How to implement your own application === The easiest way to implement your application is to adapt the Cellular_App content to your needs.<br>Another method is to add a new entry task for this new application and start it from main (do not forget to remove entry task start for Cellular_App to avoid conflicts).<br>Your application is in charge of initializing and starting the Cellular middleware (for this, copy and paste the required lines from Cellular_App). === How to setup iSIM for GMS01Q === There are 2 STMod+ boards with Monarch Sequans modem, one with GM01Q (the default in the X-CUBE-CELLULAR delivery) and one with GMS01Q.<br> The GMS01Q is a GM01Q with an iSIM.<br> To use GMS01Q, a small modification must be made in the source code, ''.h'' file.<br> The file to update is ''Projects\<board>\Demonstrations\Cellular\STM32_Cellular\Config\plf_cellular_config.h''<br> With <board> = B-L4S5I-IOT01A or 32L496GDISCOVERY or STWINKT1 or ... according the STM32 board with which you are working.<br> Patch the file as below and rebuild the binary.<br> #define PLF_CELLULAR_SIM_SLOT_NB (1U) #define PLF_CELLULAR_SIM_INDEX_0 (2U) /*!< SIM SLOT 0 interface */ #define PLF_CELLULAR_SIM_INDEX_1 (99U) /*!< SIM SLOT 1 interface */ #define PLF_CELLULAR_SIM_INDEX_2 (99U) /*!< SIM SLOT 2 interface */ #define PLF_CELLULAR_SIM_INDEX_3 (99U) /*!< SIM SLOT 3 interface */<br> === How to update APN name table === For B-L462E-CELL1 the SW embeds a APN name list. In the case of remote SIM provisioning, it is possible find the APN name automatically.<br> The user can modify the default APN name list and rebuild the firmware to have their own APN list. === How to enable Quectel software to change the BG96 modem firmware === To be completed. === How to manage EEprom on B-L462E-CELL1 === The EEprom is filled at Factory process with some data, main information are extract from modem, however a PSK automatically generated is also added. So in case of needs to write the EEprom, backup the parameters to be able to restore them, specially the PSK before. Here is the EEprom first bytes structure (length is 274 bytes): *<br> <syntaxhighlight lang="c"> // Global parameters**uint8_t Board[20]; //={"B-L462-CELL1"};**uint8_t Version [20]; // Version FG displayed on sticker {"EBL462ECELL1$KU4"};**uint8_t Revision [20]; // Revision displayed on sticker {"MB1508-L462E-C01"};**uint8_t Serial[20]; // Serial number displayed on sticker {"K192700022"};*// Modem Related**uint8_t BaseBoard[20];//={"LBAD0XX1SE"};**uint8_t Brand[16]; //={"MURATA"};**uint8_t Model[16]; //={"ALT125X"}; // returned by AT+GMM**uint8_t ModemSoftRevNumber[30]; //={"RK_02_01_02_00_57"} // returned by AT+GMR**uint8_t IMEI[16]; // returned by AT+CGSN**uint8_t PSK[20]; // Pre shared Key - randomly generated*// eSim related**uint8_t eICCID[24]; // EMBEDDED SIM CHIP, returned by AT%CCID**uint8_t eIMSI[16]; // EMBEDDED SIM CHIP, returned by AT+CIMI**uint8_t EID [32]; ///262//270**uint32_t signature; ///266//274</syntaxhighlight> Note: it is easy to read and write (using HAL services HAL_I2C_Mem_Read / HAL_I2C_Mem_Write) the EEprom after calling the I2C initialization. {{PublicationRequestId | 19451| 2021-03-29 | Ronan Gabou}} {{ArticleBasedOnModel | Example tech domain article}} <noinclude> [[Category:Using models]] [[Category:Cellular]]</noinclude>
Line 133: | Line 133: | ||
=== How to manage EEprom on B-L462E-CELL1 === |
=== How to manage EEprom on B-L462E-CELL1 === |
||
The EEprom is filled at Factory process with some data, main information are extract from modem, however a PSK automatically generated is also added. So in case of needs to write the EEprom, backup the parameters to be able to restore them, specially the PSK before. |
The EEprom is filled at Factory process with some data, main information are extract from modem, however a PSK automatically generated is also added. So in case of needs to write the EEprom, backup the parameters to be able to restore them, specially the PSK before. |
||
− | Here is the EEprom first bytes structure (length is 274 bytes): |
+ | Here is the EEprom first bytes structure (length is 274 bytes):<br>
|
− | + | <syntaxhighlight lang="c"> |
|
− | + | // Global parameters |
|
− | + | uint8_t Board[20]; //={"B-L462-CELL1"}; |
|
− | + | uint8_t Version [20]; // Version FG displayed on sticker {"EBL462ECELL1$KU4"}; |
|
− | + | uint8_t Revision [20]; // Revision displayed on sticker {"MB1508-L462E-C01"}; |
|
− | + | uint8_t Serial[20]; // Serial number displayed on sticker {"K192700022"}; |
|
− | + | // Modem Related |
|
− | + | uint8_t BaseBoard[20];//={"LBAD0XX1SE"}; |
|
− | + | uint8_t Brand[16]; //={"MURATA"}; |
|
− | + | uint8_t Model[16]; //={"ALT125X"}; // returned by AT+GMM |
|
− | + | uint8_t ModemSoftRevNumber[30]; //={"RK_02_01_02_00_57"} // returned by AT+GMR |
|
− | + | uint8_t IMEI[16]; // returned by AT+CGSN |
|
− | + | uint8_t PSK[20]; // Pre shared Key - randomly generated |
|
− | + | // eSim related |
|
− | + | uint8_t eICCID[24]; // EMBEDDED SIM CHIP, returned by AT%CCID |
|
− | + | uint8_t eIMSI[16]; // EMBEDDED SIM CHIP, returned by AT+CIMI |
|
− | + | uint8_t EID [32]; ///262//270 |
|
+ | uint32_t signature; ///266//274 |
||
+ | </syntaxhighlight> |
||
Note: it is easy to read and write (using HAL services HAL_I2C_Mem_Read / HAL_I2C_Mem_Write) the EEprom after calling the I2C initialization. |
Note: it is easy to read and write (using HAL services HAL_I2C_Mem_Read / HAL_I2C_Mem_Write) the EEprom after calling the I2C initialization. |
||