1 What is NanoEdge AI Library for 1-class classification (outlier detection)?
NanoEdge™ AI Library is an Artificial Intelligence (AI) static library originally developed by Cartesiam, for embedded C software running on Arm® Cortex® microcontrollers.
When embedded on microcontrollers, it gives them the ability to easily "identify" outliers from sensor patterns, by themselves, without the need for the user to have additional skills in Mathematics, Machine Learning, or data science.
The NanoEdge AI static library for 1-class classification is the code that contains an AI model (for example, as a bundle of signal treatment, Machine Learning model, and optimally tuned hyperparameters) designed to identify if a sensor pattern is inside the class or outside the class (outlier/anomaly). The class under consideration is defined by the user in NanoEdge AI Studio (NanoEdgeAIStudio), also called the Studio, and are used during the training process of the AI model.
2 Install / Getting started
The main functions available via the library are:
oneclass_init()
|
run first before the classification process to load the knowledge |
oneclass()
|
run a classification iteration to identify if the pattern is inside or outside the class (inference) |
2.1 Static library
- In NanoEdge AI Studio, after obtaining a library, click Compile (on the "Deployment" screen, which follows the "Benchmark" and "Emulator" screens)
- Open the .zip file obtained
- Select and copy the static library
libneai.a
- Link this static library to your project code
2.2 NanoEdge AI Library functions
Most NanoEdge AI function return the status of the library in the following enum, neai_state
:
enum neai_state {
NEAI_OK = 0,
NEAI_INIT_FCT_NOT_CALLED = 123,
NEAI_BOARD_ERROR,
NEAI_KNOWLEDGE_BUFFER_ERROR,
NEAI_NOT_ENOUGH_CALL_TO_LEARNING,
NEAI_UNKNOWN_ERROR};
Here are the possible statuses:
NEAI_OK
: the library is working as expectedNEAI_INIT_FCT_NOT_CALLED
: the learn or detect function has been called without running the init function before. Initialize your library.NEAI_BOARD_ERROR
: the board detected is not authorized. For instance, it may happen if you are trying to use a limited library (for instance obtained from the free version of NanoEdge AI Studio) with a non-supported STM32 board.NEAI_KNOWLEDGE_BUFFER_ERROR
: the knowledge loaded is not compatible with this library. Make sure that the knowledge being used is the one obtained with this exact library.NEAI_NOT_ENOUGH_CALL_TO_LEARNING
: this is a fail-safe to prevent users from running an insufficient (only one or a few) number of iterations of the learning function. Run more learning iterations.NEAI_UNKNOWN_ERROR
: there is an unknown error with the library.
2.2.1 Initialization
enum neai_state neai_oneclass_init(const float knowledge_buffer[]);
Initialization must be called at the beginning to load the knowledge.
- Input:
const float knowledge_buffer[]
, this buffer is defined in the header file knowledge.h provided in the .zip file containing the static NanoEdge AI Library.
- Output:
- the
neai_state
enum (NEAI_OK == 0, in case of success).
- the
For more details on the output of the initialization function, refer to the header file NanoEdgeAI.h provided in the .zip file containing the static NanoEdge AI Library, or in the code examples below.
2.2.2 1-class classification
enum neai_state neai_oneclass(float input_buffer[], uint8_t *is_outlier);
This function returns the result of outlier detection, whether or not the detected buffer is an outlier.
- Input:
float input_buffer[]
, the length of the buffer isDATA_INPUT_USER * AXIS_NUMBER
.
- Output:
1
if the input pattern is detected as an outlier (outside the class considered), and0
if it is not an outlier (it belongs to the class).- The
neai_state
enum (NEAI_OK == 0, in case of success).
2.3 Example "Hello World!"
Header files:
NanoEdgeAI.h and knowledge.h (provided in the .zip file that you download by clicking Compile in NanoEdge AI Studio (on the "Deploy" screen after obtaining a library)
Example of NanoEdge AI Library header file:
/* =============
Copyright (c) 2021, STMicroelectronics
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that
the following conditions are met:
* Redistributions of source code must retain the above copyright notice, this list of conditions and the
following disclaimer.
* Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the
following disclaimer in the documentation and/or other materials provided with the distribution.
* Neither the name of the copyright holders nor the names of its contributors may be used to endorse or promote
products derived from this software without specific prior written permission.
*THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES,
INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE
DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER / OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR
SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE
USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.*
*/
#ifndef __NANOEDGEAI_H__
#define __NANOEDGEAI_H__
/* Includes */
#include <stdint.h>
/* Define */
#define AXIS_NUMBER 3
#define DATA_INPUT_USER 512
enum neai_state {
NEAI_OK = 0,
NEAI_INIT_FCT_NOT_CALLED = 123,
NEAI_BOARD_ERROR,
NEAI_KNOWLEDGE_BUFFER_ERROR,
NEAI_NOT_ENOUGH_CALL_TO_LEARNING, //This is a fail-safe to prevent users from learning one or even no signals.
NEAI_UNKNOWN_ERROR};
/* Input buffer */
float input_user_buffer[DATA_INPUT_USER * AXIS_NUMBER];
/* Function prototypes */
#ifdef __cplusplus
extern "C" {
#endif
enum neai_state neai_oneclass_init(const float knowledge_buffer[]);
enum neai_state neai_oneclass(float input_buffer[], uint8_t *is_outlier);
#ifdef __cplusplus
}
#endif
#endif
Main program: main.c
This program must be completed by the user (depending on the applications or the desired features).
/* =============
Copyright (c) 2020, STMicroelectronics
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that
the following conditions are met:
* Redistributions of source code must retain the above copyright notice, this list of conditions and the
following disclaimer.
* Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the
following disclaimer in the documentation and/or other materials provided with the distribution.
* Neither the name of the copyright holders nor the names of its contributors may be used to endorse or promote
products derived from this software without specific prior written permission.
*THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES,
INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE
DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER / OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR
SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE
USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.*
*/
/**
**************************************************************************
* Demo: NanoEdge AI process to include in main program body
*
* @note This program must be completed and customized by the user
**************************************************************************
*/
/* Includes --------------------------------------------------------------------*/
#include "NanoEdgeAI.h"
#include "knowledge.h"
/* Private define --------------------------------------------------------------*/
/* Private variables defined by user -------------------------------------------*/
/* Private function prototypes defined by user ---------------------------------*/
/*
* @brief Collect data process
*
* This function is defined by user, depends on applications and sensors
*
* @param sample_buffer: [in, out] buffer of sample values
* @retval None
* @note If AXIS_NUMBER = 3 (cf NanoEdgeAI.h), the buffer must be
* ordered as follow:
* [x0 y0 z0 x1 y1 z1 ... xn yn zn], where xi, yi and zi
* are the values for x, y and z axes, n is equal to
* DATA_INPUT_USER (cf NanoEdgeAI.h)
*/
void fill_buffer(float sample_buffer[])
{
/* USER BEGIN */
/* USER END */
}
/* -----------------------------------------------------------------------------*/
int main(void)
{
/* Initialization ----------------------------------------------------------*/
enum neai_state error_code = neai_oneclass_init(knowledge);
if (error_code != NEAI_OK) {
/* This happens if the knowledge does not correspond to the library or if the library works into a not supported board. */
}
/* Oneclass ----------------------------------------------------------------*/
uint8_t oneclass_result = 0;
while (1) {
fill_buffer(input_user_buffer);
neai_oneclass(input_user_buffer, &oneclass_result);
/* USER BEGIN */
/*
* e.g.: Trigger functions depending on oneclass_result
* (blink LED, ring alarm, etc.).
*/
/* USER END */
}
}
3 Resources
Documentation
All NanoEdge AI Studio documentation is available here.
Tutorials
Step-by-step tutorials, to use NanoEdge AI Studio to build a smart device from A to Z.