Difference between revisions of "AI:How to use transfer learning to perform image classification on STM32"

[unchecked revision] [quality revision]
m
m

This article presents a video on how to use a technique called "Transfer learning" to quickly train a deep learning model in order to classify images.

This video teaches you how to use ST ecosystem to build a computer vision application from the ground up. It describes how the FP-AI-VISION1 allows easy image collection with an STM32 Discovery kit, how to use transfer learning with Tensorflow to quickly train an image classification model, and eventually how to use STM32Cube.AI to convert this model into optimized code for ST microcontrollers.

The Jupyter notebook used in this video is available on Github. It can be opened with Colab.

How to use transfer learning to perform image classification on STM32

The article below describes step by step the video tutorial. For another complete example on how to use your own models with the FP-AI-VISION1 and Teachable Machine check out this article. In addition, this series of videos gives a good overview of the Vision function package.

1 Dataset generation[edit]

First you need a dataset of images representative of your classes. It can be generated either by following the steps described below or by using an already existing dataset (see related Github page for pasta datasets to jump start, note that it has been recorded with a fix distance of 13 cm and good light conditions). It is a good idea to use the same sensor for the dataset collection as the one that will be used for inference.

In the present example, the B-CAMS-OMV board is used as camera module.

Download the FP-AI-VISION1 function package from https://www.st.com/en/embedded-software/fp-ai-vision1.html.

Using the USB Webcam application provided within FP-AI-VISION1, the board and the camera can be used as a webcam.

First plug your board onto your computer using the ST-LINK port. Make sure the JP6 jumper is set to ST-LINK.

Discovery board ST-LINK setup

After plugging the USB cable onto your computer, the board appears as a mounted device.

The binary is located under FP-AI-VISION1_V3.0.0\Projects\STM32H747I-DISCO\Applications\USB_Webcam\Binary.

Drag and drop it onto the board mounted device. This flashes the binary on the board.

Unplug the board, change the JP6 jumper to the HS position, and plug your board using the USB OTG port.

Discovery board USB OTG setup

Launch the Windows® camera application (it can be found by searching for “camera” in the Windows search bar). If your computer has already a camera, change the source of the image feed by clicking the “flip camera” button.

The capture can be done either in VGA or QVGA, the resolution can be changed with the menu settings -> Photos -> Quality. The images will be resized to the input resolution of the neural network in the Python notebook.

Take enough picture samples to fill your dataset. It must be structured as follows:

Dataset
    ├── cats
    │   ├── cat0001.jpg
    │   ├── cat0002.jpg
    │   └── ...
    ├── dogs
    └── horses

The dataset must to be large enough. The one used for the video includes 1408 files belonging to 8 classes. It is recommended to use at least 100 pictures per class.

2 Model generation[edit]

The Python notebook used to generate the model can be found at https://github.com/STMicroelectronics/stm32ai/blob/master/AI_resources/VISION/transfer_learning/TransferLearning.ipynb

It can be open either with Google Colab (as in the present example) or by using any Python environment.

Just click (or Ctrl + Click) the Open in Colab icon at the top of the notebook on Github. This takes you to the Colab notebook project.

Zip your dataset folder and import it to the Colab project.

Colab import

You can run the script either step by step or run the whole script by pressing Ctrl + F9.

All the steps are described in details in the script but what they do is straightforward :

  • Import all the necessary libraries.
  • Unzip the dataset.
  • Import the dataset (this step also automatically resizes images to match the model input size).
  • Display samples from the dataset
  • Perform data augmentation by adding duplicate images with random contrast/translation/rotation/zoom.
  • Display new samples.
  • Normalize data.
  • Import a pretrained MobileNet model without the last layer and add new ones at the end.
  • Train the model.
  • Plot training loss history.
  • Quantize the model to reduce its size.
  • Export the quantized model.

The trained and quantized model appears as model_quant.tflite.

3 Model deployment[edit]

This section describes how to generate a model that can be used on STM32 platforms, starting from a model produced by a high-level library such a Keras/Tensorlflow.

It also describes how to use your model in an already existing project.

3.1 Model generation for STM32[edit]

Warning white.png Warning
Warning, the latest version of FP-AI-VISION1 is based on STM32Cube.AI 6.0.0. Make sure your are using this version.

First convert the tflite model to be used on a STM32 platform.

There are two ways to achieve this goal, one by using STM32CubeMX and generating an entire project (recommended at first), the other by using the command line interface to generate only the required files.

3.1.1 Project generation with STM32CubeMX (Option 1)[edit]

Start STM32CubeMX and create a new project. In this example, the STM32H747I-DISCO board is used. Select the board in the Board Selector and start the project.

A new window opens showing the board configuration. Click Software Packs -> Select Components.

Adding components to STM32CubeMX

Select the components for the Arm® Cortex®-M7 core under STMicroelectronics X-CUBE-AI, check the core box, select Application as application, then click Ok.

Components selector

The stm32-ai library will be download if it has not been downloaded yet. When it is complete, click Ok.

Go to Software Packs (on the left) -> STMicroelectronics XCUBE AI. A pop up window opens to configure peripherals and clock.Click Yes.

Click Add network, call your network network, select TFLite from the scrollable menu, and browse to the last section to find the generated model.

Once the model is selected, click Analyze. This provides a quick overview of the model memory footprint. Click the Show graph button for more in-depth information on the model topology and RAM memory usage layer by layer including activation buffers.

Memory Usage windows

To customize how the model is stored in memory, click the gear icon (Advanced Settings) and specify if you want to use external Flash memory and/or RAM. Check the Use activation buffer for input buffer to make them share the same buffer in order to reduce memory usage.

X-Cube-AI model loading

Click Analyze again. You can see that the RAM occupation has been significantly reduced (refer to the memory graph for more details).

Memory Usage window after enabling input buffer space sharing

Check that the model works properly by validating it either on the PC or on the target.

To generate the code for STM32CubeIDE (or Arm® KEIL® or IAR SYSTEMS®) go to Project manager, specify a project name and location. Select STM32CubeIDE as toolchain, then click GENERATE CODE on the top right corner.

Project manager window

This generates the necessary code for the whole project. In the present example, only the files related to the neural network are required.

They are located under YourProjectName\CM7\X-CUBE-AI\App\ and are called network.c,network.h ,network_data.c, network_data.h and network_config.h. They represent the model and its weight.

3.1.2 Command line interface (Option 2)[edit]

The other way to generate the necessary files is to use the command line interface. The main advantage is to produce only the required files.

The documentation related to X CUBE AI is located under C:\Users\<USERNAME>\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\6.0.0\Documentation/.

The CLI is called stm32ai.exe for Windows. It is located under C:\Users\<USERNAME>\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\6.0.0\Utilities\windows and $HOME/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/6.0.0/Utilities/ for UNIX®-based systems.

If there is no utilities folder, create a CUBE MX project and add Core AI in the Software Package (see section Project generation). This downloads all the necessary files.

For ease of usage, add the folder to your Windows path:

PC $> set CUBE_FW_DIR=C:\Users\<USERNAME>\STM32Cube\Repository
PC $> set X_CUBE_AI_DIR=%CUBE_FW_DIR%\Packs\STMicroelectronics\X-CUBE-AI\6.0.0
PC $> set PATH=%X_CUBE_AI_DIR%\Utilities\windows;%PATH%

Once added, go to the folder where you wish to generate the network files in command line (using PowerShell or similar) and run the following command:

PC $> stm32ai.exe generate -m .\model_quant.tflite --allocate-inputs # (change the path to the model if needed).

This creates all the necessary files under the stm32ai_output folder.

3.2 Model integration[edit]

Now that the C files are generated for your model, integrate them in an already existing project.

In this example, the application is based on the 'Person detection AI function package project.

Launch the STM32CubeIDE project with the .project located under FP-AI-VISION1_V3.0.0\FP-AI-VISION1_V3.0.0\Projects\STM32H747I-DISCO\Applications\PersonDetection\MobileNetv2_Model\STM32CubeIDE. Double click it to open STM32CubeIDE.

Select the CM7 subproject and build it. The resulting workspace is shown below:

STM32CubeIDE Project window

Replace the model files (network.c,network.h ,network_data.c, network_config.h and network_config.h) by those generated previously with STM32CubeMX.

Replace them in Windows explorer. Below the file location:

PersonDetection
+-- MobileNetv2_Model
|   +-- Inc
|   |   network.h
|   |   network_data.h
|   |   network_config.h
|   +-- Src
|   |   network.c
|   |   network_data.c

Change the name of your classes. Go to fp_vision_app.c and change output_labels to your class names. Be careful that there are as many labels as your model output size.

Clean your project under STM32CubeIDE with Project->Clean....

Make sure that your board is connected to the ST-LINK port and properly powered (set the jumper position to ST-LINK).

Build your project and run it with the play button.

A ST-Application pack splash window appears followed by the camera view and the model classification. If either of these window is not displayed properly, go through the wiki article to check if steps have been skipped.


This article presents a video on how to use a technique called "Transfer learning" to quickly train a deep learning model in order to classify images. 

This video teaches you how to use ST ecosystem to build a computer vision application from the ground up. It describes how the FP-AI-VISION1 allows easy image collection with an STM32 Discovery kit, how to use transfer learning with Tensorflow to quickly train an image classification model, and eventually how to use STM32Cube.AI to convert this model into optimized code for ST microcontrollers.

The Jupyter notebook used in this video is [https://github.com/STMicroelectronics/stm32ai/blob/master/AI_resources/VISION/transfer_learning/TransferLearning.ipynb available on Github]. It can be opened with Colab.
<div class="res-img">

[[File:Video ST CV TL.png|center||link=https://www.youtube.com/watch?v=NDshmSH7WnA&list=PLnMKNibPkDnG9IC5Nl9vJg1CKMAO1kODW|How to use transfer learning to perform image classification on STM32]]</div>


The article below describes step by step the video tutorial. For another complete example on how to use your own models with the FP-AI-VISION1 and Teachable Machine [[How to use Teachable Machine to create an image classification application on STM32|check out this article]]. In addition, [https://www.youtube.com/watch?v=ftM2D6qgrtI this series of videos] gives a good overview of the Vision function package.

== Dataset generation ==

First you need a dataset of images representative of your classes. It can be generated either by following the steps described below or by using an already existing dataset (see related [https://github.com/STMicroelectronics/stm32ai/tree/master/AI_resources/VISION/transfer_learning Github page] for pasta datasets to jump start, note that it has been recorded with a fix distance of 13 cm and good light conditions). It is a good idea to use the same sensor for the dataset collection as the one that will be used for inference.

In the present example, the [https://www.st.com/en/development-tools/b-cams-omv.html B-CAMS-OMV] board is used as camera module.

Download the FP-AI-VISION1 function package from [https://www.st.com/en/development-tools/b-cams-omv.html https://www.st.com/en/embedded-software/fp-ai-vision1.html].

Using the USB Webcam application provided within FP-AI-VISION1, the board and the camera can be used as a webcam.

First plug your board onto your computer using the '''ST-LINK''' port. Make sure the '''JP6''' jumper is set to '''ST-LINK'''.
<div class="res-img">

[[File:discordBoard.jpg|center|Discovery board ST-LINK setup]]</div>


After plugging the USB cable onto your computer, the board appears as a mounted device.

The binary is located under <code>FP-AI-VISION1_V3.0.0\Projects\STM32H747I-DISCO\Applications\USB_Webcam\Binary</code>.

Drag and drop it onto the board mounted device. This flashes the binary on the board.

Unplug the board, change the '''JP6''' jumper to the '''HS''' position, and plug your board using the '''USB OTG''' port.
<div class="res-img">

[[File:discordBoard2.jpg|center|Discovery board USB OTG setup]]</div>


Launch the Windows<sup>&reg;</sup> camera application (it can be found by searching for “camera” in the Windows search bar). If your computer has already a camera, change the source of the image feed by clicking the “flip camera” button.

The capture can be done either in '''VGA''' or '''QVGA''', the resolution can be changed with the menu <code>settings -&gt; Photos -&gt; Quality</code>.
The images will be resized to the input resolution of the neural network in the Python notebook.

Take enough picture samples to fill your dataset. It must be structured as follows:
<pre>Dataset
    ├── cats
    │   ├── cat0001.jpg
    │   ├── cat0002.jpg
    │   └── ...
    ├── dogs
    └── horses</pre>

The dataset must to be large enough. The one used for the video includes 1408 files belonging to 8 classes. It is recommended to use at least 100 pictures per class.

== Model generation ==

The Python notebook used to generate the model can be found at https://github.com/STMicroelectronics/stm32ai/blob/master/AI_resources/VISION/transfer_learning/TransferLearning.ipynb

It can be open either with Google Colab (as in the present example) or by using any Python environment.

Just click (or <code>Ctrl + Click</code>) the <code>Open in Colab</code> icon at the top of the notebook on Github. This takes you to the Colab notebook project.

Zip your dataset folder and import it to the Colab project.
<div class="res-img">

[[File:ColabImport.png|center|Colab import]]</div>


You can run the script either step by step or run the whole script by pressing <code>Ctrl + F9</code>.

All the steps are described in details in the script but what they do is straightforward :

* Import all the necessary libraries.
* Unzip the dataset.
* Import the dataset (this step also automatically resizes images to match the model input size).
* Display samples from the dataset
* Perform data augmentation by adding duplicate images with random contrast/translation/rotation/zoom.
* Display new samples.
* Normalize data.
* Import a pretrained <code>MobileNet</code> model without the last layer and add new ones at the end.
* Train the model.
* Plot training loss history.
* Quantize the model to reduce its size.
* Export the quantized model.

The trained and quantized model appears as <code>model_quant.tflite</code>.

== Model deployment ==

This section describes how to generate a model that can be used on STM32 platforms, starting from a model produced by a high-level library such a Keras/Tensorlflow.

It also describes how to use your model in an already existing project.

=== Model generation for STM32 ===
{{Warning|Warning, the latest version of FP-AI-VISION1 is based on STM32Cube.AI 6.0.0. Make sure your are using this version.}}

First convert the <code>tflite</code> model to be used on a STM32 platform.

There are two ways to achieve this goal, one by using STM32CubeMX and generating an entire project (recommended at first), the other by using the command line interface to generate only the required files.

==== Project generation with STM32CubeMX (Option 1) ====

Start STM32CubeMX and create a new project. In this example, the STM32H747I-DISCO board is used. Select the board in the <code>Board Selector</code> and start the project.

A new window opens showing the board configuration. Click <code>Software Packs -&gt; Select Components</code>.
<div class="res-img">

[[File:CubeMXScreenShot.png|center|Adding components to STM32CubeMX]]</div>


Select the components for the Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-M7 core under STMicroelectronics X-CUBE-AI, check the core box, select <code>Application</code> as application, then click Ok.
<div class="res-img">

[[File:CubeMXScreenShot2.png|center|Components selector]]</div>


The stm32-ai library will be download if it has not been downloaded yet. When it is complete, click Ok.

Go to <code>Software Packs (on the left) -&gt; STMicroelectronics XCUBE AI</code>. A pop up window opens to configure peripherals and clock.Click Yes.

Click <code>Add network</code>, call your network <code>network</code>, select TFLite from the scrollable menu, and browse to the last section to find the generated model.

Once the model is selected, click <code>Analyze</code>. This provides a quick overview of the model memory footprint. Click the <code>Show graph</code> button for more in-depth information on the model topology and RAM memory usage layer by layer including activation buffers.
<div class="res-img">

[[File:Graph1.png|center|Memory Usage windows]]</div>


To customize how the model is stored in memory, click the gear icon (<code>Advanced Settings</code>) and specify if you want to use external Flash memory and/or RAM. Check the <code>Use activation buffer for input buffer</code> to make them share the same buffer in order to reduce memory usage.
<div class="res-img">

[[File:CubeMXScreenShot3.png|950px|center|X-Cube-AI model loading]]</div>


Click <code>Analyze</code> again. You can see that the RAM occupation has been significantly reduced  (refer to the memory graph for more details).
<div class="res-img">

[[File:Graph2.png|center|Memory Usage window after enabling input buffer space sharing]]</div>


Check that the model works properly by validating it either on the PC or on the target.

To generate the code for STM32CubeIDE (or Arm<sup>&reg;</sup> KEIL<sup>&reg;</sup> or IAR SYSTEMS<sup>&reg;</sup>) go to <code>Project manager</code>, specify a project name and location. Select STM32CubeIDE as toolchain, then click <code>GENERATE CODE</code> on the top right corner.
<div class="res-img">

[[File:CubeMXScreenShot4.png|950px|center|Project manager window]]</div>


This generates the necessary code for the whole project. In the present example, only the files related to the neural network are required.

They are located under <code>YourProjectName\CM7\X-CUBE-AI\App\</code> and are called <code>network.c</code>,<code>network.h</code> ,<code>network_data.c</code>, <code>network_data.h</code> and <code>network_config.h</code>. They represent the model and its weight.

==== Command line interface (Option 2) ====

The other way to generate the necessary files is to use the command line interface. The main advantage is to produce only the required files.

The documentation related to X CUBE AI is located under <code>C:\Users\&lt;USERNAME&gt;\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\6.0.0\Documentation/</code>.

The CLI is called <code>stm32ai.exe</code> for Windows. It is located under <code>C:\Users\&lt;USERNAME&gt;\STM32Cube\Repository\Packs\STMicroelectronics\X-CUBE-AI\6.0.0\Utilities\windows</code> and <code>$HOME/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/6.0.0/Utilities/</code> for UNIX<sup>&reg;</sup>-based systems.

If there is no <code>utilities</code> folder, create a CUBE MX project and add Core AI in the Software Package (see section Project generation). This  downloads all the necessary files.

For ease of usage, add the folder to your Windows path:
 {{PC$}} set CUBE_FW_DIR=C:\Users\&lt;USERNAME&gt;\STM32Cube\Repository
 {{PC$}} set X_CUBE_AI_DIR=%CUBE_FW_DIR%\Packs\STMicroelectronics\X-CUBE-AI\6.0.0
 {{PC$}} set PATH=%X_CUBE_AI_DIR%\Utilities\windows;%PATH%

Once added, go to the folder where you wish to generate the network files in command line (using PowerShell or similar) and run the following command:

 {{PC$}} stm32ai.exe generate -m .\model_quant.tflite --allocate-inputs # (change the path to the model if needed).

This creates all the necessary files under the <code>stm32ai_output</code> folder.

=== Model integration ===

Now that the C files are generated for your model, integrate them in an already existing project.

In this example, the application is based on the '''Person detection'' AI function package project.

Launch the STM32CubeIDE project with the <code>.project</code> located under <code>FP-AI-VISION1_V3.0.0\FP-AI-VISION1_V3.0.0\Projects\STM32H747I-DISCO\Applications\PersonDetection\MobileNetv2_Model\STM32CubeIDE</code>. Double click it to open STM32CubeIDE.

Select the <code>CM7</code> subproject and build it. The resulting workspace is shown below: 
<div class="res-img">

[[File:CubeIDEScreenShot.png|center|STM32CubeIDE Project window]]</div>


Replace the model files (<code>network.c</code>,<code>network.h</code> ,<code>network_data.c</code>, <code>network_config.h</code> and <code>network_config.h</code>) by those generated previously with STM32CubeMX.

Replace them in Windows explorer. Below the file location:
<pre>PersonDetection
+-- MobileNetv2_Model
|   +-- Inc
|   |   network.h
|   |   network_data.h
|   |   network_config.h
|   +-- Src
|   |   network.c
|   |   network_data.c</pre>


Change the name of your classes. Go to <code>fp_vision_app.c</code> and change <code>output_labels</code> to your class names. Be careful that there are as many labels as your model output size.

Clean your project under STM32CubeIDE with <code>Project-&gt;Clean...</code>.

Make sure that your board is connected to the ST-LINK port and properly powered (set the jumper position to <code>ST-LINK</code>).

Build your project and run it with the play button.

A ST-Application pack splash window appears followed by the camera view and the model classification. If either of these window is not displayed properly, go through the wiki article to check if steps have been skipped.
<noinclude>

[[Category:Vision|How to add AI model to OpenMV ecosystem30]]
{{PublicationRequestId | 20512| 2021-07-12 | AnneJ ?}}</noinclude>
Line 213: Line 213:
   
 
<noinclude>
 
<noinclude>
[[Category:Vision|How to add AI model to OpenMV ecosystem]]
+
[[Category:Vision|30]]
 
{{PublicationRequestId | 20512| 2021-07-12 | AnneJ ?}}
 
{{PublicationRequestId | 20512| 2021-07-12 | AnneJ ?}}
 
</noinclude>
 
</noinclude>