Last edited 3 days ago

Snippet

1. Usage

The Snippet template is used to display snippet of code and to provide license/copyrights and component information at the same time.

Usage:  {{Snippet | category=<category> | component=<component> | snippet=<snippet>}}

Where:

  • <category> is the mandatory category article to which the licenses and copyright associated to the snippet are refering to:
    • AI: to refer to the AI licences page
  • <component> is the mandatory component name the snippet is refering to.
  • <snippet> is the mandatory source code of the snippet.

2. Basic examples

You type You get
Snippet usage
{{Snippet | category=AI | component=Application | snippet=
<source lang="c" highlight="4-9">
/* USER CODE BEGIN 4 */
/*...*/

void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
  if (GPIO_Pin == GPIO_PIN_11) {
    dataRdyIntReceived++;
  }
}
/* USER CODE END 4 */
</source>
}}
This snippet is provided AS IS, and by taking it, you agree to be bound to the license terms which can be found here for the component: Application.
/* USER CODE BEGIN 4 */
/*...*/

void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
  if (GPIO_Pin == GPIO_PIN_11) {
    dataRdyIntReceived++;
  }
}
/* USER CODE END 4 */
Snippet error if category or component are not set
{{Snippet | snippet=
<source lang="c" highlight="4-9">
/* USER CODE BEGIN 4 */
/*...*/

void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
  if (GPIO_Pin == GPIO_PIN_11) {
    dataRdyIntReceived++;
  }
}
/* USER CODE END 4 */
</source>
}}
This snippet is provided AS IS, and by taking it, you agree to be bound to the license terms which can be found [[unknown category|here]] for the component: unknown component.
/* USER CODE BEGIN 4 */
/*...*/

void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
  if (GPIO_Pin == GPIO_PIN_11) {
    dataRdyIntReceived++;
  }
}
/* USER CODE END 4 */
Snippet error if category as a wrong value
{{Snippet | category=Toto | component=Application | snippet=
<source lang="c" highlight="4-9">
/* USER CODE BEGIN 4 */
/*...*/

void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
  if (GPIO_Pin == GPIO_PIN_11) {
    dataRdyIntReceived++;
  }
}
/* USER CODE END 4 */
</source>
}}
This snippet is provided AS IS, and by taking it, you agree to be bound to the license terms which can be found [[unknown category|here]] for the component: Application.
/* USER CODE BEGIN 4 */
/*...*/

void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
  if (GPIO_Pin == GPIO_PIN_11) {
    dataRdyIntReceived++;
  }
}
/* USER CODE END 4 */

3. More examples

You type You get
Check that spaces before and after the snippet
BEFORE{{Snippet | category=AI | component=Application | snippet=
<source lang="c" highlight="4-9">
/* USER CODE BEGIN 4 */
/*...*/

void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
  if (GPIO_Pin == GPIO_PIN_11) {
    dataRdyIntReceived++;
  }
}
/* USER CODE END 4 */
</source>
}}AFTER<br>
BEFORE
{{Snippet | category=AI | component=Application | snippet=
<source lang="c" highlight="4-9">
/* USER CODE BEGIN 4 */
/*...*/

void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
  if (GPIO_Pin == GPIO_PIN_11) {
    dataRdyIntReceived++;
  }
}
/* USER CODE END 4 */
</source>
}}
AFTER
BEFORE
This snippet is provided AS IS, and by taking it, you agree to be bound to the license terms which can be found here for the component: Application.
/* USER CODE BEGIN 4 */
/*...*/

void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
  if (GPIO_Pin == GPIO_PIN_11) {
    dataRdyIntReceived++;
  }
}
/* USER CODE END 4 */
AFTER

BEFORE

This snippet is provided AS IS, and by taking it, you agree to be bound to the license terms which can be found here for the component: Application.
/* USER CODE BEGIN 4 */
/*...*/

void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
  if (GPIO_Pin == GPIO_PIN_11) {
    dataRdyIntReceived++;
  }
}
/* USER CODE END 4 */

AFTER

4. Code

This snippet is provided AS IS, and by taking it, you agree to be bound to the license terms which can be found [[unknown category|here]] for the component: unknown component.

{{{snippet}}}