![]() |
Coming soon |
Please understand this is draft, thank you
1. X-CUBE-WW4 Pack content
The X-Cube Firmware is organized in the typical way as most of packs delivered by STM.
This Wiki page will focus on the part of the pack specific to the Wi-Fi,
giving a brief description of the Middlewares and Applications folder organization.
Third party Middlerewas (LWIP, MbedTLS, FreeRTOS, etc) are not covered by this page, because their folder structure is inherited from the public code.
2. ST Middlewares
2.1. WLAN_Driver
It is basically the code allowing the two chips communication (host and ww4) and ww4 fw download.
Umac interface, RPC (Remote Procedure Call) and COM abstraction.
It is provided in source code.
Linux oriented. Folders shared `between MCU host, MPU host and with STM32WW4 device.
It occupies about 10 kb (mw) + 5 kb (sdio) flash (on the host)
2.2. WLAN_Lib and WPA supplicant
WLAN_API, wpa_supplicant, wpa_supplicant MCU customization.
WPA supplicant is given is source code, this comes from Linux distribution.
The customization of the WPA supplicant for MCU devices is given in library.
The WLAN_Lib is a bridge between application, WPA Supplicant, LWIP and WLAN_Driver.
This code is given in libraries.
Part of the WLAN_Lib is given in source code and part as a compiled libraries (.a)
These the principal directories of the WLAN_Lib middleware:
- Api: include files with type definitions and functions prototypes offered by the WLAN_Lib to the application.
- Config: wlan_lib_config_template.h should be copied to the project space and to be used to configure the WLAN_Lib according to the specific project needs.
- Interface: the Wlan_Lib requests via these include files a set of callbacks or functions that the project must provide to allow the Wlan_Lib to be functional. Few examples, a way to allocate memory, a way to log messages, an interface with an IP stack, etc.
- Libraries: part of the implementation not provided in source. libwlancore.a and libwlancommon.a are always required by the linker. The other libraries only for projects requiring the correspondent features.
- WLAN_Driver_Shim: It is a specific interface WLAN_Lib vs WLAN_Driver.
- wpa_supplicant_bsd3: pubblic WPA supplicant from Linux world.
- wpa_supplicant/ST_customization: Customisation to STM32 MCUs.
Big code size, depends on the config and the libraries linked.
3. Projects
Projects are available for U5 and H7 boards.
Each project has similar structure, the picture below refers to CLI project, but other project are similar.
Basically, a project consists in five main entities:
- IDEs: directories containing the workspace for different IDEs (EWARM, STM32CubeIDE, Keil in future).
- Core: files related to the device (U5, H7, etc.) typically generated with CubeMX. Interrupt handling, MSP HW configuration (uart, dma, tim, etc)
- MWs configuration and interfaces: Similarly to WLAN_Lib above described, often MWs modules need to be configures and requires some interfaces. The directories LWIP/, MBEDTLS/, Trace/, WLAN_DRIVER/ are meant to provide to the correspondent MW the necessary code to be functional.
- WW4 binary: It is placed in WLAN_Lib_Driver/Target. It is downloaded to the STM32WW4 by the application during initialization.
- Application: The application resides on the top, it uses several middleware modules and drivers. It needs to be centralized in a common place; due to some CubeFw restriction, it is decided to place* the application in the WLAN_Lib/App directory (in spite it handles also other MWs then WLAN_LIb).
(*) The project WLAN_Driver_Prod application is an exception, since it does not use WLAN_Lib middleware, the application is placed in WLAN_Driver/App
Depending on the project other directories might be added for specific cases:
- iperf : used by WLAN_Lib_CLI project to group iperf2 files
- dbgww4 : used by WLAN_Driver_Prod and WLAN_Lib_CLI projects to have direct communication with STM32WW4.
- Eeprom: used by WLAN_Lib_Fota and WLAN_Lib_Provisioning to emulate EPROM (read/store data in flash memory).
- Html: used by WLAN_Lib_HTTP_Server and WLAN_Lib_Provisioning to keep the web pages of the server.
other might come.
3.1. IDEs: Build and Install
/* (copied from readme.md). Can be done better */
- Build the chosen project
- Open your preferred toolchain
- Rebuild all files and load your image into target memory
- (Optional) Attach to the running target if you want to debug
- Use the application through the serial link
- Open a Terminal client connected to the Host ST-LINK COM port
- UART Config = 921600, 8b, 1 stopbit, no parity, no flow control
- (Optional) Connect an additional STLINK-V3SET on the X-NUCLEO-WW432 expansion board (CN1 -STDC14 debug header) and open another serial link
- Open a Terminal client connected to the STLINK-V3SET COM port
- UART Config = 921600, 8b, 1 stopbit, no parity, no flow control
- Press Reset button of the Host board
3.2. Core
Compatible with CubeMX generation. Typical to CubeFw, no need to detail about it.
3.3. MWs configuration and interfaces
Code is placed in the /Target directories: WLAN_LIB/Target, WLAN_DRIVER/Target, LWIP/Target, etc.
3.3.1. MWs configuration
Most important configuration files of the middlewares are:
- "WLAN_LIB/Target/wlan_lib_config.h": few definitions to configure the WLAN_Lib ans wpa supplicant provided in source code.
- "WLAN_DRIVER/Target/wlan_driver_config.h": definitions to configure the WLAN_Driver.
- "Core/Inc/FreeRTOSConfig.h": definitions to configure the FreeRTOS. There is no dedicated /Target directory for it.
- "LWIP/Target/lwipopts.h and lwippools.h": definitions to configure the WLAN_Driver.
LwIP pull buffers configuration and FreeRTOS heap memory configuration will be discussed in a separate chapter dedicated to memory, transversal to application and MWs.
Logs configuration will be discussed in a separate chapter dedicated to logs and traces, transversal to application and MWs.
3.3.2. MWs interfaces
The interfaces often don't belong strictly to a specific MW but they make bridges between MWs or are used by more the one MW.
In such cases interfaces are put in the WLAN_LIB/Target (similarly the application cross MWs which is put in the WLAN_LIB/App directory)
Let's mention the most important:
- "wlan_netif_lwip.c", "wlan_netbuf_lwip.c" and "app_lwip_cb.c" make the bridge bewwen the "WLAN_Lib" and the "LWIP" middlewares.
- "wlan_os.c" mainly operative system abstraction requested by both "WLAN_Lib" and "WLAN_Driver" it is placed in the "WLAN_LIB/Target" directory.
- "com_sdio.c" and "sdio_drv.c" allow the Host device to communicate with the WW4 device (via SDIO or SPI). For the moment only SDIO implementation is provided. The files are placed in the WLAN_DRIVER/Target directory.
3.4. WW4 binary
Binary placed in the WLAN_DRIVER/Target directory.
Remind: STM32WW4 does not have flash memory. During initialization phase the host device downloads the code into the STM32WW4 RAM where it is executed.
3.5. Application
While the above files and directories remains pretty similar between different projects, the code that makes them different between one and the other is the application, placed in the directory WLAN_Lib/App.
Here there are several files and again most of them are common between applications, few are completely different.
Let's see this more in detail.
Most applications use a "didactical" layer, providing functions that groups a sequence of LWIP and WLAN_Lib functions call, and other functions to print out on the hyper terminal didactical messages about the state of the application. This layer also provides function for facilitate the debug and to get performance or memory usage statistics.
This layer is constituted by files like : "app_common.c, app_handlers.c, uart_if.c, util_led_pb.c, util_net_address.c, util_net_mem.c, util_net_perf.c "
Actually, only WLAN_Lib_Ping does not use this "didactical" layer, because is targeted for experienced developers that want to start writing their application from zero, by interfacing directly with the MWs with minimal overhead.
The file that that really change from one application to the other is : "main_app.c" (in the WLAN_Lib/App )
It is the entry point, often other specific files come to complement it depending on the application, for example:
"generic_mqtt.c, httpserver.c, ping_addr.c, ping_url.c, console.c, etc"
More details about them will be given in the wiki pages specific to each application.
Other two files deserve to be mentioned because users need to configure them for adapting any application to their environment:
The files are "app_conf.h" and "credentials_and_ip_static_addr.h".
The first contains general definition depending on the specific application.
The second contains the SSID, Password, Ip address, netmask, etc. of the Local access point to which user wants to connect.
Next chapters refer to code placed in the WLAN_Lib/App but their scope sometime is more general than just the application or in any case the deserve to be discussed in a general context. For example, the file "msg.h" configures the application logs, but it is wise to talk about it in a unique cross chapter that explain how to configure logs as well in the other modules.
3.6. Memory setting
3.6.1. Use of FreeRTOS heap instead Lib-C heap
The application code in util_net_mem.c redirect all calls to "malloc", "calloc", "realloc" and "free" form the classical Lib-C HEAP to the FreeRTOS memory basically using "pvPortMalloc()" and "vPortFree()".
The advantage is that no matter which module, it could be also Third_Party MW with hardcoded calls to "malloc", all dynamic memory allocation centralized in the FreeRTOS memory.
The classical HEAP memory instantiated in the linker file is therefore no more used and can be minimized, on the other hand the FreeRTOS HEAP shall be configure depending on the project. Configuration is done in the "/Core/Inc/FreeRTOSConfig.h".
Examples of values for the different applications: #define configTOTAL_HEAP_SIZE ((size_t)15000) /* APP_PROD */ #define configTOTAL_HEAP_SIZE ((size_t)130000) /* APP_CLI */ #define configTOTAL_HEAP_SIZE ((size_t)100000) /* APP_PROVISIONING*/ #define configTOTAL_HEAP_SIZE ((size_t)100000) /* APP_HTTPSERVER*/ #define configTOTAL_HEAP_SIZE ((size_t)130000) /* APP_P2P*/ #define configTOTAL_HEAP_SIZE ((size_t)100000) /* APP_WPS*/ #define configTOTAL_HEAP_SIZE ((size_t)100000) /* APP_ENTERPRISE*/ #define configTOTAL_HEAP_SIZE ((size_t)60000) /* APP_ECHO*/ #define configTOTAL_HEAP_SIZE ((size_t)60000) /* APP_MQTT*/ #define configTOTAL_HEAP_SIZE ((size_t)60000) /* APP_PING*/ #define configTOTAL_HEAP_SIZE ((size_t)80000) /* APP_FOTA */
3.6.2. LWIP Pull buffers ( lwippools.h and lwipopts.h)
Pull buffers are defined in the "LWIP/Target/lwippools.h" but a cople of parameters that determines the final size are in the "LWIP/Target/lwipopts.h"
LWIP_MALLOC_MEMPOOL_START LWIP_MALLOC_MEMPOOL(TX_COUNT - 1, TX_POOL_BUFSIZE) LWIP_MALLOC_MEMPOOL(1, 1664) LWIP_MALLOC_MEMPOOL_END
"TX_POOL_BUFSIZE" is 1580 for all projects but the number of the buffers "TX_COUNT" can be quite different depending on the size to be transferred or on the performance that we want to achieve.
For most projects "TX_COUNT" is configured to 5. But when we need high performance like to get a good IPERF throughput in the WLAN_Lib_CLI project, the number of pull buffers is increased to 44. Also provisioning requires a larger number of TX buffers, because when acting as HTTP server it needs to send images with relatively big size to the connected devices.
3.6.3. Memory footprint
Should an overview be given here, for example depending on the above options (logs, pulls, tracealyzer, etc)
3.7. Debug: Logs, Trace, Performance measurements
3.7.1. Logging configuration
There are many flags to be tune for enabling/disabling the logs, each Middleware has its own, and the application as well.
Sometime the verbose level is selectable dynamically sometime at compilation time.
Sometimes it saves ROM memory (the sting to be printed is removed from the binary) sometime not.
In all cases the logs reach the hyper terminal via the utility ADV_TRACE that uses the the DMA to send a circular buffer of characters on the UART.
3.7.1.1. Application logs (file msg.h)
Application logs are enabled/disabled at compilation time in the file msg.h
Disabling these logs allows reducing the memory footprint, but be aware that most of logs are not in the application;
so this will only allow to save about 3KB flash memory.
#define ENABLE_APP_MSG_DEBUG 0 #define ENABLE_APP_MSG_INFO 1 #define ENABLE_APP_MSG_WARNING 1 #define ENABLE_APP_MSG_ERROR 1 #define ENABLE_APP_MSG_ASSERT 1 #define ENABLE_IPERF2_MSG 1
The file msg.h includes a descriptive part to tell where to enable\disable MWs logs, which is also done in the next paragraph of the WiKi page.
3.7.1.2. WLAN_Lib / WLAN_Driver logs
The WLAN_Lib / WLAN_Driver allow both compilation flags and dynamic level.
If the LOG compilation flags are disabled of course trace are not available at all (remove from the binary, hence flash memory saved).
If the LOG compilation flags are enabled, then verbose level can be selected dynamically via a CLI command.
Basically the filtering of logs to be displayed is done by the function "wlan_os_printf_impl(logLevel, text)" implemented in the file "wlan_os.c",
depending on the verbose level that has been previously set by the function "wlan_os_set_print_lvl(PrintLevel)".
Possible levels are:
WLAN_OS_PRINT_ALL = 0, /*!< Print all messages (DBG + INFO + ERR) */ WLAN_OS_PRINT_DBG = 1, /*!< Print debug and lower messages (DBG + INFO + ERR) */ WLAN_OS_PRINT_INFO = 2, /*!< Print info and lower messages (INFO + ERR) */ WLAN_OS_PRINT_ERR = 3, /*!< Print error messages (ERR) */ WLAN_OS_NO_PRINT = 4, /*!< Dont print any message */
If "WLAN_OS_PRINT_ALL" or "WLAN_OS_PRINT_DBG" are set by "wlan_os_set_print_lvl()" some messages might be lost.
This can be avoided by using larger buffers in "wlan_os.c" ("uint8_t a_uart_buff[4096]").
We have three modules using this method WLAN_Lib, WLAN_Lib_wpa_Supplicant and WLA_Driver.
- WLAN_Lib : it is given in libraries (.a) so it cannot be recompiled. The provided version supports logs. A version not supporting logs can be provided on request: it allows saving 30KB flash memory.
- WLAN_Lib/wpa_Supplicant : it is given in source code, logs can be enabled by the compilation flag "WLAN_LIB_WPA_LOG_ENABLE" in the "wlan_lib_config.h". This has huge impact on memory size (more then 100KB).
- WLAN_Driver : it is given in source code, logs can be enabled by the compilation flag "WW4_LOG_ENABLE" in the "wlan_driver_config.h".
3.7.1.3. Third party Middlewares logs
Each Middleware is suppposes to provied an interface for redirecting the logs.
The most important is surely the LWIP, the log configuration is done in following file:
"\Applications\WLAN_Lib\<ApplicationName>\LWIP\Target\cc.h"
Notice that mbedTLS has a log system with dedicated API, a part of enabling the compilation flags in the "mbedtls_config.h"
the implementation should be implemented in the correspondent interface file (similarly to what is done in "wlan_os.c" for WLAN_Lib\Driver.
3.7.2. Logging implementation: how logs are sent to the hyper terminal
Logs reach the hyper terminal via the utility ADV_TRACE that uses the DMA to send a circular buffer of characters on the UART.
"UTIL_ADV_TRACE_COND_FSend()" post data to the circular queue for printing.
"UTIL_ADV_TRACE_COND_Send()" would also allow to set a "VerboseLevel" for filtering but this feature is not used (always true) since already implemented by the Middlewares.
A function that deserves to be mentioned is "UTIL_ADV_TRACE_IsBufferEmpty()": when trace buffer is full it allows to wait (kind of polling mode) that there is enough space to complete the messages. This is useful when no time constraint, like when printing the help message, or the scan results. It should not be used to compensate the high verbose level (e.g. DEBUG lgs), because it has consequence on the real time. For such cases the trace buffer should be increased in the "wlan_os.c" file (as explained earlier).
3.7.3. LwIP gpio indicator
Led or GPIOs can be used to indicate LwIP activity.
This is currently implemented in the "Target/" files "wlan_netif_lwip.c" and "app_lwip_cb.c".
When RX or TX functions are called the BLUE Led on STM32U5 boards or the ORANGE Led on the STM32H7 boards is switched ON.
A SW timer is armed which switches OFF the Led 10ms later.
Notice that, when measuring the throughput with IPERF, current implementation it degrades performances.
So for CLI project this indicator has been disabled.
In final release this will be implemented better, probably using an HW timer (HAL_TIM) instead of freeRTOS timer.
Notice that before LwIP data is exchanged, the same GPIO (Led) also blinks at initialization (regularly once every second) to indicate when the STA device is alive, it is connecting to a Local Access Point and establishing the LwIP connections. This is handled by a dedicated task and it stops blinking once the connection is established. Them the GPIO is used exclusively for the LwIP tx/rx activity as described above.
3.7.4. Performance measurements
3.7.4.1. util_net_perf.c
tbd
3.7.4.2. Percepio Tracealyzer
tbd